]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/Bitcode
DAGCombine: fold (or (and X, M), (and X, N)) -> (and X, (or M, N))
[opencl/llvm.git] / test / Bitcode /
2015-01-20 David MajnemerBitcode: Don't create comdats when autoupgrading macho...
2015-01-19 Rafael EspindolaBring r226038 back.
2015-01-16 Timur IskhodzhanovRevert r226242 - Revert Revert Don't create new comdats...
2015-01-16 Filipe CabecinhasUse report_fatal_error instead of llvm_unreachable...
2015-01-16 Rafael EspindolaRevert "Revert Don't create new comdats in CodeGen"
2015-01-15 Timur IskhodzhanovRevert Don't create new comdats in CodeGen
2015-01-14 Duncan P. N. Exon... IR: Move MDLocation into place
2015-01-14 Rafael EspindolaDon't create new comdats in CodeGen.
2015-01-10 Rafael EspindolaUse the DiagnosticHandler to print diagnostics when...
2015-01-08 Rafael EspindolaMake this test a bit stricter.
2014-12-15 Duncan P. N. Exon... IR: Make metadata typeless in assembly
2014-12-11 Duncan P. N. Exon... Bitcode: Use unsigned char to record MDStrings
2014-12-11 Duncan P. N. Exon... Bitcode: Add METADATA_NODE and METADATA_VALUE
2014-12-08 Duncan P. N. Exon... IR: Fix bitcode compatability filenames
2014-12-07 Duncan P. N. Exon... IR: Add missing tests for function-local metadata
2014-12-01 Reid KlecknerParse 'ghccc' in .ll files as the GHC convention (cc 10)
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-09-23 Michael KupersteinEnsure bitcode encoding stays stable.
2014-08-30 Jordan RoseTeach llvm-bcanalyzer to use one stream's BLOCKINFO...
2014-08-19 Duncan P. N. Exon... verify-uselistorder: Force -preserve-bc-use-list-order
2014-08-18 Duncan P. N. Exon... verify-uselistorder: Call verifyModule() and improve...
2014-08-16 Duncan P. N. Exon... BitcodeReader: Only create one basic block for each...
2014-08-12 Duncan P. N. Exon... Don't upgrade global constructors when reading bitcode
2014-08-01 Duncan P. N. Exon... UseListOrder: Fix blockaddress use-list order
2014-07-31 Duncan P. N. Exon... verify-uselistorder: Change the default -num-shuffles=5
2014-07-31 Duncan P. N. Exon... UseListOrder: Handle self-users
2014-07-31 Duncan P. N. Exon... UseListOrder: Don't give constant IDs to GlobalValues
2014-07-30 Rafael EspindolaUse "weak alias" instead of "alias weak"
2014-07-30 Duncan P. N. Exon... UseListOrder: Visit global values
2014-07-30 Duncan P. N. Exon... Fix line endings before adding RUN lines, NFC
2014-07-30 Duncan P. N. Exon... Rename llvm-uselistorder => verify-uselistorder
2014-07-30 Duncan P. N. Exon... Reapply "UseListOrder: Order GlobalValue uses after...
2014-07-29 Duncan P. N. Exon... Revert "UseListOrder: Order GlobalValue uses after...
2014-07-29 Duncan P. N. Exon... UseListOrder: Additional test coverage for r214242
2014-07-29 Duncan P. N. Exon... UseListOrder: Order GlobalValue uses after initializers
2014-07-29 Duncan P. N. Exon... Bitcode: Correctly compare a Use against itself
2014-07-29 Duncan P. N. Exon... Fix line-endings, NFC
2014-07-28 Duncan P. N. Exon... llvm-uselistorder: Add -num-shuffles option
2014-07-28 Duncan P. N. Exon... Bitcode: Serialize (and recover) use-list order
2014-07-25 Duncan P. N. Exon... Move -verify-use-list-order into llvm-uselistorder
2014-07-25 Duncan P. N. Exon... IPO: Add use-list-order verifier
2014-07-23 Saleem AbdulrasoolAsmParser: remove deprecated LLIR support
2014-07-22 Hal FinkelMake use of the align parameter attribute for all point...
2014-07-21 Mark HeffernanRename metadata llvm.loop.vectorize.unroll to llvm...
2014-07-18 Hal FinkelAdd a dereferenceable attribute
2014-07-16 Reid KlecknerRoundtrip the inalloca bit on allocas through bitcode
2014-06-25 Eli BenderskyAdd some test files for r211710.
2014-06-13 Tim NorthoverIR: add "cmpxchg weak" variant to support permitted...
2014-06-05 Tom RoederAdd a new attribute called 'jumptable' that creates...
2014-06-03 Rafael EspindolaAllow alias to point to an arbitrary ConstantExpr.
2014-05-29 Adam Nemet[X86] Move test from r209863 to CodeGen/X86
2014-05-29 Adam Nemet[X86] Auto-upgrade AVX1 vbroadcast intrinsics
2014-05-20 Nick LewyckyAdd 'nonnull', a new parameter and return attribute...
2014-05-17 Rafael EspindolaHandle ConstantAggregateZero when upgrading global_ctors.
2014-05-16 Rafael EspindolaFix most of PR10367.
2014-05-07 Duncan P. N. Exon... IR: Don't allow non-default visibility on local linkage
2014-04-24 Reid KlecknerAdd 'musttail' marker to call instructions
2014-04-05 Saleem AbdulrasoolAsmParser: add a warning for compatibility parsing
2014-04-05 Saleem AbdulrasoolAsmParser: restore LLVM IR compatibility for linker_pri...
2014-03-27 Karthik BhatAll new elements except the last one initialized to...
2014-03-13 Rafael EspindolaRemove the linker_private and linker_private_weak linkages.
2014-03-11 Tim NorthoverIR: add a second ordering operand to cmpxhg for failure
2014-03-02 Michael KupersteinEnsure bitcode encoding of instructions and their opera...
2014-02-26 Michael KupersteinEnsure bitcode encoding of instructions and their opera...
2014-02-04 Manman RenUpdate testing case for r200806.
2014-01-16 Manman RenReport a warning when dropping outdated debug info...
2014-01-14 Nico RieckDecouple dllexport/dllimport from linkage
2014-01-14 Nico RieckRevert "Decouple dllexport/dllimport from linkage"
2014-01-14 Nico RieckDecouple dllexport/dllimport from linkage
2013-12-31 Nick LewyckyFold vector selects with undef elements in the conditio...
2013-12-22 Michael KupersteinEnsure bitcode encoding of calling conventions stays...
2013-12-19 Reid KlecknerBegin adding docs and IR-level support for the inalloca...
2013-12-15 Michael KupersteinEnsure bitcode encoding of global variable attributes...
2013-12-08 Michael KupersteinFixed CRLF
2013-12-08 Michael KupersteinEnsure bitcode encoding of visibility styles stays...
2013-12-02 Manman RenDebug Info: drop debug info via upgrading path if versi...
2013-12-01 Michael KupersteinEnsure bitcode encoding of linkage types stays stable...
2013-11-18 Paul RobinsonThe 'optnone' attribute means don't inline anything...
2013-11-04 Rafael EspindolaChange BitcodeReader to use error_code instead of bool...
2013-10-31 Reid KlecknerUse a larger invalid attribute bitcode number
2013-10-31 NAKAMURA Takumillvm/test/Bitcode/invalid.ll: Tweak expresion to mach...
2013-10-31 Rafael EspindolaFix a use after free on invalid input.
2013-09-28 Manman RenAutoUpgrade: upgrade from scalar TBAA format to struct...
2013-09-12 Joe AbbeyPatch provide by Tom Roeder!
2013-09-09 Bob WilsonRevert patches to add case-range support for PR1255.
2013-08-23 Andrea Di BiagioAdd function attribute 'optnone'.
2013-08-20 Bill WendlingUse -disable-output and to suppress output and don...
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-07-26 Tobias GrosserMake .bc en/decoding of AttrKind stable
2013-07-17 Tobias GrosserAdd some uncovered attribute tests
2013-02-26 Kostya SerebryanyUnify clang/llvm attributes for asan/tsan/msan (LLVM...
2013-02-20 Bill WendlingModify the LLVM assembly output so that it uses referen...
2013-02-12 Bill WendlingTest for string attributes and for attribute group...
2013-02-11 Kostya Serebryany[tsan/msan] adding thread_safety and uninitialized_chec...
2012-10-11 Jan Wen VoungChange encoding of instruction operands in bitcode...
2012-09-21 Benjamin KramerBitcodeReader: Correctly insert blockaddress constant...
2012-07-18 Joel JonesMore replacing of target-dependent intrinsics with...
2012-07-13 Joel JonesThis is one of the first steps at moving to replace...
next