]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/CodeGen/ARM/debug-info-branch-folding.ll
Revert "DI: Fold constant arguments into a single MDString"
[opencl/llvm.git] / test / CodeGen / ARM / debug-info-branch-folding.ll
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-08-06 David BlaikieDebugInfo: Assert that any CU for which debug_loc lists...
2014-07-25 David BlaikieDebugInfo: Fix up some test cases to have more correct...
2013-11-23 Manman RenDebug Info: update testing cases to specify the debug...
2013-09-06 Manman RenDebug Info Testing: updated to use NULL instead of...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-07-27 Manman RenDebug Info Verifier: verify SPs in llvm.dbg.sp.
2013-07-24 Manman RenDebug Info: improve the Finder.
2013-06-15 David BlaikieDebugInfo: follow up to 184045 to constrain the tests...
2013-06-15 David BlaikieDebugInfo: print DBG_VALUE MachineInstrs with [] for...
2013-04-30 Adrian PrantlTemporarily revert "Change the informal convention...
2013-04-30 Adrian PrantlChange the informal convention of DBG_VALUE so that...
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-22 David BlaikieReorder the DIFile field in DILexicalBlock to become...
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-03-08 David BlaikieUpgrade tests to the latest debug info format.
2012-12-04 Bill WendlingUse the 'count' attribute to calculate the upper bound...
2012-12-04 Bill WendlingAdd a 'count' field to the DWARF subrange.
2012-08-14 Nadav RotemDuring the CodeGenPrepare we often lower intrinsics...
2011-06-02 Devang PatelDuring post RA scheduling, do not try to chase reg...
2011-05-26 Devang PatelDuring branch folding avoid inserting redundant DBG_VAL...