]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/CodeGen/Generic
[X86][AVX] Simplified diff between AVX1 and SSE42 fp stack folding tests. NFC.
[opencl/llvm.git] / test / CodeGen / Generic /
2015-01-14 Philip ReamesgetMangledTypeStr: clarify how it mangles types, and...
2014-12-19 Peter CollingbourneCodeGen: do not attempt to invalidate virtual registers...
2014-12-15 Duncan P. N. Exon... IR: Make metadata typeless in assembly
2014-12-13 Akira HatanakaRename argument strings of codegen passes to avoid...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Tim NorthoverARM: yes it can (as of r218789)
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-09-20 Peter CollingbourneFix crash with an insertvalue that produces an empty...
2014-09-03 Lang HamesAdd a regression test to sanity check the PBQP allocator.
2014-07-30 Rafael EspindolaUse "weak alias" instead of "alias weak"
2014-07-25 Hal FinkelAdd @llvm.assume, lowering, and some basic properties
2014-06-05 Tom RoederAdd a new attribute called 'jumptable' that creates...
2014-05-30 Filipe CabecinhasConvert a vselect into a concat_vector if possible
2014-05-30 Tim NorthoverAArch64 & ARM: disable generic test that relies on...
2014-04-23 Saleem AbdulrasoolMC: move test from Generic to COFF
2014-04-23 Saleem AbdulrasoolMC: honour IMAGE_SCN_CNT_INITIALIZED_DATA
2014-02-28 Justin BognerCommandLine: Exit successfully for -version and -help
2014-02-13 Daniel SandersRe-commit: Demote EmitRawText call in AsmPrinter::EmitI...
2014-02-12 Daniel SandersRevert r201237+r201238: Demote EmitRawText call in...
2014-02-12 Daniel SandersDemote EmitRawText call in AsmPrinter::EmitInlineAsm...
2014-02-06 Juergen Ributzka[DAG] Don't pull the binary operation though the shift...
2014-01-27 Stepan DyatkovskiyAdditional fix for 200201: due to dependence on bitwidt...
2014-01-27 Stepan DyatkovskiyFix for PR18102.
2014-01-23 Eric ChristopherMove test to x86 directory.
2014-01-23 Eric ChristopherAvoid emitting a DWARF type attribute for an ObjC prope...
2014-01-06 Bill WendlingRemove a failing test to get the buildbots back to...
2014-01-06 Bill WendlingTry to fix s390x build bot.
2014-01-05 Bill WendlingAttempt to fix buildbots by XFAILing some architectures.
2014-01-05 Bill WendlingEmit an error message if the value passed to __builtin_...
2013-12-13 Rafael EspindolaFix pr18235.
2013-11-21 NAKAMURA TakumiRevert r195317 (and r195333), "Teach ISel not to optimi...
2013-11-21 Kostya Serebryanyadd 'REQUIRES: asserts' to a test that uses 'llc -debug...
2013-11-21 Paul RobinsonTeach ISel not to optimize 'optnone' functions.
2013-11-14 Rafael EspindolaError if we see an alias to a declaration.
2013-10-07 Matt ArsenaultChange objectsize intrinsic to accept different address...
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-06-28 Manman RenDebug Info: clean up usage of Verify.
2013-05-21 Justin HolewinskiDrop @llvm.annotation and @llvm.ptr.annotation intrinsi...
2013-04-30 Manman RenTBAA: remove !tbaa from testing cases if not used.
2013-03-25 Jyotsna VermaXFAIL some of the generic CodeGen tests for Hexagon.
2013-03-20 Hao LiuAdd a test case for PR15318 fixed in r177472
2013-01-11 Eric ChristopherFor inline asm:
2012-12-19 Nadav RotemAfter reducing the size of an operation in the DAG...
2012-12-11 Paul Redmondmove X86-specific test
2012-11-13 Duncan SandsCodegen support for arbitrary vector getelementptrs.
2012-08-24 Manman RenBranchProb: modify the definition of an edge in BranchP...
2012-08-17 Benjamin KramerFix broken check lines.
2012-08-10 Eli FriedmanThe normal edge of an invoke is not allowed to branch...
2012-07-15 Nadav RotemFix a bug in the scalarization of BUILD_VECTOR. BUILD_V...
2012-07-02 Bob WilsonExtend TargetPassConfig to allow running only a subset...
2012-07-02 Chandler CarruthConvert the uses of '|&' to use '2>&1 |' instead, which...
2012-06-28 Nuno Lopesadd a new @llvm.donothing intrinsic that, well, does...
2012-06-26 Rafael EspindolaFix llc's -print-before=pass and -print-after=pass.
2012-06-26 Jack CarterThere are a number of generic inline asm operand modifi...
2012-06-25 Jakob Stoklund OlesenEnforce stricter liveness rules for PHIs.
2012-06-22 NAKAMURA Takumitest/CodeGen/Generic/asm-large-immediate.ll: Mark it...
2012-06-21 Jack CarterThe inline asm operand modifier 'n' is suppose
2012-06-21 NAKAMURA TakumiRevert r158209, "test/CodeGen/Generic/APIntLoadStore...
2012-06-11 Jakob Stoklund OlesenFix test case to work on ARM.
2012-06-08 Jakob Stoklund OlesenDon't run RAFast in the optimizing regalloc pipeline.
2012-06-08 Chad RosierFix a crash in APInt::lshr when shiftAmt > BitWidth.
2012-06-08 NAKAMURA Takumitest/CodeGen/Generic/APIntLoadStore.ll: Mark as XFAIL...
2012-05-30 Bob WilsonAdd an insertPass API to TargetPassConfig. <rdar:...
2012-05-22 Nuno Lopesrevert my previous patches that introduced an additiona...
2012-05-09 Nuno Lopeschange the objectsize intrinsic signature: add a 3rd...
2012-04-16 Bill WendlingMove to X86 directory because this fails on non-X86...
2012-04-10 Rafael EspindolaDon't try to zExt just to check if an integer constant...
2012-04-03 Pete CooperAdd VSELECT to LegalizeVectorTypes::ScalariseVectorResu...
2012-03-30 Bill WendlingAdd testcase for r153705
2012-03-21 Andrew Trickmisched: tag a few XFAILs that I plan to fix
2012-03-21 Andrew TrickI meant to disable this test, not XFAIL it
2012-03-21 Andrew Trickmisched: beginning to add unit tests
2012-02-16 Eli BenderskyReplace all instances of dg.exp file with lit.local...
2012-02-02 NAKAMURA TakumiMove test/CodeGen/Generic/2012-02-01-CoalescerBug.ll...
2012-02-02 Lang HamesPR11868. The previous loop in LiveIntervals::join would...
2012-01-31 Bill WendlingRemove all references to the old EH.
2011-12-12 Chandler CarruthManually upgrade the test suite to specify the flag...
2011-10-16 Nadav RotemRemove the the test which checks the saving of a vector...
2011-09-26 David MeyerPR11004: Inline memcpy to avoid generating nested call...
2011-09-20 Bill WendlingThis test is completely invalid with the modern EH...
2011-09-08 Nadav RotemThis test is already covered by llvm/trunk/test/CodeGen...
2011-09-08 Nadav RotemAdd X86-SSE4 codegen support for vector-select.
2011-09-03 Dan GohmanRevert r129875, XFAILing this test for arm, since the...
2011-09-02 Bill WendlingTry to eliminate the use of the 'unwind' instruction.
2011-09-01 Benjamin KramerXFAIL this test on arm until the backend is fixed.
2011-08-31 Bill WendlingRevert r138894. This was failing on cmake-clang-i686...
2011-08-31 Bill WendlingUpdate more tests to the new EH scheme.
2011-08-26 Bill WendlingRevert r138606 until LowerInvoke has been converted...
2011-08-25 Bill WendlingUpdate to the new EH scheme.
2011-08-25 Bill WendlingLSR wants to split the landing pad's critical edge...
2011-07-12 Andrew TrickComment correction.
2011-07-09 Chris LattnerLand the long talked about "type system rewrite" patch...
2011-07-09 Chris Lattnermore tests not making the jump into the brave new world.
2011-07-07 Lang HamesAdded a testcase for PR10220.
2011-07-06 Jakub StaszakIntroduce "expect" intrinsic instructions.
2011-06-24 Devang PatelHandle debug info for i128 constants.
next