]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/DebugInfo/X86/DW_AT_specification.ll
IR: Make metadata typeless in assembly
[opencl/llvm.git] / test / DebugInfo / X86 / DW_AT_specification.ll
2014-12-15 Duncan P. N. Exon... IR: Make metadata typeless in assembly
2014-10-06 Frederic Riss[dwarfdump] Print the name for referenced specification...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-06-24 David BlaikieFix up scoping in a few tests (and delete one that...
2014-05-21 David BlaikieDebugInfo: Simplify subprogram declaration creation...
2014-05-14 David BlaikieDebugInfo: Sure up subprogram variable list handling...
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2013-11-22 Manman RenDebug Info: update testing cases to specify the debug...
2013-10-29 Manman RenDebug Info: use createAndAddDIE for newly-created Subpr...
2013-10-04 Rafael EspindolaFix this test.
2013-10-04 David BlaikieDebugInfo: Fix ordering of members after r191928
2013-09-08 Manman RenDebug Info Testing: update context from empty string...
2013-09-06 Manman RenDebug Info Testing: updated to use NULL instead of...
2013-09-06 Manman RenDebug Info Testing: Updated to use null instead of...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-08-19 David Blaikiellvm-dwarfdump: Do not include address offsets for...
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-21 David BlaikieMove the DIFile in DISubprogram to the beginning to...
2013-03-21 David BlaikieRemove unused field in DISubprogram
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-12 David BlaikieUpdate debug info test cases with empty SplitDebugFilen...
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-02-02 David BlaikieRemove the (apparently) unnecessary debug info metadata...
2013-01-25 Eli BenderskyNow that llvm-dwarfdump supports flags to specify which...
2012-08-01 Eric ChristopherTemporarily revert c23b933d5f8be9b51a1d22e717c0311f65f8...
2012-07-27 Eric ChristopherAdd a DW_AT_high_pc for CUs that are a single address...
2012-03-15 Eric ChristopherFor types with a parent of the compile unit make sure...
2012-03-15 Eric ChristopherRevert the removal of DW_AT_MIPS_linkage_name when...
2012-03-14 Eric ChristopherRemove the DW_AT_MIPS_linkage name attribute when we...
2012-02-22 Eric ChristopherOnly add DW_AT_prototyped if we're working with a C...
2012-02-21 Eric ChristopherThere's no need for a DW_AT_byte_size on a pointer...
2012-01-24 Eric ChristopherFix the testcases for the previous patch.
2011-11-11 Devang PatelMove X86 specific test in X86 directory.