Regenerate this stale testcase from source.
[opencl/llvm.git] / test / DebugInfo / X86 / block-capture.ll
2014-12-05 Adrian PrantlRegenerate this stale testcase from source.
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-08-06 David BlaikieDebugInfo: Assert that any CU for which debug_loc lists...
2014-06-30 Adrian PrantlDebug info: split out complex DIVariable address expres...
2014-06-24 David BlaikieFix up scoping in a few tests (and delete one that...
2014-06-13 David BlaikieDebugInfo: Refactor some tests to allow DW_AT_name...
2014-05-23 David BlaikieDebugInfo: Generalize a test case to not depend on...
2014-05-14 David BlaikieDebugInfo: Sure up subprogram variable list handling...
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2013-11-22 Manman RenDebug Info: update testing cases to specify the debug...
2013-11-21 Eric ChristopherIn Dwarf 3 (and Dwarf 2) attributes whose value are...
2013-11-16 Eric ChristopherFor dwarf4 use the correct form for referencing debug_l...
2013-09-08 Manman RenDebug Info Testing: update context from empty string...
2013-09-06 Manman RenDebug Info Testing: Updated to use null instead of...
2013-09-04 Eric ChristopherRemove hack ensuring that darwin didn't produce dwarf...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-08-19 David Blaikiellvm-dwarfdump: Do not include address offsets for...
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-21 David BlaikieMove the DIFile in DISubprogram to the beginning to...
2013-03-21 David BlaikieRemove unused field in DISubprogram
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRemove the unused 4th operand for DIFile debug info...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-12 David BlaikieUpdate debug info test cases with empty SplitDebugFilen...
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-02-02 David BlaikieRemove the (apparently) unnecessary debug info metadata...
2013-01-25 Eli BenderskyNow that llvm-dwarfdump supports flags to specify which...
2012-08-01 Eric ChristopherTemporarily revert c23b933d5f8be9b51a1d22e717c0311f65f8...
2012-07-27 Eric ChristopherAdd a DW_AT_high_pc for CUs that are a single address...
2012-02-24 Eric ChristopherIf the Address of a variable is an argument then treat...