]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/DebugInfo/X86/concrete_out_of_line.ll
Debug info: (bugfix) C++ C/Dtors can be compiled to multiple functions,
[opencl/llvm.git] / test / DebugInfo / X86 / concrete_out_of_line.ll
2014-04-12 Adrian PrantlDebug info: (bugfix) C++ C/Dtors can be compiled to...
2014-03-07 David BlaikieDebugInfo: Refactor test to not rely on fixed DIE offsets
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2014-01-24 Eric ChristopherRevert "Use DW_AT_high_pc and DW_AT_low_pc for the...
2014-01-24 Eric ChristopherUse DW_AT_high_pc and DW_AT_low_pc for the high and...
2014-01-03 David BlaikieRevert "Reverting r193835 due to weirdness with Go..."
2014-01-03 David BlaikieReverting r193835 due to weirdness with Go...
2013-11-22 Manman RenDebug Info: update testing cases to specify the debug...
2013-11-01 David BlaikieDebugInfo: Emit member variable locations as data inste...
2013-10-04 David BlaikieDebugInfo: Fix ordering of members after r191928
2013-09-08 Manman RenDebug Info Testing: update context from empty string...
2013-09-06 Manman RenDebug Info Testing: updated to use NULL instead of...
2013-09-06 Manman RenDebug Info Testing: Updated to use null instead of...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-05-09 Eric ChristopherRevert "Make sure debug info contains linkage names...
2013-05-08 Eric ChristopherMake sure debug info contains linkage names (DW_AT_MIPS...
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-22 David BlaikieReorder the DIFile field in DILexicalBlock to become...
2013-03-21 David BlaikieMove the DIFile in DISubprogram to the beginning to...
2013-03-21 David BlaikieRemove unused field in DISubprogram
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-12 David BlaikieUpdate debug info test cases with empty SplitDebugFilen...
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-02-04 David Blaikie[DebugInfo] remove more node indirection (this time...
2013-02-02 David BlaikieRemove the (apparently) unnecessary debug info metadata...
2013-01-25 Eli BenderskyNow that llvm-dwarfdump supports flags to specify which...
2012-08-24 Eric ChristopherUse DW_FORM_flag_present to save space in debug informa...
2012-08-23 Eric ChristopherRemove the DW_AT_MIPS_linkage name attribute when we...
2012-08-01 Eric ChristopherTemporarily revert c23b933d5f8be9b51a1d22e717c0311f65f8...
2012-07-27 Eric ChristopherAdd a DW_AT_high_pc for CUs that are a single address...
2012-03-15 Eric ChristopherFor types with a parent of the compile unit make sure...
2012-03-15 Eric ChristopherRevert the removal of DW_AT_MIPS_linkage_name when...
2012-03-14 Eric ChristopherRemove the DW_AT_MIPS_linkage name attribute when we...
2012-02-22 Eric ChristopherOnly add DW_AT_prototyped if we're working with a C...
2012-02-21 Eric ChristopherThere's no need for a DW_AT_byte_size on a pointer...
2012-01-24 Eric ChristopherFix the testcases for the previous patch.
2011-11-12 Rafael EspindolaThe dwarf standard says that the only differences betwe...