]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/DebugInfo/X86/dbg-value-inlined-parameter.ll
IR: Move MDLocation into place
[opencl/llvm.git] / test / DebugInfo / X86 / dbg-value-inlined-parameter.ll
2015-01-14 Duncan P. N. Exon... IR: Move MDLocation into place
2014-12-15 Duncan P. N. Exon... IR: Make metadata typeless in assembly
2014-10-10 Frederic Riss[dwarfdump] Resolve also variable specifications/abstra...
2014-10-06 Frederic Riss[dwarfdump] Print the name for referenced specification...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-08-06 David BlaikieDebugInfo: Assert that any CU for which debug_loc lists...
2014-06-13 David BlaikieDebugInfo: Reference abstract definitions from variable...
2014-06-13 David BlaikieDebugInfo: Refactor some tests to allow DW_AT_name...
2014-05-31 Alp TokerFix typos
2014-05-27 David BlaikieDebugInfo: Create abstract function definitions even...
2014-05-27 David BlaikieDebugInfo: Lazily attach definition attributes to defin...
2014-05-27 David BlaikieDebugInfo: Fix argument ordering in test by adding...
2014-05-23 David BlaikieDebugInfo: Generalize some tests to handle variations...
2014-03-07 Adrian PrantlRemove unnecessary test for Darwin and update testcase...
2014-03-07 David BlaikieDebugInfo: Use DW_FORM_data4 for DW_AT_high_pc in inlin...
2014-03-07 David BlaikieDebugInfo: Update test to cover linux (with a FIXME...
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2013-11-22 Manman RenDebug Info: update testing cases to specify the debug...
2013-09-06 Manman RenDebug Info Testing: updated to use NULL instead of...
2013-09-06 Manman RenDebug Info Testing: Updated to use null instead of...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-07-29 Manman RenDebug Info: update testing cases to pass verifier.
2013-07-24 Manman RenUpdate testing cases to pass debug info verifier.
2013-07-19 Manman RenDebug Info: enable verifying by default and disable...
2013-06-20 David BlaikieDebugInfo: don't use location lists when the location...
2013-05-02 Manman RenTBAA: remove !tbaa from testing cases if not used.
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-22 David BlaikieReorder the DIFile field in DILexicalBlock to become...
2013-03-21 David BlaikieMove the DIFile in DISubprogram to the beginning to...
2013-03-21 David BlaikieRemove unused field in DISubprogram
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRemove the unused 4th operand for DIFile debug info...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-03-08 David BlaikieUpgrade tests to the latest debug info format.
2013-01-25 Eli BenderskyNow that llvm-dwarfdump supports flags to specify which...
2012-12-27 Eric ChristopherFileCheck-ize.
2012-12-21 Eric ChristopherMove these files over to the debug info directory.