]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/DebugInfo/X86/pr11300.ll
Move the complex address expression out of DIVariable and into an extra
[opencl/llvm.git] / test / DebugInfo / X86 / pr11300.ll
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-05-23 David BlaikieDebugInfo: Generalize some tests to handle variations...
2014-05-21 David BlaikieDebugInfo: Simplify subprogram declaration creation...
2014-05-14 David BlaikieDebugInfo: Sure up subprogram variable list handling...
2014-02-04 David BlaikieDebugInfo: Remove some unneeded conditionals now that...
2013-11-22 Manman RenDebug Info: update testing cases to specify the debug...
2013-10-29 Manman RenDebug Info: use createAndAddDIE for newly-created Subpr...
2013-10-04 David BlaikieDebugInfo: Fix ordering of members after r191928
2013-09-08 Manman RenDebug Info Testing: update context from empty string...
2013-09-06 Manman RenDebug Info Testing: updated to use NULL instead of...
2013-09-04 Eric ChristopherRemove hack ensuring that darwin didn't produce dwarf...
2013-08-26 Manman RenDebug Info: add an identifier field to DICompositeType.
2013-08-19 David Blaikiellvm-dwarfdump: Do not include address offsets for...
2013-04-22 David BlaikieRevert "Revert "PR14606: debug info imported_module...
2013-04-19 Eric ChristopherRevert "PR14606: debug info imported_module support"
2013-04-19 David BlaikiePR14606: debug info imported_module support
2013-03-28 David BlaikieRevert "Adding DIImportedModules to DIScopes."
2013-03-27 David BlaikieAdding DIImportedModules to DIScopes.
2013-03-22 David BlaikieReorder the DIFile field in DILexicalBlock to become...
2013-03-21 David BlaikieMove the DIFile in DISubprogram to the beginning to...
2013-03-21 David BlaikieRemove unused field in DISubprogram
2013-03-20 David BlaikieDebug info: refactor the first field of DICompileUnit...
2013-03-20 David BlaikieDebug Info: Swap the 2nd and 3rd parameters to DICompil...
2013-03-20 David BlaikieRemove unused field in DICompileUnit
2013-03-20 David BlaikieRefactor the DIFile (2nd) parameter to DITypes to be...
2013-03-19 David BlaikieMove the DIFile operand to DITypes from the 4th operand...
2013-03-17 David BlaikieSplit out filename & directory from DIFile to start...
2013-03-13 David BlaikieRemove the unused 4th operand for DIFile debug info...
2013-03-13 David BlaikieRefactor filename/directory in DICompileUnit into a...
2013-03-12 David BlaikieRemove unused "isMain" field from DICompileUnit
2013-03-12 David BlaikieUpdate debug info test cases with empty SplitDebugFilen...
2013-03-11 David BlaikieUpgrading debug info test cases to be (more) compatible...
2013-02-02 David BlaikieRemove the (apparently) unnecessary debug info metadata...
2013-01-25 Eli BenderskyNow that llvm-dwarfdump supports flags to specify which...
2012-08-01 Eric ChristopherTemporarily revert c23b933d5f8be9b51a1d22e717c0311f65f8...
2012-07-27 Eric ChristopherAdd a DW_AT_high_pc for CUs that are a single address...
2012-03-15 Eric ChristopherFor types with a parent of the compile unit make sure...
2012-03-15 Eric ChristopherRevert the removal of DW_AT_MIPS_linkage_name when...
2012-03-14 Eric ChristopherRemove the DW_AT_MIPS_linkage name attribute when we...
2012-02-22 Eric ChristopherOnly add DW_AT_prototyped if we're working with a C...
2012-02-21 Eric ChristopherThere's no need for a DW_AT_byte_size on a pointer...
2012-01-24 Eric ChristopherFix the testcases for the previous patch.
2011-11-11 Devang PatelMove X86 specific test in X86 directory.