]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/DebugInfo
[X86][AVX] Simplified diff between AVX1 and SSE42 fp stack folding tests. NFC.
[opencl/llvm.git] / test / DebugInfo /
2015-01-20 Adrian PrantlDebugLocs without a scope should fail the verification.
2015-01-20 Adrian PrantlReapply: Teach SROA how to update debug info for fragme...
2015-01-19 Adrian PrantlRemove support for DIVariable's FlagIndirectVariable...
2015-01-14 Duncan P. N. Exon... IR: Move MDLocation into place
2015-01-13 Adrian PrantlDebug Info: Move the complex expression handling (...
2015-01-13 Will SchmidtUpdate multiline.ll testcase to handle (ppc64le) .local...
2015-01-12 Adrian PrantlDebug info: Factor out the creation of DWARF expression...
2015-01-08 Adrian PrantlRevert "Reapply: Teach SROA how to update debug info...
2015-01-07 Adrian PrantlReapply: Teach SROA how to update debug info for fragme...
2015-01-07 Adrian PrantlDebug info: Allow aggregate types to be described by...
2015-01-06 Adrian PrantlRevert "Reapply: Teach SROA how to update debug info...
2015-01-06 Adrian PrantlReapply: Teach SROA how to update debug info for fragme...
2014-12-31 Colin LeMahieuReverting 225045 and 225043 and XFAIL multiline.ll...
2014-12-30 David BlaikieFix a test case to not depend on asm comment syntax...
2014-12-30 David BlaikieGeneralize even further, for ARM comment syntax (@)
2014-12-30 David BlaikieGeneralize test case to handle different asm syntax...
2014-12-30 David BlaikieDebugInfo: Omit is_stmt from line table entries on...
2014-12-26 Timur IskhodzhanovBand-aid fix for PR22032: don't emit DWARF debug info...
2014-12-24 Saleem AbdulrasoolIAS: correct debug line info for asm macros
2014-12-24 Adrian PrantlDebug Info: In symmetry to DW_TAG_pointer_type, do...
2014-12-23 Chandler CarruthRevert r224739: Debug info: Teach SROA how to update...
2014-12-22 Adrian PrantlThumb1 frame lowering: Mark CFI instructions with the...
2014-12-22 Adrian PrantlDebug info: Teach SROA how to update debug info for...
2014-12-17 David BlaikiePR21875: codegen for non-type template parameters of...
2014-12-16 Adrian PrantlARM/AArch64: Attach the FrameSetup MIFlag to CFI instru...
2014-12-15 Duncan P. N. Exon... IR: Make metadata typeless in assembly
2014-12-12 Ekaterina RomanovaA fix for PR21176.
2014-12-11 Ekaterina RomanovaReverting commit 223981, because the test that I added...
2014-12-10 Ekaterina RomanovaA fix for PR21176.
2014-12-09 Frederic RissCorrectly handle complex locations expressions in repla...
2014-12-05 Adrian PrantlFix a bug when pretty-printing DW_OP_deref.
2014-12-05 Adrian PrantlRegenerate this stale testcase from source.
2014-12-05 Adrian PrantlAdd a comment.
2014-12-04 Adrian PrantlSimplify implementation and testcase of r223401 based...
2014-12-04 Adrian PrantlDebug info: If the RegisterCoalescer::reMaterializeTriv...
2014-11-29 Hans WennborgSwitch lowering: Fix broken 'Figure out which block...
2014-11-21 Manman RenDebug Info: revert r222195, r222210 and r222239.
2014-11-18 Manman RenRemove triple in testing case to recover an arm bot.
2014-11-18 Frederic RissAllow DwarfCompileUnit::constructImportedEntityDIE...
2014-11-18 Manman RenUpdate testing case that was accidently duplicated.
2014-11-18 Manman RenDebug Info: In DIBuilder, the context field of a global...
2014-11-14 Frederic RissAdd a test for r222029 that doesn't rely on the default...
2014-11-14 Frederic Riss[dwarfdump] Handle relocations in Dwarf accelerator...
2014-11-14 Frederic RissTentatively appease the bots.
2014-11-14 Frederic RissReapply "[dwarfdump] Add support for dumping accelerato...
2014-11-13 Frederic RissAdd an assert and a test that verify r221709's fix.
2014-11-13 Frederic RissRevert "[dwarfdump] Add support for dumping accelerator...
2014-11-12 Frederic RissFix emission of Dwarf accelerator table when there...
2014-11-12 Frederic Riss[dwarfdump] Add support for dumping accelerator tables.
2014-11-12 Timur IskhodzhanovTemporary fix for PR21528 - use mangled C++ function...
2014-11-12 Timur Iskhodzhanov[COFF] Make it clearer that the symbols subsection...
2014-11-04 David BlaikieProvide gmlt-like inline scope information in the skele...
2014-11-04 NAKAMURA TakumiRemove "REQUIRES:shell" from tests. They work for me.
2014-11-04 David MajnemerCodeGen: Enable DWARF emission for MS ABI targets
2014-11-03 Oliver StannardRevert r221150, as it broke sanitizer tests
2014-11-03 Oliver StannardEmit .eh_frame with relocations to functions, rather...
2014-11-01 David BlaikieTest 221067 in a fixed-target test so as not to fail...
2014-11-01 David BlaikieRemove test coverage added in 221067 due to it being...
2014-11-01 David BlaikieRemove DwarfUnit::LabelEnd in favor of computing the...
2014-10-30 David BlaikiePR21408: Workaround the appearance of duplicate variabl...
2014-10-24 Timur IskhodzhanovFix PR21189 -- Emit symbol subsection required to debug...
2014-10-23 David BlaikieDebugInfo: Remove DwarfDebug::CurrentFnArguments since...
2014-10-23 David BlaikieDebugInfo: Simplify/tidy/correct global variable decl...
2014-10-23 Frederic Riss[dwarfdump] Dump DW_AT_ranges values inline in the...
2014-10-21 Rafael EspindolaFix a bit of confusion about .set and produce more...
2014-10-21 Paul RobinsonDo not attribute static allocas to the call site's...
2014-10-10 Frederic Riss[dwarfdump] Prettyprint DW_AT_APPLE_property_attribute...
2014-10-10 Frederic Riss[dwarfdump] Resolve also variable specifications/abstra...
2014-10-08 Timur IskhodzhanovFix COFF section index relocation should be 16 bits...
2014-10-08 David Majnemerllvm-dwarfdump: Add support for some COFF relocations
2014-10-06 Eric ChristopherFor biendian targets like ARM and AArch64, it is useful...
2014-10-06 Eric ChristopherAdd support for ARM and AArch64 big endian objects to
2014-10-06 Eric ChristopherAdd some tests for RelocVisitor.
2014-10-06 Frederic Riss[dwarfdump] Print the name for referenced specification...
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Justin Bognertest: XFAIL the non-darwin gmlt test on darwin
2014-10-01 David BlaikieImplement DW_TAG_subrange_type with DW_AT_count rather...
2014-10-01 NAKAMURA Takumillvm/test/DebugInfo/X86/gmlt.test: Get rid of %llc_dwar...
2014-09-30 David BlaikieOmit DW_AT_inline under -gmlt to save a little more...
2014-09-30 David BlaikieAdjust test case addition in r218702 so as not to fail...
2014-09-30 David BlaikieDisable the -gmlt optimization implemented in r218129...
2014-09-24 Renato GolinRemoving empty tests from failed revert
2014-09-24 Renato GolinRevert 218406 - Refactor the RelocVisitor::visit method
2014-09-24 Renato GolinRevert 218411 - XFAIL reloc test on x86/hexagon
2014-09-24 Renato GolinXFAIL reloc test on x86/hexagon
2014-09-24 Renato GolinRefactor the RelocVisitor::visit method
2014-09-24 Kaelyn TakataRevert "Refactor the RelocVisitor::visit method"
2014-09-24 Renato GolinRefactor the RelocVisitor::visit method
2014-09-23 Oliver StannardFix segfault in AArch64 backend with -g and -mbig-endian
2014-09-23 Timur IskhodzhanovFix a small typo in the test comment
2014-09-22 Frederic RissFix a test introduced in r218246 to work also on Windows.
2014-09-22 Frederic Riss[dwarfdump] Dump full filenames as DW_AT_(decl|call...
2014-09-22 Frederic RissAllow DWARFDebugInfoEntryMinimal::getSubroutineName...
2014-09-20 David MajnemerUpdate tests which broke from r218189
2014-09-19 David BlaikieFix test case to be portable to different architectures.
next