]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/Transforms/InstSimplify
Updates to sync with changes in upstream.
[opencl/llvm.git] / test / Transforms / InstSimplify /
2014-12-20 David MajnemerInstSimplify: Optimize away pointless comparisons
2014-12-18 David MajnemerConstantFold: Shifting undef by zero results in undef
2014-12-17 David MajnemerInstSimplify: shl nsw/nuw undef, %V -> undef
2014-12-11 David MajnemerInstSimplify: Remove usesless %a parameter from tests
2014-12-10 David MajnemerConstantFold: an undef shift amount results in undef
2014-12-10 David MajnemerConstantFold: div undef, 0 should fold to undef, not...
2014-12-10 David MajnemerInstSimplify: [al]shr exact undef, %X -> undef
2014-12-10 David MajnemerInstSimplify: div %X, 0 -> undef
2014-12-08 David MajnemerInstSimplify: Try to bring back the rest of r223583
2014-12-08 NAKAMURA TakumiRevert a part of r223583, for now. It seems causing...
2014-12-06 David MajnemerInstSimplify: Optimize away useless unsigned comparisons
2014-12-04 Hal FinkelRevert "r223364 - Revert r223347 which has caused crash...
2014-12-04 Alexander PotapenkoRevert r223347 which has caused crashes on bootstrap...
2014-12-04 Hal FinkelRestrict somewhat the memory-allocation pointer cmp...
2014-12-01 Hal FinkelSimplify pointer comparisons involving memory allocatio...
2014-11-27 David MajnemerInstSimplify: Restore optimizations lost in r210006
2014-11-25 David MajnemerInstSimplify: Handle some simple tautological comparisons
2014-11-22 David MajnemerInstSimplify: Simplify (sub 0, X) -> X if it's NUW
2014-11-05 David MajnemerInstSimplify: Exact shifts of X by Y are X if X has...
2014-10-22 Bruno Cardoso Lopes[InstSimplify] Support constant folding to vector of...
2014-10-21 David MajnemerInstCombine: Simplify FoldICmpCstShrCst
2014-10-20 Philip ReamesIntroduce a 'nonnull' metadata on Load instructions.
2014-10-14 Hal FinkelRevert "r216914 - Revert: [APFloat] Fixed a bug in...
2014-10-11 David MajnemerInstCombine, InstSimplify: (%X /s C1) /s C2 isn't alway...
2014-09-17 David MajnemerInstSimplify: Don't allow (x srem y) urem y -> x srem y
2014-09-17 David MajnemerInstSimplify: ((X % Y) % Y) -> (X % Y)
2014-09-15 David MajnemerInstSimplify: Simplify trivial and/or of icmps
2014-09-02 Andrea Di BiagioRevert: [APFloat] Fixed a bug in method 'fusedMultiplyAdd'.
2014-09-02 Andrea Di Biagio[APFloat] Fixed a bug in method 'fusedMultiplyAdd'.
2014-08-28 David MajnemerInstSimplify: Move a transform from InstCombine to...
2014-08-27 David MajnemerInstSimplify: Don't simplify gep X, (Y-X) to Y if types...
2014-08-27 Nico WeberReland r216439 215441, majnemer has a real fix for...
2014-08-27 Nico WeberRevert r216439 (and r216441, else the former doesn...
2014-08-27 David MajnemerInstSimplify: Compute comparison ranges for left shift...
2014-08-26 David MajnemerInstSimplify: Fold gep X, (sub 0, ptrtoint(X)) to null
2014-08-26 David MajnemerInstSimplify: Simplify trivial pointer expressions...
2014-08-22 David MajnemerValueTracking: Figure out more bits when looking at...
2014-07-31 David MajnemerInstSimplify: Simplify (X - (0 - Y)) if the second...
2014-07-25 Hal FinkelAdd @llvm.assume, lowering, and some basic properties
2014-07-18 Hal FinkelAdd a dereferenceable attribute
2014-07-17 Suyog SardaMove ashr optimization from InstCombineShift to InstSim...
2014-07-14 David MajnemerFix a test broken in r212981
2014-07-14 David MajnemerInstSimplify: Correct sdiv x / -1
2014-07-14 David MajnemerInstSimplify: The upper bound of X / C was missing...
2014-07-04 David MajnemerInstSimplify: Fix a bug when INT_MIN is in a sdiv
2014-06-26 Dinesh DwivediThis patch removed duplicate code for matching patterns
2014-06-19 Nick LewyckyMove optimization of some cases of (A & C1)|(B & C2...
2014-06-19 Nick LewyckyMake instsimplify's analysis of icmp eq/ne use computeK...
2014-05-20 Nick LewyckyTeach isKnownNonNull that a nonnull return is not null...
2014-05-16 David MajnemerInstSimplify: Improve handling of ashr/lshr
2014-05-16 David MajnemerInstSimplify: Optimize using dividend in sdiv
2014-05-14 David MajnemerInstSimplify: Optimize signed icmp of -(zext V)
2014-04-26 Gerolf HoflehnerRecursivelyDeleteTriviallyDeadInstructions() could...
2014-04-26 Gerolf HoflehnerRevert commit r207302 since build failures
2014-04-26 Gerolf HoflehnerRecursivelyDeleteTriviallyDeadInstructions() could...
2014-01-24 Benjamin KramerInstSimplify: Make shift, select and GEP simplification...
2013-09-28 Benjamin KramerAdd a test that large offsets on GEPs on 32 bits target...
2013-09-24 Benjamin KramerVerify that we don't optimize null return checks to...
2013-09-24 Benjamin KramerMemoryBuiltins: Fix operator new bits.
2013-09-24 Benjamin KramerTeach MemoryBuiltins and InstructionSimplify that opera...
2013-09-23 Benjamin KramerExpand test case a bit.
2013-09-23 Benjamin KramerInstSimplify: Fold equality comparisons between non...
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-07-14 Stephen LinUpdate Transforms tests to use CHECK-LABEL for easier...
2013-07-12 Nick LewyckyFix logic error optimizing "icmp pred (urem X, Y),...
2013-07-09 David MajnemerInstSimplify: X >> X -> 0
2013-04-19 Benjamin KramerConstantFolding: ComputeMaskedBits wants the scalar...
2013-04-11 Benjamin KramerAdd missing colons to check lines.
2013-03-18 Manman RenCheck whether a pointer is non-null (isKnownNonNull...
2013-02-08 Chad Rosier[SimplifyLibCalls] Library call simplification doen...
2013-02-07 Michael IlsemanIdentify and simplify idempotent intrinsics. Test case...
2013-02-05 Benjamin KramerConstantFolding: Fix a crash when encoutering a truncat...
2013-02-01 Dan GohmanAdd a testcase for some past-the-end address subtleties.
2013-02-01 Benjamin KramerInstSimplify: stripAndComputeConstantOffsets can be...
2013-02-01 Dan GohmanRewrite instsimplify's handling if icmp on pointer...
2013-01-31 Dan GohmanAn alloca can be equal to an argument. It can't *alias...
2012-12-30 Dmitri GribenkoTests: rewrite 'opt ... %s' to 'opt ... < %s' so that...
2012-12-28 Chandler CarruthTeach instsimplify to use the constant folder where...
2012-12-12 Michael IlsemanAdded a slew of SimplifyInstruction floating-point...
2012-12-07 Chandler CarruthAdd support to ValueTracking for determining that a...
2012-11-27 Michael IlsemanFast-math test for SimplifyInstruction: fold multiply...
2012-11-16 Duncan SandsInstructionSimplify should be able to simplify A+B...
2012-03-28 Chad RosierRevert r153521 as it's causing large regressions on...
2012-03-27 Chad RosierReapply r153423; the original commit was fine. The...
2012-03-26 Chad RosierRevert r153423 as this is causing failures on our inter...
2012-03-26 Rafael EspindolaUse the new range metadata in computeMaskedBits and...
2012-03-25 Chandler CarruthTeach instsimplify how to simplify comparisons of point...
2012-03-25 Chandler CarruthSwitch the pointer-difference simplification logic...
2012-03-13 Duncan SandsGeneralize the "trunc(ptrtoint(x)) - trunc(ptrtoint...
2012-03-12 Chandler CarruthTeach instsimplify how to constant fold pointer differe...
2012-03-05 Eli FriedmanMake sure we don't return bits outside the mask in...
2012-02-26 Nick LewyckyReinstate the optimization from r151449 with a fix...
2012-02-25 Nick LewyckyRoll these back to r151448 until I figure out how they...
2012-02-25 Nick LewyckyAn argument and a local identified object (eg. a noalia...
2012-02-25 Nick LewyckyTeach instsimplify to be more aggressive when analyzing...
2012-02-24 Chris Lattnerfix PR12075, a regression in a recent transform I added...
2012-02-20 Chris Lattnerfold comparisons of gep'd alloca points with null to...
2012-02-18 Eli FriedmanFix a rather nasty regression from r150690: LHS !=...
2012-02-16 Benjamin KramerInstSimplify: Ignore pointer casts when constant foldin...
2012-02-16 Eli BenderskyReplace all instances of dg.exp file with lit.local...
next