]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/lit.cfg
Remove unnecessary test for Darwin and update testcase to be a little less
[opencl/llvm.git] / test / lit.cfg
2014-02-17 Duncan P. N. Exon... PGO: llvm-profdata: tool for merging profiles
2014-01-30 Timur IskhodzhanovReland r200340 - 'Add line table debug info to COFF...
2014-01-22 Alp TokerEliminate inappropriate use of FindProgramByName()...
2013-12-03 NAKAMURA Takumicheck-llvm: Ask llvm-config about assertion mode, inste...
2013-10-28 Alp Tokerlit: add missing substitutions for recently added tools
2013-10-26 NAKAMURA Takumillvm/test/lit.cfg: Tighten conditions to enable 'native'.
2013-10-23 Anders WaldenborgAdd llvm-c-test tool for testing llvm-c
2013-10-02 Chandler CarruthRemove the very substantial, largely unmaintained legac...
2013-10-02 Chandler CarruthDon't layout items in a list in columns. That requires...
2013-09-30 Eric ChristopherAdd llvm-readobj to the list of programs to find in...
2013-09-20 Andrew KaylorFix some more MCJIT PIC test XFAILs (for i386)
2013-09-19 Peter CollingbourneFix LTO handling of module-level assembly (PR14152).
2013-09-13 Amaury de la VieuvilleAdd "native" to config.available_features, to make...
2013-08-30 Alexey SamsonovRestore llvm-ranlib expansion in RUN-lines removed...
2013-08-21 Daniel Dunbar[tests] Update fma3 check to work with Py3.
2013-08-21 Nadav RotemAdd the FMA3 feature in order to test FMA encoding...
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-08-09 Daniel Dunbar[tests] Update to use lit_config and lit package, as...
2013-08-08 Daniel Dunbar[lit] Remove on_clone member, which is no longer used.
2013-08-07 Daniel Dunbar[tests] Make string encoding issues explicit.
2013-08-04 Bob WilsonRemove "lto_on_osx" xfails, now that -rdynamic works...
2013-07-11 David DeanAdd the ability to use guarded malloc when running...
2013-06-26 NAKAMURA TakumiSuppress llvm/test/Other/can-execute.txt on msys bash.
2013-06-14 Rafael EspindolaRemove the LLVM specific archive index.
2013-06-14 Eli BenderskyDo not to perform RUN line substitution of llc if that...
2013-05-06 Tim NorthoverAArch64: use MCJIT by default and enable related tests.
2013-05-06 Ulrich Weigand[SystemZ] Set up JIT/MCJIT test cases
2013-04-23 Alexey SamsonovUse zlib to uncompress debug sections in DWARF parser.
2013-04-12 Nico RieckRemove obsolete object file dumpers
2013-04-10 Jyotsna VermaAdd object-emission flag for lit tests. This flag is...
2013-04-10 Reid Kleckner[test] Use lit's shell test runner on Windows
2013-04-04 Alexey SamsonovPropagate path to ASan/MSan symbolizer into test enviro...
2013-03-27 Evgeniy StepanovDisable ASan/MSan symbolization of reports in tests.
2013-03-26 Alexey SamsonovAdd asan/msan to the list of available features in...
2013-03-15 Alexey SamsonovFixup for r176933: more careful setup of path to llvm...
2013-03-13 Evgeniy StepanovSet symbolizer path in the test environment.
2013-01-16 Peter CollingbourneIntroduce llvm::sys::getProcessTriple() function.
2012-11-21 Andrew KaylorAdding tests for the Intel JIT event listener's MCJIT...
2012-11-01 NAKAMURA Takumillvm/test/lit.cfg: Don't use mcjit to ppc32 yet, not...
2012-10-30 Ulrich WeigandSet %defaultjit to use MCJIT for PowerPC targets.
2012-10-26 Rafael EspindolaFix unexpected passes. These test do work with LTO...
2012-10-19 Daniel Dunbartests: Stop mangling '-vg' into the triple, we don...
2012-10-18 Daniel Dunbartest: Add a lit config variable to check if LTO is...
2012-10-18 Sebastian PopUse pre-python 2.5 syntax in lit.cfg.
2012-10-05 NAKAMURA TakumiEnable llvm/test/ExecutionEngine/MCJIT also for cygwin.
2012-10-03 NAKAMURA Takumitest/ExecutionEngine/MCJIT: MCJIT should work also...
2012-10-02 Andrew KaylorSupport for generating ELF objects on Windows.
2012-10-02 James MolloyAdd default JIT LIT variable.
2012-07-03 NAKAMURA Takumillvm/test/lit.cfg: Retweak for Win32 to fix testing.
2012-07-02 Chandler CarruthConvert all tests using TCL-style quoting to use shell...
2012-07-02 Chandler CarruthSwitch a bunch of Linker tests from using elaborate...
2012-06-28 Chandler CarruthRemove 'site.exp' building from both CMake and configur...
2012-04-19 Michael J. SpencerRemove llvm-ld and llvm-stub (which is only used by...
2012-04-13 Sylvestre LedruCatch the Python exception when subprocess.Popen is...
2012-03-25 Eli BenderskyContinue cleanup of LIT, getting rid of the remaining...
2012-02-16 Eli BenderskyReplace all instances of dg.exp file with lit.local...
2012-01-16 Eli BenderskyAdding a basic ELF dynamic loader and MC-JIT for ELF...
2011-11-28 NAKAMURA Takumitest/lit.cfg: Enable the feature 'asserts' to check...
2011-11-05 Benjamin KramerUpdate lit's list of tools.
2011-10-27 Daniel Dunbartests: Rip out a bunch of now unused test code relating...
2011-10-06 Peter Collingbournes/tblgen/llvm-tblgen/g in a few missed places, includin...
2011-10-04 David DeanFix PR9833/PR11054 (patch provided by Patrik Hägglund)
2011-09-20 Eric ChristopherRemove llvm-gcc and various compiler handling from...
2011-08-30 Andrew TrickLit option for ignoring stderr output.
2011-06-22 Andrew Tricklit support for REQUIRES: asserts.
2011-02-24 NAKAMURA Takumitest/lit.cfg: Add PATHEXT to 'substitution', to recogni...
2011-02-22 Sean CallananFixed lit.cfg to no longer recognize the old
2011-02-09 NAKAMURA Takumitest/lit.cfg: Seek sane tools(and bash) in directories...
2011-01-05 Frits van BommelFix lit for people whose LLVM path contains 'opt',...
2011-01-04 Tobias GrosserInclude llvm-gcc dir before llvm_tools_dir
2011-01-04 David GreeneDon't pattern match "/clang" so we don't mangle directo...
2011-01-03 David GreeneDon't pattern match "clang-" as it may be part of a...
2011-01-03 David GreeneReapply 122341 to fix PR8199 now that clang changes...
2010-12-21 David GreeneRevert 122341. It breaks some darwin tests.
2010-12-21 David GreeneFix PR 8199. This patch prepends the build tool dir...
2010-12-07 NAKAMURA Takumitest: Add the feature 'shell' on LLVM_ON_UNIX.
2010-12-07 Michael J. SpencerTest: Fix Support.Path and _all_ of the unittest death...
2010-11-29 NAKAMURA Takumitest: Use $SharedLibDir for loadable modules. On Cygmin...
2010-11-29 NAKAMURA Takumitest: Add the new feature 'loadable_module'.
2010-11-25 Duncan SandsUse LLVMCC_EMITIR_FLAG rather than hard-coding "-emit...
2010-09-13 Duncan SandsSpelling fixes in comments.
2010-08-30 Michael J. SpencerTest: Fix LLVMC tests on CMake.
2010-08-20 Bob WilsonThe %ocamlopt setting has embedded quotes. Copy the...
2010-08-19 Daniel Dunbartests: Haste makes waste.
2010-08-19 Daniel Dunbartests: Ignore whitespace in llvm_supports_binding(...
2010-08-10 Daniel Dunbartests: Don't error out if HOME isn't present in t the...
2010-06-23 Daniel Dunbartests: Tweak lit.cfg to fix breakage with out-of-dir...
2010-06-12 Daniel Dunbartests: Propogate LLVM_SRC_ROOT and PYTHON_EXECUTABLE...
2010-03-20 Jeffrey YasskinAdd support for XFAILing valgrind runs with memory...
2010-03-20 Daniel Dunbartests: Mangle '-vg' onto the end of the triple when...
2010-03-08 John McCallRevert r97726 and r97728 at ddunbar's request; we want...
2010-03-04 John McCallTeach lit to honor conditional directives. The syntax is:
2010-02-25 Daniel Dunbartests: Propogate the HOME environment variable through...
2010-02-23 Daniel Dunbartests: Don't make a missing llvm-gcc dir a fatal error.
2010-02-23 Daniel DunbarFix a thinko in the lit.cfg.
2010-02-04 Benjamin KramerGet the LLVMC tests working with clang++ by removing...
2010-02-02 Daniel DunbarMCAssembler/Darwin: Add a test (on Darwin) that we...
2010-01-16 Daniel DunbarFix llvm_supports_binding for lit, problem noticed...
2009-12-08 Daniel DunbarCMake/lit: Add llvm_{unit_,}site_config parameters...
2009-11-08 Daniel DunbarDerive the right paths to use during testing instead...
next