For llvm-objdump, hook up existing options to work when using -macho (the Mach-O...
[opencl/llvm.git] / test / tools / llvm-readobj /
2015-01-05 Charlie TurnerEmit the build attribute Tag_conformance.
2015-01-03 Saleem Abdulrasoolllvm-readobj: add support to dump COFF export tables
2014-11-28 Charlie TurnerTest all <build attribute, value> pairs.
2014-11-27 Charlie TurnerStop uppercasing build attribute data.
2014-11-26 Will NewtonUpdate AArch64 ELF relocations to ABI 1.0
2014-11-26 Will NewtonUpdate ARM ELF relocations to ABI 2.09
2014-11-25 David MajnemerForgot to add a file for r222734
2014-11-25 David MajnemerCOFF: Add another test for r222124
2014-11-20 Jyoti Allur[ELF] Prevent ARM ELF object writer from generating...
2014-11-20 David MajnemerAdd a test for r221870
2014-11-19 Rui Ueyamallvm-readobj: fix off-by-one error in COFFDumper
2014-11-19 Rui Ueyamallvm-readobj: teach it how to dump COFF base relocation...
2014-11-18 David Majnemerllvm-readobj: Don't print the Characteristics field...
2014-11-17 David MajnemerObject, COFF: Tighten the object file parser
2014-11-17 Frederic RissImplement MachODumper::printFileHeaders
2014-11-13 Rui Ueyamallvm-readobj: Print out address table when dumping...
2014-11-12 Timur Iskhodzhanov[COFF] Make it clearer that the symbols subsection...
2014-11-05 David Majnemerllvm-readobj: Add support for dumping the DOS header...
2014-10-23 Timur IskhodzhanovPR21189: Teach llvm-readobj to dump bits of COFF symbol...
2014-10-13 Timur IskhodzhanovAdd VS2012-generated test inputs for test/tools/llvm...
2014-10-08 Rui Ueyamallvm-readobj: add test for r219228
2014-10-06 Timur IskhodzhanovFix dumping codeview line tables when there are multipl...
2014-10-03 Rui Ueyamallvm-readobj: print out the fields of the COFF delay...
2014-10-03 Rui Ueyamallvm-readobj: print COFF delay-load import table
2014-10-02 Rui Ueyamallvm-readobj: add a test for COFF import-by-ordinal...
2014-10-02 Rui Ueyamallvm-readobj: print COFF imported symbols
2014-10-02 Rui UeyamaThis patch adds a new flag "-coff-imports" to llvm...
2014-09-23 Timur IskhodzhanovRebuild the inputs for the codeview-linetables.test...
2014-09-20 David Majnemerllvm-readobj: pretty-print special COFF section names
2014-09-16 David Majnemeryaml2obj: Support bigobj
2014-09-10 David MajnemerObject: Add support for bigobj
2014-08-11 Tim NorthoverAArch64: add support for dynamic-loader relocations
2014-08-11 Tim Northoverllvm-readobj: zero out timestamp in COFF auto-generated...
2014-07-13 Simon Atanasyan[Mips] Support SHT_MIPS_ABIFLAGS section type flag...
2014-07-05 Simon Atanasyan[llvm-readobj] Fix output of MIPS GOT without local...
2014-07-04 Tim Northoverllvm-readobj: fix MachO relocatoin printing a bit.
2014-06-27 Simon Atanasyan[ELF][Mips] Fix recognition of MIPS 64-bit arch in...
2014-06-18 Simon Atanasyan[llvm-readobj][ELF] New `-mips-plt-got` command line...
2014-06-09 Alp TokerReduce verbiage of lit.local.cfg files
2014-05-11 Simon Atanasyan[llvm-readobj] Print values of FLAGS and MIPS_FLAGS...
2014-04-16 Saleem Abdulrasooltools: fix invalid printing, buffer overrun in llvm...
2014-04-14 Saleem Abdulrasooltools: address possible non-null terminated filenames
2014-03-24 Rafael EspindolaTeach llvm-readobj to print human friendly description...
2014-03-18 Rui UeyamaObject/COFF: Add function to check if section number...
2014-03-17 Nico Rieckllvm-readobj: Print referred symbol name for CLR token...
2014-03-17 Nico Rieckllvm-readobj: Add test for COFF auxiliary symbols as...
2014-03-13 Saleem AbdulrasoolSupport: add support to identify WinCOFF/ARM objects
2014-03-06 Rafael EspindolaFix the printing of n_type.
2014-02-26 Nico RieckRelax COFF string table check
2014-01-30 Saleem Abdulrasooltools: add support for decoding ARM attributes
2014-01-27 Rui UeyamaRename IMAGE_DLL_CHARACTERISTICS_HIGH_ENTROPY_VA.
2014-01-26 Rui UeyamaCOFF: Add a missing enum value for high entropy ASLR.
2014-01-26 Rui Ueyamallvm-readobj: add support for PE32+ (Windows 64 bit...
2014-01-21 Saleem Abdulrasooltools: support decoding ARM EHABI opcodes in readobj
2014-01-09 Saleem Abdulrasoolllvm-readobj: address review comments for ARM EHABI...
2014-01-08 Saleem Abdulrasooltests: disable ARM unwinding tests if ARM is unavailable
2014-01-08 Saleem Abdulrasoolllvm-readobj: add support for ARM EHABI unwind info
2014-01-05 Simon Atanasyan[Mips] Add support for DT_MIPS_RLD_MAP and DT_MIPS_PLTG...
2014-01-05 Simon Atanasyan[Mips] Rename the test case input file. No functional...
2013-12-19 Timur IskhodzhanovTeach the llvm-readobj COFF dumper to dump debug line...
2013-12-19 Timur IskhodzhanovRemove the COFF files with Z7 debug info from the repo
2013-12-17 Timur IskhodzhanovAdd some simple COFF files with Z7 debug info
2013-11-15 Rui UeyamaPath: Recognize COFF import library file magic.
2013-11-14 Rui UeyamaRecognize 0x0000 as a COFF file magic.
2013-11-11 Simon AtanasyanAdd support for DT_VERxxx and DT_MIPS_xxx .dynamic...
2013-10-07 Simon Atanasyan[Mips] Teach llvm-readobj to print MIPS-specific ELF...
2013-09-03 Joerg SonnenbergerPrint string value for DT_RPATH and DT_RUNPATH.
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-07-25 Rafael EspindolaRemove the mblaze backend from llvm.
2013-07-19 Rui UeyamaRetry submitting r186623: COFFDumper: Dump data directo...
2013-07-18 Rui UeyamaRevert "COFFDumper: Dump data directory entries."
2013-07-18 Rui UeyamaCOFFDumper: Dump data directory entries.
2013-06-12 Rui Ueyamareadobj: Dump PE/COFF optional records.
2013-06-05 Rafael EspindolaDon't hide the first ELF symbol.
2013-05-30 Rafael EspindolaChange how we iterate over relocations on ELF.
2013-04-24 Rafael EspindolaUse pointers to iterate over symbols.
2013-04-18 Rafael EspindolaAt Jim Grosbach's request detemplate Object/MachO.h.
2013-04-13 Rafael EspindolaFinish templating MachObjectFile over endianness.
2013-04-12 Nico RieckTeach llvm-readobj to print ELF program headers
2013-04-12 Nico RieckAdd extensive relocation tests for llvm-readobj
2013-04-12 Rafael EspindolaAdd 179294 back, but don't use bit fields so that it...
2013-04-11 Rafael EspindolaRevert my last two commits while I debug what is wrong...
2013-04-11 Rafael EspindolaPrint more information about relocations.
2013-04-11 Rafael EspindolaAdd MachO-x86-64 tests.
2013-04-05 Rafael EspindolaDon't fetch pointers from a InMemoryStruct.
2013-04-05 Rafael EspindolaThe ppc bots say this is the last broken line, so lets...
2013-04-05 Rafael EspindolaOne more try before I just delete the macho bits until...
2013-04-05 Rafael EspindolaMore test loosening.
2013-04-05 Rafael EspindolaLoosen this test too.
2013-04-05 Rafael EspindolaLoosen this test.
2013-04-03 Eric ChristopherImplements low-level object file format specific output...