]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/tools
Revert "This reapplies r207130 with an additional testcase+and a missing check for"
[opencl/llvm.git] / test / tools /
2014-04-23 Justin Bognerllvm-cov: Add support for gcov's --long-file-names...
2014-04-18 Justin Bognerllvm-profdata: Avoid writing to /dev/null in tests
2014-04-18 Justin Bognertest: Add extra run lines to investigate an error on...
2014-04-18 Justin BognerProfileData: Add support for the indexed instrprof...
2014-04-16 Saleem Abdulrasooltools: fix invalid printing, buffer overrun in llvm...
2014-04-14 Saleem Abdulrasooltools: fix heap-buffer-overrun detected via ASAN
2014-04-14 Saleem Abdulrasooltools: address possible non-null terminated filenames
2014-04-13 Saleem Abdulrasooltools: teach objdump about FILE aux records
2014-03-26 Justin Bognerllvm-cov: Move XFAIL after the body of the test
2014-03-26 Justin Bognerllvm-cov: Disable test on big endian machines
2014-03-26 Justin Bognerllvm-cov: Handle functions with no line number
2014-03-24 Rafael EspindolaTeach llvm-readobj to print human friendly description...
2014-03-23 Justin Bognerllvm-profdata: Check for bad data in the show command
2014-03-23 Duncan P. N. Exon... InstrProf: Check pointer size in raw profile
2014-03-22 Justin Bognerllvm-profdata: Don't pipe stderr into show for the...
2014-03-21 Duncan P. N. Exon... InstrProf: Cleanup binary profdata testcase
2014-03-21 Duncan P. N. Exon... InstrProf: Change magic number to have non-text characters
2014-03-21 Duncan P. N. Exon... InstrProf: Actually detect bad headers
2014-03-21 Duncan P. N. Exon... InstrProf: Read raw binary profile in llvm-profdata
2014-03-21 Justin BognerProfileData: Introduce InstrProfWriter using the naive...
2014-03-21 Justin BognerProfileData: Introduce the InstrProfReader interface...
2014-03-21 Rui UeyamaObject/COFF: Support large relocation table.
2014-03-20 Greg Fitzgeraldllvm-objdump output hex to match binutils' objdump
2014-03-19 Justin Bognerllvm-profdata: Make "merge" into a subcommand.
2014-03-19 Justin Bognerllvm-profdata: Update to use the naive text format...
2014-03-18 Rui UeyamaObject/COFF: Add function to check if section number...
2014-03-17 Nico Rieckllvm-readobj: Print referred symbol name for CLR token...
2014-03-17 Nico Rieckllvm-readobj: Add test for COFF auxiliary symbols as...
2014-03-13 Saleem AbdulrasoolSupport: add support to identify WinCOFF/ARM objects
2014-03-12 Justin BognerBack out Profile library and dependent commits
2014-03-12 Justin Bognerllvm-profdata: Use the Profile library, implement show...
2014-03-06 Rafael EspindolaFix the printing of n_type.
2014-03-04 Rui Ueyamallvm-objdump: Indent unwind info contents.
2014-03-04 Rui Ueyamallvm-objdump: Fix typo in output.
2014-03-04 Rui Ueyamallvm-objdump: Print x64 unwind info in executable.
2014-03-04 Rui UeyamaMake a test for llvm-objdump a little bit more readable.
2014-02-26 Nico RieckRelax COFF string table check
2014-02-24 Simon Atanasyanllvm-objdump: Do not attempt to disassemble symbols...
2014-02-24 Reed KotlerFor lcov tests, don't Xfail mips littl endian (mipsel...
2014-02-20 Rui Ueyamallvm-objdump/COFF: Print SEH table addresses.
2014-02-20 Rui UeyamaObject/COFF: Fix padding between CSDVersion and EditList.
2014-02-19 Rui Ueyamallvm-objdump/COFF: Print load configuration table.
2014-02-18 Justin Bognerllvm-cov: Support gcov's extermely lenient treatment...
2014-02-17 Duncan P. N. Exon... PGO: llvm-profdata: tool for merging profiles
2014-02-04 Justin Bognerllvm-cov: Implement the preserve-paths flag
2014-02-04 Justin Bognerllvm-cov: Implement the object-directory flag
2014-02-04 Justin Bognerllvm-cov: Ignore missing .gcda files
2014-02-04 Justin Bognerllvm-cov: Document the llvm-cov tests
2014-01-30 Saleem Abdulrasooltools: add support for decoding ARM attributes
2014-01-29 Justin Bognerllvm-cov: Expect a source file as a positional parameter
2014-01-27 Rui UeyamaRename IMAGE_DLL_CHARACTERISTICS_HIGH_ENTROPY_VA.
2014-01-26 Rui UeyamaCOFF: Add a missing enum value for high entropy ASLR.
2014-01-26 Rui Ueyamallvm-readobj: add support for PE32+ (Windows 64 bit...
2014-01-25 Venkatraman Govind... [Sparc] Add sparc to the list of XFAIL architecture...
2014-01-21 Saleem Abdulrasooltools: support decoding ARM EHABI opcodes in readobj
2014-01-17 Rui Ueyamallvm-objdump/COFF: Print ordinal base number.
2014-01-16 Rui Ueyamallvm-objdump/COFF: Print DLL name in the export table...
2014-01-16 Rui Ueyamallmv-objdump/COFF: Print export table contents.
2014-01-09 Saleem Abdulrasoolllvm-readobj: address review comments for ARM EHABI...
2014-01-08 Saleem Abdulrasooltests: disable ARM unwinding tests if ARM is unavailable
2014-01-08 Saleem Abdulrasoolllvm-readobj: add support for ARM EHABI unwind info
2014-01-05 Simon Atanasyan[Mips] Add support for DT_MIPS_RLD_MAP and DT_MIPS_PLTG...
2014-01-05 Simon Atanasyan[Mips] Rename the test case input file. No functional...
2013-12-19 Timur IskhodzhanovTeach the llvm-readobj COFF dumper to dump debug line...
2013-12-19 Timur IskhodzhanovRemove the COFF files with Z7 debug info from the repo
2013-12-19 Yuchen Wullvm-cov: Added -f option for function summaries.
2013-12-18 Yuchen Wullvm-cov: Print coverage summary to STDOUT.
2013-12-18 Yuchen Wullvm-cov: Added -c option for branch counts.
2013-12-17 Timur IskhodzhanovAdd some simple COFF files with Z7 debug info
2013-12-16 Yuchen Wullvm-cov: Added -u option for unconditional branch...
2013-12-13 Yuchen Wullvm-cov: Added -b option for branch probabilities.
2013-12-10 Yuchen Wullvm-cov: Added -a option for block data.
2013-12-07 Yuchen Wullvm-cov: Added test.h header to tests.
2013-12-06 Yuchen Wullvm-cov: Regenerated gcov files with r195513 changes.
2013-12-05 Yuchen Wullvm-cov: Changed extension from .llcov to .gcov.
2013-12-04 Daniel JasperUn-revert r196358: "llvm-cov: Added support for functio...
2013-12-04 Daniel JasperRevert r196358: "llvm-cov: Added support for function...
2013-12-04 Yuchen Wullvm-cov: Added support for function checksums.
2013-12-03 Yuchen Wullvm-cov: Another fix to llvm-cov test.
2013-12-03 Daniel JasperFurther fix to llvm-cov test.
2013-12-03 Daniel JasperFix llvm-cov test as suggested in r196228's post commit...
2013-12-03 Daniel JasperCopy input files to test directory.
2013-12-03 NAKAMURA Takumillvm-cov.test: Resurrect part of r194694 for win32...
2013-12-03 Yuchen Wullvm-cov: Removed output to STDOUT/specified file.
2013-11-29 Petar Jovanovicmips: XFAIL llvm-cov test
2013-11-20 Yuchen Wullvm-cov: Added file checksum to gcno and gcda files.
2013-11-15 Rui UeyamaPath: Recognize COFF import library file magic.
2013-11-14 Rui UeyamaRecognize 0x0000 as a COFF file magic.
2013-11-14 NAKAMURA Takumillvm-cov.test: Remove XFAIL:arm. Seems this is passing...
2013-11-14 NAKAMURA Takumillvm-cov.test: Tweak win32 hosts not confused by \r...
2013-11-14 NAKAMURA TakumiSuppress llvm-cov.test on Win32, with REQUIRES: shell
2013-11-14 Yuchen Wullvm-cov: Removed StringMap holding GCOVLines.
2013-11-14 Yuchen Wullvm-cov: Replaced asserts with proper error handling.
2013-11-13 Yuchen Wullvm-cov: Changed XFAIL targets to be more generic.
2013-11-13 Yuchen WuAdded basic unit test for llvm-cov.
2013-11-12 Yuchen WuRevert "Added basic unit test for llvm-cov."
2013-11-12 Yuchen Wullvm-cov: Added call to update run/program counts.
2013-11-12 Yuchen WuAdded basic unit test for llvm-cov.
2013-11-11 Simon AtanasyanAdd support for DT_VERxxx and DT_MIPS_xxx .dynamic...
2013-11-05 Yuchen WuRevert "Added basic unit test for llvm-cov."
next