]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/tools
Regenerate this stale testcase from source.
[opencl/llvm.git] / test / tools /
2014-12-04 Kevin EnderbyRe-add support to llvm-objdump for Mach-O universal...
2014-12-03 Rafael EspindolaThis reverts commit r223306 and r223277.
2014-12-03 Kevin EnderbyMove tests for llvm-objdump for universal files to...
2014-12-03 Kevin EnderbyAdd support to llvm-objdump for Mach-O universal files...
2014-11-28 Charlie TurnerTest all <build attribute, value> pairs.
2014-11-27 Charlie TurnerStop uppercasing build attribute data.
2014-11-26 Will NewtonUpdate AArch64 ELF relocations to ABI 1.0
2014-11-26 Will NewtonUpdate ARM ELF relocations to ABI 2.09
2014-11-25 Rafael EspindolaThis test requires asserts because of -stats.
2014-11-25 Rafael Espindolagold plugin: call llvm_shutdown so that -stats works.
2014-11-25 David MajnemerForgot to add a file for r222734
2014-11-25 David MajnemerCOFF: Add another test for r222124
2014-11-24 Rafael EspindolaAdd a disable-output option to the gold plugin.
2014-11-20 Jyoti Allur[ELF] Prevent ARM ELF object writer from generating...
2014-11-20 David MajnemerAdd a test for r221870
2014-11-19 Rui Ueyamallvm-readobj: fix off-by-one error in COFFDumper
2014-11-19 Rui Ueyamallvm-readobj: teach it how to dump COFF base relocation...
2014-11-18 David Majnemerllvm-readobj: Don't print the Characteristics field...
2014-11-17 David MajnemerObject, COFF: Tighten the object file parser
2014-11-17 Frederic RissImplement MachODumper::printFileHeaders
2014-11-14 Kevin EnderbyAdd the code and test cases for 64-bit ARM to llvm...
2014-11-13 Rui Ueyamallvm-readobj: Print out address table when dumping...
2014-11-12 Timur Iskhodzhanov[COFF] Make it clearer that the symbols subsection...
2014-11-12 Rafael EspindolaFix the test.
2014-11-11 Colin LeMahieu[llvm-mc] Fixing case where if a file ended with non...
2014-11-11 David Majnemerllvm-objdump: Skip empty sections when dumping contents
2014-11-11 Manuel KlimekWas convinced in commit comments that requiring a speci...
2014-11-10 Manuel KlimekMark test using python as REQUIRES: python27.
2014-11-07 NAKAMURA Takumillvm/test/tools/llvm-symbolizer/ppc64.test: Avoid subshell.
2014-11-07 Jay Foadllvm-symbolizer: teach it about PowerPC64 ELF function...
2014-11-06 Kevin EnderbyPlumb in the ARM thumb symbolizer in llvm-objdump’s...
2014-11-05 David Majnemerllvm-readobj: Add support for dumping the DOS header...
2014-11-04 Kevin EnderbyAdd the code and test cases for 32-bit Intel to llvm...
2014-11-03 David MajnemerForgot to add input file for test added in r221133
2014-11-03 David Majnemerllvm-vtabledump: Handle Itanium VTables
2014-11-01 Diego NovilloAdd show and merge tools for sample PGO profiles.
2014-10-30 Rafael EspindolaEnable the slp vectorizer in the gold plugin.
2014-10-30 Rafael EspindolaEnable the loop vectorizer in the gold plugin.
2014-10-29 Rafael EspindolaReplace also-emit-llvm with save-temps.
2014-10-29 NAKAMURA Takumimacho-symbolized-disassembly.test: Don't check C++...
2014-10-28 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to demangl...
2014-10-23 Timur IskhodzhanovPR21189: Teach llvm-readobj to dump bits of COFF symbol...
2014-10-23 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code for Object...
2014-10-18 Nick Kledzik[llvm-objdump] don't test timestamp dump as that is...
2014-10-18 Nick Kledzik[llvm-objdump] enhance test case for mach-o -private...
2014-10-18 Nick Kledzik[llvm-objdump] Fix mach-o binding decompression error
2014-10-17 Alexander Potapenko[llvm-symbolizer] Introduce the -dsym-hint option.
2014-10-14 Nick Kledzik[llvm-objdump] Update error message and add test case...
2014-10-13 Timur IskhodzhanovAdd VS2012-generated test inputs for test/tools/llvm...
2014-10-08 Rui Ueyamallvm-readobj: add test for r219228
2014-10-07 Rafael Espindolagold plugin: Handle gold selecting a linkonce GV when...
2014-10-07 Rafael Espindolagold plugin: create internal replacement with original...
2014-10-07 Rafael Espindolagold plugin: Remap function arguments when creating...
2014-10-06 Timur IskhodzhanovFix dumping codeview line tables when there are multipl...
2014-10-03 Rui Ueyamallvm-readobj: print out the fields of the COFF delay...
2014-10-03 Rui Ueyamallvm-readobj: print COFF delay-load import table
2014-10-02 Rui Ueyamallvm-readobj: add a test for COFF import-by-ordinal...
2014-10-02 Rui Ueyamallvm-readobj: print COFF imported symbols
2014-10-02 Rui UeyamaThis patch adds a new flag "-coff-imports" to llvm...
2014-10-02 Eric ChristopherRemove test directories with no tests.
2014-09-30 Alex LorenzRevert r218673 'llvm-cov: add test for report's functio...
2014-09-30 Alex Lorenzllvm-cov: add test for report's function & file associa...
2014-09-30 Alex Lorenzllvm-cov: Use the number of executed functions for...
2014-09-26 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to print...
2014-09-26 David Majnemerllvm-vtabledump: strip trailing NUL bytes
2014-09-26 David Majnemerllvm-vtabledump: Dump RTTI structures for the MS ABI
2014-09-25 Justin Bognerllvm-cov: Combine segments that cover the same location
2014-09-24 Kevin EnderbyFlush out enough of llvm-objdump’s SymbolizerSymbolLook...
2014-09-24 Renato GolinRemoving empty ARM tests from failed revert
2014-09-24 Renato GolinRemoving empty tests from failed revert
2014-09-24 Renato GolinRevert 218407 - Add support for ARM and AArch64 BE...
2014-09-24 Renato GolinRevert 218408 - Report endianness in output of {dwarf...
2014-09-24 Renato GolinReport endianness in output of {dwarf, obj}dump
2014-09-24 Renato GolinAdd support for ARM and AArch64 BE object files
2014-09-24 Kaelyn TakataRevert "Add support for ARM and AArch64 BE object files"
2014-09-24 Kaelyn TakataRevert "Report endianness in output of {dwarf, obj...
2014-09-24 Renato GolinReport endianness in output of {dwarf, obj}dump
2014-09-24 Renato GolinAdd support for ARM and AArch64 BE object files
2014-09-23 Timur IskhodzhanovRebuild the inputs for the codeview-linetables.test...
2014-09-20 David Majnemerllvm-readobj: pretty-print special COFF section names
2014-09-19 Justin Bognerllvm-cov: Prevent a test from matching its own check...
2014-09-19 Justin Bognerllvm-cov: Fix dropped lines when filters were applied
2014-09-18 Peter CollingbourneLTO: introduce object file-based on-disk module format.
2014-09-17 Nick Kledzik[llvm-objdump] clean up test cases now that build bots...
2014-09-17 Justin Bognerllvm-cov: Push some more debug output into the View...
2014-09-17 Rafael EspindolaInternalize common symbols when we can.
2014-09-17 Alexey SamsonovExclude known and bugzilled failures from UBSan bootstrap
2014-09-17 Nick Kledzik[llvm-objdump] properly use c_str() with format("%s...
2014-09-16 Nick Kledziktweak test case for debugging bot
2014-09-16 Kevin EnderbyHookup the MCSymbolizer to llvm-objdump’s disassembly...
2014-09-16 Nick Kledziktweak test case to help build bot
2014-09-16 David Majnemeryaml2obj: Support bigobj
2014-09-16 Nick Kledziktweak test case to help solve why failing on one build bot
2014-09-16 Nick Kledzik[llvm-objdump] for mach-o add -bind, -lazy-bind, and...
2014-09-15 Justin Bognerllvm-cov: Make debug output more consistent
2014-09-15 Justin Bognerllvm-cov: Fix an issue with showing regions but not...
2014-09-12 Nick KledzikStop suppress error messages in test case to see why...
2014-09-12 Nick Kledzik[llvm-objdump] support -rebase option for mach-o to...
2014-09-12 Justin Bognerllvm-profdata: Avoid undefined behaviour when reading...
2014-09-11 Justin BognerRevert "llvm-cov: Remove an overly system specific...
next