For llvm-objdump, hook up existing options to work when using -macho (the Mach-O...
[opencl/llvm.git] / test / tools /
2015-01-20 Kevin EnderbyFor llvm-objdump, hook up existing options to work...
2015-01-19 Frederic Riss[dsymutil] Add the detected target triple to the debug...
2015-01-16 Kevin EnderbyChange the test case for llvm-objdump’s -archive-header...
2015-01-16 Kevin EnderbyFix the Archive::Child::getRawSize() method used by...
2015-01-16 Kevin EnderbyWork around to get the build bot clang-cmake-armv7...
2015-01-16 Kevin EnderbyAnother attempt to fix the build bot clang-cmake-armv7...
2015-01-15 Kevin EnderbyAdd the option, -archive-headers, used with -macho...
2015-01-14 Rafael EspindolaFix linking of shared libraries.
2015-01-14 Rafael EspindolaFix handling of extern_weak. This was broken by r225983.
2015-01-14 Rafael EspindolaHandle a symbol being undefined.
2015-01-09 Kevin EnderbyAdd the option, -universal-headers, used with -macho...
2015-01-07 Kevin EnderbySlightly refactor things for llvm-objdump and the ...
2015-01-06 Rafael EspindolaChange the .ll syntax for comdats and add a syntactic...
2015-01-05 Frederic Riss[dsymutil] Implement the BinaryHolder object and gain...
2015-01-05 Charlie TurnerEmit the build attribute Tag_conformance.
2015-01-03 Saleem Abdulrasoolllvm-readobj: add support to dump COFF export tables
2014-12-23 Kevin EnderbyAdd printing the LC_THREAD load commands with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_ROUTINES load commands with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_CLIENT load command with llvm...
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_LIBRARY load command with llvm...
2014-12-18 Kevin EnderbyAdd printing the LC_SUB_UMBRELLA load command with...
2014-12-18 Kevin EnderbyAdd printing the LC_SUB_FRAMEWORK load command with...
2014-12-18 Kevin EnderbyAdd printing the LC_LINKER_OPTION load command with...
2014-12-17 Kevin EnderbyAdd printing the LC_ENCRYPTION_INFO_64 load command...
2014-12-16 Kevin EnderbyAdd printing the LC_ENCRYPTION_INFO load command with...
2014-12-16 Kevin EnderbyFix a bug in llvm-objdump’s -private-headers for the...
2014-12-16 Kevin EnderbyFix a bug in llvm-objdump’s -private-headers for 32...
2014-12-12 Reid KlecknerRelax debug-map-parsing.test error message check for...
2014-12-12 Frederic RissInitial dsymutil tool commit.
2014-12-09 Frederic RissRevert "Initial dsymutil tool commit."
2014-12-09 Frederic RissInitial dsymutil tool commit.
2014-12-09 Rafael EspindolaRemember the unmangled name in the plugin.
2014-12-04 Kevin EnderbyRe-add support to llvm-objdump for Mach-O universal...
2014-12-03 Rafael EspindolaThis reverts commit r223306 and r223277.
2014-12-03 Kevin EnderbyMove tests for llvm-objdump for universal files to...
2014-12-03 Kevin EnderbyAdd support to llvm-objdump for Mach-O universal files...
2014-11-28 Charlie TurnerTest all <build attribute, value> pairs.
2014-11-27 Charlie TurnerStop uppercasing build attribute data.
2014-11-26 Will NewtonUpdate AArch64 ELF relocations to ABI 1.0
2014-11-26 Will NewtonUpdate ARM ELF relocations to ABI 2.09
2014-11-25 Rafael EspindolaThis test requires asserts because of -stats.
2014-11-25 Rafael Espindolagold plugin: call llvm_shutdown so that -stats works.
2014-11-25 David MajnemerForgot to add a file for r222734
2014-11-25 David MajnemerCOFF: Add another test for r222124
2014-11-24 Rafael EspindolaAdd a disable-output option to the gold plugin.
2014-11-20 Jyoti Allur[ELF] Prevent ARM ELF object writer from generating...
2014-11-20 David MajnemerAdd a test for r221870
2014-11-19 Rui Ueyamallvm-readobj: fix off-by-one error in COFFDumper
2014-11-19 Rui Ueyamallvm-readobj: teach it how to dump COFF base relocation...
2014-11-18 David Majnemerllvm-readobj: Don't print the Characteristics field...
2014-11-17 David MajnemerObject, COFF: Tighten the object file parser
2014-11-17 Frederic RissImplement MachODumper::printFileHeaders
2014-11-14 Kevin EnderbyAdd the code and test cases for 64-bit ARM to llvm...
2014-11-13 Rui Ueyamallvm-readobj: Print out address table when dumping...
2014-11-12 Timur Iskhodzhanov[COFF] Make it clearer that the symbols subsection...
2014-11-12 Rafael EspindolaFix the test.
2014-11-11 Colin LeMahieu[llvm-mc] Fixing case where if a file ended with non...
2014-11-11 David Majnemerllvm-objdump: Skip empty sections when dumping contents
2014-11-11 Manuel KlimekWas convinced in commit comments that requiring a speci...
2014-11-10 Manuel KlimekMark test using python as REQUIRES: python27.
2014-11-07 NAKAMURA Takumillvm/test/tools/llvm-symbolizer/ppc64.test: Avoid subshell.
2014-11-07 Jay Foadllvm-symbolizer: teach it about PowerPC64 ELF function...
2014-11-06 Kevin EnderbyPlumb in the ARM thumb symbolizer in llvm-objdump’s...
2014-11-05 David Majnemerllvm-readobj: Add support for dumping the DOS header...
2014-11-04 Kevin EnderbyAdd the code and test cases for 32-bit Intel to llvm...
2014-11-03 David MajnemerForgot to add input file for test added in r221133
2014-11-03 David Majnemerllvm-vtabledump: Handle Itanium VTables
2014-11-01 Diego NovilloAdd show and merge tools for sample PGO profiles.
2014-10-30 Rafael EspindolaEnable the slp vectorizer in the gold plugin.
2014-10-30 Rafael EspindolaEnable the loop vectorizer in the gold plugin.
2014-10-29 Rafael EspindolaReplace also-emit-llvm with save-temps.
2014-10-29 NAKAMURA Takumimacho-symbolized-disassembly.test: Don't check C++...
2014-10-28 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to demangl...
2014-10-23 Timur IskhodzhanovPR21189: Teach llvm-readobj to dump bits of COFF symbol...
2014-10-23 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code for Object...
2014-10-18 Nick Kledzik[llvm-objdump] don't test timestamp dump as that is...
2014-10-18 Nick Kledzik[llvm-objdump] enhance test case for mach-o -private...
2014-10-18 Nick Kledzik[llvm-objdump] Fix mach-o binding decompression error
2014-10-17 Alexander Potapenko[llvm-symbolizer] Introduce the -dsym-hint option.
2014-10-14 Nick Kledzik[llvm-objdump] Update error message and add test case...
2014-10-13 Timur IskhodzhanovAdd VS2012-generated test inputs for test/tools/llvm...
2014-10-08 Rui Ueyamallvm-readobj: add test for r219228
2014-10-07 Rafael Espindolagold plugin: Handle gold selecting a linkonce GV when...
2014-10-07 Rafael Espindolagold plugin: create internal replacement with original...
2014-10-07 Rafael Espindolagold plugin: Remap function arguments when creating...
2014-10-06 Timur IskhodzhanovFix dumping codeview line tables when there are multipl...
2014-10-03 Rui Ueyamallvm-readobj: print out the fields of the COFF delay...
2014-10-03 Rui Ueyamallvm-readobj: print COFF delay-load import table
2014-10-02 Rui Ueyamallvm-readobj: add a test for COFF import-by-ordinal...
2014-10-02 Rui Ueyamallvm-readobj: print COFF imported symbols
2014-10-02 Rui UeyamaThis patch adds a new flag "-coff-imports" to llvm...
2014-10-02 Eric ChristopherRemove test directories with no tests.
2014-09-30 Alex LorenzRevert r218673 'llvm-cov: add test for report's functio...
2014-09-30 Alex Lorenzllvm-cov: add test for report's function & file associa...
2014-09-30 Alex Lorenzllvm-cov: Use the number of executed functions for...
2014-09-26 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to print...
2014-09-26 David Majnemerllvm-vtabledump: strip trailing NUL bytes
2014-09-26 David Majnemerllvm-vtabledump: Dump RTTI structures for the MS ABI
2014-09-25 Justin Bognerllvm-cov: Combine segments that cover the same location
2014-09-24 Kevin EnderbyFlush out enough of llvm-objdump’s SymbolizerSymbolLook...
next