]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test/tools
DebugInfo: Don't include the name of the CU file in the line table file list when...
[opencl/llvm.git] / test / tools /
2014-02-04 Justin Bognerllvm-cov: Implement the preserve-paths flag
2014-02-04 Justin Bognerllvm-cov: Implement the object-directory flag
2014-02-04 Justin Bognerllvm-cov: Ignore missing .gcda files
2014-02-04 Justin Bognerllvm-cov: Document the llvm-cov tests
2014-01-30 Saleem Abdulrasooltools: add support for decoding ARM attributes
2014-01-29 Justin Bognerllvm-cov: Expect a source file as a positional parameter
2014-01-27 Rui UeyamaRename IMAGE_DLL_CHARACTERISTICS_HIGH_ENTROPY_VA.
2014-01-26 Rui UeyamaCOFF: Add a missing enum value for high entropy ASLR.
2014-01-26 Rui Ueyamallvm-readobj: add support for PE32+ (Windows 64 bit...
2014-01-25 Venkatraman Govind... [Sparc] Add sparc to the list of XFAIL architecture...
2014-01-21 Saleem Abdulrasooltools: support decoding ARM EHABI opcodes in readobj
2014-01-17 Rui Ueyamallvm-objdump/COFF: Print ordinal base number.
2014-01-16 Rui Ueyamallvm-objdump/COFF: Print DLL name in the export table...
2014-01-16 Rui Ueyamallmv-objdump/COFF: Print export table contents.
2014-01-09 Saleem Abdulrasoolllvm-readobj: address review comments for ARM EHABI...
2014-01-08 Saleem Abdulrasooltests: disable ARM unwinding tests if ARM is unavailable
2014-01-08 Saleem Abdulrasoolllvm-readobj: add support for ARM EHABI unwind info
2014-01-05 Simon Atanasyan[Mips] Add support for DT_MIPS_RLD_MAP and DT_MIPS_PLTG...
2014-01-05 Simon Atanasyan[Mips] Rename the test case input file. No functional...
2013-12-19 Timur IskhodzhanovTeach the llvm-readobj COFF dumper to dump debug line...
2013-12-19 Timur IskhodzhanovRemove the COFF files with Z7 debug info from the repo
2013-12-19 Yuchen Wullvm-cov: Added -f option for function summaries.
2013-12-18 Yuchen Wullvm-cov: Print coverage summary to STDOUT.
2013-12-18 Yuchen Wullvm-cov: Added -c option for branch counts.
2013-12-17 Timur IskhodzhanovAdd some simple COFF files with Z7 debug info
2013-12-16 Yuchen Wullvm-cov: Added -u option for unconditional branch...
2013-12-13 Yuchen Wullvm-cov: Added -b option for branch probabilities.
2013-12-10 Yuchen Wullvm-cov: Added -a option for block data.
2013-12-07 Yuchen Wullvm-cov: Added test.h header to tests.
2013-12-06 Yuchen Wullvm-cov: Regenerated gcov files with r195513 changes.
2013-12-05 Yuchen Wullvm-cov: Changed extension from .llcov to .gcov.
2013-12-04 Daniel JasperUn-revert r196358: "llvm-cov: Added support for functio...
2013-12-04 Daniel JasperRevert r196358: "llvm-cov: Added support for function...
2013-12-04 Yuchen Wullvm-cov: Added support for function checksums.
2013-12-03 Yuchen Wullvm-cov: Another fix to llvm-cov test.
2013-12-03 Daniel JasperFurther fix to llvm-cov test.
2013-12-03 Daniel JasperFix llvm-cov test as suggested in r196228's post commit...
2013-12-03 Daniel JasperCopy input files to test directory.
2013-12-03 NAKAMURA Takumillvm-cov.test: Resurrect part of r194694 for win32...
2013-12-03 Yuchen Wullvm-cov: Removed output to STDOUT/specified file.
2013-11-29 Petar Jovanovicmips: XFAIL llvm-cov test
2013-11-20 Yuchen Wullvm-cov: Added file checksum to gcno and gcda files.
2013-11-15 Rui UeyamaPath: Recognize COFF import library file magic.
2013-11-14 Rui UeyamaRecognize 0x0000 as a COFF file magic.
2013-11-14 NAKAMURA Takumillvm-cov.test: Remove XFAIL:arm. Seems this is passing...
2013-11-14 NAKAMURA Takumillvm-cov.test: Tweak win32 hosts not confused by \r...
2013-11-14 NAKAMURA TakumiSuppress llvm-cov.test on Win32, with REQUIRES: shell
2013-11-14 Yuchen Wullvm-cov: Removed StringMap holding GCOVLines.
2013-11-14 Yuchen Wullvm-cov: Replaced asserts with proper error handling.
2013-11-13 Yuchen Wullvm-cov: Changed XFAIL targets to be more generic.
2013-11-13 Yuchen WuAdded basic unit test for llvm-cov.
2013-11-12 Yuchen WuRevert "Added basic unit test for llvm-cov."
2013-11-12 Yuchen Wullvm-cov: Added call to update run/program counts.
2013-11-12 Yuchen WuAdded basic unit test for llvm-cov.
2013-11-11 Simon AtanasyanAdd support for DT_VERxxx and DT_MIPS_xxx .dynamic...
2013-11-05 Yuchen WuRevert "Added basic unit test for llvm-cov."
2013-11-05 Yuchen WuAdded basic unit test for llvm-cov.
2013-10-07 Simon Atanasyan[Mips] Teach llvm-readobj to print MIPS-specific ELF...
2013-09-27 Rui UeyamaResurrect lit.local.cfg to un-break hexagon buildbot.
2013-09-27 Rui UeyamaRe-submit r191472 with a fix for big endian.
2013-09-27 Rui UeyamaRevert "llvm-objdump: Dump COFF import table if -privat...
2013-09-27 Rui Ueyamallvm-objdump: Dump COFF import table if -private-header...
2013-09-24 Peter CollingbourneMove LTO support library to a component, allowing it...
2013-09-23 NAKAMURA Takumillvm/test/tools/lto/lit.local.cfg: Add "MingW" for...
2013-09-20 NAKAMURA Takumitest/tools/lto/lit.local.cfg: Suppress llvm-lto test...
2013-09-19 Peter CollingbourneFix LTO handling of module-level assembly (PR14152).
2013-09-15 Kai NackeGenerate IMAGE_REL_AMD64_ADDR32NB relocations for SEH
2013-09-03 Joerg SonnenbergerPrint string value for DT_RPATH and DT_RUNPATH.
2013-08-27 Kai NackeFix wrong code offset for unwind code SET_FPREG.
2013-08-16 Daniel Dunbar[tests] Cleanup initialization of test suffixes.
2013-07-25 Rafael EspindolaRemove the mblaze backend from llvm.
2013-07-19 Rui UeyamaRetry submitting r186623: COFFDumper: Dump data directo...
2013-07-18 Rui UeyamaRevert "COFFDumper: Dump data directory entries."
2013-07-18 Rui UeyamaCOFFDumper: Dump data directory entries.
2013-07-08 Kai NackeRevert: Fix wrong code offset for unwind code SET_FPREG.
2013-07-08 Kai NackeRevert: Generate IMAGE_REL_AMD64_ADDR32NB relocations...
2013-07-06 Kai NackeGenerate IMAGE_REL_AMD64_ADDR32NB relocations for SEH
2013-07-06 Kai NackeFix wrong code offset for unwind code SET_FPREG.
2013-06-12 Rui Ueyamareadobj: Dump PE/COFF optional records.
2013-06-05 Rafael EspindolaDon't hide the first ELF symbol.
2013-05-30 Rafael EspindolaChange how we iterate over relocations on ELF.
2013-04-24 Rafael EspindolaUse pointers to iterate over symbols.
2013-04-18 Rafael EspindolaAt Jim Grosbach's request detemplate Object/MachO.h.
2013-04-13 Rafael EspindolaFinish templating MachObjectFile over endianness.
2013-04-12 Nico RieckTeach llvm-readobj to print ELF program headers
2013-04-12 Nico RieckAdd extensive relocation tests for llvm-readobj
2013-04-12 Rafael EspindolaAdd 179294 back, but don't use bit fields so that it...
2013-04-11 Rafael EspindolaRevert my last two commits while I debug what is wrong...
2013-04-11 Rafael EspindolaPrint more information about relocations.
2013-04-11 Rafael EspindolaAdd MachO-x86-64 tests.
2013-04-05 Rafael EspindolaDon't fetch pointers from a InMemoryStruct.
2013-04-05 Rafael EspindolaThe ppc bots say this is the last broken line, so lets...
2013-04-05 Rafael EspindolaOne more try before I just delete the macho bits until...
2013-04-05 Rafael EspindolaMore test loosening.
2013-04-05 Rafael EspindolaLoosen this test too.
2013-04-05 Rafael EspindolaLoosen this test.
2013-04-03 Eric ChristopherImplements low-level object file format specific output...
2012-12-05 Richard SmithPR10867: Analogue of r169441 for when using external...
2012-12-05 Richard SmithPR10867. lit would interpret
2012-12-05 Michael J. SpencerAdd dump of Win64 EH unwind data.
next