]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test
Move the complex address expression out of DIVariable and into an extra
[opencl/llvm.git] / test /
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Duncan P. N. Exon... LTO: Add missing target triple from r218784
2014-10-01 Reed KotlerAdd fptrunc to mips fast-sel
2014-10-01 Duncan P. N. Exon... LTO: Ignore disabled diagnostic remarks
2014-10-01 Adrian PrantlRevert r218778 while investigating buldbot breakage.
2014-10-01 Adrian PrantlMove the complex address expression out of DIVariable...
2014-10-01 Tom StellardR600: Call EmitFunctionHeader() in the AsmPrinter to...
2014-10-01 Jingyue WuRevert r216862 due to a performance regression
2014-10-01 Oliver Stannard[ARM] Allow selecting VRINT[APMXZR] and VCVT[BT] instru...
2014-10-01 Chandler Carruth[x86] Fix a few more tiny patterns with the new vector...
2014-10-01 Tom Coxon[AArch64] Allow access to all system registers with...
2014-10-01 Evgeniy StepanovRevert r218721, r218735.
2014-10-01 Asiri RathnayakeAdd missing natual vector cast.
2014-10-01 Oliver Stannard[ARM] Add support for Cortex-M7, FPv5-SP and FPv5-DP...
2014-10-01 Daniel Sanders[mips] Fix disassembly of [ls][wd]c[23], cache, and...
2014-10-01 Sasa Stankovic[mips] For indirect calls we don't need $gp to point...
2014-10-01 Justin Bognertest: XFAIL the non-darwin gmlt test on darwin
2014-10-01 Chandler Carruth[x86] Teach the new vector shuffle lowering to be even...
2014-10-01 Chandler Carruth[x86] Hoist the zext-lowering up in the v4i32 lowering...
2014-10-01 David BlaikieImplement DW_TAG_subrange_type with DW_AT_count rather...
2014-10-01 Chandler Carruth[x86] Teach the new vector shuffle lowering about VBROA...
2014-10-01 NAKAMURA Takumillvm/test/DebugInfo/X86/gmlt.test: Get rid of %llc_dwar...
2014-10-01 Gerolf Hoflehner[InstCombine] Optimize icmp-select-icmp
2014-09-30 David BlaikieOmit DW_AT_inline under -gmlt to save a little more...
2014-09-30 Hal Finkel[BasicAA] Make better use of zext and sign information
2014-09-30 Jingyue Wu[SimplifyCFG] threshold for folding branches with commo...
2014-09-30 Chandler Carruth[x86] Add AVX1 and AVX2 testing to all of the 128-bit...
2014-09-30 Chandler Carruth[x86] Update the exact FileCheck syntax of the 256...
2014-09-30 David BlaikieAdjust test case addition in r218702 so as not to fail...
2014-09-30 Chandler Carruth[x86] Rework all of the 128-bit vector shuffle tests...
2014-09-30 David BlaikieDisable the -gmlt optimization implemented in r218129...
2014-09-30 Juergen RibutzkaRecommit r218010 [FastISel][AArch64] Fold bit test...
2014-09-30 Matt ArsenaultR600/SI: Fix printing of clamp and omod
2014-09-30 Bradley SmithExtend C disassembler API to allow specifying target...
2014-09-30 Reed KotlerAdd numeric extend, trunctate to mips fast-isel
2014-09-30 Alex LorenzRevert r218673 'llvm-cov: add test for report's functio...
2014-09-30 Alex Lorenzllvm-cov: add test for report's function & file associa...
2014-09-30 Alex Lorenzllvm-cov: Use the number of executed functions for...
2014-09-30 Lorenzo MartignoniIntroduce support for custom wrappers for vararg functions.
2014-09-30 Robert Khasanov[AVX512] Added intrinsics for 128-, 256- and 512-bit...
2014-09-30 Robert Khasanov[AVX512] Added intrinsics for 128- and 256-bit versions...
2014-09-30 Robert Khasanov[AVX512] Added intrinsics for VPCMPEQB and VPCMPEQW.
2014-09-30 Robert Khasanov[AVX512] Enabled intrinsics for VPCMPEQD and VPCMPEQQ.
2014-09-30 Chad Rosier[IndVarSimplify] Widen loop unsigned compares.
2014-09-30 Chandler Carruth[x86] Revert r218588, r218589, and r218600. These patch...
2014-09-30 Chandler Carruth[x86] Add some vector-register broadcast operations...
2014-09-30 Matt ArsenaultR600: Fix broken check lines, missing scalar case.
2014-09-30 Juergen Ributzka[FastISel][AArch64] Fold sign-/zero-extends into the...
2014-09-29 Hans WennborgWinCOFFObjectWriter: optimize the string table for...
2014-09-29 Eric ChristopherAdd soft-float to the key for the subtarget lookup...
2014-09-29 Matt ArsenaultR600/SI: Also fix fsub + fadd a, a to mad combines
2014-09-29 Matt ArsenaultR600/SI: Fix using mad with multiplies by 2
2014-09-29 Chad Rosier[AArch64] Improve cost model to handle sdiv by a pow...
2014-09-29 Kevin QinUse a loop to simplify the runtime unrolling prologue.
2014-09-29 Oliver Stannard[Thumb2] ldrexd and strexd are not defined on v7M
2014-09-29 Chandler Carruth[x86] Make the new vector shuffle lowering lower blends...
2014-09-29 Chandler Carruth[x86] Delete a bunch of really bad and totally unnecess...
2014-09-29 Chandler Carruth[x86] Add the dispatch skeleton to the new vector shuff...
2014-09-28 Chandler Carruth[x86] Teach the new vector shuffle lowering to fall...
2014-09-28 Chandler Carruth[x86] Fix the new vector shuffle lowering's use of...
2014-09-28 Chandler Carruth[x86] Fix a really silly bug that I introduced fixing...
2014-09-28 Chandler Carruth[x86] Fix yet another bug in the new vector shuffle...
2014-09-27 James Molloy[AArch64] Redundant store instructions should be remove...
2014-09-27 Craig TopperUpdate test case to match minor formatting change intro...
2014-09-27 Chandler Carruth[x86] Fix terrible bugs everywhere in the new vector...
2014-09-27 Chandler Carruth[x86] Flip the sentinel values used in the target shuff...
2014-09-27 Craig TopperFix TableGen -gen-disassembler output for bit fields...
2014-09-26 Sanjay PatelRefactor reciprocal and reciprocal square root estimate...
2014-09-26 David MajnemerObject: BSS/virtual sections don't have contents
2014-09-26 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to print...
2014-09-26 Chandler Carruth[x86] Fix a moderately terrifying bug in the new 128...
2014-09-26 Chad Rosier[IndVar] Don't widen loop compare unless IV user is...
2014-09-26 Matt ArsenaultR600/SI: Add strict check lines to div_scale tests.
2014-09-26 Matt ArsenaultR600/SI Allow same SGPR to be used for multiple operands
2014-09-26 Matt ArsenaultR600/SI: Partially move operand legalization to post...
2014-09-26 Matt ArsenaultR600/SI: Don't move operands that are required to be...
2014-09-26 Matt ArsenaultR600/SI: Fix using wrong operand indices when commuting
2014-09-26 David PeixottoIgnore annotation function calls in cost computation
2014-09-26 Chandler Carruth[x86] In the new vector shuffle lowering, when trying...
2014-09-26 Chandler Carruth[x86] Fix a large collection of bugs that crept in...
2014-09-26 Renato GolinElide repeated register operand in Thumb1 instructions
2014-09-26 Robert Khasanov[AVX512] Added load/store from BW/VL subsets to Registe...
2014-09-26 David Majnemerllvm-vtabledump: strip trailing NUL bytes
2014-09-26 David Majnemerllvm-vtabledump: Dump RTTI structures for the MS ABI
2014-09-26 David XuRevert patch of r218493, delete the test case
2014-09-26 David XuRedundant store instructions should be removed as dead...
2014-09-26 Eric ChristopherAdd the first backend support for on demand subtarget...
2014-09-26 Matt ArsenaultR600: Avoid repeated check lines
2014-09-26 Matt ArsenaultR600/SI: Fix emitting trailing whitespace after s_waitcnt
2014-09-25 Adam Nemet[AVX512] Make vextract*x4/vinsert*x4 tests check for...
2014-09-25 Matt ArsenaultR600: Fix some missing conversion testcases
2014-09-25 Matt ArsenaultRemove duplicated RUN lines in middle of test
2014-09-25 Bruno Cardoso Lopes[MachineSink+PGO] Teach MachineSink to use BlockFrequen...
2014-09-25 Tom StellardR600/SI: Add support for global atomic add
2014-09-25 Robin MorissetLower idempotent RMWs to fence+load
2014-09-25 Sid ManningAdd missing attributes !cmp.[eq,gt,gtu] instructions.
2014-09-25 Daniel Sanders[mips] Add CCValAssign::[ASZ]ExtUpper and CCPromoteToUp...
2014-09-25 Renato GolinAdd aliases for VAND imm to VBIC ~imm
2014-09-25 Chandler Carruth[x86] Teach the new vector shuffle lowering to use...
2014-09-25 Chandler Carruth[x86] Teach the new vector shuffle lowering a fancier...
next