]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - test
Debug info: Support variadic functions.
[opencl/llvm.git] / test /
2014-02-25 Adrian PrantlDebug info: Support variadic functions.
2014-02-25 Adrian PrantlRevert "Debug info: Support variadic functions."
2014-02-25 Adrian PrantlDebug info: Support variadic functions.
2014-02-25 Richard Osborne[XCore] Add intrinsic for CLRPT (clear port time) instr...
2014-02-25 Richard Osborne[XCore] Add intrinsic for EDU (event disable unconditio...
2014-02-25 Logan ChienKeep the link register for uwtable.
2014-02-25 Richard Osborne[XCore] Prefer to word align functions.
2014-02-25 Renato GolinIgnore old JIT tests in AARch64 - CMake style
2014-02-25 Alp TokerFix typos
2014-02-25 Chandler Carruth[SROA] Fix another instability in SROA with respect...
2014-02-24 David Blaikiellvm-dwarfdump: Support for debug_line.dwo section...
2014-02-24 Simon Atanasyanllvm-objdump: Do not attempt to disassemble symbols...
2014-02-24 Matt ArsenaultR600/SI - Add new CI arithmetic instructions.
2014-02-24 Arnold SchwaighoferSLPVectorizer: Try vectorizing 'splat' stores
2014-02-24 Reed KotlerFor lcov tests, don't Xfail mips littl endian (mipsel...
2014-02-24 Alexey Samsonov[CMake] Remove dependency on non-existing profile_rt...
2014-02-24 Kostya Serebryany[asan] remove test that should have been removed in...
2014-02-23 Saleem AbdulrasoolAsm Parser: support .error directive
2014-02-23 Saleem AbdulrasoolAsmParser: support .ifeqs directive
2014-02-23 Benjamin KramerSPARC: Implement TRAP lowering. Matches what GCC emits.
2014-02-23 Saleem AbdulrasoolARM IAS: support .align without parameters
2014-02-23 Saleem AbdulrasoolMCAsmParser: support .ifne
2014-02-23 Saleem AbdulrasoolMCAsmParser: handle space properly for .ifc/.ifnc
2014-02-23 Saleem AbdulrasoolMCAsmParser: add support for .err directive
2014-02-23 Elena DemikhovskyAVX-512: Fixed encoding of VPTESTMQ
2014-02-23 Saleem AbdulrasoolARM IAS: support .short and .hword
2014-02-22 Benjamin KramerMake test more resilient against scheduling decisions.
2014-02-22 Nico RieckMC: Support COFF string tables larger than 10MB
2014-02-22 NAKAMURA Takumillvm/test/CodeGen/X86/shift-pcmp.ll: Tweak to appease...
2014-02-22 Quentin Colombet[CodeGenPrepare] Fix the check of the legality of an...
2014-02-21 Quentin Colombet[DAGCombiner] PCMP* sets its result to all ones or...
2014-02-21 Rafael EspindolaAdd a SymbolicFile interface between Binary and ObjectFile.
2014-02-21 Sebastian Popadd -da-delinearize runs and checks to MIV testcases
2014-02-21 Kevin Qin[AArch64] Add register constraints to avoid generating...
2014-02-20 Nick LewyckyMake sure that value handle users see the transformatio...
2014-02-20 Oliver StannardAArch64: __va_list.__stack must be 8-byte aligned
2014-02-20 Daniel Sanders[mips] Make it impossible to have UnknownABI in CodeGen...
2014-02-20 Benjamin KramerAsmParser: Disable Darwin-style macro argument expansio...
2014-02-20 Daniel Sanders[mips] Make mips64 the default CPU for the mips64 archi...
2014-02-20 Elena DemikhovskyAVX-512: added a lit test for truncate operation
2014-02-20 Rui Ueyamallvm-objdump/COFF: Print SEH table addresses.
2014-02-20 Elena DemikhovskyAVX-512: Assembly parsing of broadcast semantic in...
2014-02-20 Rui UeyamaObject/COFF: Fix padding between CSDVersion and EditList.
2014-02-20 Eric ChristopherAdd support for hashing attributes with DW_FORM_block...
2014-02-19 Roman DivackyExpand 64bit {SHL,SHR,SRA}_PARTS on sparcv9.
2014-02-19 Rafael EspindolaAdd back r201608, r201622, r201624 and r201625
2014-02-19 Daniel Sanders[mips] Use multiple FileCheck prefixes rather than...
2014-02-19 Venkatraman Govind... [Sparc] Remove spurious checks from a testcase.
2014-02-19 Rafael EspindolaThis reverts commit r201625 and r201624.
2014-02-19 Daniel Sanders[mips] Add explicit N32 and N64 tests to nabi-regs...
2014-02-19 Cameron McInallyFix AVX512 vector sqrt assembly strings.
2014-02-19 Daniel JasperRevert r201622 and r201608.
2014-02-19 Tim NorthoverX86: move test requiring X86TargetLowering info into...
2014-02-19 Tim NorthoverTry addding datalayout in case that's what Hexagon...
2014-02-19 Tim NorthoverX86 CodeGenPrep: sink shufflevectors before shifts
2014-02-19 Craig TopperRemove special FP opcode maps and instead add enough...
2014-02-19 Craig TopperRemove A6/A7 opcode maps. They can all be handled with...
2014-02-19 Rui Ueyamallvm-objdump/COFF: Print load configuration table.
2014-02-19 Saleem AbdulrasoolMCAsmParser: support required parameters
2014-02-19 Rafael EspindolaNow that llvm always does the right thing with private...
2014-02-19 Rafael EspindolaAvoid an infinite cycle with private linkage and -f...
2014-02-18 Rafael EspindolaFix PR18743.
2014-02-18 Ana Pazos[AArch64] Expanded sin, cos, pow with FP vector types...
2014-02-18 Robert LyttonXCore target: Handle common linkage
2014-02-18 Robert LyttonXCore target: Fix llvm.eh.return and EH info register...
2014-02-18 Tim NorthoverX86: use vpsllvd (& friends) for 16-bit shifts on Haswell
2014-02-18 Justin Bognerllvm-cov: Support gcov's extermely lenient treatment...
2014-02-18 Jiangning LiuFix a typo about lowering AArch64 va_copy.
2014-02-17 Duncan P. N. Exon... PGO: llvm-profdata: tool for merging profiles
2014-02-17 Kevin EnderbyFix the arm assembler so that this malformed instruction:
2014-02-17 Anders WaldenborgAdd support for assigning to . in AsmParser.
2014-02-17 Craig TopperFix diassembler handling of rex.b when mod=00/01/10...
2014-02-17 Elena DemikhovskyAVX-512: implemented zext fron i1 to i16
2014-02-17 Gerolf Hoflehnerfix for null VectorizedValue assertion in the SLP Vecto...
2014-02-17 Saleem AbdulrasoolMCAsmParser: add some mixed argument tests
2014-02-17 Saleem AbdulrasoolMCAsmParser: better handling for named arguments
2014-02-16 Mark SeabornUse 16 byte stack alignment for NaCl on ARM
2014-02-16 Arnold SchwaighoferSCEVExpander: Try hard not to create derived induction...
2014-02-16 Nico RieckFix more broken CHECK lines
2014-02-16 Nico RieckAdd extra CHECK prefix to tests with explicit prefix
2014-02-16 Nico RieckActually call FileCheck in tests
2014-02-16 Elena DemikhovskyAVX-512: simpyfied BUILD_VECTOR for masks; fixed cmp...
2014-02-16 Eric ChristopherAdd a DIELoc class to cover the DW_FORM_exprloc set...
2014-02-16 Nico RieckFix broken CHECK lines
2014-02-16 Saleem AbdulrasoolMCAsmParser: relax declaration parsing
2014-02-16 Saleem AbdulrasoolARM IAS: (partially) support .arch_extension directive
2014-02-15 David BlaikieDebugInfo: Deduplicate entries in the fission address...
2014-02-15 Arnold SchwaighoferRevert "SCEVExpander: Try hard not to create derived...
2014-02-15 Arnold SchwaighoferSCEVExpander: Try hard not to create derived induction...
2014-02-15 Craig TopperAdd opcode extension forms of MOV8ri/MOV16ri/MOV32ri.
2014-02-14 David BlaikieDebugInfo: Implement DW_AT_stmt_list for type units
2014-02-14 Quentin Colombet[CodeGenPrepare][AddressingModeMatcher] Give up on...
2014-02-14 Tom StellardTargetLowering: n * r where n > 2 should be an illegal...
2014-02-14 David BlaikieDebugInfo: Don't include the name of the CU file in...
2014-02-14 Diego NovilloSupport DWARF discriminators in object streamer.
2014-02-14 Reed KotlerThis patch has two main functions:
2014-02-14 Artyom SkrobovGenerate the DWARF stack frame decode operations in...
2014-02-14 Kevin Qin[AArch64 NEON] Fix a bug to avoid using floating type...
2014-02-14 Eric ChristopherRevert "DebugInfo: Don't include the name of the CU...
2014-02-14 NAKAMURA Takumillvm/test/DebugInfo/empty.ll: Mark it as XFAIL:win32...
next