]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - tools/llvm-nm
For llvm-objdump, hook up existing options to work when using -macho (the Mach-O...
[opencl/llvm.git] / tools / llvm-nm /
2015-01-14 Chandler Carruth[cleanup] Re-sort all the #include lines in LLVM using
2014-12-09 Rafael EspindolaReturn ErrorOr<std::unique_ptr<Archive>> form getAsArchive.
2014-10-31 David MajnemerObject, COFF: Cleanup symbol type code, improve binutil...
2014-09-18 Peter CollingbourneLTO: introduce object file-based on-disk module format.
2014-09-10 David MajnemerObject: Add support for bigobj
2014-08-19 Rafael EspindolaDon't own the buffer in object::Binary.
2014-08-08 Rafael EspindolaUse a simpler predicate. NFC.
2014-08-01 Rafael EspindolaRemove some calls to std::move.
2014-07-31 Rafael EspindolaReplaces a few pointers with references in llvm-nm...
2014-07-31 Rafael EspindolaUse std::unique_ptr to make the ownership explicit.
2014-07-28 Kevin EnderbyTweak llvm-nm’s -undefined-only (aka -u) printing for...
2014-07-24 Kevin EnderbyAdd an implementation for llvm-nm’s -print-file-name...
2014-07-21 David BlaikieCorrect the ownership passing semantics of object:...
2014-07-17 Kevin EnderbyTweak formating to match what clang-format would be...
2014-07-17 Kevin EnderbyAdd printing of Mach-O stabs in llvm-nm.
2014-07-16 Kevin EnderbyAdd the "-x" flag to llvm-nm for Mach-O files that...
2014-07-14 NAKAMURA Takumi[CMake] Update libdeps.
2014-07-11 Kevin EnderbyAdd the "-s" flag to llvm-nm for Mach-O files that...
2014-07-08 Kevin EnderbyChanged the lvm-nm alias "-s" for -print-armap to ...
2014-07-06 Rafael EspindolaUpdate the MemoryBuffer API to use ErrorOr.
2014-07-03 Kevin EnderbyAdd the -just-symbol-name (aka -j) flag to llvm-nm...
2014-07-03 Rafael Espindolafix configure+make build
2014-07-03 Rafael EspindolaAdd support for inline asm symbols to IRObjectFile.
2014-07-03 Kevin EnderbyAdd the -U flag to llvm-nm as an alias to -defined...
2014-07-02 Kevin EnderbyAdd the -reverse-sort flag (aka -r) to llvm-nm
2014-07-01 Kevin EnderbyAlso run clang-format on llvm-nm.cpp to tidy things...
2014-06-30 Kevin EnderbyAdd the -arch flag support to llvm-nm to select the...
2014-06-23 Rafael EspindolaPass a std::unique_ptr& to the create??? methods is...
2014-06-23 Rafael EspindolaMake ObjectFile and BitcodeReader always own the Memory...
2014-06-23 Rafael EspindolaConvert a few methods to use ErrorOr.
2014-06-23 Kevin EnderbyChange the default input for llvm-nm to be a.out instea...
2014-06-20 Kevin EnderbyFix some double printing of filenames for archives...
2014-06-20 Kevin EnderbyAdded the -m option as an alias for -format=darwin...
2014-06-19 Kevin EnderbyFix the output of llvm-nm for Mach-O files to use the...
2014-06-19 Kevin EnderbyChange the output of llvm-nm and llvm-size for Mach...
2014-06-16 Rafael EspindolaConvert the Archive API to use ErrorOr.
2014-06-13 Rafael EspindolaRemove 'using std::error_code' from tools.
2014-06-12 Rafael EspindolaDon't use 'using std::error_code' in include/llvm.
2014-06-12 Rafael EspindolaRemove system_error.h.
2014-06-05 Kevin EnderbyAdd "-format darwin" to llvm-nm to be like darwin's...
2014-06-03 Rafael EspindolaAllow alias to point to an arbitrary ConstantExpr.
2014-05-30 Tim NorthoverMachO: support N_INDR aliases in assembly files.
2014-05-16 Rafael EspindolaDelete getAliasedGlobal.
2014-05-14 Kevin EnderbyTeach llvm-nm to know about fat archives (aka MachOUniv...
2014-05-12 Kevin EnderbySuggested improvement by Rafael Espindola to use isa...
2014-05-09 Kevin EnderbyFix llvm-nm to print the full 64-bit address for symbol...
2014-04-03 Rafael EspindolaRevert "Fix a nomenclature error in llvm-nm."
2014-04-02 Rafael EspindolaFix a nomenclature error in llvm-nm.
2014-03-19 David MajnemerObject: Provide a richer means of describing auxiliary...
2014-03-18 Rui UeyamaObject/COFF: Add function to check if section number...
2014-03-18 Alexey Samsonov[C++11] Change the interface of getCOFF{Section,Relocat...
2014-03-15 Rui UeyamaObject/COFF: change data type of SymbolNumber from...
2014-03-06 Ahmed CharlesReplace OwningPtr<T> with std::unique_ptr<T>.
2014-03-05 Ahmed Charles[C++11] Replace OwningPtr::take() with OwningPtr::relea...
2014-03-04 Chandler Carruth[cleanup] Re-sort all the includes with utils/sort_incl...
2014-02-26 Alexey SamsonovMove getELFDynamicSymbolIterators to a public header.
2014-02-21 Rafael EspindolaAdd a SymbolicFile interface between Binary and ObjectFile.
2014-02-10 Rafael EspindolaChange the begin and end methods in ObjectFile to match...
2014-02-05 Rafael EspindolaUse the information provided by getFlags to unify some...
2014-02-04 Rafael EspindolaSmall fix for llvm-nm handling of weak symbols on ELF...
2014-02-04 Rafael EspindolaMove error handling down to getSymbolNMTypeChar.
2014-01-31 Rafael EspindolaSimplify getSymbolFlags.
2014-01-30 Rafael EspindolaThis file already has a "using namespace object;",...
2014-01-30 Rafael EspindolaOnly ELF has a dynamic symbol table. Remove it from...
2014-01-30 Rafael EspindolaUse early returns and factor the object::Binary creation.
2014-01-30 Rafael EspindolaSimplify the handling of iterators in ObjectFile.
2014-01-30 Rafael EspindolaFix TLS handling in ELF's getAddress and llvm-nm to...
2014-01-29 Rafael EspindolaNormalize the style in llvm-nm.cpp.
2014-01-22 Rafael EspindolaPass the computed magic to createBinary and createObjec...
2014-01-21 Rafael EspindolaRename these methods to match the style guide.
2014-01-15 Rafael EspindolaReturn an ErrorOr<Binary *> from createBinary.
2014-01-15 Rafael EspindolaMake parseBitcodeFile return an ErrorOr<Module *>.
2013-12-10 NAKAMURA Takumi[CMake] Update LLVM_LINK_COMPONENTS for each CMakeLists...
2013-11-02 Rafael Espindolamove getSymbolNMTypeChar to the one program that needs...
2013-09-19 Andrew TrickRevert "Encapsulate PassManager debug flags to avoid...
2013-09-18 Andrew TrickEncapsulate PassManager debug flags to avoid static...
2013-07-10 Rafael EspindolaDon't crash in 'llvm -s' when an archive has no symtab.
2013-07-03 Rafael EspindolaMake llvm-nm return 1 on error.
2013-06-18 Alexey SamsonovBasic support for parsing Mach-O universal binaries...
2013-06-17 Rafael EspindolaDon't link with the archive library programs that don...
2013-06-14 Rafael EspindolaRemove unused header.
2013-06-12 Rafael EspindolaRemove the program class.
2013-02-03 Michael J. Spencer[Object][Archive] Improve performance.
2013-01-02 Chandler CarruthMove all of the header files which are involved in...
2012-12-04 Chandler CarruthSort the #include lines for tools/...
2012-11-13 Daniel Dunbarllvm-nm: Make sort more stable when symbol names are...
2012-11-13 Shankar EaswaranAdding changes to support GNU style archive library...
2012-09-18 Jan SjödinAdd hidden flag to exclude aliases from output.
2012-08-17 Bill WendlingChange the `linker_private_weak_def_auto' linkage to...
2012-06-06 Michael J. Spencer[llvm-nm] Update documentation to cover object file...
2012-03-10 Benjamin KramerFix uses of the C99 PRI format macros not to conflict...
2012-02-28 David MeyerIn the ObjectFile interface, replace isInternal(),...
2012-02-28 Michael J. Spencer[Object] Add {begin,end}_dynamic_symbols stubs and...
2011-12-25 Rafael EspindolaRemove unused variables.
2011-12-13 Michael J. Spencerllvm-nm: refactor in order to support reading files...
2011-12-12 Daniel DunbarLLVMBuild: Remove trailing newline, which irked me.
2011-11-29 Danil MalyshevFixed ObjectFile functions:
2011-11-27 Chandler CarruthRevert r145180 as it is causing test failures on all...
2011-11-27 Danil MalyshevFixed ObjectFile functions:
2011-11-11 Daniel DunbarLLVMBuild: Add description files for the LLVM tools.
next