]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - unittests
cleanup.
[opencl/llvm.git] / unittests /
2015-01-13 Duncan P. N. Exon... IR: Add MDLocation class
2015-01-13 Aaron BallmanSilence warnings about unknown pragmas for compilers...
2015-01-13 NAKAMURA TakumiIR/MetadataTest.cpp: Appease msc17 to avoid initializer...
2015-01-13 Richard TrieuDisable a warning for self move since the test is check...
2015-01-13 Duncan P. N. Exon... IR: Use unique_ptr, NFC
2015-01-13 Duncan P. N. Exon... IR: Remove an invalid assertion when replacing resolved...
2015-01-13 Duncan P. N. Exon... Revert "IR: Fix an inverted assertion when replacing...
2015-01-13 Duncan P. N. Exon... IR: Fix an inverted assertion when replacing resolved...
2015-01-12 Duncan P. N. Exon... IR: Fix unit test memory leak reported by ASan
2015-01-12 Duncan P. N. Exon... IR: Make MDNodeFwdDecl destructor public
2015-01-12 Duncan P. N. Exon... IR: Add test for handleChangedOperand() recursion
2015-01-12 Duncan P. N. Exon... IR: Make temporary nodes distinct
2015-01-10 Dmitri GribenkoConvertUTFTest: fix misleading empty line
2015-01-07 Duncan P. N. Exon... IR: Add MDNode::getDistinct()
2015-01-07 Duncan P. N. Exon... IR: Add MDNode::isDistinct()
2015-01-05 Duncan P. N. Exon... IR: Don't drop MDNode uniquing on null operands
2015-01-05 Frederic RissMake DIE.h a public CodeGen header.
2015-01-05 Chandler Carruth[PM] Add names and debug logging for analysis passes...
2015-01-05 Chandler Carruth[PM] Switch the new pass manager to use a reference...
2015-01-04 Lang Hames[APFloat][ADT] Fix sign handling logic for FMA results...
2015-01-01 Chandler CarruthRevert r225053: Add an ArrayRef upcasting constructor...
2014-12-31 Michael GottesmanAdd 2x constructors for TinyPtrVector, one that takes...
2014-12-31 Michael GottesmanAdd a SmallMapVector class that is a MapVector with...
2014-12-31 Michael GottesmanAdd an ArrayRef upcasting constructor from ArrayRef...
2014-12-29 Chandler Carruth[cmake] Start making LLVM_LIBDIR_SUFFIX effective by...
2014-12-23 Rafael EspindolaFix a leak found by asan.
2014-12-22 Peter Zotov[C API] Expose LLVMGetGlobalValueAddress and LLVMGetFun...
2014-12-22 Rafael EspindolaThe leak detector is dead, long live asan and valgrind.
2014-12-16 Duncan P. N. Exon... Remove 'metadata' from comments
2014-12-16 Duncan P. N. Exon... IR: Stop printing 'metadata' in Metadata::print()
2014-12-16 Duncan P. N. Exon... IR: Make MDNode::dump() useful by adding addresses
2014-12-15 David MajnemerStringPool: Cleanup typos in unittest comments
2014-12-15 David MajnemerThreadLocal: Return a mutable pointer if templated...
2014-12-12 Duncan P. N. Exon... IR: Don't track nullptr on metadata RAUW
2014-12-12 Rafael EspindolaMove the resize file feature from mapped_file_region...
2014-12-12 Rafael EspindolaPass a FD to resise_file and add a testcase.
2014-12-12 Rafael EspindolaRemove unused feature. NFC.
2014-12-11 Rafael EspindolaRemove a convoluted way of calling close by moving...
2014-12-11 Rafael EspindolaRemove dead code. NFC.
2014-12-09 Duncan P. N. Exon... IR: Split Metadata from Value
2014-12-07 Duncan P. N. Exon... IR: Drop uniquing for self-referencing MDNodes
2014-12-07 Duncan P. N. Exon... IR: Remove reference to ENABLE_MDNODE_UNIQUING
2014-12-04 Rafael EspindolaRemove dead code. NFC.
2014-12-03 Aaron BallmanSilencing several "multiple copy constructors" warnings...
2014-12-03 Duncan P. N. Exon... ADT: Add SmallVector<>::emplace_back()
2014-12-03 Lang Hames[MCJIT] Unique-ptrify the RTDyldMemoryManager member...
2014-11-29 Duncan P. N. Exon... DebugIR: Delete -debug-ir
2014-11-25 Colin LeMahieuCleaning out google tests from MC.
2014-11-24 Paul RobinsonMore long path name support on Windows, this time in...
2014-11-24 Duncan P. N. Exon... Support: Add *cast_or_null<> for pointer wrappers
2014-11-21 Rafael EspindolaFix a silly bug in StreamingMemoryObject.cpp.
2014-11-20 Michael IlsemanCompilation test for PostOrderIterator.
2014-11-20 Alexey SamsonovRemove support for undocumented SpecialCaseList entries.
2014-11-19 Lang Hames[ADT] Fix PR20728 - Incorrect APFloat::fusedMultiplyAdd...
2014-11-19 David BlaikieRemove StringMap::GetOrCreateValue in favor of StringMa...
2014-11-18 NAKAMURA TakumiCallGraphTest.cpp: Remove invalid tests. ++S might...
2014-11-17 Rafael EspindolaFix the autoconf build.
2014-11-17 Rafael EspindolaFactor common code it Linker::init.
2014-11-17 Rafael EspindolaFix GraphTraits for "const CallGraphNode *" and "const...
2014-11-15 Benjamin KramerDispose disassembler after use in unit test.
2014-11-14 David BlaikieStringMap: Test and finish off supporting perfectly...
2014-11-13 Rafael EspindolaFix the other build system.
2014-11-13 Rafael EspindolaFix a regression on the disassembling C API.
2014-11-13 Aaron BallmanFixing some sign comparison warnings from MSVC; NFC.
2014-11-13 Paul RobinsonDrop a few unneeded ctor calls (missed code review...
2014-11-13 Paul RobinsonImprove long path name support on Windows.
2014-11-13 Jordan Rose[Bitcode] AtEndOfStream should only check against the...
2014-11-12 David BlaikieEnsure function_refs are copyable even from non-const...
2014-11-07 NAKAMURA Takumi[CMake] LLVMSupport: Give system_libs PRIVATE scope...
2014-11-04 Colin LeMahieu[Hexagon] Reverting 220584 to address ASAN errors.
2014-10-28 Rafael EspindolaRemove the PreserveSource linker mode.
2014-10-27 Michael GottesmanAdd MapVector::rbegin(), MapVector::rend() to completme...
2014-10-25 Rafael EspindolaUpdate the error handling of lib/Linker.
2014-10-24 Rafael EspindolaModernize the error handling of the Materialize function.
2014-10-24 Colin LeMahieu[Hexagon] Resubmission of 220427
2014-10-23 Rafael EspindolaAdd unittest for extreme alignments.
2014-10-23 NAKAMURA Takumi[CMake] Prune trailing whitespace.
2014-10-23 NAKAMURA TakumiRevert r220427, "[Hexagon] Adding encoding bits for...
2014-10-22 Lang Hames[MCJIT] Make repeat calls to MCJIT::getPointerToFunctio...
2014-10-22 Colin LeMahieu[Hexagon] Adding encoding bits for add opcode.
2014-10-22 Filipe CabecinhasSilence gcc's -Wcomment
2014-10-21 Aaron BallmanSilence a -Wcast-qual warning; NFC.
2014-10-19 Lang Hames[ADT] Add a 'find_as' operation to DenseSet.
2014-10-10 Chandler Carruth[ADT] Add an (ADL-friendly) abs free function for APFlo...
2014-10-10 Matt ArsenaultAdd minnum / maxnum to APFloat
2014-10-10 Chandler Carruth[ADT] Replace the logb implementation with the simpler...
2014-10-10 Chandler Carruth[ADT] Add the scalbn function for APFloat.
2014-10-10 Chandler Carruth[ADT] Implement the 'logb' functionality for APFloat...
2014-10-09 Chandler Carruth[ADT] Add basic operator overloads for arithmetic to...
2014-10-08 Nick Kledzik[Support] Add MemoryBuffer::getFileSlice()
2014-10-07 Kaelyn TakataAdd return value and negative checks to MapVector:...
2014-10-07 Kaelyn TakataAdd size_t MapVector::erase(KeyT) similar to the one...
2014-10-05 NAKAMURA Takumi[CMake] HexagonTests: Update LINK_COMPONENTS.
2014-10-03 Sid ManningAdd unit tests to verify Hexagon emission.
2014-10-03 Duncan P. N. Exon... Revert "Revert "DI: Fold constant arguments into a...
2014-10-03 Sid ManningAdding skeleton for unit testing Hexagon Code Emission
2014-10-02 Duncan P. N. Exon... Revert "DI: Fold constant arguments into a single MDString"
2014-10-02 Duncan P. N. Exon... DI: Fold constant arguments into a single MDString
2014-10-01 David BlaikieUpdate test name to match changes made in r218783
2014-10-01 Argyrios KyrtzidisAdds 'override' to overriding methods. NFC.
next