]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - utils/unittest
Updates to sync with changes in upstream.
[opencl/llvm.git] / utils / unittest /
2015-01-20 Rafael EspindolaUse -Wl,defs when linking.
2014-03-14 Galina KistanovaReverted r203879.
2014-03-14 Galina KistanovaFixed misuse of isascii. Also fixes mingw32 build,...
2014-02-26 NAKAMURA Takumi[CMake] Use LINK_LIBS instead of target_link_libraries().
2014-02-19 Alexey SamsonovSupport GTest for FreeBSD platforms (9.x)
2014-02-10 NAKAMURA Takumi[CMake] Add dependencies to gtest.
2014-01-30 Renato GolinComment out unused macro because of warning
2014-01-10 NAKAMURA TakumiSink add_llvm_library(gtest_main) to UnitTestMain/CMake...
2013-11-19 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-18 Alexey SamsonovUnbreak the build after r194997
2013-11-18 Alexey SamsonovRevert r194865 and r194874.
2013-11-16 NAKAMURA Takumigtest-death-test.cc: Move ~DeathTestFactory() to unbrea...
2013-11-15 Juergen RibutzkaFix previous commit (r194865)
2013-11-15 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-15 Chandler CarruthMove all of the GoogleTest files back to the same locat...
2013-05-14 Duncan SandsGet the unittests compiling when building with cmake...
2013-04-30 Reid KlecknerTry to fix ProgramTest on FreeBSD
2013-02-25 Matt Beaumont-Gay'Hexadecimal' has two 'a's and only one 'i'.
2013-01-18 Manuel KlimekAdd basic command line parsing to TestMain.
2012-12-07 NAKAMURA Takumiunittest/googletest/Makefile: Unbreak out-of-tree build.
2012-12-06 Alexey SamsonovTry to unbreak makefile build by excluding gtest-all...
2012-12-06 Alexey SamsonovModify the LLVM checkout of googletest:
2012-11-27 Richard SmithRemove unused internal linkage variable.
2012-09-27 Sylvestre LedruRevert 'Fix a typo 'iff' => 'if''. iff is an abreviatio...
2012-09-27 Sylvestre LedruFix a typo 'iff' => 'if'
2012-09-10 Evgeniy StepanovGTest on Android needs a custom tmpdir path.
2012-09-04 Evgeniy StepanovFix Android build of gtest and lib/Support.
2012-07-23 Sylvestre LedruFix a typo (the the => the)
2012-06-06 Benjamin KramerRemove dead private member variables from gtest.
2012-06-06 Justin HolewinskiFix gtest build issue on Visual Studio 2012 RC
2012-05-15 Daniel Dunbarllvm-build: Add support for non-installed libraries...
2012-01-22 David BlaikieHelp GCC along with code that's actually unreachable.
2012-01-21 David BlaikieRemove unreachable defaults from gtest.
2011-12-15 Daniel Dunbarbuild/unittests: Fix llvm-config names for gtest librar...
2011-11-29 Daniel Dunbarbuild/CMake: Finish removal of add_llvm_library_depende...
2011-11-12 Daniel DunbarLLVMBuild: Add info for gtest.
2011-10-19 Joe AbbeyAdding dependencies to allow -DBUILD_SHARED_LIBS=true...
2011-07-27 Frits van BommelUpdate CMake build for new gtest file.
2011-07-27 Jay FoadMerge gtest-1.6.0.
2011-04-15 Chris LattnerFix a ton of comment typos found by codespell. Patch by
2011-03-01 Oscar FuentesFixes warnings emitted by Visual Studio 2010 compiler.
2011-02-28 NAKAMURA TakumiDon't install libUnitTestMain.a. It might be useless...
2011-02-04 NAKAMURA TakumiMake Win32's header file name lower for cross build...
2010-11-29 Michael J. SpencerMerge System into Support.
2010-10-19 Michael J. SpencerFix VC2010 build.
2010-10-17 Oscar FuentesBuild with RTTI and exceptions disabled. Only in GCC...
2010-10-07 Michael J. Spencergtest: Fix warnings on MinGW.
2010-10-07 Michael J. SpencerCMake: Fix warning in gtest.
2010-10-02 Francois PichetFix MSVC release mode compilation error.
2010-09-25 Oscar FuentesReverting "CMake: Don't include tools, unittets, or...
2010-09-24 Michael J. SpencerCMake: Don't include tools, unittets, or examples as...
2010-09-24 Michael J. SpencerFix line endings from my last commit.
2010-09-24 Michael J. Spencerunittests: Support Windows.
2010-09-24 Michael J. SpencerCMake: Build unittests.
2010-09-04 Chris Lattnerdelete dead code.
2010-08-15 Argyrios KyrtzidisRevert r111082. No warnings for this common pattern.
2010-08-14 Argyrios KyrtzidisAdd ATTRIBUTE_UNUSED to methods that are not supposed...
2010-07-12 Jakob Stoklund OlesenSilence a warning.
2010-06-23 Nick LewyckyDon't link against libm and libpthread which don't...
2010-06-03 Benjamin KramerForgot to update the most important part of the gtest...
2010-06-03 Benjamin KramerDisable pthread support in googletest if llvm was confi...
2010-06-03 Benjamin KramerTurns out gtest still prefers the system <tr1/tuple...
2010-06-02 Benjamin KramerUpdate Readme and Makefiles for the new gtest.
2010-06-02 Benjamin KramerMerge gtest-1.5.0.
2010-06-02 Benjamin KramerMerge gtest-1.4.0.
2010-06-02 Benjamin KramerMerge gtest-1.3.0.
2010-04-18 Chris Lattnersilence some -Wmissing-field-initializers warnings.
2010-04-13 Daniel DunbarFix -Asserts warnings.
2010-04-09 Chris Lattneradd minix support, patch by Kees van Reeuwijk! PR6797
2010-03-09 Chandler CarruthContinue propagating the GoogleTest flags until we...
2010-03-09 Chandler CarruthConsolidate GoogleTest make options and duplicate them...
2010-01-24 Chris Lattnermake -fno-rtti the default unless a directory builds...
2009-12-18 Eli FriedmanFix an issue in googletest where a name was used before...
2009-12-16 Bill WendlingRemove superfluous 'extern' variable that was causing...
2009-10-26 Julien LerougeRemove / use flags that are now set in the Makefile...
2009-10-12 Edward O'CallaghanHaiku porting patches, Credit to Paul Davey.
2009-09-20 Daniel DunbarFollow googletest logic for suppressing warnings in...
2009-09-13 Daniel DunbarMove unittest driver to utils/unittest/UnitTestMain.
2009-09-05 Jeffrey YasskinTeach googletest to use raw_ostream instead of just...
2009-08-18 Anton KorobeynikovThe attached patches attempt to fix cross builds. For...
2009-07-27 Benjamin KramerRemove trailing slashes from include paths. Some versio...
2009-05-08 Chris LattnerChange 'make install' to install tblgen, for better...
2009-02-12 Julien LerougeFix MingW build: define GTEST_OS_WINDOWS if OS is MingW...
2009-02-05 Mike StumpFIx spelling.
2009-02-05 Mike StumpProbe for flags before using them to try to help compil...
2009-01-05 Misha BrukmanRenamed Google Test license file from COPYING to LICENS...
2009-01-02 Misha BrukmanWe also removed gtest-all.cc from the distribution...
2009-01-01 Misha Brukman* Removed gtest-all.cc; .cc files including other ...
2009-01-01 Misha BrukmanMoved Google Test code up one directory so that we...
2008-12-31 Misha BrukmanImport of Google Test 1.2.1, with the non-essential...