FileCheck: Print a nice error message for missing closing ']' in regex vars.
[opencl/llvm.git] / utils /
2014-01-03 Adrian PrantlFileCheck: Print a nice error message for missing closi...
2014-01-02 Hal Finkel[TableGen] Handle ValueType in CodeGenDAGPatterns GetNu...
2014-01-02 Craig TopperMark REX64_PREFIX as In64BitMode, remove hack from...
2014-01-02 Craig TopperRemove unused HasFROperands field from disassembler.
2014-01-02 Craig TopperMark PUSHFS64/PUSHGS64/POPFS64/POPGS64 as In64BitMode...
2014-01-02 Craig TopperRemove unnecessary stirng comparison from disassembler.
2014-01-02 Craig TopperMark all x86 Int_ and _Int patterns as isCodeGenOnly...
2014-01-02 Craig TopperRemove unused function argument.
2014-01-01 Craig TopperRemove modifierType/Base from X86 disassembler tables...
2014-01-01 Craig TopperRemove need for MODIFIER_OPCODE in the disassembler...
2014-01-01 Elena DemikhovskyAVX-512: Added intrinsics for vcvt, vcvtt, vrndscale...
2014-01-01 Craig TopperSecond attempt at Removing special form of AddRegFrm...
2013-12-31 Craig TopperRevert r198238 and add FP disassembler tests. It didn...
2013-12-30 Craig TopperRemove special form of AddRegFrm used by FP instruction...
2013-12-30 Craig TopperRemove EscapeFilter. It's funcionality can be covered...
2013-12-30 Craig TopperSimplify filter accepts function to just return 'condit...
2013-12-30 NAKAMURA Takumi[CMake] Generate ${BUILD_MODE}/llvm-lit for each $...
2013-12-29 Alp TokerPython compatibility fix for r198150
2013-12-29 Alp TokerProspective Python 3 fix for r198150
2013-12-29 Alp Tokerlit: Incremental test scheduling
2013-12-25 Elena DemikhovskyAVX-512: decoder for AVX-512, made by Alexey Bader.
2013-12-20 NAKAMURA TakumiInstall three utils, "FileCheck", "count", and "not...
2013-12-20 Eric Christopher[x86] Rename In32BitMode predicate to Not64BitMode
2013-12-19 Hal FinkelAdd support for positionally-encoded operands to FixedL...
2013-12-19 Hal FinkelAdd support for PointerLikeRegClass to FixedLenDecoderE...
2013-12-17 Hal FinkelSupport little-endian encodings in the FixedLenDecoderE...
2013-12-17 NAKAMURA TakumiTweak lit/TestingConfig.py Py3-compatible. has_key...
2013-12-17 Reid KlecknerAdd missing trailing comma in llvm-lit.in
2013-12-17 Reid KlecknerAdd the lit site config for unittests to bin/llvm-lit
2013-12-16 Elena DemikhovskyAVX-512: Added legal type MVT::i1 and VK1 register...
2013-12-12 Hans WennborgExpose FileCheck's AddFixedStringToRegEx as Regex:...
2013-12-05 Alp TokerCorrect word hyphenations
2013-12-03 NAKAMURA Takumiutils/llvm-lit: Generate "llvm-lit.py" rather than...
2013-12-03 Bill WendlingRemove superfluous label.
2013-12-02 Rafael EspindolaRemove dead code.
2013-11-24 Bill WendlingDefault to a better compression algorithm.
2013-11-20 Daniel SandersFileCheck: fix a bug with multiple --check-prefix optio...
2013-11-20 Bill WendlingAdd -triple option.
2013-11-19 Bill WendlingAdd lld to projects to tag.
2013-11-19 Juergen Ributzka[weak vtables] Place class definitions into anonymous...
2013-11-19 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-18 Arnaud A. de Grand... test-release.sh: tweak RPATH for the binary packages.
2013-11-18 Alexey SamsonovUnbreak the build after r194997
2013-11-18 Alexey SamsonovRevert r194865 and r194874.
2013-11-17 Ahmed BougachaTableGen: Generate an enum for all named Operand types...
2013-11-16 NAKAMURA Takumigtest-death-test.cc: Move ~DeathTestFactory() to unbrea...
2013-11-16 Owen AndersonSmall improvement to InstrinsicEmitter::EmitAttributes...
2013-11-15 Juergen RibutzkaFix previous commit (r194865)
2013-11-15 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-15 Chandler CarruthMove all of the GoogleTest files back to the same locat...
2013-11-15 Matt ArsenaultAdd addrspacecast instruction.
2013-11-14 Matt ArsenaultUpdate emacs llvm mode.
2013-11-13 Alexey SamsonovFileCheck: fix matching of one check-prefix is a prefix...
2013-11-13 Alexey SamsonovFileCheck: fix a bug with multiple --check-prefix options.
2013-11-10 Matt ArsenaultAllow multiple check prefixes in FileCheck.
2013-11-03 Elena DemikhovskyAVX-512: added VPCONFLICT instruction and intrinsics,
2013-11-03 Bob WilsonConfigure with --enable-terminfo=no for Apple's llvmCor...
2013-11-01 Rafael EspindolaRemove linkonce_odr_auto_hide.
2013-10-31 Andrew TrickLower stackmap intrinsics directly to their target...
2013-10-31 Andrew TrickEnable variable arguments support for intrinsics.
2013-10-31 Andrew Trickwhitespace
2013-10-28 Ahmed BougachaTableGen: remove unused variable.
2013-10-28 Ahmed BougachaTableGen: Refactor DAG patterns to enable parsing one...
2013-10-28 Ahmed BougachaTableGen: Refactor AsmWriterEmitter to keep AsmWriterInsts.
2013-10-28 Alp Tokerlit: multiprocessing platform fix attempt
2013-10-27 Alp TokerClarify the comment about BSD versions in r193465
2013-10-26 Joerg Sonnenbergerself.path may be empty or otherwise miss the normal...
2013-10-26 Alp Tokerlit: Issue a note when multiprocessing fails to load
2013-10-26 Alp TokerFix a referenced before assignment in r193463
2013-10-26 Alp Tokerlit: handle late multiprocessing errors gracefully
2013-10-26 Alp TokerAttempt to fix the FreeBSD build, disable multiprocessing
2013-10-25 Rafael EspindolaTry to fix the openbsd bot.
2013-10-23 Rafael EspindolaActually switch the default to use multiprocessing
2013-10-23 Daniel Dunbar[lit] Stop hacking the GIL check interval.
2013-10-23 Daniel Dunbar[lit] Use multiprocessing based parallelism by default...
2013-10-20 Peter CollingbourneTypo.
2013-10-18 NAKAMURA TakumiYAMLBench.cpp: Use llvm_move instead of std::move also...
2013-10-18 Michael J. Spencer[Support][YAML] Add support for accessing tags and...
2013-10-17 NAKAMURA TakumiLit: LIT_PRESERVES_TMP should be aware of TMPDIR, too.
2013-10-17 NAKAMURA TakumiLit: Introduce an environment variable, $LIT_PRESERVES_...
2013-10-14 Rafael EspindolaRemove utils/profile.pl.
2013-10-14 Craig TopperAllow pinsrw/pinsrb/pextrb/pextrw/movmskps/movmskpd...
2013-10-12 Craig TopperRemove more filters from the disassembler. Mark some...
2013-10-12 Craig TopperMark some more instructions as CodeGenOnly. Remove...
2013-10-12 Will DietzAdd missing #include's to cctype when using isdigit...
2013-10-11 Stephen LinReally fix CHECK-LABEL and CHECK-DAG interaction. This...
2013-10-11 Rafael EspindolaFix handling of CHECK-DAG inside of CHECK-LABEL.
2013-10-11 Craig TopperRemove another unnecessary filter from the disassembler.
2013-10-10 Craig TopperFix so CRC32r64r8 isn't accidentally filtered from...
2013-10-09 Craig TopperMore x86 disassembler filtering cleanup.
2013-10-09 Craig TopperRemove some old filters from the x86 disassembler table...
2013-10-08 Craig TopperRemove unneeded MMX instruction definition by moving...
2013-10-08 Craig TopperRemove some instructions that existed to provide aliase...
2013-10-07 Craig TopperRemove some instructions that seem to only exist to...
2013-10-07 Craig TopperAdd disassembler support for long encodings for INC...
2013-10-07 David MajnemerRevert "Revert "Windows: Add support for unicode comman...
2013-10-06 David MajnemerRevert "Windows: Add support for unicode command lines"
2013-10-06 David MajnemerWindows: Add support for unicode command lines
2013-10-05 Craig TopperAdd OPC_CheckChildSame0-3 to the DAG isel matcher....
2013-10-04 Craig TopperRevert r191940 to see if it fixes the build bots.
next