]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/history - utils
Provide an API to temporarily suppress DebugLocations from being attached
[opencl/llvm.git] / utils /
2013-04-30 Reid KlecknerTry to fix ProgramTest on FreeBSD
2013-04-27 Ulrich WeigandHandle tied sub-operands in AsmMatcherEmitter
2013-04-26 Michael GottesmanUse 'git svn find-rev' in git-svnrevert instead of...
2013-04-26 Michael GottesmanAdded the scripts git-svnup/git-svnrevert to utils...
2013-04-25 Michael LiaoRemove SMLoc paired with CHECK-NOT patterns. Not functi...
2013-04-25 Michael LiaoRemove tailing whitespaces
2013-04-23 Andrew TrickMachine model: Generate table entries for super-resources.
2013-04-23 Andrew TrickMachine model: verify well-formed processor resource...
2013-04-23 Andrew TrickMachine model: rewrite a tablegen loop to avoid compari...
2013-04-18 Chad Rosier[asm parser] Add support for predicating MnemonicAlias...
2013-04-12 Daniel Dunbarlit: Fix infinite recursion when an out-of-tree test...
2013-04-12 Daniel Dunbarlit: Add a test for discovery w/ test_exec_root (out...
2013-04-11 Michael LiaoAdd CLAC/STAC instruction encoding/decoding support
2013-04-11 Daniel Dunbarlit: Don't descend into .git directories during test...
2013-04-11 Daniel Dunbarlit: Shorten a metavar to make --help look nicer.
2013-04-11 Daniel Dunbarlit: Add a test for discovery when exact test names...
2013-04-11 Daniel Dunbarlit: Add a trivial test of the basic progress bar.
2013-04-05 Rafael EspindolaMove yaml2obj to tools too.
2013-04-05 Rafael EspindolaUse ScalarBitSetTraits.
2013-04-05 Rafael EspindolaMove obj2yaml to tools to sort out make's dependencies.
2013-04-05 Rafael EspindolaBuild obj2yaml with configure+make.
2013-04-04 Rafael EspindolaAdd back parsing of header charactestics.
2013-04-03 Rafael EspindolaRemove anonymous namespace.
2013-04-02 Rafael EspindolaUse yaml::IO in yaml2obj.cpp.
2013-03-29 Andrew TrickFix TableGen subtarget-emitter to handle A9/Swift.
2013-03-29 Dan GohmanRevert r178166. According to Howard, this code is actua...
2013-03-27 Dan GohmanAvoid undefined behavior from passing a std::vector...
2013-03-26 Andrew TrickTableGen SubtargetEmitter fix to allow A9 and Swift...
2013-03-25 Dave Zarzyckix86 -- add the XTEST instruction
2013-03-24 Jakob Stoklund OlesenAllow types to be omitted in output patterns.
2013-03-24 Jakob Stoklund OlesenAllow direct value types to be used in instruction...
2013-03-23 Jakob Stoklund OlesenAllow direct value types in pattern definitions.
2013-03-23 Jakob Stoklund OlesenMake all unnamed RegisterClass TreePatternNodes typed...
2013-03-23 Benjamin KramerPlug a memory leak in FileCheck when the input file...
2013-03-21 Sean SilvaAdd TableGen ctags(1) emitter and helper script.
2013-03-20 Reid Kleckner[lit] Avoid CRLFs in bash scripts on Windows
2013-03-19 Ulrich WeigandExtend TableGen instruction selection matcher to improv...
2013-03-18 Andrew TrickTableGen fix for the new machine model.
2013-03-18 Jakob Stoklund OlesenExtract a method.
2013-03-17 Jakob Stoklund OlesenUse ArrayRef<MVT::SimpleValueType> when possible.
2013-03-16 Andrew TrickMachine model. Allow mixed itinerary classes and SchedR...
2013-03-15 Jakob Stoklund OlesenAdd SchedRW as an Instruction field.
2013-03-14 Andrew TrickFix r177112: Add ProcResGroup.
2013-03-14 Andrew TrickMachineModel: Add a ProcResGroup class.
2013-03-13 NAKAMURA Takumilit.TestFormats.GoogleTest: Honor LitConfig.noExecute...
2013-03-11 Kevin EnderbyFixes disassembler crashes on 2013 Haswell RTM instruct...
2013-03-01 Andrew TrickMIsched machine model: tablegen subtarget emitter impro...
2013-02-28 Bill WendlingEnable syntax highlighting for reStructuredText files.
2013-02-26 Michael J. Spencer[TableGen] Fix ICE on MSVC 2012 Release builds.
2013-02-26 Kostya SerebryanyUnify clang/llvm attributes for asan/tsan/msan (LLVM...
2013-02-25 Matt Beaumont-Gay'Hexadecimal' has two 'a's and only one 'i'.
2013-02-14 Jyotsna VermaFix for bug 15246 -- out-of-bound error in the TableGen...
2013-02-13 David PeixottoPR14992 - Tablegen incorrectly converts ARM tLDMIA_UPD...
2013-02-12 Guy BenyeiAdd static cast to unsigned char whenever a character...
2013-02-12 Kay Tiong KhooAdded 0x0D to 2-byte opcode extension table for prefetc...
2013-02-11 Kostya Serebryany[tsan/msan] adding thread_safety and uninitialized_chec...
2013-02-07 Daniel Dunbar[lit] Add a display function for lit.Test.TestResult.
2013-02-06 Guy BenyeiCanonicalize line endings to Linux style also when...
2013-02-06 Jim GrosbachAllow targets to add custom asm operand matching logic.
2013-02-05 Bob WilsonPreprocess Apple llvmCore headers to reflect NDEBUG...
2013-02-05 Bob WilsonSet the deployment target for Apple llvmCore builds...
2013-02-05 Eli BenderskyFix comments
2013-02-05 Jack CarterThis patch that sets the EmitAlias flag in td files
2013-02-01 Andrew TrickMachineModel: Inconsequential TableGen SubtargetEmitter...
2013-01-31 Daniel Dunbar[lit] Add a test for internal shell execution behaviors.
2013-01-31 Daniel Dunbar[lit] Change to raise InternalShellError for all comman...
2013-01-31 Daniel Dunbar[lit] Fix bug where InternalShellError messages were...
2013-01-31 Daniel Dunbar[lit] Fix a shell parsing bug with ';' not separated...
2013-01-31 Daniel Dunbar[lit] Add a test for the various ShTest format features.
2013-01-31 Daniel Dunbar[lit] TestRunner: Eliminate failDueToStderr argument...
2013-01-31 Daniel Dunbar[lit] Delete the now-unused SyntaxCheckTest format.
2013-01-31 Jakob Stoklund OlesenClarify intent.
2013-01-31 Derek Schuff[MC] bundle alignment: prevent padding instructions...
2013-01-31 Tim NorthoverAdd AArch64 as an experimental target.
2013-01-31 Daniel Dunbar[lit] Move unittest adaptor code into discovery module.
2013-01-31 Daniel Dunbar[lit] Run the ShUtil tests as part of the test suite.
2013-01-31 Daniel Dunbar[lit] Set parallel mode for coverage tests.
2013-01-31 Daniel Dunbar[lit] Move discovery code into its own module.
2013-01-31 Daniel Dunbar[lit] Add a MANIFEST file and a script for sanity check...
2013-01-31 Daniel Dunbar[lit] Add a basic discovery test.
2013-01-31 Daniel Dunbar[lit] Add a script for checking test coverage.
2013-01-31 Daniel Dunbar[lit] Add a test suite for lit itself.
2013-01-30 Alexey Samsonov[lit] Make GoogleTest test runner correctly discover...
2013-01-30 Daniel Dunbar[lit] Add some TODO notes to myself.
2013-01-28 David GreeneAvoid Unnecessary Builds
2013-01-27 NAKAMURA Takumi[CMake][Lit][unittests] Deprecate CMAKE_BUILD_TYPE...
2013-01-27 Bill WendlingUse the AttributeSet instead of AttributeWithIndex.
2013-01-25 Aaron BallmanA port of the Visual Studio 2012 debugger visualizers...
2013-01-25 Bob WilsonUse xcrun to find the right compiler when building...
2013-01-25 NAKAMURA Takumilit/ShUtil.py: Deprecate '!' in shell expression. It...
2013-01-23 Bill WendlingAdd the IR attribute 'sspstrong'.
2013-01-20 NAKAMURA Takumillvm/utils/valgrind/x86_64-pc-linux-gnu.supp: Add ...
2013-01-18 Manuel KlimekAdd basic command line parsing to TestMain.
2013-01-18 Dmitri GribenkoRemove support for Tcl test format since nobody uses it
2013-01-17 Daniel Dunbar[utils] Update find-rev utility to take a branch argume...
2013-01-16 David GreeneUse --enable-werror
2013-01-15 Chad Rosier[ms-inline asm] Address the FIXME in AsmParser.cpp.
2013-01-12 Bob WilsonFix quoting problems from my previous change. <rdar...
2013-01-11 Michael IlsemanSupport for half intrinsics. Pushes MMX into slower...
2013-01-10 Bob WilsonUpdate Apple's build script for llvmCore. <rdar://probl...
next