opencl/llvm.git
6 years ago[PM] Move the LazyCallGraph printing functionality to a print method.
Chandler Carruth [Tue, 13 Jan 2015 23:53:50 +0000 (23:53 +0000)]
[PM] Move the LazyCallGraph printing functionality to a print method.

I'm adding generic analysis printing utility pass support which will
require such a method (or a specialization) so this will let the
existing printing logic satisfy that.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225854 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Bail out of AddMachineRegPiece() if MachineReg is not a
Adrian Prantl [Tue, 13 Jan 2015 23:39:15 +0000 (23:39 +0000)]
Debug Info: Bail out of AddMachineRegPiece() if MachineReg is not a
physical register. The call to getMinimalPhysRegClass() later on asserts
on this condition.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225852 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Move the complex expression handling (=the remainder) of
Adrian Prantl [Tue, 13 Jan 2015 23:39:11 +0000 (23:39 +0000)]
Debug Info: Move the complex expression handling (=the remainder) of
emitDebugLocValue() into DwarfExpression.

Ought to be NFC, but it actually uncovered a bug in the debug-loc-asan.ll
testcase. The testcase checks that the address of variable "y" is stored
at [RSP+16], which also lines up with the comment.
It also check(ed) that the *value* of "y" is stored in RDI before that,
but that is actually incorrect, since RDI is the very value that is
stored in [RSP+16]. Here's the assembler output:

movb 2147450880(%rcx), %r8b
#DEBUG_VALUE: bar:y <- RDI
cmpb $0, %r8b
movq %rax, 32(%rsp)          # 8-byte Spill
movq %rsi, 24(%rsp)          # 8-byte Spill
movq %rdi, 16(%rsp)          # 8-byte Spill
.Ltmp3:
#DEBUG_VALUE: bar:y <- [RSP+16]

Fixed the comment to spell out the correct register and the check to
expect an address rather than a value.

Note that the range that is emitted for the RDI location was and is still
wrong, it claims to begin at the function prologue, but really it should
start where RDI is first assigned.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225851 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[AVX512] Add 16x32 unpck tests as well
Adam Nemet [Tue, 13 Jan 2015 23:27:55 +0000 (23:27 +0000)]
[AVX512] Add 16x32 unpck tests as well

Forgot this from r225838.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225850 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agocleanup.
Adrian Prantl [Tue, 13 Jan 2015 23:11:51 +0000 (23:11 +0000)]
cleanup.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225848 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDocument, cleanup, and clang-format DwarfExpression.h
Adrian Prantl [Tue, 13 Jan 2015 23:11:07 +0000 (23:11 +0000)]
Document, cleanup, and clang-format DwarfExpression.h

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225847 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Turn DIExpression::getFrameRegister() into an isFrameRegister()
Adrian Prantl [Tue, 13 Jan 2015 23:10:43 +0000 (23:10 +0000)]
Debug Info: Turn DIExpression::getFrameRegister() into an isFrameRegister()
function.

NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225846 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoR600/SI: Add pattern for bitcasting fp immediates to integers
Tom Stellard [Tue, 13 Jan 2015 22:59:41 +0000 (22:59 +0000)]
R600/SI: Add pattern for bitcasting fp immediates to integers

The backend now assumes that all immediates are integers.  This allows
us to simplify immediate handling code, becasue we no longer need to
handle fp and integer immediates differently.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225844 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Remove the defunt CGSCC-specific debug flag.
Chandler Carruth [Tue, 13 Jan 2015 22:45:13 +0000 (22:45 +0000)]
[PM] Remove the defunt CGSCC-specific debug flag.

Even before I sunk the debug flag into the opt tool this had been made
obsolete by factoring the pass and analysis managers into a single set
of templates that all used the core flag. No functionality changed here.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225842 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Push the debug option for the new pass manager into the opt tool
Chandler Carruth [Tue, 13 Jan 2015 22:42:38 +0000 (22:42 +0000)]
[PM] Push the debug option for the new pass manager into the opt tool
and expose the necessary hooks in the API directly.

This makes it much cleaner for example to log the usage of a pass
manager from a library. It also makes it more obvious that this
functionality isn't "optional" or "asserts-only" for the pass manager.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225841 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoFix function names in tests from r225838.
Adam Nemet [Tue, 13 Jan 2015 22:40:15 +0000 (22:40 +0000)]
Fix function names in tests from r225838.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225840 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[AVX512] Unpack support in new shuffle lowering
Adam Nemet [Tue, 13 Jan 2015 22:20:18 +0000 (22:20 +0000)]
[AVX512] Unpack support in new shuffle lowering

This now handles both 32 and 64-bit element sizes.

In this version, the test are in vector-shuffle-512-v8.ll, canonicalized by
Chandler's update_llc_test_checks.py.

Part of <rdar://problem/17688758>

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225838 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[AVX512] Add pretty-printing of shuffle mask for unpacks
Adam Nemet [Tue, 13 Jan 2015 22:20:14 +0000 (22:20 +0000)]
[AVX512] Add pretty-printing of shuffle mask for unpacks

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225837 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDAGCombiner: simplify by using condition variables; NFC
Matthias Braun [Tue, 13 Jan 2015 22:17:46 +0000 (22:17 +0000)]
DAGCombiner: simplify by using condition variables; NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225836 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Sink the convenience typedefs after the class template they are
Chandler Carruth [Tue, 13 Jan 2015 21:30:27 +0000 (21:30 +0000)]
[PM] Sink the convenience typedefs after the class template they are
referring to and give them nice comments.

Previously, these were used, but now things use the generic form of the
AnalysisManager.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225833 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser/Bitcode: Add support for MDLocation
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 21:10:44 +0000 (21:10 +0000)]
AsmParser/Bitcode: Add support for MDLocation

This adds assembly and bitcode support for `MDLocation`.  The assembly
side is rather big, since this is the first `MDNode` subclass (that
isn't `MDTuple`).  Part of PR21433.

(If you're wondering where the mountains of testcase updates are, we
don't need them until I update `DILocation` and `DebugLoc` to actually
use this class.)

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225830 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoR600: Implement getRecipEstimate
Matt Arsenault [Tue, 13 Jan 2015 20:53:23 +0000 (20:53 +0000)]
R600: Implement getRecipEstimate

This requires a new hook to prevent expanding sqrt in terms
of rsqrt and reciprocal. v_rcp_f32, v_rsq_f32, and v_sqrt_f32 are
all the same rate, so this expansion would just double the number
of instructions and cycles.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225828 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoR600: Implement getRsqrtEstimate
Matt Arsenault [Tue, 13 Jan 2015 20:53:18 +0000 (20:53 +0000)]
R600: Implement getRsqrtEstimate

Only do for f32 since I'm unclear on both what this is expecting
for the refinement steps in terms of accuracy, and what
f64 instruction actually provides.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225827 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Fix GCC error from MDLocation::getInlinedAt()
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 20:50:21 +0000 (20:50 +0000)]
IR: Fix GCC error from MDLocation::getInlinedAt()

Apparently GCC didn't like my ternary operator from r225824.  Use an
`if`.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225826 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Add MDLocation class
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 20:44:56 +0000 (20:44 +0000)]
IR: Add MDLocation class

Add a new subclass of `UniquableMDNode`, `MDLocation`.  This will be the
IR version of `DebugLoc` and `DILocation`.  The goal is to rename this
to `DILocation` once the IR classes supersede the `DI`-prefixed
wrappers.

This isn't used anywhere yet.  Part of PR21433.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225824 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoR600: Make cttz / ctlz cheap to speculate
Matt Arsenault [Tue, 13 Jan 2015 19:46:48 +0000 (19:46 +0000)]
R600: Make cttz / ctlz cheap to speculate

Speculating things is generally good. SI+ has instructions for these
for 32-bit values. This is still probably better even with the expansion
for 64-bit values, although it is odd that this callback doesn't have
the size as a parameter.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225822 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoFix non-determinism issue in SLP
Julien Lerouge [Tue, 13 Jan 2015 19:45:52 +0000 (19:45 +0000)]
Fix non-determinism issue in SLP

The issue was introduced in r214638:

+  for (auto &BSIter : BlocksSchedules) {
+    scheduleBlock(BSIter.second.get());
+  }

Because BlocksSchedules is a DenseMap with BasicBlock* keys, blocks are
scheduled in non-deterministic order, resulting in unpredictable IR.

Patch by Daniel Reynaud!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225821 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoUse the integrated assembler as default on SystemZ
Ulrich Weigand [Tue, 13 Jan 2015 19:45:16 +0000 (19:45 +0000)]
Use the integrated assembler as default on SystemZ

This was already done in clang, this commit now uses the integrated
assembler as default when using LLVM tools directly.

A number of test cases deliberately using an invalid instruction in
inline asm now have to use -no-integrated-as.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225820 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoUse the integrated assembler as default on PowerPC
Ulrich Weigand [Tue, 13 Jan 2015 19:43:45 +0000 (19:43 +0000)]
Use the integrated assembler as default on PowerPC

This was already done in clang, this commit now uses the integrated
assembler as default when using LLVM tools directly.

A number of test cases using inline asm had to be adapted, either by
updating the expected output, or by using -no-integrated-as (for such
tests that deliberately use an invalid instruction in inline asm).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225819 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRunning clang-format on CommandLine.h and CommandLine.cpp.
Chris Bieneman [Tue, 13 Jan 2015 19:14:20 +0000 (19:14 +0000)]
Running clang-format on CommandLine.h and CommandLine.cpp.

No functional changes, I'm just going to be doing a lot of work in these files and it would be helpful if they had more current LLVM style.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225817 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAdd link to Go bindings documentation.
Peter Collingbourne [Tue, 13 Jan 2015 18:49:42 +0000 (18:49 +0000)]
Add link to Go bindings documentation.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225815 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRevert "r225808 - [PowerPC] Add StackMap/PatchPoint support"
Hal Finkel [Tue, 13 Jan 2015 18:25:05 +0000 (18:25 +0000)]
Revert "r225808 - [PowerPC] Add StackMap/PatchPoint support"

Reverting this while I investiage buildbot failures (segfaulting in
GetCostForDef at ScheduleDAGRRList.cpp:314).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225811 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoUpdate multiline.ll testcase to handle (ppc64le) .localentry directive
Will Schmidt [Tue, 13 Jan 2015 18:17:08 +0000 (18:17 +0000)]
Update multiline.ll testcase to handle (ppc64le) .localentry directive

The ppc64le platform will emit a .localentry directive. This is triggering
a false-positive against a CHECK-NOT: .loc in multiline.ll.
Add a space "{{ }}" to the check-not line to allow for arguments, and
prevent .localentry from matching.

Differential Revision: http://reviews.llvm.org/D6935

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225810 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PowerPC] Add missing override keyword
Hal Finkel [Tue, 13 Jan 2015 18:02:22 +0000 (18:02 +0000)]
[PowerPC] Add missing override keyword

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225809 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PowerPC] Add StackMap/PatchPoint support
Hal Finkel [Tue, 13 Jan 2015 17:48:12 +0000 (17:48 +0000)]
[PowerPC] Add StackMap/PatchPoint support

This commit does two things:

 1. Refactors PPCFastISel to use more of the common infrastructure for call
    lowering (this lets us take advantage of this common code for lowering some
    common intrinsics, stackmap/patchpoint among them).

 2. Adds support for stackmap/patchpoint lowering. For the most part, this is
    very similar to the support in the AArch64 target, with the obvious differences
    (different registers, NOP instructions, etc.). The test cases are adapted
    from the AArch64 test cases.

One difference of note is that the patchpoint call sequence takes 24 bytes, so
you can't use less than that (on AArch64 you can go down to 16). Also, as noted
in the docs, we take the patchpoint address to be the actual code address
(assuming the call is local in the TOC-sharing sense), which should yield
higher performance than generating the full cross-DSO indirect-call sequence
and is likely just as useful for JITed code (if not, we'll change it).

StackMaps and Patchpoints are still marked as experimental, and so this support
is doubly experimental. So go ahead and experiment!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225808 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[StackMaps] Use CurrentFnSymForSize
Hal Finkel [Tue, 13 Jan 2015 17:48:07 +0000 (17:48 +0000)]
[StackMaps] Use CurrentFnSymForSize

When computing the call-site offset, use AP.CurrentFnSymForSize instead of
AP.CurrentFnSym. There should be no change for other targets, but this is
necessary for generating valid expressions for PPC64/ELF.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225807 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[StackMaps] Mark in CallLoweringInfo when lowering a patchpoint
Hal Finkel [Tue, 13 Jan 2015 17:48:04 +0000 (17:48 +0000)]
[StackMaps] Mark in CallLoweringInfo when lowering a patchpoint

While, generally speaking, the process of lowering arguments for a patchpoint
is the same as lowering a regular indirect call, on some targets it may not be
exactly the same. Targets may not, for example, want to add additional register
dependencies that apply only to making cross-DSO calls through linker stubs,
may not want to load additional registers out of function descriptors, and may
not want to add additional side-effect-causing instructions that cannot be
removed later with the call itself being generated.

The PowerPC target will use this in a future commit (for all of the reasons
stated above).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225806 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[StackMaps] Allow the target to pre-process the live-out mask
Hal Finkel [Tue, 13 Jan 2015 17:47:59 +0000 (17:47 +0000)]
[StackMaps] Allow the target to pre-process the live-out mask

Some targets, PowerPC for example, have pseudo-registers (such as that used to
represent the rounding mode), that don't have DWARF register numbers or a
register class. These are used only for internal dependency tracking, and
should not appear in the recorded live-outs. This adds a callback allowing the
target to pre-process the live-out mask in order to remove these kinds of
registers so that the StackMaps code does not complain about them and/or
attempt to include them in the output.

This will be used by the PowerPC target in a future commit.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225805 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PowerPC] Split the blr definition into BLR and BLR8
Hal Finkel [Tue, 13 Jan 2015 17:47:54 +0000 (17:47 +0000)]
[PowerPC] Split the blr definition into BLR and BLR8

We really need a separate 64-bit version of this instruction so that it can be
marked as clobbering LR8 (instead of just LR). No change in functionality
(although the verifier might be slightly happier), however, it is required for
stackmap/patchpoint support. Thus, this will be covered by stackmap test cases
once those are added.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225804 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PowerPC] Add DWARF numbers for CA (XER), etc.
Hal Finkel [Tue, 13 Jan 2015 17:45:11 +0000 (17:45 +0000)]
[PowerPC] Add DWARF numbers for CA (XER), etc.

For registers that have DWARF numbers (like CA, which is really part of XER),
add them. Also, RM is not an SPR, and the declaration hack (where it is
declared as an SPR with an arbitrary number) is not needed, so just declare it
as a register.

NFC; although CA's register number will be needed when stackmap/patchpoint
support is added.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225800 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[mips][microMIPS] Fix issue with 16b instructions in jr instruction delay slot
Jozef Kolek [Tue, 13 Jan 2015 15:59:17 +0000 (15:59 +0000)]
[mips][microMIPS] Fix issue with 16b instructions in jr instruction delay slot

16 bit instructions are not allowed in jr delay slot. Same stands for
PseudoIndirectBranch and PseudoReturn.

Differential Revision: http://reviews.llvm.org/D6815

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225798 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAdded a Mips lld milestone to the release notes for the 3.6 release.
Daniel Sanders [Tue, 13 Jan 2015 15:17:00 +0000 (15:17 +0000)]
Added a Mips lld milestone to the release notes for the 3.6 release.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225797 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAdded TLI hook for isFPExtFree. Some of the FMA combine heuristics are now guarded...
Olivier Sallenave [Tue, 13 Jan 2015 15:06:36 +0000 (15:06 +0000)]
Added TLI hook for isFPExtFree. Some of the FMA combine heuristics are now guarded with that hook.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225795 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRevert "SLPVectorizer: Cache results from memory alias checking."
Erik Eckstein [Tue, 13 Jan 2015 14:36:46 +0000 (14:36 +0000)]
Revert "SLPVectorizer: Cache results from memory alias checking."

The alias cache has a problem of incorrect collisions in case a new instruction is allocated at the same address as a previously deleted instruction.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225790 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoSilence warnings about unknown pragmas for compilers that are not Clang. NFC.
Aaron Ballman [Tue, 13 Jan 2015 14:30:07 +0000 (14:30 +0000)]
Silence warnings about unknown pragmas for compilers that are not Clang. NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225788 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[OCaml] Allow out-of-tree builds of LLVM bindings.
Peter Zotov [Tue, 13 Jan 2015 12:17:56 +0000 (12:17 +0000)]
[OCaml] Allow out-of-tree builds of LLVM bindings.

In order to use this feature, configure LLVM as usual,
but then build and install it as:

   make all install SYSTEM_LLVM_CONFIG=llvm-config

where llvm-config is the llvm-config binary installed on your
system (possibly llvm-config-VERSION on e.g. Debian).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225787 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoSLPVectorizer: Cache results from memory alias checking.
Erik Eckstein [Tue, 13 Jan 2015 11:37:51 +0000 (11:37 +0000)]
SLPVectorizer: Cache results from memory alias checking.

This speeds up the dependency calculations for blocks with many load/store/call instructions.
Beside the improved runtime, there is no functional change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225786 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] In the PassManager template, remove a pointless indirection through
Chandler Carruth [Tue, 13 Jan 2015 11:36:43 +0000 (11:36 +0000)]
[PM] In the PassManager template, remove a pointless indirection through
a nested class template for the PassModel, and use the T-suffix for the
two typedefs to match the code in the AnalysisManager.

This is the last of the fairly fundamental code cleanups here. Will be
focusing on the printing of analyses next to finish that aspect off.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225785 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Remove the 'AnalysisManagerT' type parameter from numerous layers
Chandler Carruth [Tue, 13 Jan 2015 11:31:43 +0000 (11:31 +0000)]
[PM] Remove the 'AnalysisManagerT' type parameter from numerous layers
of templates in the new pass manager.

The analysis manager is now itself just a template predicated on the IR
unit. This makes lots of the templates really trivial and more clear:
they are all parameterized on a single type, the IR unit's type.
Everything else is a function of that. To me, this is a really nice
cleanup of the APIs and removes a layer of 'magic' and 'indirection'
that really wasn't there and just got in the way of understanding what
is going on here.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225784 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Refactor the new pass manager to use a single template to implement
Chandler Carruth [Tue, 13 Jan 2015 11:13:56 +0000 (11:13 +0000)]
[PM] Refactor the new pass manager to use a single template to implement
the generic functionality of the pass managers themselves.

In the new infrastructure, the pass "manager" isn't actually interesting
at all. It just pipelines a single chunk of IR through N passes. We
don't need to know anything about the IR or the passes to do this really
and we can replace the 3 implementations of the exact same functionality
with a single generic PassManager template, complementing the single
generic AnalysisManager template.

I've left typedefs in place to give convenient names to the various
obvious instantiations of the template.

With this, I think I've nuked almost all of the redundant logic in the
managers, and I think the overall design is actually simpler for having
single templates that clearly indicate there is no special logic here.
The logging is made somewhat more annoying by this change, but I don't
think the difference is worth having heavy-weight traits to help log
things.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225783 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoUpdate release notes wrt OCaml bindings.
Peter Zotov [Tue, 13 Jan 2015 09:48:02 +0000 (09:48 +0000)]
Update release notes wrt OCaml bindings.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225779 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[OCaml] Use $CAMLORIGIN, an rpath-$ORIGIN-like mechanism in OCaml.
Peter Zotov [Tue, 13 Jan 2015 09:47:59 +0000 (09:47 +0000)]
[OCaml] Use $CAMLORIGIN, an rpath-$ORIGIN-like mechanism in OCaml.

As a result, installations of LLVM in non-standard locations
will not require passing custom -ccopt -L flags when building
the binary, nor absolute paths would be embedded in the cma/cmxa
files. Additionally, the executables will not require changes
to LD_LIBRARY_PATH, although CAML_LD_LIBRARY_PATH still
has to be set for ocamlc without -custom.

See http://caml.inria.fr/mantis/view.php?id=6642.
Note that the patch is approved, but not merged yet.
It will be released in 4.03 and likely 4.02.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225778 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR/MetadataTest.cpp: Appease msc17 to avoid initializer list.
NAKAMURA Takumi [Tue, 13 Jan 2015 08:13:46 +0000 (08:13 +0000)]
IR/MetadataTest.cpp: Appease msc17 to avoid initializer list.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225775 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoPeephole opt needs optimizeSelect() to keep track of newly created MIs
Mehdi Amini [Tue, 13 Jan 2015 07:07:13 +0000 (07:07 +0000)]
Peephole opt needs optimizeSelect() to keep track of newly created MIs

Peephole optimizer is scanning a basic block forward. At some point it
needs to answer the question "given a pointer to an MI in the current
BB, is it located before or after the current instruction".
To perform this, it keeps a set of the MIs already seen during the scan,
if a MI is not in the set, it is assumed to be after.
It means that newly created MIs have to be inserted in the set as well.

This commit passes the set as an argument to the target-dependent
optimizeSelect() so that it can properly update the set with the
(potentially) newly created MIs.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225772 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agofix {typo, build failure} in r225760
Ramkumar Ramachandra [Tue, 13 Jan 2015 04:17:47 +0000 (04:17 +0000)]
fix {typo, build failure} in r225760

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225762 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoStandardize {pred,succ,use,user}_empty()
Ramkumar Ramachandra [Tue, 13 Jan 2015 03:46:47 +0000 (03:46 +0000)]
Standardize {pred,succ,use,user}_empty()

The functions {pred,succ,use,user}_{begin,end} exist, but many users
have to check *_begin() with *_end() by hand to determine if the
BasicBlock or User is empty. Fix this with a standard *_empty(),
demonstrating a few usecases.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225760 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoARM: prepare prefix parsing for improved AAELF support
Saleem Abdulrasool [Tue, 13 Jan 2015 03:22:49 +0000 (03:22 +0000)]
ARM: prepare prefix parsing for improved AAELF support

AAELF specifies a number of ELF specific relocation types which have custom
prefixes for the symbol reference.  Switch the parser to be more table driven
with an idea of file formats for which they apply.  NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225758 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Fold all three analysis managers into a single AnalysisManager
Chandler Carruth [Tue, 13 Jan 2015 02:51:47 +0000 (02:51 +0000)]
[PM] Fold all three analysis managers into a single AnalysisManager
template.

This consolidates three copies of nearly the same core logic. It adds
"complexity" to the ModuleAnalysisManager in that it makes it possible
to share a ModuleAnalysisManager across multiple modules... But it does
so by deleting *all of the code*, so I'm OK with that. This will
naturally make fixing bugs in this code much simpler, etc.

The only down side here is that we have to use 'typename' and 'this->'
in various places, and the implementation is lifted into the header.
I'll take that for the code size reduction.

The convenient names are still typedef-ed and used throughout so that
users can largely ignore this aspect of the implementation.

The follow-up change to this will do the exact same refactoring for the
PassManagers. =D

It turns out that the interesting different code is almost entirely in
the adaptors. At the end, that should be essentially all that is left.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225757 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDisable a warning for self move since the test is checking for this behavior.
Richard Trieu [Tue, 13 Jan 2015 02:10:33 +0000 (02:10 +0000)]
Disable a warning for self move since the test is checking for this behavior.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225754 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agofix typo; NFC
Sanjay Patel [Tue, 13 Jan 2015 01:51:52 +0000 (01:51 +0000)]
fix typo; NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225753 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRename llvm.recoverframeallocation to llvm.framerecover
Reid Kleckner [Tue, 13 Jan 2015 01:51:34 +0000 (01:51 +0000)]
Rename llvm.recoverframeallocation to llvm.framerecover

This name is less descriptive, but it sort of puts things in the
'llvm.frame...' namespace, relating it to frameallocate and
frameaddress. It also avoids using "allocate" and "allocation" together.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225752 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Fix another place where I was using an overly generic T&& for the
Chandler Carruth [Tue, 13 Jan 2015 01:44:56 +0000 (01:44 +0000)]
[PM] Fix another place where I was using an overly generic T&& for the
IR unit to directly use IRUnitT& for now.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225750 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Use unique_ptr, NFC
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 00:57:27 +0000 (00:57 +0000)]
IR: Use unique_ptr, NFC

Use `std::unique_ptr<>`, as suggested by David Blaikie.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225749 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoPhabricator calls it "subscriber" not "cc"
Paul Robinson [Tue, 13 Jan 2015 00:50:31 +0000 (00:50 +0000)]
Phabricator calls it "subscriber" not "cc"

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225747 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAdd the llvm.frameallocate and llvm.recoverframeallocation intrinsics
Reid Kleckner [Tue, 13 Jan 2015 00:48:10 +0000 (00:48 +0000)]
Add the llvm.frameallocate and llvm.recoverframeallocation intrinsics

These intrinsics allow multiple functions to share a single stack
allocation from one function's call frame. The function with the
allocation may only perform one allocation, and it must be in the entry
block.

Functions accessing the allocation call llvm.recoverframeallocation with
the function whose frame they are accessing and a frame pointer from an
active call frame of that function.

These intrinsics are very difficult to inline correctly, so the
intention is that they be introduced rarely, or at least very late
during EH preparation.

Reviewers: echristo, andrew.w.kaylor

Differential Revision: http://reviews.llvm.org/D6493

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225746 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Remove an invalid assertion when replacing resolved operands
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 00:46:34 +0000 (00:46 +0000)]
IR: Remove an invalid assertion when replacing resolved operands

This adds back the testcase from r225738, and adds to it.  Looks like we
need both sides for now (the assertion was incorrect both ways, and
although it seemed reasonable (when written correctly) it wasn't
particularly important).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225745 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoCombine fcmp + select to fminnum / fmaxnum if no nans and legal
Matt Arsenault [Tue, 13 Jan 2015 00:43:00 +0000 (00:43 +0000)]
Combine fcmp + select to fminnum / fmaxnum if no nans and legal

Also require unsafe FP math for no since there isn't a way to
test for signed zeros.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225744 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Re-clang-format much of this code as the code has changed some and
Chandler Carruth [Tue, 13 Jan 2015 00:36:47 +0000 (00:36 +0000)]
[PM] Re-clang-format much of this code as the code has changed some and
so has clang-format. Notably, this fixes a bunch of formatting in the
CGSCC pass manager side of things that has been improved in clang-format
recently.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225743 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRevert "IR: Fix an inverted assertion when replacing resolved operands"
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 00:34:21 +0000 (00:34 +0000)]
Revert "IR: Fix an inverted assertion when replacing resolved operands"

This reverts commit r225738.  Maybe the assertion is just plain wrong,
but this version fails on WAY more bots.  I'll make sure both ways work
in a follow-up but I want to get bots green in the meantime.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225742 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoGrammar and spelling.
Eric Christopher [Tue, 13 Jan 2015 00:21:14 +0000 (00:21 +0000)]
Grammar and spelling.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225740 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Fix an inverted assertion when replacing resolved operands
Duncan P. N. Exon Smith [Tue, 13 Jan 2015 00:10:38 +0000 (00:10 +0000)]
IR: Fix an inverted assertion when replacing resolved operands

Add a unit test, since this bug was only exposed by clang tests.  Thanks
to Rafael for tracking this down!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225738 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRelease merge script: don't actually commit the merge
Hans Wennborg [Tue, 13 Jan 2015 00:07:31 +0000 (00:07 +0000)]
Release merge script: don't actually commit the merge

Instead, just present the command for committing it. This way,
the user can test the merge locally, resolve conflicts, etc.
before committing, which seems much safer to me.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225737 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRelease tag script: add -revision option
Hans Wennborg [Tue, 13 Jan 2015 00:07:29 +0000 (00:07 +0000)]
Release tag script: add -revision option

It seems useful to be able to create the branch at a revision that looks good
on the buildbots.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225736 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRelease tag script: add -dry-run flag
Hans Wennborg [Tue, 13 Jan 2015 00:07:22 +0000 (00:07 +0000)]
Release tag script: add -dry-run flag

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225735 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Move support for constants into DwarfExpression.
Adrian Prantl [Tue, 13 Jan 2015 00:04:06 +0000 (00:04 +0000)]
Debug Info: Move support for constants into DwarfExpression.
Move the declaration of DebugLocDwarfExpression into DwarfExpression.h
because it needs to be accessed from AsmPrinterDwarf.cpp and DwarfDebug.cpp

NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225734 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Split out writeMDTuple(), NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 23:45:31 +0000 (23:45 +0000)]
IR: Split out writeMDTuple(), NFC

Prepare for more subclasses of `UniquableMDNode` than `MDTuple`.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225732 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoMake DwarfExpression store the AsmPrinter instead of the TargetMachine.
Adrian Prantl [Mon, 12 Jan 2015 23:36:56 +0000 (23:36 +0000)]
Make DwarfExpression store the AsmPrinter instead of the TargetMachine.
NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225731 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoremove extra semicolon
Adrian Prantl [Mon, 12 Jan 2015 23:36:50 +0000 (23:36 +0000)]
remove extra semicolon

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225730 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agomusttail: Only set the inreg flag for fastcall and vectorcall
Reid Kleckner [Mon, 12 Jan 2015 23:28:23 +0000 (23:28 +0000)]
musttail: Only set the inreg flag for fastcall and vectorcall

Otherwise we'll attempt to forward ECX, EDX, and EAX for cdecl and
stdcall thunks, leaving us with no scratch registers for indirect call
targets.

Fixes PR22052.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225729 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoR600/SI: Remove redundant setting expand on f64 vectors
Matt Arsenault [Mon, 12 Jan 2015 23:13:00 +0000 (23:13 +0000)]
R600/SI: Remove redundant setting expand on f64 vectors

None of these are legal types already, so they default to
Expand.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225728 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Unbreak the MSVC build after r225689
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 23:09:14 +0000 (23:09 +0000)]
IR: Unbreak the MSVC build after r225689

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225727 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoRun clang-format on the parts of AsmPrinterDwarf where it improves the
Adrian Prantl [Mon, 12 Jan 2015 23:03:23 +0000 (23:03 +0000)]
Run clang-format on the parts of AsmPrinterDwarf where it improves the
readability.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225726 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Add a virtual destructor to DwarfExpression.
Adrian Prantl [Mon, 12 Jan 2015 22:59:28 +0000 (22:59 +0000)]
Debug Info: Add a virtual destructor to DwarfExpression.
Thanks Chandler for noticing!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225724 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[PM] Sink the reference vs. value decision for IR units out of the
Chandler Carruth [Mon, 12 Jan 2015 22:53:31 +0000 (22:53 +0000)]
[PM] Sink the reference vs. value decision for IR units out of the
templated interface.

So far, every single IR unit I can come up with has address-identity.
That is, when two units of IR are both active in LLVM, their addresses
will be distinct of the IR is distinct. This is clearly true for
Modules, Functions, BasicBlocks, and Instructions. It turns out that the
only practical way to make the CGSCC stuff work the way we want is to
make it true for SCCs as well. I expect this pattern to continue.

When first designing the pass manager code, I kept this dimension of
freedom in the type parameters, essentially allowing for a wrapper-type
whose address did not form identity. But that really no longer makes
sense and is making the code more complex or subtle for no gain. If we
ever have an actual use case for this, we can figure out what makes
sense then and there. It will be better because then we will have the
actual example in hand.

While the simplifications afforded in this patch are fairly small
(mostly sinking the '&' out of many type parameters onto a few
interfaces), it would have become much more pronounced with subsequent
changes. I have a sequence of changes that will completely remove the
code duplication that currently exists between all of the pass managers
and analysis managers. =] Should make things much cleaner and avoid bug
fixing N times for the N pass managers.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225723 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Remove incorrect comment, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:53:18 +0000 (22:53 +0000)]
IR: Remove incorrect comment, NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225722 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Fix unit test memory leak reported by ASan
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:46:15 +0000 (22:46 +0000)]
IR: Fix unit test memory leak reported by ASan

http://lab.llvm.org:8011/builders/sanitizer-x86_64-linux-fast/builds/603/steps/check-llvm%20asan/logs/stdio

Thanks Alexey for pointing me to this!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225721 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoUntwine this expression. Thanks to David for noticing!
Adrian Prantl [Mon, 12 Jan 2015 22:39:14 +0000 (22:39 +0000)]
Untwine this expression. Thanks to David for noticing!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225720 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago[X86][SSE] Minor regression fix for r225551
Simon Pilgrim [Mon, 12 Jan 2015 22:38:08 +0000 (22:38 +0000)]
[X86][SSE] Minor regression fix for r225551

r225551 vector byte shuffle optimization caused an assertion as fully zeroable vectors can be produced under certain circumstances. This fix drops the assert and returns a zero vector where the assert would have failed.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225718 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Implement DwarfUnit::addRegisterOpPiece() using DwarfExpression.
Adrian Prantl [Mon, 12 Jan 2015 22:37:16 +0000 (22:37 +0000)]
Debug Info: Implement DwarfUnit::addRegisterOpPiece() using DwarfExpression.
NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225717 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoBitcode: Range-based for, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:35:34 +0000 (22:35 +0000)]
Bitcode: Range-based for, NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225716 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoBitcode: Add abbreviation for METADATA_NAME
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:34:10 +0000 (22:34 +0000)]
Bitcode: Add abbreviation for METADATA_NAME

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225715 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoBitcode: Range-based for, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:33:00 +0000 (22:33 +0000)]
Bitcode: Range-based for, NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225714 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoBitcode: Range-based for, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:31:35 +0000 (22:31 +0000)]
Bitcode: Range-based for, NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225713 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoBitcode: Simplify emission of METADATA_BLOCK
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:30:34 +0000 (22:30 +0000)]
Bitcode: Simplify emission of METADATA_BLOCK

Refactor logic so that we know up-front whether to open a block and
whether we need an MDString abbreviation.

This is almost NFC, but will start emitting `MDString` abbreviations
when the first record is not an `MDString`.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225712 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Use subclass API instead of MDNode wrappers, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:27:39 +0000 (22:27 +0000)]
AsmParser: Use subclass API instead of MDNode wrappers, NFC

Use subclass API instead of the wrappers in `MDNode` in the assembly
parser.  This will make the code easier to follow once we have multiple
subclasses.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225711 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Factor duplicated code into ParseMDNode(), NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:26:48 +0000 (22:26 +0000)]
AsmParser: Factor duplicated code into ParseMDNode(), NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225710 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Reorder ParseMetadata() logic, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:24:50 +0000 (22:24 +0000)]
AsmParser: Reorder ParseMetadata() logic, NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225709 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Simplify ParseMDTuple(), NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 22:23:04 +0000 (22:23 +0000)]
AsmParser: Simplify ParseMDTuple(), NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225708 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug Info: Implement DwarfUnit::addRegisterOffset using DwarfExpression.
Adrian Prantl [Mon, 12 Jan 2015 22:19:26 +0000 (22:19 +0000)]
Debug Info: Implement DwarfUnit::addRegisterOffset using DwarfExpression.
No functional change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225707 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoDebug info: Factor out the creation of DWARF expressions from AsmPrinter
Adrian Prantl [Mon, 12 Jan 2015 22:19:22 +0000 (22:19 +0000)]
Debug info: Factor out the creation of DWARF expressions from AsmPrinter
into a new class DwarfExpression that can be shared between AsmPrinter
and DwarfUnit.

This is the first step towards unifying the two entirely redundant
implementations of dwarf expression emission in DwarfUnit and AsmPrinter.

Almost no functional change — Testcases were updated because asm comments
that used to be on two lines now appear on the same line, which is
actually preferable.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225706 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: ParseMDNode() => ParseMDTuple(), NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 21:23:11 +0000 (21:23 +0000)]
AsmParser: ParseMDNode() => ParseMDTuple(), NFC

This isn't parsing arbitrary subclasses of `MDNode`, just `MDTuple`.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225702 91177308-0d34-0410-b5e6-96231b3b80d8

6 years ago80-cols; NFC
Sanjay Patel [Mon, 12 Jan 2015 21:21:28 +0000 (21:21 +0000)]
80-cols; NFC

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225700 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Remove unused version of ParseMDNodeID()
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 21:14:38 +0000 (21:14 +0000)]
AsmParser: Remove unused version of ParseMDNodeID()

Merge the two versions of `ParseMDNodeID()` now that no one needs
special forward references.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225699 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoAsmParser: Use normal references for metadata attachments, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 21:13:09 +0000 (21:13 +0000)]
AsmParser: Use normal references for metadata attachments, NFC

Remove special parsing logic for metadata attachments.  Now that
`DebugLoc` is stored normally (since the metadata/value split), we don't
need this special forward referencing logic.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225698 91177308-0d34-0410-b5e6-96231b3b80d8

6 years agoIR: Prepare for a new UniquableMDNode subclass, NFC
Duncan P. N. Exon Smith [Mon, 12 Jan 2015 20:56:33 +0000 (20:56 +0000)]
IR: Prepare for a new UniquableMDNode subclass, NFC

Add generic dispatch for the parts of `UniquableMDNode` that cast to
`MDTuple`.  This makes adding other subclasses (like PR21433's
`MDLocation`) easier.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@225697 91177308-0d34-0410-b5e6-96231b3b80d8