Reflow this comment.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215160 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215160 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Fix overwriting/loss of inlined arguments to recursively inlined functions.
Due to an unnecessary special case, inlined arguments that happened to
be from the same function as they were inlined into were misclassified
as non-inline arguments and would overwrite the non-inlined arguments.
Assert that we never overwrite a function's arguments, and stop
misclassifying inlined arguments as non-inline arguments to fix this
issue.
Excuse the rather crappy test case - handcrafted IR might do better, or
someone who understands better how to tickle the inliner to create a
recursive inlining situation like this (though it may also be necessary
to tickle the variable in a particular way to cause it to be recorded in
the MMI side table and go down this particular path for location
information).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215157 91177308-0d34-0410-b5e6-96231b3b80d8
Due to an unnecessary special case, inlined arguments that happened to
be from the same function as they were inlined into were misclassified
as non-inline arguments and would overwrite the non-inlined arguments.
Assert that we never overwrite a function's arguments, and stop
misclassifying inlined arguments as non-inline arguments to fix this
issue.
Excuse the rather crappy test case - handcrafted IR might do better, or
someone who understands better how to tickle the inliner to create a
recursive inlining situation like this (though it may also be necessary
to tickle the variable in a particular way to cause it to be recorded in
the MMI side table and go down this particular path for location
information).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215157 91177308-0d34-0410-b5e6-96231b3b80d8
fix materialization of one bit constants and global values which are accessed through
a base GOT entry.
Summary:
get tip of tree mips fast-isel to pass test-suite
Two bugs were fixed:
1) one bit booleans were treated as 1 bit signed integers and so the literal '1' could become sign extended.
2) mips uses got for pic but in certain cases, as with string constants for example, many items can be referenced from the same got entry and this case was not handled properly.
Test Plan: test-suite
Reviewers: dsanders
Reviewed By: dsanders
Subscribers: mcrosier
Differential Revision: http://reviews.llvm.org/D4801
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215155 91177308-0d34-0410-b5e6-96231b3b80d8
a base GOT entry.
Summary:
get tip of tree mips fast-isel to pass test-suite
Two bugs were fixed:
1) one bit booleans were treated as 1 bit signed integers and so the literal '1' could become sign extended.
2) mips uses got for pic but in certain cases, as with string constants for example, many items can be referenced from the same got entry and this case was not handled properly.
Test Plan: test-suite
Reviewers: dsanders
Reviewed By: dsanders
Subscribers: mcrosier
Differential Revision: http://reviews.llvm.org/D4801
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215155 91177308-0d34-0410-b5e6-96231b3b80d8
Temporarily Revert "Nuke the old JIT." as it's not quite ready to
be deleted. This will be reapplied as soon as possible and before
the 3.6 branch date at any rate.
Approved by Jim Grosbach, Lang Hames, Rafael Espindola.
This reverts commits r215111, 215115, 215116, 215117, 215136.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215154 91177308-0d34-0410-b5e6-96231b3b80d8
be deleted. This will be reapplied as soon as possible and before
the 3.6 branch date at any rate.
Approved by Jim Grosbach, Lang Hames, Rafael Espindola.
This reverts commits r215111, 215115, 215116, 215117, 215136.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215154 91177308-0d34-0410-b5e6-96231b3b80d8
Debugging Utility - optional ability for dumping critical path length
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215153 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215153 91177308-0d34-0410-b5e6-96231b3b80d8
MachineCombiner Pass for selecting faster instruction sequence on AArch64
Re-commit of r214832,r21469 with a work-around that
avoids the previous problem with gcc build compilers
The work-around is to use SmallVector instead of ArrayRef
of basic blocks in preservesResourceLen()/MachineCombiner.cpp
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215151 91177308-0d34-0410-b5e6-96231b3b80d8
Re-commit of r214832,r21469 with a work-around that
avoids the previous problem with gcc build compilers
The work-around is to use SmallVector instead of ArrayRef
of basic blocks in preservesResourceLen()/MachineCombiner.cpp
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215151 91177308-0d34-0410-b5e6-96231b3b80d8
Add two missing ARM cpusubtypes to the switch statement in
MachOObjectFile::getArch(uint32_t CPUType, uint32_t CPUSubType) .
Upcoming changes will cause existing test cases to use this but
I wanted to check in this obvious change separately.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215150 91177308-0d34-0410-b5e6-96231b3b80d8
MachOObjectFile::getArch(uint32_t CPUType, uint32_t CPUSubType) .
Upcoming changes will cause existing test cases to use this but
I wanted to check in this obvious change separately.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215150 91177308-0d34-0410-b5e6-96231b3b80d8
Fix a case in SROA where lifetime intrinsics could inhibit alloca promotion. In
this case, the code path dealing with vector promotion was missing the explicit
checks for lifetime intrinsics that were present on the corresponding integer
promotion path.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215148 91177308-0d34-0410-b5e6-96231b3b80d8
this case, the code path dealing with vector promotion was missing the explicit
checks for lifetime intrinsics that were present on the corresponding integer
promotion path.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215148 91177308-0d34-0410-b5e6-96231b3b80d8
[MCJIT] Replace a c-style cast with reinterpret_cast + static_cast.
C-style casts (and reinterpret_casts) result in implementation defined
values when a pointer is cast to a larger integer type. On some platforms
this was leading to bogus address computations in RuntimeDyldMachOAArch64.
This should fix http://llvm.org/PR20501.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215143 91177308-0d34-0410-b5e6-96231b3b80d8
C-style casts (and reinterpret_casts) result in implementation defined
values when a pointer is cast to a larger integer type. On some platforms
this was leading to bogus address computations in RuntimeDyldMachOAArch64.
This should fix http://llvm.org/PR20501.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215143 91177308-0d34-0410-b5e6-96231b3b80d8
Remove Support/IncludeFile.h and its only user. This is actively harmful, since
it breaks the modules builds (where CallGraph.h can be quite reasonably
transitively included by an unimported portion of a module, and CallGraph.cpp
not linked in), and appears to have been entirely redundant since PR780 was
fixed back in 2008.
If this breaks anything, please revert; I have only tested this with a single
configuration, and it's possible that this is still somehow fixing something
(though I doubt it, since no other similar file uses this mechanism any more).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215142 91177308-0d34-0410-b5e6-96231b3b80d8
it breaks the modules builds (where CallGraph.h can be quite reasonably
transitively included by an unimported portion of a module, and CallGraph.cpp
not linked in), and appears to have been entirely redundant since PR780 was
fixed back in 2008.
If this breaks anything, please revert; I have only tested this with a single
configuration, and it's possible that this is still somehow fixing something
(though I doubt it, since no other similar file uses this mechanism any more).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215142 91177308-0d34-0410-b5e6-96231b3b80d8
Fix test failure on ARM.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215140 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215140 91177308-0d34-0410-b5e6-96231b3b80d8
[modules] Update module map workaround to cope with the problematic file having
been relocated.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215139 91177308-0d34-0410-b5e6-96231b3b80d8
been relocated.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215139 91177308-0d34-0410-b5e6-96231b3b80d8
test commit: remove trailing whitespace.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215138 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215138 91177308-0d34-0410-b5e6-96231b3b80d8
Remove a few XFAILs.
These tests now pass with MCJIT.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215136 91177308-0d34-0410-b5e6-96231b3b80d8
These tests now pass with MCJIT.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215136 91177308-0d34-0410-b5e6-96231b3b80d8
[Branch probability] Recompute branch weights of tail-merged basic blocks.
BranchFolderPass was not correctly setting the basic block branch weights when
tail-merging created or merged blocks. This patch recomutes the weights of
tail-merged blocks using the following formula:
branch_weight(merged block to successor j) =
sum(block_frequency(bb) * branch_probability(bb -> j))
bb is a block that is in the set of merged blocks.
<rdar://problem/16256423>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215135 91177308-0d34-0410-b5e6-96231b3b80d8
BranchFolderPass was not correctly setting the basic block branch weights when
tail-merging created or merged blocks. This patch recomutes the weights of
tail-merged blocks using the following formula:
branch_weight(merged block to successor j) =
sum(block_frequency(bb) * branch_probability(bb -> j))
bb is a block that is in the set of merged blocks.
<rdar://problem/16256423>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215135 91177308-0d34-0410-b5e6-96231b3b80d8
Add the majority of the remaining SPE instructions.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215131 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215131 91177308-0d34-0410-b5e6-96231b3b80d8
FileCheck: Add a flag to allow checking empty input
Currently FileCheck errors out on empty input. This is usually the
right thing to do, but makes testing things like "this command does
not emit some error message" hard to test. This usually leads to
people using "command 2>&1 | count 0" instead, and then the bots that
use guard malloc fail a few hours later.
By adding a flag to FileCheck that allows empty inputs, we can make
tests that consist entirely of "CHECK-NOT" lines feasible.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215127 91177308-0d34-0410-b5e6-96231b3b80d8
Currently FileCheck errors out on empty input. This is usually the
right thing to do, but makes testing things like "this command does
not emit some error message" hard to test. This usually leads to
people using "command 2>&1 | count 0" instead, and then the bots that
use guard malloc fail a few hours later.
By adding a flag to FileCheck that allows empty inputs, we can make
tests that consist entirely of "CHECK-NOT" lines feasible.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215127 91177308-0d34-0410-b5e6-96231b3b80d8
Indent
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215126 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215126 91177308-0d34-0410-b5e6-96231b3b80d8
[AVX512] Generate masking instruction variants with tablegen
After adding the masking variants to several instructions, I have decided to
experiment with generating these from the non-masking/unconditional
variant. This will hopefully reduce the amount repetition that we currently
have in order to define an instruction with all its variants (for a reg/mem
instruction this would be 6 instruction defs and 2 Pat<> for the intrinsic).
The patch is the first cut that is currently only applied to valignd/q to make
the patch small.
A few notes on the approach:
* In order to stitch together the dag for both the conditional and the
unconditional patterns I pass the RHS of the set rather than the full
pattern (set dest, RHS).
* Rather than subclassing each instruction base class (e.g. AVX512AIi8),
with a masking variant which wouldn't scale, I derived the masking
instructions from a new base class AVX512 (this is just I<> with
Requires<HasAVX512>). The instructions derive from this now, plus a new set
of classes that add the format bits and everything else that instruction
base class provided (i.e. AVX512AIi8 vs. AVX512AIi8Base).
I hope we can go incrementally from here. I expect that:
* We will need different variants of the masking class. One example is
instructions requiring three vector sources. In this case we tie one of the
source operands to dest rather than a new implicit source operand ($src0)
* Add the zero-masking variant
* Add more AVX512*Base classes as new uses are added
I've looked at X86.td.expanded before and after to make sure that nothing got
lost for valignd/q.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215125 91177308-0d34-0410-b5e6-96231b3b80d8
After adding the masking variants to several instructions, I have decided to
experiment with generating these from the non-masking/unconditional
variant. This will hopefully reduce the amount repetition that we currently
have in order to define an instruction with all its variants (for a reg/mem
instruction this would be 6 instruction defs and 2 Pat<> for the intrinsic).
The patch is the first cut that is currently only applied to valignd/q to make
the patch small.
A few notes on the approach:
* In order to stitch together the dag for both the conditional and the
unconditional patterns I pass the RHS of the set rather than the full
pattern (set dest, RHS).
* Rather than subclassing each instruction base class (e.g. AVX512AIi8),
with a masking variant which wouldn't scale, I derived the masking
instructions from a new base class AVX512 (this is just I<> with
Requires<HasAVX512>). The instructions derive from this now, plus a new set
of classes that add the format bits and everything else that instruction
base class provided (i.e. AVX512AIi8 vs. AVX512AIi8Base).
I hope we can go incrementally from here. I expect that:
* We will need different variants of the masking class. One example is
instructions requiring three vector sources. In this case we tie one of the
source operands to dest rather than a new implicit source operand ($src0)
* Add the zero-masking variant
* Add more AVX512*Base classes as new uses are added
I've looked at X86.td.expanded before and after to make sure that nothing got
lost for valignd/q.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215125 91177308-0d34-0410-b5e6-96231b3b80d8
llvm/test/tools/llvm-objdump: Reorganize target-dependent some tests.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215122 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215122 91177308-0d34-0410-b5e6-96231b3b80d8
Fix the ocaml bindings.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215117 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215117 91177308-0d34-0410-b5e6-96231b3b80d8
fix configure+make build
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215116 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215116 91177308-0d34-0410-b5e6-96231b3b80d8
Remove empty directories.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215115 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215115 91177308-0d34-0410-b5e6-96231b3b80d8
Nuke the old JIT.
I am sure we will be finding bits and pieces of dead code for years to
come, but this is a good start.
Thanks to Lang Hames for making MCJIT a good replacement!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215111 91177308-0d34-0410-b5e6-96231b3b80d8
I am sure we will be finding bits and pieces of dead code for years to
come, but this is a good start.
Thanks to Lang Hames for making MCJIT a good replacement!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215111 91177308-0d34-0410-b5e6-96231b3b80d8
Add mfasr and mtasr
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215110 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215110 91177308-0d34-0410-b5e6-96231b3b80d8
Add mfrtcu and mfrtcl instructions
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215109 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215109 91177308-0d34-0410-b5e6-96231b3b80d8
Support mttbl and mttbu mnemonic
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215108 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215108 91177308-0d34-0410-b5e6-96231b3b80d8
Add RFID instruction.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215105 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215105 91177308-0d34-0410-b5e6-96231b3b80d8
Fix Itineray class of rfi
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215104 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215104 91177308-0d34-0410-b5e6-96231b3b80d8
Spell e500 feature in lower case.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215103 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215103 91177308-0d34-0410-b5e6-96231b3b80d8
Add first bunch of SPE instructions. As they overlap with Altivec, mark
them as parser-only until the disassembler is extended to handle
predicates properly.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215102 91177308-0d34-0410-b5e6-96231b3b80d8
them as parser-only until the disassembler is extended to handle
predicates properly.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215102 91177308-0d34-0410-b5e6-96231b3b80d8
Insert parens to avoid a warning:
suggest parentheses around arithmetic in operand of '^' [-Wparentheses]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215101 91177308-0d34-0410-b5e6-96231b3b80d8
suggest parentheses around arithmetic in operand of '^' [-Wparentheses]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215101 91177308-0d34-0410-b5e6-96231b3b80d8
Silencing an MSVC C4334 warning ('<<' : result of 32-bit shift implicitly converted to 64 bits (was 64-bit shift intended?)). No functional changes intended.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215100 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215100 91177308-0d34-0410-b5e6-96231b3b80d8
[mips] Add assembler support for .set msa/nomsa directive.
Summary:
These directives are used to toggle whether the assembler accepts MSA-specific instructions or not.
Patch by Matheus Almeida and Toma Tabacu.
Reviewers: dsanders
Reviewed By: dsanders
Differential Revision: http://reviews.llvm.org/D4783
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215099 91177308-0d34-0410-b5e6-96231b3b80d8
Summary:
These directives are used to toggle whether the assembler accepts MSA-specific instructions or not.
Patch by Matheus Almeida and Toma Tabacu.
Reviewers: dsanders
Reviewed By: dsanders
Differential Revision: http://reviews.llvm.org/D4783
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215099 91177308-0d34-0410-b5e6-96231b3b80d8
Fix lld-x86_64-win7 Build #11969
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215097 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215097 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix another miscompile found through fuzz testing the new vector
shuffle lowering.
This is closely related to the previous one. Here we failed to use the
source offset when swapping in the other case -- where we end up
swapping the *final* shuffle. The cause of this bug is a bit different:
I simply wasn't thinking about the fact that this mask is actually
a slice of a wide mask and thus has numbers that need SourceOffset
applied. Simple fix. Would be even more simple with an algorithm-y thing
to use here, but correctness first. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215095 91177308-0d34-0410-b5e6-96231b3b80d8
shuffle lowering.
This is closely related to the previous one. Here we failed to use the
source offset when swapping in the other case -- where we end up
swapping the *final* shuffle. The cause of this bug is a bit different:
I simply wasn't thinking about the fact that this mask is actually
a slice of a wide mask and thus has numbers that need SourceOffset
applied. Simple fix. Would be even more simple with an algorithm-y thing
to use here, but correctness first. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215095 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix another miscompile in the new vector shuffle lowering found
via the fuzz tester.
Here I missed an offset when round-tripping a value through a shuffle
mask. I got it right 2 lines below. See a problem? I do. ;] I'll
probably be adding a little "swap" algorithm which accepts a range and
two values and swaps those values where they occur in the range. Don't
really have a name for it, let me know if you do.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215094 91177308-0d34-0410-b5e6-96231b3b80d8
via the fuzz tester.
Here I missed an offset when round-tripping a value through a shuffle
mask. I got it right 2 lines below. See a problem? I do. ;] I'll
probably be adding a little "swap" algorithm which accepts a range and
two values and swaps those values where they occur in the range. Don't
really have a name for it, let me know if you do.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215094 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix another miscompile in the new vector shuffle lowering found
through the new fuzzer.
This one is great: bad operator precedence led the modulus to happen at
the wrong point. All the asserts didn't fire because there were usually
the right values past the end of the 4 element region we were looking
at. Probably could have gotten a crash here with ASan + fuzzing, but the
correctness tests pinpointed this really nicely.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215092 91177308-0d34-0410-b5e6-96231b3b80d8
through the new fuzzer.
This one is great: bad operator precedence led the modulus to happen at
the wrong point. All the asserts didn't fire because there were usually
the right values past the end of the 4 element region we were looking
at. Probably could have gotten a crash here with ASan + fuzzing, but the
correctness tests pinpointed this really nicely.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215092 91177308-0d34-0410-b5e6-96231b3b80d8
[x32] Use ebp/esp as frame and stack pointer
Summary:
Since pointers are 32-bit on x32 we can use ebp and esp as frame and stack
pointer. Some operations like PUSH/POP and CFI_INSTRUCTION still
require 64-bit register, so using 64-bit MachineFramePtr where required.
X86_64 NaCl uses 64-bit frame/stack pointers, however it's been found that
both isTarget64BitLP64 and isTarget64BitILP32 are true for NaCl. Addressing
this issue here as well by making isTarget64BitLP64 false.
Also mark hasReservedSpillSlot unreachable on X86. See inlined comments.
Test Plan: Add one new simple test and upgrade 2 existing with x32 target case.
Reviewers: nadav, dschuff
Subscribers: llvm-commits, zinovy.nis
Differential Revision: http://reviews.llvm.org/D4617
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215091 91177308-0d34-0410-b5e6-96231b3b80d8
Summary:
Since pointers are 32-bit on x32 we can use ebp and esp as frame and stack
pointer. Some operations like PUSH/POP and CFI_INSTRUCTION still
require 64-bit register, so using 64-bit MachineFramePtr where required.
X86_64 NaCl uses 64-bit frame/stack pointers, however it's been found that
both isTarget64BitLP64 and isTarget64BitILP32 are true for NaCl. Addressing
this issue here as well by making isTarget64BitLP64 false.
Also mark hasReservedSpillSlot unreachable on X86. See inlined comments.
Test Plan: Add one new simple test and upgrade 2 existing with x32 target case.
Reviewers: nadav, dschuff
Subscribers: llvm-commits, zinovy.nis
Differential Revision: http://reviews.llvm.org/D4617
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215091 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix a miscompile in the new shuffle lowering found through the new
fuzz testing.
The function which tested for adjacency did what it said on the tin, but
when I called it, I wanted it to do something more thorough: I wanted to
know if the *pairs* of shuffle elements were adjacent and started at
0 mod 2. In one place I had the decency to try to test for this, but in
the other it was completely skipped, miscompiling this test case. Fix
this by making the helper actually do what I wanted it to do everywhere
I called it (and removing the now redundant code in one place).
I *really* dislike the name "canWidenShuffleElements" for this
predicate. If anyone can come up with a better name, please let me know.
The other name I thought about was "canWidenShuffleMask" but is it
really widening the mask to reduce the number of lanes shuffled? I don't
know. Naming things is hard.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215089 91177308-0d34-0410-b5e6-96231b3b80d8
fuzz testing.
The function which tested for adjacency did what it said on the tin, but
when I called it, I wanted it to do something more thorough: I wanted to
know if the *pairs* of shuffle elements were adjacent and started at
0 mod 2. In one place I had the decency to try to test for this, but in
the other it was completely skipped, miscompiling this test case. Fix
this by making the helper actually do what I wanted it to do everywhere
I called it (and removing the now redundant code in one place).
I *really* dislike the name "canWidenShuffleElements" for this
predicate. If anyone can come up with a better name, please let me know.
The other name I thought about was "canWidenShuffleMask" but is it
really widening the mask to reduce the number of lanes shuffled? I don't
know. Naming things is hard.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215089 91177308-0d34-0410-b5e6-96231b3b80d8
Update Tablegen documents given that binary literals are now sized
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215088 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215088 91177308-0d34-0410-b5e6-96231b3b80d8
Update BitRecTy::convertValue to allow if expressions with bit values on both sides of the if
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215087 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215087 91177308-0d34-0410-b5e6-96231b3b80d8
Change the { } expression in tablegen to accept sized binary literals which are not just 0 and 1.
It also allows nested { } expressions, as now that they are sized, we can merge pull bits from the nested value.
In the current behaviour, everything in { } must have been convertible to a single bit.
However, now that binary literals are sized, its useful to be able to initialize a range of bits.
So, for example, its now possible to do
bits<8> x = { 0, 1, { 0b1001 }, 0, 0b0 }
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215086 91177308-0d34-0410-b5e6-96231b3b80d8
It also allows nested { } expressions, as now that they are sized, we can merge pull bits from the nested value.
In the current behaviour, everything in { } must have been convertible to a single bit.
However, now that binary literals are sized, its useful to be able to initialize a range of bits.
So, for example, its now possible to do
bits<8> x = { 0, 1, { 0b1001 }, 0, 0b0 }
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215086 91177308-0d34-0410-b5e6-96231b3b80d8
Change BitsInit to inherit from TypedInit.
This is useful in a later patch where binary literals such as 0b000 will become BitsInit values instead of IntInit values.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215085 91177308-0d34-0410-b5e6-96231b3b80d8
This is useful in a later patch where binary literals such as 0b000 will become BitsInit values instead of IntInit values.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215085 91177308-0d34-0410-b5e6-96231b3b80d8
Change TableGen so that binary literals such as 0b001 are now sized.
Instead of these becoming an integer literal internally, they now become bits<n> values.
Prior to this change, 0b001 was 1 bit long. This is confusing as clearly the user gave 3 bits.
This new type holds both the literal value and the size, and so can ensure sizes match on initializers.
For example, this used to be legal
bits<1> x = 0b00;
but now it must be written as
bits<2> x = 0b00;
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215084 91177308-0d34-0410-b5e6-96231b3b80d8
Instead of these becoming an integer literal internally, they now become bits<n> values.
Prior to this change, 0b001 was 1 bit long. This is confusing as clearly the user gave 3 bits.
This new type holds both the literal value and the size, and so can ensure sizes match on initializers.
For example, this used to be legal
bits<1> x = 0b00;
but now it must be written as
bits<2> x = 0b00;
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215084 91177308-0d34-0410-b5e6-96231b3b80d8
TableGen: Change { } to only accept bits<n> entries when n == 1.
Prior to this change, it was legal to do something like
bits<2> opc = { 0, 1 };
bits<2> opc2 = { 1, 0 };
bits<2> a = { opc, opc2 };
This involved silently dropping bits from opc and opc2 which is very hard to debug.
Now the above test would be an error. Having tested with an assert, none of LLVM/clang was relying on this behaviour.
Thanks to Adam Nemet for the above test.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215083 91177308-0d34-0410-b5e6-96231b3b80d8
Prior to this change, it was legal to do something like
bits<2> opc = { 0, 1 };
bits<2> opc2 = { 1, 0 };
bits<2> a = { opc, opc2 };
This involved silently dropping bits from opc and opc2 which is very hard to debug.
Now the above test would be an error. Having tested with an assert, none of LLVM/clang was relying on this behaviour.
Thanks to Adam Nemet for the above test.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215083 91177308-0d34-0410-b5e6-96231b3b80d8
Fix a whole bunch of binary literals which were the wrong size. All were being silently zero extended to the correct width.
The commit after this changes { } and 0bxx literals to be of type bits<n> and not int. This means we need to write exactly the right number of bits, and not rely on the values being silently zero extended for us.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215082 91177308-0d34-0410-b5e6-96231b3b80d8
The commit after this changes { } and 0bxx literals to be of type bits<n> and not int. This means we need to write exactly the right number of bits, and not rely on the values being silently zero extended for us.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215082 91177308-0d34-0410-b5e6-96231b3b80d8
Add an option to the shuffle fuzzer that lets you fuzz exclusively
within a single bit-width of vectors. This is particularly useful for
when you know you have bugs in a certain area and want to find simpler
test cases than those produced by an open-ended fuzzing that ends up
legalizing the vector in addition to shuffling it.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215056 91177308-0d34-0410-b5e6-96231b3b80d8
within a single bit-width of vectors. This is particularly useful for
when you know you have bugs in a certain area and want to find simpler
test cases than those produced by an open-ended fuzzing that ends up
legalizing the vector in addition to shuffling it.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215056 91177308-0d34-0410-b5e6-96231b3b80d8
Use the minor number for the revision numbers.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215055 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215055 91177308-0d34-0410-b5e6-96231b3b80d8
Add a vector shuffle fuzzer.
This is a python script which for a given seed generates a random
sequence of random shuffles of a random vector width. It embeds this
into a function and emits a main function which calls the test routine
and checks that the results (where defined) match the obvious results.
I'll be using this to drive out miscompiles from the new vector shuffle
logic now that it is clean of any crashes I can find with llvm-stress.
Note, my python skills are very poor. Sorry if this is terrible code,
and feel free to tell me how I should write this or just patch it as
necessary.
The tests generated try to be very portable and use boring C routines.
It technically will mis-declare the C routines and pass 32-bit integers
to parametrs that expect 64-bit integers. If someone wants to fix this
and has less terrible ideas of how to do it, I'm all ears. Fortunately,
this "just works" for x86. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215054 91177308-0d34-0410-b5e6-96231b3b80d8
This is a python script which for a given seed generates a random
sequence of random shuffles of a random vector width. It embeds this
into a function and emits a main function which calls the test routine
and checks that the results (where defined) match the obvious results.
I'll be using this to drive out miscompiles from the new vector shuffle
logic now that it is clean of any crashes I can find with llvm-stress.
Note, my python skills are very poor. Sorry if this is terrible code,
and feel free to tell me how I should write this or just patch it as
necessary.
The tests generated try to be very portable and use boring C routines.
It technically will mis-declare the C routines and pass 32-bit integers
to parametrs that expect 64-bit integers. If someone wants to fix this
and has less terrible ideas of how to do it, I'm all ears. Fortunately,
this "just works" for x86. =]
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215054 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Make a test more portable
mach-o doesn't like sections without segments, and elf is perfectly
happy with commas in section names, so use a Darwin-like section name.
Suggestion by Eric Christopher.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215052 91177308-0d34-0410-b5e6-96231b3b80d8
mach-o doesn't like sections without segments, and elf is perfectly
happy with commas in section names, so use a Darwin-like section name.
Suggestion by Eric Christopher.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215052 91177308-0d34-0410-b5e6-96231b3b80d8
MC: split Win64EHUnwindEmitter into a shared streamer
This changes Win64EHEmitter into a utility WinEH UnwindEmitter that can be
shared across multiple architectures and a target specific bit which is
overridden (Win64::UnwindEmitter). This enables sharing the section selection
code across X86 and the intended use in ARM for emitting unwind information for
Windows on ARM.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215050 91177308-0d34-0410-b5e6-96231b3b80d8
This changes Win64EHEmitter into a utility WinEH UnwindEmitter that can be
shared across multiple architectures and a target specific bit which is
overridden (Win64::UnwindEmitter). This enables sharing the section selection
code across X86 and the intended use in ARM for emitting unwind information for
Windows on ARM.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215050 91177308-0d34-0410-b5e6-96231b3b80d8
[X86][SchedModel] Fixed missing/wrong scheduling model found by code inspection.
Source: Agner Fog's Instruction tables.
Related to <rdar://problem/15607571>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215045 91177308-0d34-0410-b5e6-96231b3b80d8
Source: Agner Fog's Instruction tables.
Related to <rdar://problem/15607571>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215045 91177308-0d34-0410-b5e6-96231b3b80d8
Add the -mcpu= option to llvm-objdump for use with the disassemblers.
Also make the disassembler created with the Mach-O parser (the -m option)
pick up the Target specific attributes specified with -mattr option.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215032 91177308-0d34-0410-b5e6-96231b3b80d8
Also make the disassembler created with the Mach-O parser (the -m option)
pick up the Target specific attributes specified with -mattr option.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215032 91177308-0d34-0410-b5e6-96231b3b80d8
MC X86: Accept ".att_syntax prefix" and diagnose noprefix
Fixes PR18916. I don't think we need to implement support for either
hybrid syntax. Nobody should write Intel assembly with '%' prefixes on
their registers or AT&T assembly without them.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215031 91177308-0d34-0410-b5e6-96231b3b80d8
Fixes PR18916. I don't think we need to implement support for either
hybrid syntax. Nobody should write Intel assembly with '%' prefixes on
their registers or AT&T assembly without them.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@215031 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "Reapply "DebugInfo: Ensure that all debug location scope chains from instructions within a function, lead to the function itself.""
This reverts commit r214761.
Revert while Reid investigates & provides a reproduction for an
assertion failure for this on Windows.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214999 91177308-0d34-0410-b5e6-96231b3b80d8
This reverts commit r214761.
Revert while Reid investigates & provides a reproduction for an
assertion failure for this on Windows.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214999 91177308-0d34-0410-b5e6-96231b3b80d8
fix typo
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214995 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214995 91177308-0d34-0410-b5e6-96231b3b80d8
getNewMemBuffer memsets the buffer to zeros,
the caller don't have to initialize it.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214994 91177308-0d34-0410-b5e6-96231b3b80d8
the caller don't have to initialize it.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214994 91177308-0d34-0410-b5e6-96231b3b80d8
Fix a test that has no checks.
X86 doesn't have fneg, so check for xor.
Differential Revision: http://reviews.llvm.org/D4812
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214992 91177308-0d34-0410-b5e6-96231b3b80d8
X86 doesn't have fneg, so check for xor.
Differential Revision: http://reviews.llvm.org/D4812
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214992 91177308-0d34-0410-b5e6-96231b3b80d8
R600: Cleanup fadd and fsub tests
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214991 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214991 91177308-0d34-0410-b5e6-96231b3b80d8
Revert "r214897 - Remove dead zero store to calloc initialized memory"
It broke msan.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214989 91177308-0d34-0410-b5e6-96231b3b80d8
It broke msan.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214989 91177308-0d34-0410-b5e6-96231b3b80d8
Remove the target machine from CCState. Previously it was only used
to get the subtarget and that's accessible from the MachineFunction
now. This helps clear the way for smaller changes where we getting
a subtarget will require passing in a MachineFunction/Function as
well.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214988 91177308-0d34-0410-b5e6-96231b3b80d8
to get the subtarget and that's accessible from the MachineFunction
now. This helps clear the way for smaller changes where we getting
a subtarget will require passing in a MachineFunction/Function as
well.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214988 91177308-0d34-0410-b5e6-96231b3b80d8
Improve performance of calculateDbgValueHistory.
In r210492 the logic of calculateDbgValueHistory was changed to end
register variable live ranges at the end of MBB conditionally on
the fact that the register was or not clobbered by the function body.
This requires an initial scan of all the operands of the function
to collect all clobbered registers. In a second pass over all
instructions, we compare this set with the set of clobbered
registers for the current MachineInstruction. This modification
incurred a compilation time regression on some benchmarks: the
debug info emission phase takes ~10% more time.
While a small performance hit is unavoidable due to the initial
scan requirement, we can improve the situation by avoiding to
create too many temporary sets and just use lambdas to work directly
on the result of the initial scan.
Fixes <rdar://problem/17884104>
Patch by Frederic Riss!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214987 91177308-0d34-0410-b5e6-96231b3b80d8
In r210492 the logic of calculateDbgValueHistory was changed to end
register variable live ranges at the end of MBB conditionally on
the fact that the register was or not clobbered by the function body.
This requires an initial scan of all the operands of the function
to collect all clobbered registers. In a second pass over all
instructions, we compare this set with the set of clobbered
registers for the current MachineInstruction. This modification
incurred a compilation time regression on some benchmarks: the
debug info emission phase takes ~10% more time.
While a small performance hit is unavoidable due to the initial
scan requirement, we can improve the situation by avoiding to
create too many temporary sets and just use lambdas to work directly
on the result of the initial scan.
Fixes <rdar://problem/17884104>
Patch by Frederic Riss!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214987 91177308-0d34-0410-b5e6-96231b3b80d8
Cleanup collectChangingRegs
The handling of the epilogue is best expressed as an early exit and
there is no reason to look for register defs in DbgValue MIs.
Patch by Frederic Riss!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214986 91177308-0d34-0410-b5e6-96231b3b80d8
The handling of the epilogue is best expressed as an early exit and
there is no reason to look for register defs in DbgValue MIs.
Patch by Frederic Riss!
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214986 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Fix ranges+gmlt test case to actually exercise the gmlt situation.
Originally this test case tested the specified behavior (that -gmlt
would not produce DW_AT_ranges and that when no CU DW_AT_ranges were
produced, no debug_ranges section (not even an empty list) would be
produced) but then the ranges emission code was improved not to create
ranges of a single element (instead favoring high_pc/low_pc) and so this
test case no longer exercised the -gmlt portion of the behavior.
This caused me some confusion when reading the comments and trying to
update this test case for future changes to -gmlt. I've made this test
resilient to those changes (by using the {{DW_TAG|NULL}} pattern to
block the end of the attribute search at the end of the CU's attribute
list without mandating that it must (or must not) be followed by another
tag (the future changes to -gmlt should produce no subprograms in this
CU))
Fix the test case to have two functions in distinct sections to force
the use of DW_AT_ranges.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214985 91177308-0d34-0410-b5e6-96231b3b80d8
Originally this test case tested the specified behavior (that -gmlt
would not produce DW_AT_ranges and that when no CU DW_AT_ranges were
produced, no debug_ranges section (not even an empty list) would be
produced) but then the ranges emission code was improved not to create
ranges of a single element (instead favoring high_pc/low_pc) and so this
test case no longer exercised the -gmlt portion of the behavior.
This caused me some confusion when reading the comments and trying to
update this test case for future changes to -gmlt. I've made this test
resilient to those changes (by using the {{DW_TAG|NULL}} pattern to
block the end of the attribute search at the end of the CU's attribute
list without mandating that it must (or must not) be followed by another
tag (the future changes to -gmlt should produce no subprograms in this
CU))
Fix the test case to have two functions in distinct sections to force
the use of DW_AT_ranges.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214985 91177308-0d34-0410-b5e6-96231b3b80d8
Add a triple to this test to get the right IR mangling
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214982 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214982 91177308-0d34-0410-b5e6-96231b3b80d8
Don't count inreg params when mangling fastcall functions
This is consistent with MSVC.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214981 91177308-0d34-0410-b5e6-96231b3b80d8
This is consistent with MSVC.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214981 91177308-0d34-0410-b5e6-96231b3b80d8
Round up the size of byval arguments to MinAlign
Otherwise we can end up with an argument frame size that is not a
multiple of stack slot size, which is very awkward.
This fixes PR20547, which was a bug in x86_64 Sys V vararg handling.
However, it's much easier to test this with x86 callee-cleanup
functions, which previously ended in "retl $6" instead of "retl $8".
This does affect behavior of all backends, but it presumably fixes the
same bug in all of them.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214980 91177308-0d34-0410-b5e6-96231b3b80d8
Otherwise we can end up with an argument frame size that is not a
multiple of stack slot size, which is very awkward.
This fixes PR20547, which was a bug in x86_64 Sys V vararg handling.
However, it's much easier to test this with x86 callee-cleanup
functions, which previously ended in "retl $6" instead of "retl $8".
This does affect behavior of all backends, but it presumably fixes the
same bug in all of them.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214980 91177308-0d34-0410-b5e6-96231b3b80d8
UseListOrder: Use std::vector
I initially used a `SmallVector<>` for `UseListOrder::Shuffle`, which
was a silly choice. When I realized my error I quickly rolled a custom
data structure.
This commit simplifies it to a `std::vector<>`. Now that I've had a
chance to measure performance, this data structure isn't part of a
bottleneck, so the additional complexity is unnecessary.
This is part of PR5680.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214979 91177308-0d34-0410-b5e6-96231b3b80d8
I initially used a `SmallVector<>` for `UseListOrder::Shuffle`, which
was a silly choice. When I realized my error I quickly rolled a custom
data structure.
This commit simplifies it to a `std::vector<>`. Now that I've had a
chance to measure performance, this data structure isn't part of a
bottleneck, so the additional complexity is unnecessary.
This is part of PR5680.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214979 91177308-0d34-0410-b5e6-96231b3b80d8
[AArch64] Add a few isTarget* API to AArch64 Subtarget.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214977 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214977 91177308-0d34-0410-b5e6-96231b3b80d8
Add test case omitted in r214974.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214975 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214975 91177308-0d34-0410-b5e6-96231b3b80d8
[AArch64] Fix OS ABI flag for aarch64-linux-gnu target.
For triple aarch64-linux-gnu we were incorrectly setting IRIX.
For triple aarch64 we are correctly setting SYSV.
Patch by Ana Pazos <apazos@codeaurora.org>.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214974 91177308-0d34-0410-b5e6-96231b3b80d8
For triple aarch64-linux-gnu we were incorrectly setting IRIX.
For triple aarch64 we are correctly setting SYSV.
Patch by Ana Pazos <apazos@codeaurora.org>.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214974 91177308-0d34-0410-b5e6-96231b3b80d8
use register iterators that include self to reduce code duplication in CriticalAntiDepBreaker
This patch addresses 2 FIXME comments that I added to CriticalAntiDepBreaker while fixing PR20020.
Initialize an MCSubRegIterator and an MCRegAliasIterator to include the self reg.
Assuming that works as advertised, there should be functional difference with this patch, just less code.
Also, remove the associated asserts - we're setting those values just before, so the asserts don't do anything meaningful.
Differential Revision: http://reviews.llvm.org/D4566
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214973 91177308-0d34-0410-b5e6-96231b3b80d8
This patch addresses 2 FIXME comments that I added to CriticalAntiDepBreaker while fixing PR20020.
Initialize an MCSubRegIterator and an MCRegAliasIterator to include the self reg.
Assuming that works as advertised, there should be functional difference with this patch, just less code.
Also, remove the associated asserts - we're setting those values just before, so the asserts don't do anything meaningful.
Differential Revision: http://reviews.llvm.org/D4566
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214973 91177308-0d34-0410-b5e6-96231b3b80d8
[AVX512] Added load/store instructions to Register2Memory opcode tables.
Added lowering tests for load/store.
Reviewed by Elena Demikhovsky <elena.demikhovsky@intel.com>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214972 91177308-0d34-0410-b5e6-96231b3b80d8
Added lowering tests for load/store.
Reviewed by Elena Demikhovsky <elena.demikhovsky@intel.com>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214972 91177308-0d34-0410-b5e6-96231b3b80d8
[AArch64] Add a testcase for r214957.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214965 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214965 91177308-0d34-0410-b5e6-96231b3b80d8
Add a new option -run-slp-after-loop-vectorization.
This swaps the order of the loop vectorizer and the SLP/BB vectorizers. It is disabled by default so we can do performance testing - ideally we want to change to having the loop vectorizer running first, and the SLP vectorizer using its leftovers instead of the other way around.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214963 91177308-0d34-0410-b5e6-96231b3b80d8
This swaps the order of the loop vectorizer and the SLP/BB vectorizers. It is disabled by default so we can do performance testing - ideally we want to change to having the loop vectorizer running first, and the SLP vectorizer using its leftovers instead of the other way around.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214963 91177308-0d34-0410-b5e6-96231b3b80d8
ARM: do not generate BLX instructions on Cortex-M CPUs.
Particularly on MachO, we were generating "blx _dest" instructions on M-class
CPUs, which don't actually exist. They happen to get fixed up by the linker
into valid "bl _dest" instructions (which is why such a massive issue has
remained largely undetected), but we shouldn't rely on that.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214959 91177308-0d34-0410-b5e6-96231b3b80d8
Particularly on MachO, we were generating "blx _dest" instructions on M-class
CPUs, which don't actually exist. They happen to get fixed up by the linker
into valid "bl _dest" instructions (which is why such a massive issue has
remained largely undetected), but we shouldn't rely on that.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214959 91177308-0d34-0410-b5e6-96231b3b80d8
ARM-MachO: materialize callee address correctly on v4t.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214958 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214958 91177308-0d34-0410-b5e6-96231b3b80d8
[AArch64] Conditional selects are expensive on out-of-order cores.
Specifically Cortex-A57. This probably applies to Cyclone too but I haven't enabled it for that as I can't test it.
This gives ~4% improvement on SPEC 174.vpr, and ~1% in 471.omnetpp.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214957 91177308-0d34-0410-b5e6-96231b3b80d8
Specifically Cortex-A57. This probably applies to Cyclone too but I haven't enabled it for that as I can't test it.
This gives ~4% improvement on SPEC 174.vpr, and ~1% in 471.omnetpp.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214957 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix two independent miscompiles in the process of getting the same
test case to actually generate correct code.
The primary miscompile fixed here is that we weren't correctly handling
in-place elements in one half of a single-input v8i16 shuffle when
moving a dword of elements from that half to the other half. Some times,
we would clobber the in-place elements in forming the dword to move
across halves.
The fix to this involves forcibly marking the in-place inputs even when
there is no need to gather them into a dword, and to much more carefully
re-arrange the elements when grouping them into a dword to move across
halves. With these two changes we would generate correct shuffles for
the test case, but found another miscompile. There are also some random
perturbations of the generated shuffle pattern in SSE2. It looks like
a wash; more instructions in some cases fewer in others.
The second miscompile would corrupt the results into nonsense. This is
a buggy pattern in one of the added DAG combines. Mapping elements
through a PSHUFD when pairing redundant half-shuffles is *much* harder
than this code makes it out to be -- it requires reasoning about *all*
of where the input is used in the PSHUFD, not just one part of where it
is used. Plus, we can't combine a half shuffle *into* a PSHUFD but the
code didn't guard against it. I think this was just a bad idea and I've
just removed that aspect of the combine. No tests regress as
a consequence so seems OK.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214954 91177308-0d34-0410-b5e6-96231b3b80d8
test case to actually generate correct code.
The primary miscompile fixed here is that we weren't correctly handling
in-place elements in one half of a single-input v8i16 shuffle when
moving a dword of elements from that half to the other half. Some times,
we would clobber the in-place elements in forming the dword to move
across halves.
The fix to this involves forcibly marking the in-place inputs even when
there is no need to gather them into a dword, and to much more carefully
re-arrange the elements when grouping them into a dword to move across
halves. With these two changes we would generate correct shuffles for
the test case, but found another miscompile. There are also some random
perturbations of the generated shuffle pattern in SSE2. It looks like
a wash; more instructions in some cases fewer in others.
The second miscompile would corrupt the results into nonsense. This is
a buggy pattern in one of the added DAG combines. Mapping elements
through a PSHUFD when pairing redundant half-shuffles is *much* harder
than this code makes it out to be -- it requires reasoning about *all*
of where the input is used in the PSHUFD, not just one part of where it
is used. Plus, we can't combine a half shuffle *into* a PSHUFD but the
code didn't guard against it. I think this was just a bad idea and I've
just removed that aspect of the combine. No tests regress as
a consequence so seems OK.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214954 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Switch to a formulation of a for loop that is much more obviously
not corrupting the mask by mutating it more times than intended. No
functionality changed (the results were non-overlapping so the old
version "worked" but was non-obvious).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214953 91177308-0d34-0410-b5e6-96231b3b80d8
not corrupting the mask by mutating it more times than intended. No
functionality changed (the results were non-overlapping so the old
version "worked" but was non-obvious).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214953 91177308-0d34-0410-b5e6-96231b3b80d8
[X86] Fixes commit r214890 to match the posted patch
This was another fallout from my local rebase where something went wrong :(
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214951 91177308-0d34-0410-b5e6-96231b3b80d8
This was another fallout from my local rebase where something went wrong :(
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214951 91177308-0d34-0410-b5e6-96231b3b80d8
Correct comment
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214945 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214945 91177308-0d34-0410-b5e6-96231b3b80d8
[dfsan] Try not to create too many additional basic blocks in functions which
already have a large number of blocks. Works around a performance issue with
the greedy register allocator.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214944 91177308-0d34-0410-b5e6-96231b3b80d8
already have a large number of blocks. Works around a performance issue with
the greedy register allocator.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214944 91177308-0d34-0410-b5e6-96231b3b80d8
R600: Increase nearby load scheduling threshold.
This partially fixes weird looking load scheduling
in memcpy test. The load clustering doesn't seem
particularly smart, but this method seems to be partially
deprecated so it might not be worth trying to fix.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214943 91177308-0d34-0410-b5e6-96231b3b80d8
This partially fixes weird looking load scheduling
in memcpy test. The load clustering doesn't seem
particularly smart, but this method seems to be partially
deprecated so it might not be worth trying to fix.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214943 91177308-0d34-0410-b5e6-96231b3b80d8
R600/SI: Implement areLoadsFromSameBasePtr
This currently has a noticable effect on the kernel argument loads.
LDS and global loads are more problematic, I think because of how copies
are currently inserted to ensure that the address is a VGPR.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214942 91177308-0d34-0410-b5e6-96231b3b80d8
This currently has a noticable effect on the kernel argument loads.
LDS and global loads are more problematic, I think because of how copies
are currently inserted to ensure that the address is a VGPR.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214942 91177308-0d34-0410-b5e6-96231b3b80d8
[X86][SchedModel] Fixed some wrong scheduling model found by code inspection.
Source: Agner Fog's Instruction tables.
Related to <rdar://problem/15607571>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214940 91177308-0d34-0410-b5e6-96231b3b80d8
Source: Agner Fog's Instruction tables.
Related to <rdar://problem/15607571>
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214940 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Assert that any CU for which debug_loc lists are emitted, has at least one range.
This was coming in weird debug info that had variables (and hence
debug_locs) but was in GMLT mode (because it was missing the 13th field
of the compile_unit metadata) so no ranges were constructed. We should
always have at least one range for any CU with a debug_loc in it -
because the range should cover the debug_loc.
The assertion just ensures that the "!= 1" range case inside the
subsequent loop doesn't get entered for the case where there are no
ranges at all, which should never reach here in the first place.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214939 91177308-0d34-0410-b5e6-96231b3b80d8
This was coming in weird debug info that had variables (and hence
debug_locs) but was in GMLT mode (because it was missing the 13th field
of the compile_unit metadata) so no ranges were constructed. We should
always have at least one range for any CU with a debug_loc in it -
because the range should cover the debug_loc.
The assertion just ensures that the "!= 1" range case inside the
subsequent loop doesn't get entered for the case where there are no
ranges at all, which should never reach here in the first place.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214939 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Fix a bunch of tests that, owing to their compile_unit metadata not including a 13th field, had some subtle behavior.
Without the 13th field, the "emission kind" field defaults to 0 (which
is not equal to either of the values of the emission kind enum (1 ==
full debug info, 2 == line tables only)).
In this particular instance, the comparison with "FullDebugInfo" was
done when adding elements to the ranges list - so for these test cases
no values were added to the ranges list.
This got weirder when emitting debug_loc entries as the addresses should
be relative to the range of the CU if the CU has only one range (the
reasonable assumption is that if we're emitting debug_loc lists for a CU
that CU has at least one range - but due to the above situation, it has
zero) so the ranges were emitted relative to the start of the section
rather than relative to the start of the CU's singular range.
Fix these tests by accounting for the difference in the description of
debug_loc entries (in some cases making the test ignorant to these
differences, in others adding the extra label difference expression,
etc) or the presence/absence of high/low_pc on the CU, and add the 13th
field to their CUs to enable proper "full debug info" emission here.
In a future commit I'll fix up a bunch of other test cases that are not
so rigorously depending on this behavior, but still doing similarly
weird things due to the missing 13th field.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214937 91177308-0d34-0410-b5e6-96231b3b80d8
Without the 13th field, the "emission kind" field defaults to 0 (which
is not equal to either of the values of the emission kind enum (1 ==
full debug info, 2 == line tables only)).
In this particular instance, the comparison with "FullDebugInfo" was
done when adding elements to the ranges list - so for these test cases
no values were added to the ranges list.
This got weirder when emitting debug_loc entries as the addresses should
be relative to the range of the CU if the CU has only one range (the
reasonable assumption is that if we're emitting debug_loc lists for a CU
that CU has at least one range - but due to the above situation, it has
zero) so the ranges were emitted relative to the start of the section
rather than relative to the start of the CU's singular range.
Fix these tests by accounting for the difference in the description of
debug_loc entries (in some cases making the test ignorant to these
differences, in others adding the extra label difference expression,
etc) or the presence/absence of high/low_pc on the CU, and add the 13th
field to their CUs to enable proper "full debug info" emission here.
In a future commit I'll fix up a bunch of other test cases that are not
so rigorously depending on this behavior, but still doing similarly
weird things due to the missing 13th field.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214937 91177308-0d34-0410-b5e6-96231b3b80d8
R600/SI: Add definitions for ds_read2st64_ / ds_write2st64_
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214936 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214936 91177308-0d34-0410-b5e6-96231b3b80d8
Fix typos in comments and doc
Committing http://reviews.llvm.org/D4798 for Robin Morisset (morisset@google.com)
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214934 91177308-0d34-0410-b5e6-96231b3b80d8
Committing http://reviews.llvm.org/D4798 for Robin Morisset (morisset@google.com)
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214934 91177308-0d34-0410-b5e6-96231b3b80d8
DebugInfo: Move the reference to the CU from the location list entry to the list itself, since it is constant across an entire list.
This simplifies construction and usage while making the data structure
smaller. It was a holdover from the days when we didn't have a separate
DebugLocList and all we had was a flat list of DebugLocEntries.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214933 91177308-0d34-0410-b5e6-96231b3b80d8
This simplifies construction and usage while making the data structure
smaller. It was a holdover from the days when we didn't have a separate
DebugLocList and all we had was a flat list of DebugLocEntries.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214933 91177308-0d34-0410-b5e6-96231b3b80d8
Remove a virtual function from TargetMachine. NFC.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214929 91177308-0d34-0410-b5e6-96231b3b80d8
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214929 91177308-0d34-0410-b5e6-96231b3b80d8
Re-apply r214881: Fix return sequence on armv4 thumb
This reverts r214893, re-applying r214881 with the test case relaxed a bit to
satiate the build bots.
POP on armv4t cannot be used to change thumb state (unilke later non-m-class
architectures), therefore we need a different return sequence that uses 'bx'
instead:
POP {r3}
ADD sp, #offset
BX r3
This patch also fixes an issue where the return value in r3 would get clobbered
for functions that return 128 bits of data. In that case, we generate this
sequence instead:
MOV ip, r3
POP {r3}
ADD sp, #offset
MOV lr, r3
MOV r3, ip
BX lr
http://reviews.llvm.org/D4748
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214928 91177308-0d34-0410-b5e6-96231b3b80d8
This reverts r214893, re-applying r214881 with the test case relaxed a bit to
satiate the build bots.
POP on armv4t cannot be used to change thumb state (unilke later non-m-class
architectures), therefore we need a different return sequence that uses 'bx'
instead:
POP {r3}
ADD sp, #offset
BX r3
This patch also fixes an issue where the return value in r3 would get clobbered
for functions that return 128 bits of data. In that case, we generate this
sequence instead:
MOV ip, r3
POP {r3}
ADD sp, #offset
MOV lr, r3
MOV r3, ip
BX lr
http://reviews.llvm.org/D4748
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214928 91177308-0d34-0410-b5e6-96231b3b80d8
[MCJIT] Make llvm-rtdyld check RuntimeDyld's error state when running in -verify
mode.
This will cause -verify mode to report failure when RuntimeDyld encounters an
internal error (e.g. overflows in relocation computations). Previously we had
let these errors slip past unreported.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214925 91177308-0d34-0410-b5e6-96231b3b80d8
mode.
This will cause -verify mode to report failure when RuntimeDyld encounters an
internal error (e.g. overflows in relocation computations). Previously we had
let these errors slip past unreported.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214925 91177308-0d34-0410-b5e6-96231b3b80d8
[PowerPC] Swap arguments and adjust shift count for vsldoi on little endian
Commits r213915 and r214718 fix recognition of shuffle masks for vmrg*
and vpku*um instructions for a little-endian target, by swapping the
input arguments. The vsldoi instruction requires similar treatment,
and also needs its shift count adjusted for little endian.
Reviewed by Ulrich Weigand.
This is a bug fix candidate for release 3.5 (and hopefully the last of
those for PowerPC).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214923 91177308-0d34-0410-b5e6-96231b3b80d8
Commits r213915 and r214718 fix recognition of shuffle masks for vmrg*
and vpku*um instructions for a little-endian target, by swapping the
input arguments. The vsldoi instruction requires similar treatment,
and also needs its shift count adjusted for little endian.
Reviewed by Ulrich Weigand.
This is a bug fix candidate for release 3.5 (and hopefully the last of
those for PowerPC).
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214923 91177308-0d34-0410-b5e6-96231b3b80d8
Improved test cases that were added with r214892.
1. Added ':' to CHECK-LABELs
2. Added more CHECKs
3. Added CHECK-NEXTs
4. Added verbose hex immediate comments to CHECKs
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214921 91177308-0d34-0410-b5e6-96231b3b80d8
1. Added ':' to CHECK-LABELs
2. Added more CHECKs
3. Added CHECK-NEXTs
4. Added verbose hex immediate comments to CHECKs
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214921 91177308-0d34-0410-b5e6-96231b3b80d8
Don't internalize all but main by default.
This is mostly a cleanup, but it changes a fairly old behavior.
Every "real" LTO user was already disabling the silly internalize pass
and creating the internalize pass itself. The difference with this
patch is for "opt -std-link-opts" and the C api.
Now to get a usable behavior out of opt one doesn't need the funny
looking command line:
opt -internalize -disable-internalize -internalize-public-api-list=foo,bar -std-link-opts
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214919 91177308-0d34-0410-b5e6-96231b3b80d8
This is mostly a cleanup, but it changes a fairly old behavior.
Every "real" LTO user was already disabling the silly internalize pass
and creating the internalize pass itself. The difference with this
patch is for "opt -std-link-opts" and the C api.
Now to get a usable behavior out of opt one doesn't need the funny
looking command line:
opt -internalize -disable-internalize -internalize-public-api-list=foo,bar -std-link-opts
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214919 91177308-0d34-0410-b5e6-96231b3b80d8
Add a test showing the interaction of linker scripts and plugin.
In particular, the linker script is processed early enough for function g
to be internalized.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214916 91177308-0d34-0410-b5e6-96231b3b80d8
In particular, the linker script is processed early enough for function g
to be internalized.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214916 91177308-0d34-0410-b5e6-96231b3b80d8
[x86] Fix a crasher due to shuffles which cancel each other out and add
a test case.
We also miscompile this test case which is showing a serious flaw in the
single-input v8i16 shuffle code. I've left the specific instruction
checks FIXME-ed out until I can address the bug in the single-input
code, but I wanted to separate out a significant functionality change to
produce correct code from a very simple and targeted crasher fix.
The miscompile problem stems from keeping track of inputs by value
rather than by index. As a consequence of doing this, we can't reliably
update those inputs because they might swap and we can't detect this
without copying the mask.
The blend code now uses indices for the input lists and this seems
strictly better. It also should make it easier to sort things and do
other cleanups. I think the time has come to simplify The Great Lambda
here.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214914 91177308-0d34-0410-b5e6-96231b3b80d8
a test case.
We also miscompile this test case which is showing a serious flaw in the
single-input v8i16 shuffle code. I've left the specific instruction
checks FIXME-ed out until I can address the bug in the single-input
code, but I wanted to separate out a significant functionality change to
produce correct code from a very simple and targeted crasher fix.
The miscompile problem stems from keeping track of inputs by value
rather than by index. As a consequence of doing this, we can't reliably
update those inputs because they might swap and we can't detect this
without copying the mask.
The blend code now uses indices for the input lists and this seems
strictly better. It also should make it easier to sort things and do
other cleanups. I think the time has come to simplify The Great Lambda
here.
git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@214914 91177308-0d34-0410-b5e6-96231b3b80d8