opencl/llvm.git
8 years agoDebugInfo: Simplify solution to avoid DW_AT_artificial on inlined parameters.
David Blaikie [Tue, 27 May 2014 19:34:32 +0000 (19:34 +0000)]
DebugInfo: Simplify solution to avoid DW_AT_artificial on inlined parameters.

Originally committed in r207717, I clearly didn't look very closely at
the code to understand how existing things were working...

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209680 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips] Optimize long branch for MIPS64 by removing %higher and %highest.
Sasa Stankovic [Tue, 27 May 2014 18:53:06 +0000 (18:53 +0000)]
[mips] Optimize long branch for MIPS64 by removing %higher and %highest.
%higher and %highest can have non-zero values only for offsets greater
than 2GB, which is highly unlikely, if not impossible when compiling a
single function. This makes long branch for MIPS64 3 instructions smaller.

Differential Revision: http://llvm-reviews.chandlerc.com/D3281.diff

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209678 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Create abstract function definitions even when concrete definitions precee...
David Blaikie [Tue, 27 May 2014 18:37:55 +0000 (18:37 +0000)]
DebugInfo: Create abstract function definitions even when concrete definitions preceed inline definitions.

After much puppetry, here's the major piece of the work to ensure that
even when a concrete definition preceeds all inline definitions, an
abstract definition is still created and referenced from both concrete
and inline definitions.

Variables are still broken in this case (see comment in
dbg-value-inlined-parameter.ll test case) and will be addressed in
follow up work.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209677 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Avoid an extra map lookup when finding abstract subprogram DIEs.
David Blaikie [Tue, 27 May 2014 18:37:51 +0000 (18:37 +0000)]
DebugInfo: Avoid an extra map lookup when finding abstract subprogram DIEs.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209676 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Lazily construct subprogram definition DIEs.
David Blaikie [Tue, 27 May 2014 18:37:48 +0000 (18:37 +0000)]
DebugInfo: Lazily construct subprogram definition DIEs.

A further step to correctly emitting concrete out of line definitions
preceeding inlined instances of the same program.

To do this, emission of subprograms must be delayed until required since
we don't know which (abstract only (if there's no out of line
definition), concrete only (if there are no inlined instances), or both)
DIEs are required at the start of the module.

To reduce the test churn in the following commit that actually fixes the
bug, this commit introduces the lazy DIE construction and cleans up test
cases that are impacted by the changes in the resulting DIE ordering.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209675 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Lazily attach definition attributes to definitions.
David Blaikie [Tue, 27 May 2014 18:37:43 +0000 (18:37 +0000)]
DebugInfo: Lazily attach definition attributes to definitions.

This is a precursor to fixing inlined debug info where the concrete,
out-of-line definition may preceed any inlined usage. To cope with this,
the attributes that may appear on the concrete definition or the
abstract definition are delayed until the end of the module. Then, if an
abstract definition was created, it is referenced (and no other
attributes are added to the out-of-line definition), otherwise the
attributes are added directly to the out-of-line definition.

In a couple of cases this causes not just reordering of attributes, but
reordering of types. When the creation of the attribute is delayed, if
that creation would create a type (such as for a DW_AT_type attribute)
then other top level DIEs may've been constructed during the delay,
causing the referenced type to be created and added after those
intervening DIEs. In the extreme case, in cross-cu-inlining.ll, this
actually causes the DW_TAG_basic_type for "int" to move from one CU to
another.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209674 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Separate out the addition of subprogram attribute additions so that they...
David Blaikie [Tue, 27 May 2014 18:37:38 +0000 (18:37 +0000)]
DebugInfo: Separate out the addition of subprogram attribute additions so that they can be added later depending on whether or not the function is inlined.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209673 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFixed a test in r209670
Jingyue Wu [Tue, 27 May 2014 18:12:55 +0000 (18:12 +0000)]
Fixed a test in r209670

The test was outdated with r209537.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209671 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDistribute sext/zext to the operands of and/or/xor
Jingyue Wu [Tue, 27 May 2014 18:00:00 +0000 (18:00 +0000)]
Distribute sext/zext to the operands of and/or/xor

This is an enhancement to SeparateConstOffsetFromGEP. With this patch, we can
extract a constant offset from "s/zext and/or/xor A, B".

Added a new test @ext_or to verify this enhancement.

Refactoring the code, I also extracted some common logic to function
Distributable.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209670 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Fix argument ordering in test by adding argument numbering.
David Blaikie [Tue, 27 May 2014 17:57:14 +0000 (17:57 +0000)]
DebugInfo: Fix argument ordering in test by adding argument numbering.

This old test didn't have the argument numbering that's now squirelled
away in the high bits of the line number in the DW_TAG_arg_variable
metadata.

Add the numbering and update the test to ensure arguments are in-order.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209669 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoPost-commit fixes for r209643
Filipe Cabecinhas [Tue, 27 May 2014 16:54:33 +0000 (16:54 +0000)]
Post-commit fixes for r209643

Detected by Daniel Jasper, Ilia Filippov, and Andrea Di Biagio
Fixed the argument order to select (the mask semantics to blendv* are the
inverse of select) and fixed the tests
Added parenthesis to the assert condition
Ran clang-format

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209667 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: add test for NZCV cross-copy save.
Tim Northover [Tue, 27 May 2014 16:50:09 +0000 (16:50 +0000)]
AArch64: add test for NZCV cross-copy save.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209665 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: add AArch64-specific test for 'c' and 'n'.
Tim Northover [Tue, 27 May 2014 16:50:03 +0000 (16:50 +0000)]
AArch64: add AArch64-specific test for 'c' and 'n'.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209664 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[PATCH] Correct type used for VADD_SPLAT optimization on PowerPC
Bill Schmidt [Tue, 27 May 2014 15:57:51 +0000 (15:57 +0000)]
[PATCH] Correct type used for VADD_SPLAT optimization on PowerPC

In PPCISelLowering.cpp: PPCTargetLowering::LowerBUILD_VECTOR(), there
is an optimization for certain patterns to generate one or two vector
splats followed by a vector add or subtract.  This operation is
represented by a VADD_SPLAT in the selection DAG.  Prior to this
patch, it was possible for the VADD_SPLAT to be assigned the wrong
data type, causing incorrect code generation.  This patch corrects the
problem.

Specifically, the code previously assigned the value type of the
BUILD_VECTOR node to the newly generated VADD_SPLAT node.  This is
correct much of the time, but not always.  The problem is that the
call to isConstantSplat() may return a SplatBitSize that is not the
same as the number of bits in the original element vector type.  The
correct type to assign is a vector type with the same element bit size
as SplatBitSize.

The included test case shows an example of this, where the
BUILD_VECTOR node has a type of v16i8.  The vector to be built is {0,
16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16, 0, 16}.  isConstantSplat
detects that we can generate a splat of 16 for type v8i16, which is
the type we must assign to the VADD_SPLAT node.  If we do not, we
generate a vspltisb of 8 and a vaddubm, which generates the incorrect
result {16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16, 16,
16}.  The correct code generation is a vspltish of 8 and a vadduhm.

This patch also corrected code generation for
CodeGen/PowerPC/2008-07-10-SplatMiscompile.ll, which had been marked
as an XFAIL, so we can remove the XFAIL from the test case.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209662 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips][mips64r6] Add Relocations R_MIPS_PCHI16, R_MIPS_PCLO16
Zoran Jovanovic [Tue, 27 May 2014 14:58:51 +0000 (14:58 +0000)]
[mips][mips64r6] Add Relocations R_MIPS_PCHI16, R_MIPS_PCLO16
Differential Revision: http://reviews.llvm.org/D3860

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209659 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[ARM] Emit correct build attributes for the relocation models.
Amara Emerson [Tue, 27 May 2014 13:30:21 +0000 (13:30 +0000)]
[ARM] Emit correct build attributes for the relocation models.

Patch by Asiri Rathnayake.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209656 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips][mips64r6] Add relocations R_MIPS_PC21_S2, R_MIPS_PC26_S2
Zoran Jovanovic [Tue, 27 May 2014 12:55:40 +0000 (12:55 +0000)]
[mips][mips64r6] Add relocations R_MIPS_PC21_S2, R_MIPS_PC26_S2
Differential Revision: http://reviews.llvm.org/D3824

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209655 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[asancov] Emit an initializer passing number of coverage code locations in each module.
Evgeniy Stepanov [Tue, 27 May 2014 12:39:31 +0000 (12:39 +0000)]
[asancov] Emit an initializer passing number of coverage code locations in each module.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209654 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: implement copies to/from NZCV as a last ditch effort.
Tim Northover [Tue, 27 May 2014 12:16:02 +0000 (12:16 +0000)]
AArch64: implement copies to/from NZCV as a last ditch effort.

A test in test/Generic creates a DAG where the NZCV output of an ADCS is used
by multiple nodes. This makes LLVM want to save a copy of NZCV for later, which
it couldn't do before.

This should be the last fix required for the aarch64 buildbot.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209651 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoARM: teach AAPCS-VFP to deal with Cortex-M4.
Tim Northover [Tue, 27 May 2014 10:43:38 +0000 (10:43 +0000)]
ARM: teach AAPCS-VFP to deal with Cortex-M4.

Cortex-M4 only has single-precision floating point support, so any LLVM
"double" type will have been split into 2 i32s by now. Fortunately, the
consecutive-register framework turns out to be precisely what's needed to
reconstruct the double and follow AAPCS-VFP correctly!

rdar://problem/17012966

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209650 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix bad assert.
Daniel Jasper [Tue, 27 May 2014 09:55:37 +0000 (09:55 +0000)]
Fix bad assert.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209648 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: support 'c' and 'n' inline asm modifiers.
Tim Northover [Tue, 27 May 2014 07:37:21 +0000 (07:37 +0000)]
AArch64: support 'c' and 'n' inline asm modifiers.

These are tested by test/CodeGen/Generic, so we should probably know
how to deal with them. Fortunately generic code does it if asked.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209646 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdding testcase for PR18886.
Dinesh Dwivedi [Tue, 27 May 2014 06:44:25 +0000 (06:44 +0000)]
Adding testcase for PR18886.

Differential Revision: http://reviews.llvm.org/D3837

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209645 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoConvert some X86 blendv* intrinsics into IR.
Filipe Cabecinhas [Tue, 27 May 2014 03:42:20 +0000 (03:42 +0000)]
Convert some X86 blendv* intrinsics into IR.

Summary:
Implemented an InstCombine transformation that takes a blendv* intrinsic
call and translates it into an IR select, if the mask is constant.

This will eventually get lowered into blends with immediates if possible,
or pblendvb (with an option to further optimize if we can transform the
pblendvb into a blend+immediate instruction, depending on the selector).
It will also enable optimizations by the IR passes, which give up on
sight of the intrinsic.

Both the transformation and the lowering of its result to asm got shiny
new tests.

The transformation is a bit convoluted because of blendvp[sd]'s
definition:

Its mask is a floating point value! This forces us to convert it and get
the highest bit. I suppose this happened because the mask has type
__m128 in Intel's intrinsic and v4sf (for blendps) in gcc's builtin.

I will send an email to llvm-dev to discuss if we want to change this or
not.

Reviewers: grosbach, delena, nadav

Differential Revision: http://reviews.llvm.org/D3859

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209643 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix link.
Rafael Espindola [Mon, 26 May 2014 21:30:40 +0000 (21:30 +0000)]
Fix link.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209640 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoUse existing helper function.
Rafael Espindola [Mon, 26 May 2014 19:57:55 +0000 (19:57 +0000)]
Use existing helper function.

No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209639 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[PPC] Use alias symbols in address computation.
Rafael Espindola [Mon, 26 May 2014 19:08:19 +0000 (19:08 +0000)]
[PPC] Use alias symbols in address computation.

This seems to match what gcc does for ppc and what every other llvm
backend does.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209638 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: force i1 to be zero-extended at an ABI boundary.
Tim Northover [Mon, 26 May 2014 17:22:07 +0000 (17:22 +0000)]
AArch64: force i1 to be zero-extended at an ABI boundary.

This commit is debatable. There are two possible approaches, neither
of which is really satisfactory:

1. Use "@foo(i1 zeroext)" to mean an extension to 32-bits on Darwin,
   and 8 bits otherwise.
2. Redefine "@foo(i1)" to mean that the i1 is extended by the caller
   to 8 bits. This goes against the spirit of "zeroext" I think, but
   it's a bit of a vague construct anyway (by definition you're going
   to extend to the amount required by the ABI, that's why it's the
   ABI!).

This implements option 2. The DAG machinery really isn't setup for the
first (there's a fairly strong assumption that "zeroext" goes to at
least the smallest register size), and even if it was the resulting
DAG looks like it would be inferior in many cases.

Theoretically we could add AssertZext nodes in the consumers of
ABI-passed values too now, but this actually seems to make the code
worse in practice by making truncation proceed in two steps. The code
produced is equally valid if we continue to assume only the low bit is
defined.

Should fix PR19850

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209637 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: simplify calling conventions slightly.
Tim Northover [Mon, 26 May 2014 17:21:53 +0000 (17:21 +0000)]
AArch64: simplify calling conventions slightly.

We can eliminate the custom C++ code in favour of some TableGen to
check the same things. Functionality should be identical, except for a
buffer overrun that was present in the C++ code and meant webkit
failed if any small argument needed to be passed on the stack.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209636 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSome cleanup for r209568.
Michael Zolotukhin [Mon, 26 May 2014 14:49:46 +0000 (14:49 +0000)]
Some cleanup for r209568.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209634 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoConvert a few loops to use ranges.
Rafael Espindola [Mon, 26 May 2014 13:38:51 +0000 (13:38 +0000)]
Convert a few loops to use ranges.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209628 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[AArch64] Add store + add folding regression tests for the load/store optimization...
Tilmann Scheller [Mon, 26 May 2014 13:36:47 +0000 (13:36 +0000)]
[AArch64] Add store + add folding regression tests for the load/store optimization pass.

Add tests for the following transform:

 str X, [x0, #32]
  ...
 add x0, x0, #32
  ->
 str X, [x0, #32]!

with X being either w1, x1, s0, d0 or q0.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209627 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[AArch64] Add more regression tests for the load/store optimization pass.
Tilmann Scheller [Mon, 26 May 2014 12:15:51 +0000 (12:15 +0000)]
[AArch64] Add more regression tests for the load/store optimization pass.

Cover the following cases:

  ldr X, [x0, #32]
   ...
  add x0, x0, #32
   ->
  ldr X, [x0, #32]!

with X being either w1, x1, s0, d0 or q0.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209624 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[asan] decrease asan-instrumentation-with-call-threshold from 10000 to 7000, see...
Kostya Serebryany [Mon, 26 May 2014 11:57:16 +0000 (11:57 +0000)]
[asan] decrease asan-instrumentation-with-call-threshold from 10000 to 7000, see PR17409

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209623 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: remove empty ARM64 directories from svn.
Tim Northover [Mon, 26 May 2014 11:25:33 +0000 (11:25 +0000)]
AArch64: remove empty ARM64 directories from svn.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209621 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove accidentally committed whitespace.
Tilmann Scheller [Mon, 26 May 2014 09:40:40 +0000 (09:40 +0000)]
Remove accidentally committed whitespace.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209619 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[AArch64] Add a regression test for the load store optimizer.
Tilmann Scheller [Mon, 26 May 2014 09:37:19 +0000 (09:37 +0000)]
[AArch64] Add a regression test for the load store optimizer.

We have a couple of regression tests for load/store pairing, but (to my knowledge) there are no regression tests for the load/store + add/sub folding.

As a first step towards increased test coverage of this area, this commit adds a test for one instance of a load + add to pre-indexed load transformation.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209618 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMake the LoopRotate pass's maximum header size configurable both programmatically
Owen Anderson [Mon, 26 May 2014 08:58:51 +0000 (08:58 +0000)]
Make the LoopRotate pass's maximum header size configurable both programmatically
and via the command line, mirroring similar functionality in LoopUnroll.  In
situations where clients used custom unrolling thresholds, their intent could
previously be foiled by LoopRotate having a hardcoded threshold.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209617 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Test linkonce-odr functions under LTO.
David Blaikie [Mon, 26 May 2014 06:44:52 +0000 (06:44 +0000)]
DebugInfo: Test linkonce-odr functions under LTO.

This was previously regressed/broken by r192749 (reverted due to this
issue in r192938) and I was about to break it again by accident with
some more invasive changes that deal with the subprogram lists. So to
avoid that and further issues - here's a test.

It's a pretty basic test - in both r192749 and my impending case, this
test would crash, but checking the basics (that we put a subprogram in
just one of the two CUs) seems like a good start.

We still get this wrong in weird ways if the linkonce-odr function
happens to not be identical in the metadata (because it's defined in two
different files (hence the # line directives in this test), etc) even
though it meets the language requirements (identical token stream) for
such a thing. That results in two subprogram DIEs, but only one of them
gets the parameter and high/low pc information, etc. We probably need to
use the DIRef infrastructure to deduplicate functions as we do types to
address this issue - or perhaps teach the BC linker to remove the
duplicate entries in subprogram lists?

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209614 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDwarfUnit: Remove some misleading no-op code introduced in r204162.
David Blaikie [Mon, 26 May 2014 05:32:21 +0000 (05:32 +0000)]
DwarfUnit: Remove some misleading no-op code introduced in r204162.

Post commit review feedback from Manman called this out, but it looks
like it slipped through the cracks.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209611 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoJust check the entire string.
Rafael Espindola [Mon, 26 May 2014 04:08:51 +0000 (04:08 +0000)]
Just check the entire string.

Thanks to David Blaikie for the suggestion.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209610 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoReformat linefeeds.
NAKAMURA Takumi [Mon, 26 May 2014 00:25:26 +0000 (00:25 +0000)]
Reformat linefeeds.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209609 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoTrailing whitespace.
NAKAMURA Takumi [Mon, 26 May 2014 00:25:09 +0000 (00:25 +0000)]
Trailing whitespace.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209608 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agotools: avoid use of std::function
Saleem Abdulrasool [Sun, 25 May 2014 21:37:59 +0000 (21:37 +0000)]
tools: avoid use of std::function

Remove the use of the std::function and replace the capturing lambda with a
non-capturing one, opting to pass the user data down to the context.  This is
needed as std::function is not yet available on all hosted platforms (it
requires RTTI, which breaks on Windows).

Thanks to Nico Rieck for pointing this out!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209607 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agotools: split out Win64EHDumper from COFFDumper
Saleem Abdulrasool [Sun, 25 May 2014 20:26:45 +0000 (20:26 +0000)]
tools: split out Win64EHDumper from COFFDumper

Move the implementation of the Win64 EH printer from the COFFDumper into its own
class.  This is in preparation for adding support to print ARM EH information.
The only real change here is in printUnwindInfo where we now lambda lift the
implicit this parameter for the resolveFunction.  Also setup the printing to
handle ARM.  This now has set the stage to introduce ARM EH printing.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209606 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agotools: inline simple single-use function
Saleem Abdulrasool [Sun, 25 May 2014 20:26:40 +0000 (20:26 +0000)]
tools: inline simple single-use function

This inlines the single use function in preparation for splitting the Win64EH
printing out of the COFFDumper into its own entity.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209605 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agotools: refactor COFFDumper symbol resolution logic
Saleem Abdulrasool [Sun, 25 May 2014 20:26:37 +0000 (20:26 +0000)]
tools: refactor COFFDumper symbol resolution logic

Make the use of the cache more transparent to the users.  There is no reason
that the cached entries really need to be passed along.  The overhead for doing
so is minimal: a single extra parameter.  This requires that some standalone
functions be brought into the COFFDumper class so that they may access the
cache.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209604 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agotools: use references rather than out pointers in COFFDumper
Saleem Abdulrasool [Sun, 25 May 2014 20:26:33 +0000 (20:26 +0000)]
tools: use references rather than out pointers in COFFDumper

Switch to use references for parameters that are guaranteed to be non-null.
Simplifies the code a slight bit in preparation for another change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209603 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Fix inlining with #file directives a little harder
David Blaikie [Sun, 25 May 2014 18:11:35 +0000 (18:11 +0000)]
DebugInfo: Fix inlining with #file directives a little harder

Seems my previous fix was insufficient - we were still not adding the
inlined function to the abstract scope list. Which meant it wasn't
flagged as inline, didn't have nested lexical scopes in the abstract
definition, and didn't have abstract variables - so the inlined variable
didn't reference an abstract variable, instead being described
completely inline.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209602 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoStreamline test case by avoiding a temporary file and piping llc output straight...
David Blaikie [Sun, 25 May 2014 15:38:52 +0000 (15:38 +0000)]
Streamline test case by avoiding a temporary file and piping llc output straight to llvm-dwarfdump

We still do temporary files in many cases, just updating this particular
one because I was debugging it and made this change while doing so.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209601 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoEmit data or code export directives based on the type.
Rafael Espindola [Sun, 25 May 2014 12:49:07 +0000 (12:49 +0000)]
Emit data or code export directives based on the type.

Currently we look at the Aliasee to decide what type of export
directive to use. It seems better to use the type of the alias
directly. This is similar to how we handle the alias having the
same address but other attributes (linkage, visibility) from the
aliasee.

With this patch it is now possible to do things like

target datalayout = "e-m:e-i64:64-f80:128-n8:16:32:64-S128"
target triple = "x86_64-pc-windows-msvc"
@foo = global [6 x i8] c"\B8*\00\00\00\C3", section ".text", align 16
@f = dllexport alias i32 (), [6 x i8]* @foo
!llvm.module.flags = !{!0}
!0 = metadata !{i32 6, metadata !"Linker Options", metadata !1}
!1 = metadata !{metadata !2, metadata !3}
!2 = metadata !{metadata !"/DEFAULTLIB:libcmt.lib"}
!3 = metadata !{metadata !"/DEFAULTLIB:oldnames.lib"}

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209600 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMake these CHECKs a bit more strict.
Rafael Espindola [Sun, 25 May 2014 12:43:13 +0000 (12:43 +0000)]
Make these CHECKs a bit more strict.

The " at the end of the line makes sure we matched the entire directive.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209599 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd an extension point for peephole optimizers.
Peter Collingbourne [Sun, 25 May 2014 10:27:02 +0000 (10:27 +0000)]
Add an extension point for peephole optimizers.

This extension point allows adding passes that perform peephole optimizations
similar to the instruction combiner. These passes will be inserted after
each instance of the instruction combiner pass.

Differential Revision: http://reviews.llvm.org/D3905

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209595 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix some misplaced spaces around 'override'
Hans Wennborg [Sat, 24 May 2014 20:19:40 +0000 (20:19 +0000)]
Fix some misplaced spaces around 'override'

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209589 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agobuild: sort llvm-readobj sources
Saleem Abdulrasool [Sat, 24 May 2014 20:04:21 +0000 (20:04 +0000)]
build: sort llvm-readobj sources

Sort the source files.  NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209587 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agollvm-readobj: remove some dead code
Saleem Abdulrasool [Sat, 24 May 2014 19:54:28 +0000 (19:54 +0000)]
llvm-readobj: remove some dead code

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209586 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64: disable FastISel for large code model.
Tim Northover [Sat, 24 May 2014 19:45:41 +0000 (19:45 +0000)]
AArch64: disable FastISel for large code model.

The code emitted is what would be expected for the small model, so it
shouldn't be used when objects can be the full 64-bits away.

This fixes MCJIT tests on Linux.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209585 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMachineVerifier: Clean up some syntactic weirdness left behind by find&replace.
Benjamin Kramer [Sat, 24 May 2014 13:31:10 +0000 (13:31 +0000)]
MachineVerifier: Clean up some syntactic weirdness left behind by find&replace.

No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209581 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoCodeGen: Make MachineBasicBlock::back skip to the beginning of the last bundle.
Benjamin Kramer [Sat, 24 May 2014 13:13:17 +0000 (13:13 +0000)]
CodeGen: Make MachineBasicBlock::back skip to the beginning of the last bundle.

This makes front/back symmetric with begin/end, avoiding some confusion.
Added instr_front/instr_back for the old behavior, corresponding to
instr_begin/instr_end. Audited all three in-tree users of back(), all
of them look like they don't want to look inside bundles.

Fixes an assertion (PR19815) when generating debug info on mips, where a
delay slot was bundled at the end of a branch.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209580 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64/ARM64: move ARM64 into AArch64's place
Tim Northover [Sat, 24 May 2014 12:50:23 +0000 (12:50 +0000)]
AArch64/ARM64: move ARM64 into AArch64's place

This commit starts with a "git mv ARM64 AArch64" and continues out
from there, renaming the C++ classes, intrinsics, and other
target-local objects for consistency.

"ARM64" test directories are also moved, and tests that began their
life in ARM64 use an arm64 triple, those from AArch64 use an aarch64
triple. Both should be equivalent though.

This finishes the AArch64 merge, and everyone should feel free to
continue committing as normal now.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209577 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAArch64/ARM64: remove AArch64 from tree prior to renaming ARM64.
Tim Northover [Sat, 24 May 2014 12:42:26 +0000 (12:42 +0000)]
AArch64/ARM64: remove AArch64 from tree prior to renaming ARM64.

I'm doing this in two phases for a better "git blame" record. This
commit removes the previous AArch64 backend and redirects all
functionality to ARM64. It also deduplicates test-lines and removes
orphaned AArch64 tests.

The next step will be "git mv ARM64 AArch64" and rewire most of the
tests.

Hopefully LLVM is still functional, though it would be even better if
no-one ever had to care because the rename happens straight
afterwards.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209576 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agollvm/test/Object/ar-error.test: Don't check the message "No such file or directory".
NAKAMURA Takumi [Sat, 24 May 2014 08:47:11 +0000 (08:47 +0000)]
llvm/test/Object/ar-error.test: Don't check the message "No such file or directory".

It didn't match on non-English version of Windows.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209570 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoImplement sext(C1 + C2*X) --> sext(C1) + sext(C2*X) and
Michael Zolotukhin [Sat, 24 May 2014 08:09:57 +0000 (08:09 +0000)]
Implement sext(C1 + C2*X) --> sext(C1) + sext(C2*X) and
sext{C1,+,C2} --> sext(C1) + sext{0,+,C2} transformation in Scalar
Evolution.

That helps SLP-vectorizer to recognize consecutive loads/stores.

<rdar://problem/14860614>

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209568 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoARM64: extract a 32-bit subreg when selecting an inreg extend
Tim Northover [Sat, 24 May 2014 07:05:42 +0000 (07:05 +0000)]
ARM64: extract a 32-bit subreg when selecting an inreg extend

After the load/store refactoring, we were sometimes trying to feed a
GPR64 into a 32-bit register offset operand. This failed in
copyPhysReg.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209566 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Generalize some tests to handle variations in attribute ordering.
David Blaikie [Fri, 23 May 2014 21:11:46 +0000 (21:11 +0000)]
DebugInfo: Generalize some tests to handle variations in attribute ordering.

In an effort to fix inlined debug info in situations where the out of
line definition of a function preceeds any inlined usage, the order in
which some attributes are added to subprogram DIEs may change. (in
essence, definition-necessary attributes like DW_AT_low_pc/high_pc will
be added immediately, but the names, types, and other features will be
delayed to module end where they may either be added to the subprogram
DIE or instead reference an abstract definition for those values)

These tests can be generalized to be resilient to this change. 5 or so
tests actually have to be incompatibly changed to cope with this
reordering and will go along with the change that affects the order.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209554 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Generalize a test case to not depend on abbreviation numbering.
David Blaikie [Fri, 23 May 2014 21:07:01 +0000 (21:07 +0000)]
DebugInfo: Generalize a test case to not depend on abbreviation numbering.

It's an unnecessary detail for this test and just gets in the way when
making unrelated changes to the output in this test.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209553 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoTest case comments. Fix sloppiness.
Andrew Trick [Fri, 23 May 2014 20:46:21 +0000 (20:46 +0000)]
Test case comments. Fix sloppiness.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209551 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoclang-format function.
Rafael Espindola [Fri, 23 May 2014 20:39:23 +0000 (20:39 +0000)]
clang-format function.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209550 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove a confusing use of a static method.
Rafael Espindola [Fri, 23 May 2014 20:35:47 +0000 (20:35 +0000)]
Remove a confusing use of a static method.

No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209548 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Put concrete definitions referencing abstract definitions in the same...
David Blaikie [Fri, 23 May 2014 20:25:15 +0000 (20:25 +0000)]
DebugInfo: Put concrete definitions referencing abstract definitions in the same scope as the abstract definition.

This seems like a simple cleanup/improved consistency, but also helps
lay the foundation to fix the bug mentioned in the test case: concrete
definitions preceeding any inlined usage aren't properly split into
concrete + abstract (because they're not known to need it until it's too
late).

Once we start deferring this choice until later, we won't have the
choice to put concrete definitions for inlined subroutines in a
different scope from concrete definitions for non-inlined subroutines
(since we won't know at time-of-construction which one it'll be). This
change brings those two cases into alignment ahead of that future
chaneg/fix.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209547 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix and improve SCEV ComputeBackedgeTankCount.
Andrew Trick [Fri, 23 May 2014 19:47:13 +0000 (19:47 +0000)]
Fix and improve SCEV ComputeBackedgeTankCount.

This is a follow-up to r209358: PR19799: Indvars miscompile due to an
incorrect max backedge taken count from SCEV.

That fix was incomplete as pointed out by Arnold and Michael Z. The
code was also too confusing. It needed a careful rewrite with more
unit tests. This version will also happen to optimize more cases.

<rdar://17005101> PR19799: Indvars miscompile...

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209545 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRevert part of "Fix broken FileCheck prefixes"
Nico Rieck [Fri, 23 May 2014 19:33:49 +0000 (19:33 +0000)]
Revert part of "Fix broken FileCheck prefixes"

This reverts part of commit r209538.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209544 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoUse alias linkage and visibility to decide tls access mode.
Rafael Espindola [Fri, 23 May 2014 19:16:56 +0000 (19:16 +0000)]
Use alias linkage and visibility to decide tls access mode.

This matches both what we do for the non-thread case and what gcc does.

With this patch clang would match gcc's behaviour in

static __thread int a = 42;
extern __thread int b __attribute__((alias("a")));
int *f(void) { return &a; }
int *g(void) { return &b; }

if not for pr19843. Manually writing the IL does produce the same access modes.

It is also a step in the direction of fixing pr19844.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209543 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove unused CHECK lines
Nico Rieck [Fri, 23 May 2014 19:06:44 +0000 (19:06 +0000)]
Remove unused CHECK lines

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209539 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix broken FileCheck prefixes
Nico Rieck [Fri, 23 May 2014 19:06:24 +0000 (19:06 +0000)]
Fix broken FileCheck prefixes

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209538 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd the extracted constant offset using GEP
Jingyue Wu [Fri, 23 May 2014 18:39:40 +0000 (18:39 +0000)]
Add the extracted constant offset using GEP

Fixed a TODO in r207783.

Add the extracted constant offset using GEP instead of ugly
ptrtoint+add+inttoptr. Using GEP simplifies future optimizations and makes IR
easier to understand.

Updated all affected tests, and added a new test in split-gep.ll to cover a
corner case where emitting uglygep is necessary.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209537 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[RuntimeDyld] Remove relocation bounds check introduced in r208375 (MachO only).
Lang Hames [Fri, 23 May 2014 18:35:44 +0000 (18:35 +0000)]
[RuntimeDyld] Remove relocation bounds check introduced in r208375 (MachO only).

We do all of our address arithmetic in 64-bit, and operations involving
logically negative 32-bit offsets (actually represented as unsigned 64 bit ints)
often overflow into higher bits. The overflow check could be preserved by
casting to uint32 at the callsite for applyRelocationValue, but this would
eliminate the value of the check.

The right way to handle overflow in relocations is to make relocation processing
target specific, and compute the values for RelocationEntry objects in the
appropriate types (32-bit for 32-bit targets, 64-bit for 64-bit targets). This
is coming as part of the cleanup I'm working on.

This fixes another i386 regression test.

<rdar://problem/16889891>

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209536 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd FIXME comment based on code review feedback by Hal Finkel on r209338
David Blaikie [Fri, 23 May 2014 16:53:14 +0000 (16:53 +0000)]
Add FIXME comment based on code review feedback by Hal Finkel on r209338

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209529 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoConvert test to use FileCheck.
Rafael Espindola [Fri, 23 May 2014 16:51:13 +0000 (16:51 +0000)]
Convert test to use FileCheck.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209528 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoTeach the table generated emitPseudoExpansionLowering function to not emit a switch...
Aaron Ballman [Fri, 23 May 2014 15:33:39 +0000 (15:33 +0000)]
Teach the table generated emitPseudoExpansionLowering function to not emit a switch statement containing only a default statement (and no cases). Updated some of the code to use range-based for loops as well. No functional changes.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209521 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAliases are always definition, delete dead code.
Rafael Espindola [Fri, 23 May 2014 15:18:06 +0000 (15:18 +0000)]
Aliases are always definition, delete dead code.

While at it, use a range loop.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209519 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDelete dead code.
Rafael Espindola [Fri, 23 May 2014 15:07:51 +0000 (15:07 +0000)]
Delete dead code.

GV is never used past this point. This was probably a copy and paste error.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209518 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips] Work around inconsistency in llvm-mc's placement of fixup markers
Daniel Sanders [Fri, 23 May 2014 13:35:24 +0000 (13:35 +0000)]
[mips] Work around inconsistency in llvm-mc's placement of fixup markers

Summary:
Add a second fixup table to MipsAsmBackend::getFixupKindInfo() to correctly
position llvm-mc's fixup placeholders for big-endian.

See PR19836 for full details of the issue. To summarize, the fixup placeholders
do not account for endianness properly and the implementations of
getFixupKindInfo() for each target are measuring MCFixupKindInfo.TargetOffset
from different ends of the instruction encoding to compensate.

Reviewers: jkolek, zoran.jovanovic, vmedic

Reviewed By: vmedic

Differential Revision: http://reviews.llvm.org/D3889

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209514 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips][mips64r6] t(eq|ge|lt|ne)i and t(ge|lt)iu are not available in MIPS32r6/MIPS64r6
Daniel Sanders [Fri, 23 May 2014 13:24:08 +0000 (13:24 +0000)]
[mips][mips64r6] t(eq|ge|lt|ne)i and t(ge|lt)iu are not available in MIPS32r6/MIPS64r6

Summary: Depends on D3872

Reviewers: jkolek, zoran.jovanovic, vmedic

Reviewed By: vmedic

Differential Revision: http://reviews.llvm.org/D3891

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209513 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[mips][mips64r6] [ls][dw][lr] are not available in MIPS32r6/MIPS64r6
Daniel Sanders [Fri, 23 May 2014 13:18:02 +0000 (13:18 +0000)]
[mips][mips64r6] [ls][dw][lr] are not available in MIPS32r6/MIPS64r6

Summary:
Instead the system is required to provide some means of handling unaligned
load/store without special instructions. Options include full hardware
support, full trap-and-emulate, and hybrids such as hardware support within
a cache line and trap-and-emulate for multi-line accesses.

MipsSETargetLowering::allowsUnalignedMemoryAccesses() has been configured to
assume that unaligned accesses are 'fast' on the basis that I expect few
hardware implementations will opt for pure-software handling of unaligned
accesses. The ones that do handle it purely in software can override this.

mips64-load-store-left-right.ll has been merged into load-store-left-right.ll

The stricter testing revealed a Bits!=Bytes bug in passByValArg(). This has
been fixed and the variables renamed to clarify the units they hold.

Reviewers: zoran.jovanovic, jkolek, vmedic

Reviewed By: vmedic

Differential Revision: http://reviews.llvm.org/D3872

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209512 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[asan] properly instrument memory accesses that have small alignment (smaller than...
Kostya Serebryany [Fri, 23 May 2014 11:52:07 +0000 (11:52 +0000)]
[asan] properly instrument memory accesses that have small alignment (smaller than min(8,size)) by making two checks instead of one. This may slowdown some cases, e.g. long long on 32-bit or wide loads produced after loop unrolling. The benefit is higher sencitivity.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209508 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoUpdated the llvm.mem.parallel_loop_access semantics to include the possibility
Pekka Jaaskelainen [Fri, 23 May 2014 11:35:46 +0000 (11:35 +0000)]
Updated the llvm.mem.parallel_loop_access semantics to include the possibility
to have only some of the loop's memory instructions be annotated and still _help_
the loop carried dependence analysis.

This was discussed in the llvmdev ML (topic: "parallel loop metadata question").

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209507 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFixup sys::getHostCPUFeatures crypto names so it doesn't clash with kernel headers
Bradley Smith [Fri, 23 May 2014 10:14:13 +0000 (10:14 +0000)]
Fixup sys::getHostCPUFeatures crypto names so it doesn't clash with kernel headers

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209506 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[YAML] Add an optional argument `EnumMask` to the `yaml::IO::bitSetCase()`.
Simon Atanasyan [Fri, 23 May 2014 08:07:09 +0000 (08:07 +0000)]
[YAML] Add an optional argument `EnumMask` to the `yaml::IO::bitSetCase()`.

Some bit-set fields used in ELF file headers in fact contain two parts.
The first one is a regular bit-field. The second one is an enumeraion.
For example ELF header `e_flags` for MIPS target might contain the
following values:

Bit-set values:

  EF_MIPS_NOREORDER = 0x00000001
  EF_MIPS_PIC       = 0x00000002
  EF_MIPS_CPIC      = 0x00000004
  EF_MIPS_ABI2      = 0x00000020

Enumeration:

  EF_MIPS_ARCH_32   = 0x50000000
  EF_MIPS_ARCH_64   = 0x60000000
  EF_MIPS_ARCH_32R2 = 0x70000000
  EF_MIPS_ARCH_64R2 = 0x80000000

For printing bit-sets we use the `yaml::IO::bitSetCase()`. It does not
support bit-set/enumeration combinations and prints too many flags from
an enumeration part. This patch fixes this problem. New method
`yaml::IO::maskedBitSetCase()` handle "enumeration" part of bitset
defined by provided mask.

Patch reviewed by Nick Kledzik and Sean Silva.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209504 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoTypedef NumeredTypesMapTy is not used anywhere.
Yaron Keren [Fri, 23 May 2014 07:31:25 +0000 (07:31 +0000)]
Typedef NumeredTypesMapTy is not used anywhere.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209502 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoTest commit.
Jingyue Wu [Fri, 23 May 2014 06:30:12 +0000 (06:30 +0000)]
Test commit.

The keyword "virtual" is not necessary.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209501 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agollvm-ar: Output the file we errored on.
Filipe Cabecinhas [Fri, 23 May 2014 05:52:12 +0000 (05:52 +0000)]
llvm-ar: Output the file we errored on.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209500 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRename a couple of variables to be more accurate.
David Blaikie [Fri, 23 May 2014 05:03:23 +0000 (05:03 +0000)]
Rename a couple of variables to be more accurate.

It's not really a "ScopeDIE", as such - it's the abstract function
definition's DIE. And we usually use "SP" for subprograms, rather than
"Sub".

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209499 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDebugInfo: Fix cross-CU references for scopes (and variables within those scopes...
David Blaikie [Fri, 23 May 2014 04:23:06 +0000 (04:23 +0000)]
DebugInfo: Fix cross-CU references for scopes (and variables within those scopes) in abstract definitions of cross-CU inlined functions

Found by Adrian Prantl during post-commit review of r209335.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209498 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMC: remove unnecessary restriction on tests
Saleem Abdulrasool [Fri, 23 May 2014 02:56:51 +0000 (02:56 +0000)]
MC: remove unnecessary restriction on tests

Rafael correctly pointed out that the restriction is unnecessary.  Although the
tests are intended to ensure that we dont abort due to an assertion, running the
tests in all modes is better since it also ensures that we dont crash without
assertions.  Always run these tests to ensure that we can handle invalid input
correctly.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209496 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[ARM64] Fix a bug in shuffle vector lowering to generate corect vext ISD with swapped...
Jiangning Liu [Fri, 23 May 2014 02:54:50 +0000 (02:54 +0000)]
[ARM64] Fix a bug in shuffle vector lowering to generate corect vext ISD with swapped input vectors.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209495 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAttempt to placate compilers that warn on casts between pointer-to-object and
Richard Smith [Fri, 23 May 2014 01:22:46 +0000 (01:22 +0000)]
Attempt to placate compilers that warn on casts between pointer-to-object and
pointer-to-function types.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209490 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoScalarEvolution: Fix handling of AddRecs in isKnownPredicate
Justin Bogner [Fri, 23 May 2014 00:06:56 +0000 (00:06 +0000)]
ScalarEvolution: Fix handling of AddRecs in isKnownPredicate

ScalarEvolution::isKnownPredicate() can wrongly reduce a comparison
when both the LHS and RHS are SCEVAddRecExprs. This checks that both
LHS and RHS are guarded in the case when both are SCEVAddRecExprs.

The test case is against indvars because I could not find a way to
directly test SCEV.

Patch by Sanjay Patel!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209487 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[Graph Writer] Limit the length of the graph name because Windows can't handle it.
Michael J. Spencer [Thu, 22 May 2014 23:32:18 +0000 (23:32 +0000)]
[Graph Writer] Limit the length of the graph name because Windows can't handle it.

Windows can't handle paths longer than 260 code points without \\?\. Even
with \\?\ it can't handle path components longer than 255 code points. So
limit graph names to the arbitrary length of 140. Random characters are still
added to the end, so it's ok if graph names collide.

Differential Revision: http://reviews.llvm.org/D3883

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209483 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMake these bool bitfields.
Eric Christopher [Thu, 22 May 2014 23:09:57 +0000 (23:09 +0000)]
Make these bool bitfields.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@209481 91177308-0d34-0410-b5e6-96231b3b80d8