]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/log
opencl/llvm.git
8 years agoArgumentPromotion: Propagate debug locations on calls for which arguments are promoted.
David Blaikie [Fri, 27 Jun 2014 05:32:09 +0000 (05:32 +0000)]
ArgumentPromotion: Propagate debug locations on calls for which arguments are promoted.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211872 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRevert "Revert "PR20038: DebugInfo: Inlined call sites where the caller has debug...
David Blaikie [Fri, 27 Jun 2014 05:31:49 +0000 (05:31 +0000)]
Revert "Revert "PR20038: DebugInfo: Inlined call sites where the caller has debug info but the call itself has no debug location.""

This reverts commit r211724.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211871 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoHave SystemZSelectionDAGInfo constructor take a DataLayout rather
Eric Christopher [Fri, 27 Jun 2014 05:26:28 +0000 (05:26 +0000)]
Have SystemZSelectionDAGInfo constructor take a DataLayout rather
than a target machine since it doesn't need anything past the
DataLayout.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211870 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRename getX86ConditonCode -> getX86ConditionCode
Craig Topper [Fri, 27 Jun 2014 05:18:21 +0000 (05:18 +0000)]
Rename getX86ConditonCode -> getX86ConditionCode

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211869 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoLeft out the NDEBUG in the previous checkin.
Andrew Trick [Fri, 27 Jun 2014 05:09:36 +0000 (05:09 +0000)]
Left out the NDEBUG in the previous checkin.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211867 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMachineScheduler: add some book-keeping to fix an assert.
Andrew Trick [Fri, 27 Jun 2014 04:57:05 +0000 (04:57 +0000)]
MachineScheduler: add some book-keeping to fix an assert.

Fixe for Bug 20057 - Assertion failied in llvm::SUnit* llvm::SchedBoundary::pickOnlyChoice(): Assertion `i <= (HazardRec->getMaxLookAhead() + MaxObservedStall) && "permanent hazard"'

Thanks to Chad for the test case.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211865 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoPropagate const-correctness into parseBitcodeFile()
Alp Toker [Fri, 27 Jun 2014 04:48:32 +0000 (04:48 +0000)]
Propagate const-correctness into parseBitcodeFile()

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211864 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoHave MipsSelectionDAGInfo constructor take a DataLayout rather
Eric Christopher [Fri, 27 Jun 2014 04:38:30 +0000 (04:38 +0000)]
Have MipsSelectionDAGInfo constructor take a DataLayout rather
than a target machine since it doesn't need anything past the
DataLayout.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211863 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoParseIR: don't take ownership of the MemoryBuffer
Alp Toker [Fri, 27 Jun 2014 04:33:58 +0000 (04:33 +0000)]
ParseIR: don't take ownership of the MemoryBuffer

clang was needlessly duplicating whole memory buffer contents in an attempt to
satisfy unclear ownership semantics. Let's just hide internal LLVM quirks and
present a simple non-owning interface.

The public C API preserves previous behaviour for stability.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211861 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove NVPTX subtarget dependent variables from the target machine
Eric Christopher [Fri, 27 Jun 2014 04:33:14 +0000 (04:33 +0000)]
Move NVPTX subtarget dependent variables from the target machine
to the subtarget.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211860 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoR600: Add some testcases for promote alloca pass.
Matt Arsenault [Fri, 27 Jun 2014 03:55:55 +0000 (03:55 +0000)]
R600: Add some testcases for promote alloca pass.

More complicated GEPs are skipped. Add some tests to
actually stress this skipping.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211859 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoUse the target lowering we can get off of the DAG rather than off
Eric Christopher [Fri, 27 Jun 2014 03:45:49 +0000 (03:45 +0000)]
Use the target lowering we can get off of the DAG rather than off
of the cached target machine.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211858 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSupport: update DLLCharacteristics enumeration
Saleem Abdulrasool [Fri, 27 Jun 2014 03:11:18 +0000 (03:11 +0000)]
Support: update DLLCharacteristics enumeration

Add the new AppContainer characteristic which is import for Windows Store
(Metro) compatible applications.  Add the new Control Flow Guard flag to bring
the enumeration up to date with the current values as of Windows 8.1.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211855 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSupport: tweak comment layout
Saleem Abdulrasool [Fri, 27 Jun 2014 03:11:14 +0000 (03:11 +0000)]
Support: tweak comment layout

Make the comment layout more uniform.  NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211854 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDon't force the build of toos/lto as a static lib.
Rafael Espindola [Fri, 27 Jun 2014 02:51:21 +0000 (02:51 +0000)]
Don't force the build of toos/lto as a static lib.

Any uses of tools/lto as a static lib should probably move to lib/LTO.
This was also never implemented in the configure build, so this reduces
the differences among the two.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211852 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix missing newline and simplify debug printing.
Matt Arsenault [Fri, 27 Jun 2014 02:36:59 +0000 (02:36 +0000)]
Fix missing newline and simplify debug printing.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211850 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoR600: Move load/store ReplaceNodeResults to common code.
Matt Arsenault [Fri, 27 Jun 2014 02:33:47 +0000 (02:33 +0000)]
R600: Move load/store ReplaceNodeResults to common code.

Future patches will want to custom lower loads on SI.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211848 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove the constructor for NVPTXFrameLowering into the implementation
Eric Christopher [Fri, 27 Jun 2014 02:05:24 +0000 (02:05 +0000)]
Move the constructor for NVPTXFrameLowering into the implementation
file in preparation for the subtarget move.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211847 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove unnecessary caching of the TargetMachine on NVPTXFrameLowering.
Eric Christopher [Fri, 27 Jun 2014 02:05:22 +0000 (02:05 +0000)]
Remove unnecessary caching of the TargetMachine on NVPTXFrameLowering.
Adjust the constructor accordingly.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211846 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRework the logic for setting the TargetName. This appears to
Eric Christopher [Fri, 27 Jun 2014 02:05:19 +0000 (02:05 +0000)]
Rework the logic for setting the TargetName. This appears to
be shorter and identical in goal.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211845 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove caching of the target machine in NVPTXInstrInfo and
Eric Christopher [Fri, 27 Jun 2014 01:27:08 +0000 (01:27 +0000)]
Remove caching of the target machine in NVPTXInstrInfo and
update constructor accordingly.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211840 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove comment that duplicated information in the constructor
Eric Christopher [Fri, 27 Jun 2014 01:27:06 +0000 (01:27 +0000)]
Remove comment that duplicated information in the constructor
that it's after.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211839 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove commented out code.
Eric Christopher [Fri, 27 Jun 2014 01:27:05 +0000 (01:27 +0000)]
Remove commented out code.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211838 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove extraneous parens and extraneous const cast (and fix the
Eric Christopher [Fri, 27 Jun 2014 01:27:03 +0000 (01:27 +0000)]
Remove extraneous parens and extraneous const cast (and fix the
prototype for the function to patch what we were returning).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211837 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove the subtarget dependent features from the target machine to
Eric Christopher [Fri, 27 Jun 2014 01:14:54 +0000 (01:14 +0000)]
Move the subtarget dependent features from the target machine to
the subtarget for the MSP430 target.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211836 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove uses and caches of the target machine and subtarget from
Eric Christopher [Fri, 27 Jun 2014 01:14:50 +0000 (01:14 +0000)]
Remove uses and caches of the target machine and subtarget from
both MSP430InstrInfo and MSP430RegisterInfo. Remove unused member
variable StackAlign from MSP430RegisterInfo. Update constructors
accordingly.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211835 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove caching of an unused subtarget from MSP430FrameLowering.
Eric Christopher [Fri, 27 Jun 2014 00:52:11 +0000 (00:52 +0000)]
Remove caching of an unused subtarget from MSP430FrameLowering.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211830 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[X86] AVX512: Add vbroadcasti*
Adam Nemet [Fri, 27 Jun 2014 00:43:38 +0000 (00:43 +0000)]
[X86] AVX512: Add vbroadcasti*

For now I used a separate template for these sub-vector/tuple broadcasts
rather than sharing the mem variants with avx512_int_broadcast_rm.

<rdar://problem/17402869>

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211828 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove unnecessary caching of variables by MSP430TargetLowering and
Eric Christopher [Fri, 27 Jun 2014 00:37:59 +0000 (00:37 +0000)]
Remove unnecessary caching of variables by MSP430TargetLowering and
make the constructor more general since it only needs a target
machine.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211827 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoHave MSP430SelectionDAGInfo constructor take a DataLayout rather
Eric Christopher [Fri, 27 Jun 2014 00:37:57 +0000 (00:37 +0000)]
Have MSP430SelectionDAGInfo constructor take a DataLayout rather
than a target machine since it doesn't need anything past the
DataLayout.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211826 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove all of the hexagon subtarget dependent variables from the target
Eric Christopher [Fri, 27 Jun 2014 00:27:40 +0000 (00:27 +0000)]
Move all of the hexagon subtarget dependent variables from the target
machine to the subtarget.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211824 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoHave HexagonSelectionDAGInfo take a DataLayout rather than a
Eric Christopher [Fri, 27 Jun 2014 00:18:25 +0000 (00:18 +0000)]
Have HexagonSelectionDAGInfo take a DataLayout rather than a
target machine since that's all it needs.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211822 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMake HexagonISelLowering not dependent upon a HexagonTargetMachine,
Eric Christopher [Fri, 27 Jun 2014 00:13:52 +0000 (00:13 +0000)]
Make HexagonISelLowering not dependent upon a HexagonTargetMachine,
but a normal TargetMachine and remove a few cached uses.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211821 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoReduce indentation.
Eric Christopher [Fri, 27 Jun 2014 00:13:49 +0000 (00:13 +0000)]
Reduce indentation.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211820 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove unnecessary caching of the subtarget for HexagonFrameLowering and remove the...
Eric Christopher [Fri, 27 Jun 2014 00:13:47 +0000 (00:13 +0000)]
Remove unnecessary caching of the subtarget for HexagonFrameLowering and remove the unused constructor argument.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211819 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoInstrItineraryData is already on the subtarget, no reason to
Eric Christopher [Fri, 27 Jun 2014 00:13:43 +0000 (00:13 +0000)]
InstrItineraryData is already on the subtarget, no reason to
cache it on the target as well.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211818 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[StackMaps] Enable patchpoint liveness analysis per default.
Juergen Ributzka [Thu, 26 Jun 2014 23:39:52 +0000 (23:39 +0000)]
[StackMaps] Enable patchpoint liveness analysis per default.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211817 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[Stackmaps] Remove the liveness calculation for stackmap intrinsics.
Juergen Ributzka [Thu, 26 Jun 2014 23:39:44 +0000 (23:39 +0000)]
[Stackmaps] Remove the liveness calculation for stackmap intrinsics.

There is no need to calculate the liveness information for stackmaps. The
liveness information is still available for the patchpoint intrinsic and
that is also the intended usage model.

Related to <rdar://problem/17473725>

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211816 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[RuntimeDyld] Teach MachOObjectImage to deregister itself with the debugger upon
Lang Hames [Thu, 26 Jun 2014 23:05:44 +0000 (23:05 +0000)]
[RuntimeDyld] Teach MachOObjectImage to deregister itself with the debugger upon
destruction the same way ELFObjectImage does.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211815 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRevert "Introduce a string_ostream string builder facilty"
Alp Toker [Thu, 26 Jun 2014 22:52:05 +0000 (22:52 +0000)]
Revert "Introduce a string_ostream string builder facilty"

Temporarily back out commits r211749, r211752 and r211754.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211814 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove the various Subtarget dependent members down to the subtarget
Eric Christopher [Thu, 26 Jun 2014 22:33:55 +0000 (22:33 +0000)]
Move the various Subtarget dependent members down to the subtarget
for the Sparc port. Use the same initializeSubtargetDependencies
function to handle initialization similar to the other ports to
handle dependencies.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211811 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoHave SparcSelectionDAGInfo take a DataLayout to initialize since
Eric Christopher [Thu, 26 Jun 2014 22:33:52 +0000 (22:33 +0000)]
Have SparcSelectionDAGInfo take a DataLayout to initialize since
that's all it needs.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211810 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove the storage and use of the subtarget out of the sparc frame
Eric Christopher [Thu, 26 Jun 2014 22:33:50 +0000 (22:33 +0000)]
Remove the storage and use of the subtarget out of the sparc frame
lowering code.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211809 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agofixed typo
Sanjay Patel [Thu, 26 Jun 2014 22:18:51 +0000 (22:18 +0000)]
fixed typo

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211808 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix the new LTOCodeGenerator setup in gold to parse options before using MAttrs.
Tom Roeder [Thu, 26 Jun 2014 20:43:27 +0000 (20:43 +0000)]
Fix the new LTOCodeGenerator setup in gold to parse options before using MAttrs.

This fixes a regression that made clang -flto -Wl,--plugin-opt=-mattr=+aes not
pass the "+aes" option to the LTOCodeGenerator attributes.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211804 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoGVN: Preserve invariant.load metadata
Arnold Schwaighofer [Thu, 26 Jun 2014 19:51:19 +0000 (19:51 +0000)]
GVN: Preserve invariant.load metadata

If both instructions to be replaced are marked invariant the resulting
instruction is invariant.

rdar://13358910

Fix by Erik Eckstein!

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211801 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove extraneous includes from the target machines.
Eric Christopher [Thu, 26 Jun 2014 19:30:05 +0000 (19:30 +0000)]
Remove extraneous includes from the target machines.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211800 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove all of the ARM subtarget features down onto the subtarget
Eric Christopher [Thu, 26 Jun 2014 19:30:02 +0000 (19:30 +0000)]
Move all of the ARM subtarget features down onto the subtarget
rather than the target machine.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211799 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove the frame lowering constructors out of line to avoid circular
Eric Christopher [Thu, 26 Jun 2014 19:29:59 +0000 (19:29 +0000)]
Move the frame lowering constructors out of line to avoid circular
includes.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211798 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoChanged Phab 'CC' to 'subscriber'; fixed typo
Sanjay Patel [Thu, 26 Jun 2014 18:12:42 +0000 (18:12 +0000)]
Changed Phab 'CC' to 'subscriber'; fixed typo

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211793 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoR600/SI: Add FP mode bits to binary.
Matt Arsenault [Thu, 26 Jun 2014 17:22:30 +0000 (17:22 +0000)]
R600/SI: Add FP mode bits to binary.

The default rounding mode to initialize the mode register needs
to be reported to the runtime. Fill in other bits a kernel
may be interested in setting for future use.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211791 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSilencing a warning about isZExtFree hiding an inherited virtual function. No functio...
Aaron Ballman [Thu, 26 Jun 2014 13:45:47 +0000 (13:45 +0000)]
Silencing a warning about isZExtFree hiding an inherited virtual function. No functional change intended.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211783 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSilence a warning due to a comparison between signed and unsigned.
Andrea Di Biagio [Thu, 26 Jun 2014 13:41:10 +0000 (13:41 +0000)]
Silence a warning due to a comparison between signed and unsigned.

No functional change intended.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211782 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd support for ppc64/power8 as a host
Will Schmidt [Thu, 26 Jun 2014 13:37:03 +0000 (13:37 +0000)]
Add support for ppc64/power8 as a host

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211781 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoadd ppc64/pwr8 as target
Will Schmidt [Thu, 26 Jun 2014 13:36:19 +0000 (13:36 +0000)]
add ppc64/pwr8 as target
includes handling DIR_PWR8 where appropriate
The P7Model Itinerary is currently tied in for use under the P8Model, and will be updated later.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211779 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdded parsing co-processor names starting with "cr"
Renato Golin [Thu, 26 Jun 2014 13:10:53 +0000 (13:10 +0000)]
Added parsing co-processor names starting with "cr"

Additional compliant GAS names for coprocessor register name
are enabled for all instruction with parameter MCK_CoprocReg:
LDC,LDC2,STC,STC2,CDP,CDP2,MCR,MCR2,MCRR,MCRR2,MRC,MRC2,MRRC,MRRC2

Patch by Andrey Kuharev.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211776 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[X86] Improve the selection of SSE3/AVX addsub instructions.
Andrea Di Biagio [Thu, 26 Jun 2014 10:45:21 +0000 (10:45 +0000)]
[X86] Improve the selection of SSE3/AVX addsub instructions.

This patch teaches the backend how to canonicalize a shuffle vectors
according to the rule:

 - (shuffle (FADD A, B), (FSUB A, B), Mask) ->
       (shuffle (FSUB A, -B), (FADD A, -B), Mask)

Where 'Mask' is:
  <0,5,2,7>            ;; for v4f32 and v4f64 shuffles.
  <0,3>                ;; for v2f64 shuffles.
  <0,9,2,11,4,13,6,15> ;; for v8f32 shuffles.

In general, ISel only knows how to pattern-match a canonical
'fadd + fsub + blendi' dag node sequence into an ADDSUB instruction.

This new rule allows to convert a non-canonical dag sequence into a
canonical one that will be matched by a single ADDSUB at ISel stage.

The idea of converting a non-canonical ADDSUB into a canonical one by
swapping the first two operands of the shuffle, and then negating the
second operand of the FADD and FSUB, was originally proposed by Hal Finkel.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211771 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoThis patch removed duplicate code for matching patterns
Dinesh Dwivedi [Thu, 26 Jun 2014 08:57:33 +0000 (08:57 +0000)]
This patch removed duplicate code for matching patterns
which are now handled in SimplifyUsingDistributiveLaws()
(after r211261)

Differential Revision: http://reviews.llvm.org/D4253

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211768 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdded instruction combine to transform few more negative values addition to subtracti...
Dinesh Dwivedi [Thu, 26 Jun 2014 05:40:22 +0000 (05:40 +0000)]
Added instruction combine to transform few more negative values addition to subtraction (Part 2)
This patch enables transforms for

(x + (~(y | c) + 1)   -->   x - (y | c) if c is even

Differential Revision: http://reviews.llvm.org/D4209

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211765 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoGlobalOpt: Don't optimize thread_local for initializers
David Majnemer [Thu, 26 Jun 2014 03:02:19 +0000 (03:02 +0000)]
GlobalOpt: Don't optimize thread_local for initializers

Folding a reference to a thread_local variable into another global
variable's initializer is very problematic, there is no relocation that
exists to represent such an access.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211762 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoR600: Fix vector FMA
Matt Arsenault [Thu, 26 Jun 2014 01:28:05 +0000 (01:28 +0000)]
R600: Fix vector FMA

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211757 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRemove forward decl of SmallVectorImpl now that we have the header
Reid Kleckner [Thu, 26 Jun 2014 01:03:20 +0000 (01:03 +0000)]
Remove forward decl of SmallVectorImpl now that we have the header

Follow up to r211749.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211754 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDon't build switch tables for dllimport and TLS variables in GEPs
Hans Wennborg [Thu, 26 Jun 2014 00:30:52 +0000 (00:30 +0000)]
Don't build switch tables for dllimport and TLS variables in GEPs

This is a follow-up to r211331, which failed to notice that we were
returning early from ValidLookupTableConstant for GEPs.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211753 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMSVC build fix following r211749
Alp Toker [Thu, 26 Jun 2014 00:25:41 +0000 (00:25 +0000)]
MSVC build fix following r211749

Avoid strndup()

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211752 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[X86] AVX512: Fix asm syntax for packed vcmp
Adam Nemet [Thu, 26 Jun 2014 00:21:12 +0000 (00:21 +0000)]
[X86] AVX512: Fix asm syntax for packed vcmp

The *_alt defs for vcmp are used by the InstParser (the asm string in the main
def is used by the InstPrinter) .  The former was accepting vector registers
as destination rather than mask registers.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211750 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoIntroduce a string_ostream string builder facilty
Alp Toker [Thu, 26 Jun 2014 00:00:48 +0000 (00:00 +0000)]
Introduce a string_ostream string builder facilty

string_ostream is a safe and efficient string builder that combines opaque
stack storage with a built-in ostream interface.

small_string_ostream<bytes> additionally permits an explicit stack storage size
other than the default 128 bytes to be provided. Beyond that, storage is
transferred to the heap.

This convenient class can be used in most places an
std::string+raw_string_ostream pair or SmallString<>+raw_svector_ostream pair
would previously have been used, in order to guarantee consistent access
without byte truncation.

The patch also converts much of LLVM to use the new facility. These changes
include several probable bug fixes for truncated output, a programming error
that's no longer possible with the new interface.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211749 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFor CrashRecoveryContext::RunSafelyOnThread, propagate Darwin's PRIO_DARWIN_BG to...
Argyrios Kyrtzidis [Wed, 25 Jun 2014 23:54:50 +0000 (23:54 +0000)]
For CrashRecoveryContext::RunSafelyOnThread, propagate Darwin's PRIO_DARWIN_BG to the new thread if it is
set on the calling thread.

This allows libclang's indexing threads to propagate their priority to the clang module building threads.

rdar://17459872

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211747 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix typo
Michael Liao [Wed, 25 Jun 2014 23:39:08 +0000 (23:39 +0000)]
Fix typo

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211744 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[FastISel][X86] More refactoring of select lowering and XALU folding. NFC.
Juergen Ributzka [Wed, 25 Jun 2014 22:50:59 +0000 (22:50 +0000)]
[FastISel][X86] More refactoring of select lowering and XALU folding. NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211740 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoThe includes were sorted. Revert r210578.
Eric Christopher [Wed, 25 Jun 2014 22:36:37 +0000 (22:36 +0000)]
The includes were sorted. Revert r210578.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211737 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[FastISel][X86] Refactor XALU folding. NFC.
Juergen Ributzka [Wed, 25 Jun 2014 22:17:23 +0000 (22:17 +0000)]
[FastISel][X86] Refactor XALU folding. NFC.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211735 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMention that Phabricator users should subscribe to *-commits
Reid Kleckner [Wed, 25 Jun 2014 20:25:21 +0000 (20:25 +0000)]
Mention that Phabricator users should subscribe to *-commits

This probably explains why a lot of messages get lost for first time
Phabricator users.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211731 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[FastISel][X86] Only fold the cmp into the select when both instructions are in the...
Juergen Ributzka [Wed, 25 Jun 2014 20:06:12 +0000 (20:06 +0000)]
[FastISel][X86] Only fold the cmp into the select when both instructions are in the same basic block.

If the cmp is in a different basic block, then it is possible that not all
operands of that compare have defined registers. This can happen when one of
the operands to the cmp is a load and the load gets folded into the cmp. In
this case FastISel will skip the load instruction and the vreg is never
defined.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211730 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMerge the used symbol scanning of MCObjectStreamer and RecordStreamer.
Rafael Espindola [Wed, 25 Jun 2014 18:37:33 +0000 (18:37 +0000)]
Merge the used symbol scanning of MCObjectStreamer and RecordStreamer.

This completes the refactoring of RecordStreamer.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211727 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRevert "PR20038: DebugInfo: Inlined call sites where the caller has debug info but...
David Blaikie [Wed, 25 Jun 2014 18:20:54 +0000 (18:20 +0000)]
Revert "PR20038: DebugInfo: Inlined call sites where the caller has debug info but the call itself has no debug location."

This reverts commit r211723.

Breaks the ASan/compiler-rt build... guess I didn't test very far at all
:/.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211724 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoPR20038: DebugInfo: Inlined call sites where the caller has debug info but the call...
David Blaikie [Wed, 25 Jun 2014 18:03:10 +0000 (18:03 +0000)]
PR20038: DebugInfo: Inlined call sites where the caller has debug info but the call itself has no debug location.

This situation does bad things when inlined, so I've fixed Clang not to
produce inlinable call sites without locations when the caller has debug
info (in the one case where I could find that this occurred). This
updates the PR20038 test case to be what clang now produces, and readds
the assertion that had to be removed due to this bug.

I've also beefed up the debug info verifier to help diagnose these
issues in the future, and I hope to add checks to the inliner to just
assert-fail if it encounters this situation. If, in the future, we
decide we have to cope with this situation, the right thing to do is
probably to just remove all the DebugLocs from the inlined instructions.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211723 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd Rpass-missed and Rpass-analysis reports to the loop vectorizer. The remarks give...
Tyler Nowicki [Wed, 25 Jun 2014 17:50:15 +0000 (17:50 +0000)]
Add Rpass-missed and Rpass-analysis reports to the loop vectorizer. The remarks give the vector width of vectorized loops and a brief analysis of loops that fail to be vectorized. For example, an analysis will be generated for loops containing control flow that cannot be simplified to a select. The optimization remarks also give the debug location of expressions that cannot be vectorized, for example the location of an unvectorizable call.

Reviewed by: Arnold Schwaighofer

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211721 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[X86] Always prefer to lower a VECTOR_SHUFFLE into a BLENDI instead of SHUFP (or...
Andrea Di Biagio [Wed, 25 Jun 2014 17:41:58 +0000 (17:41 +0000)]
[X86] Always prefer to lower a VECTOR_SHUFFLE into a BLENDI instead of SHUFP (or VPERM2X128).

This patch teaches method 'LowerVECTOR_SHUFFLE' to give higher precedence to
the check for 'isBlendMask'; the idea is that, when possible, we should firstly
check if a shuffle performs a blend, and in case, try to lower it into a BLENDI
instead of selecting a SHUFP or (worse) a VPERM2X128.

In general:
 - AVX VBLENDPS/D always have better latency and throughput than VPERM2F128;
 - BLENDPS/D instructions tend to always have better 'reciprocal throughput'
   than the equivalent SHUFPS/D;
 - Both BLENDPS/D and SHUFPS/D are often decoded into the same number of
   m-ops; however, a m-op obtained from a BLENDPS/D can be scheduled to more
   than one execution port.

This patch:
 - Moves the check for 'isBlendMask' immediately before the check for
   'isSHUFPMask' within method 'LowerVECTOR_SHUFFLE';
 - Updates existing tests for sse/avx shuffle/blend instructions to verify
   that we select (v)blendps/d when possible (instead of (v)shufps/d or
   vperm2f128).

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211720 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix indentation.
Juergen Ributzka [Wed, 25 Jun 2014 16:49:37 +0000 (16:49 +0000)]
Fix indentation.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211717 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix the build.
Rafael Espindola [Wed, 25 Jun 2014 15:47:36 +0000 (15:47 +0000)]
Fix the build.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211715 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoMove expression visitation logic up to MCStreamer.
Rafael Espindola [Wed, 25 Jun 2014 15:45:33 +0000 (15:45 +0000)]
Move expression visitation logic up to MCStreamer.

Remove the duplicate from MCRecordStreamer. No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211714 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd some test files for r211710.
Eli Bendersky [Wed, 25 Jun 2014 15:41:39 +0000 (15:41 +0000)]
Add some test files for r211710.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211711 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRename loop unrolling and loop vectorizer metadata to have a common prefix.
Eli Bendersky [Wed, 25 Jun 2014 15:41:00 +0000 (15:41 +0000)]
Rename loop unrolling and loop vectorizer metadata to have a common prefix.

[LLVM part]

These patches rename the loop unrolling and loop vectorizer metadata
such that they have a common 'llvm.loop.' prefix.  Metadata name
changes:

llvm.vectorizer.* => llvm.loop.vectorizer.*
llvm.loopunroll.* => llvm.loop.unroll.*

This was a suggestion from an earlier review
(http://reviews.llvm.org/D4090) which added the loop unrolling
metadata.

Patch by Mark Heffernan.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211710 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix = delete in MSVC build from r211705
JF Bastien [Wed, 25 Jun 2014 15:38:02 +0000 (15:38 +0000)]
Fix = delete in MSVC build from r211705

MSVC doesn't support = delete yet, use LLVM_DELETED_FUNCTION instead.

Related to: http://reviews.llvm.org/D3390

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211709 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSimplify the visitation of target expressions. No functionality change.
Rafael Espindola [Wed, 25 Jun 2014 15:29:54 +0000 (15:29 +0000)]
Simplify the visitation of target expressions. No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211707 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRandom Number Generator (llvm)
JF Bastien [Wed, 25 Jun 2014 15:21:42 +0000 (15:21 +0000)]
Random Number Generator (llvm)

Provides an abstraction for a random number generator (RNG) that produces a stream of pseudo-random numbers.
The current implementation uses C++11 facilities and is therefore not cryptographically secure.

The RNG is salted with the text of the current command line invocation.
In addition, a user may specify a seed (reproducible builds).

In clang, the seed can be set via

-frandom-seed=X
In the back end, the seed can be set via

-rng-seed=X
This is the llvm part of the patch.
clang part: D3391

URL: http://reviews.llvm.org/D3390
Author: yln

I'm landing this for the second time, it broke Windows bots the first time around.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211705 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoSimplify AddValueSymbols. No functionality change.
Rafael Espindola [Wed, 25 Jun 2014 14:42:14 +0000 (14:42 +0000)]
Simplify AddValueSymbols. No functionality change.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211701 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[msan] Fix bad interaction between with-calls mode and chained origin tracking.
Evgeniy Stepanov [Wed, 25 Jun 2014 14:41:57 +0000 (14:41 +0000)]
[msan] Fix bad interaction between with-calls mode and chained origin tracking.

Origin history should only be recorded for uninitialized values, because it is
meaningless otherwise. This change moves __msan_chain_origin to the runtime
library side and makes it conditional on the corresponding shadow value.

Previous code was correct, but _very_ inefficient.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211700 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoDon't leak a file descriptor.
Rafael Espindola [Wed, 25 Jun 2014 14:35:59 +0000 (14:35 +0000)]
Don't leak a file descriptor.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211699 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoCode cleanup.
Logan Chien [Wed, 25 Jun 2014 13:46:17 +0000 (13:46 +0000)]
Code cleanup.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211697 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoAdd Polly to the ignored trees.
Chandler Carruth [Wed, 25 Jun 2014 13:13:36 +0000 (13:13 +0000)]
Add Polly to the ignored trees.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211695 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[x86] Add intrinsics for the pshufd, pshuflw, and pshufhw instructions.
Chandler Carruth [Wed, 25 Jun 2014 13:12:54 +0000 (13:12 +0000)]
[x86] Add intrinsics for the pshufd, pshuflw, and pshufhw instructions.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211694 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoRe-apply r211399, "Generate native unwind info on Win64" with a fix to ignore SEH...
NAKAMURA Takumi [Wed, 25 Jun 2014 12:41:52 +0000 (12:41 +0000)]
Re-apply r211399, "Generate native unwind info on Win64" with a fix to ignore SEH pseudo ops in X86 JIT emitter.

--
This patch enables LLVM to emit Win64-native unwind info rather than
DWARF CFI.  It handles all corner cases (I hope), including stack
realignment.

Because the unwind info is not flexible enough to describe stack frames
with a gap of unknown size in the middle, such as the one caused by
stack realignment, I modified register spilling code to place all spills
into the fixed frame slots, so that they can be accessed relative to the
frame pointer.

Patch by Vadim Chugunov!

Reviewed By: rnk

Differential Revision: http://reviews.llvm.org/D4081

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211691 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoReformat.
NAKAMURA Takumi [Wed, 25 Jun 2014 12:40:56 +0000 (12:40 +0000)]
Reformat.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211689 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[X86] Add target combine rule to select ADDSUB instructions from a build_vector
Andrea Di Biagio [Wed, 25 Jun 2014 10:02:21 +0000 (10:02 +0000)]
[X86] Add target combine rule to select ADDSUB instructions from a build_vector

This patch teaches the backend how to combine a build_vector that implements
an 'addsub' between packed float vectors into a sequence of vector add
and vector sub followed by a VSELECT.

The new VSELECT is expected to be lowered into a BLENDI.
At ISel stage, the sequence 'vector add + vector sub + BLENDI' is
pattern-matched against ISel patterns added at r211427 to select
'addsub' instructions.
Added three more ISel patterns for ADDSUB.

Added test sse3-avx-addsub-2.ll to verify that we correctly emit 'addsub'
instructions.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211679 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFactor out part of LICM::sink into a helper function.
Evgeniy Stepanov [Wed, 25 Jun 2014 09:17:21 +0000 (09:17 +0000)]
Factor out part of LICM::sink into a helper function.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211678 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix unresolved symbols when loading gold plugin
Alexey Volkov [Wed, 25 Jun 2014 08:04:58 +0000 (08:04 +0000)]
Fix unresolved symbols when loading gold plugin

Differential Revision: http://reviews.llvm.org/D4275

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211675 91177308-0d34-0410-b5e6-96231b3b80d8

8 years ago[LICM] Don't create more than one copy of an instruction per loop exit block when...
Evgeniy Stepanov [Wed, 25 Jun 2014 07:54:58 +0000 (07:54 +0000)]
[LICM] Don't create more than one copy of an instruction per loop exit block when sinking.

Fixes exponential compilation complexity in PR19835, caused by
LICM::sink not handling the following pattern well:

f = op g
e = op f, g
d = op e
c = op d, e
b = op c
a = op b, c

When an instruction with N uses is sunk, each of its operands gets N
new uses (all of them - phi nodes). In the example above, if a had 1
use, c would have 2, e would have 4, and g would have 8.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211673 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix another asserting method in the null streamer.
Rafael Espindola [Wed, 25 Jun 2014 05:37:58 +0000 (05:37 +0000)]
Fix another asserting method in the null streamer.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211668 91177308-0d34-0410-b5e6-96231b3b80d8

8 years agoFix a regression from r211653.
Rafael Espindola [Wed, 25 Jun 2014 05:31:22 +0000 (05:31 +0000)]
Fix a regression from r211653.

The method was empty in the null streamer but I mistakenly replaced it with
the aborting one in MCStreamer.

git-svn-id: https://llvm.org/svn/llvm-project/llvm/trunk@211666 91177308-0d34-0410-b5e6-96231b3b80d8