opencl/llvm.git
2014-06-27 David BlaikieRevert "Revert "Revert "PR20038: DebugInfo: Inlined...
2014-06-27 David BlaikieArgumentPromotion: Propagate debug locations on calls...
2014-06-27 David BlaikieRevert "Revert "PR20038: DebugInfo: Inlined call sites...
2014-06-27 Eric ChristopherHave SystemZSelectionDAGInfo constructor take a DataLay...
2014-06-27 Craig TopperRename getX86ConditonCode -> getX86ConditionCode
2014-06-27 Andrew TrickLeft out the NDEBUG in the previous checkin.
2014-06-27 Andrew TrickMachineScheduler: add some book-keeping to fix an assert.
2014-06-27 Alp TokerPropagate const-correctness into parseBitcodeFile()
2014-06-27 Eric ChristopherHave MipsSelectionDAGInfo constructor take a DataLayout...
2014-06-27 Alp TokerParseIR: don't take ownership of the MemoryBuffer
2014-06-27 Eric ChristopherMove NVPTX subtarget dependent variables from the targe...
2014-06-27 Matt ArsenaultR600: Add some testcases for promote alloca pass.
2014-06-27 Eric ChristopherUse the target lowering we can get off of the DAG rathe...
2014-06-27 Saleem AbdulrasoolSupport: update DLLCharacteristics enumeration
2014-06-27 Saleem AbdulrasoolSupport: tweak comment layout
2014-06-27 Rafael EspindolaDon't force the build of toos/lto as a static lib.
2014-06-27 Matt ArsenaultFix missing newline and simplify debug printing.
2014-06-27 Matt ArsenaultR600: Move load/store ReplaceNodeResults to common...
2014-06-27 Eric ChristopherMove the constructor for NVPTXFrameLowering into the...
2014-06-27 Eric ChristopherRemove unnecessary caching of the TargetMachine on...
2014-06-27 Eric ChristopherRework the logic for setting the TargetName. This appea...
2014-06-27 Eric ChristopherRemove caching of the target machine in NVPTXInstrInfo and
2014-06-27 Eric ChristopherRemove comment that duplicated information in the const...
2014-06-27 Eric ChristopherRemove commented out code.
2014-06-27 Eric ChristopherRemove extraneous parens and extraneous const cast...
2014-06-27 Eric ChristopherMove the subtarget dependent features from the target...
2014-06-27 Eric ChristopherRemove uses and caches of the target machine and subtar...
2014-06-27 Eric ChristopherRemove caching of an unused subtarget from MSP430FrameL...
2014-06-27 Adam Nemet[X86] AVX512: Add vbroadcasti*
2014-06-27 Eric ChristopherRemove unnecessary caching of variables by MSP430Target...
2014-06-27 Eric ChristopherHave MSP430SelectionDAGInfo constructor take a DataLayo...
2014-06-27 Eric ChristopherMove all of the hexagon subtarget dependent variables...
2014-06-27 Eric ChristopherHave HexagonSelectionDAGInfo take a DataLayout rather...
2014-06-27 Eric ChristopherMake HexagonISelLowering not dependent upon a HexagonTa...
2014-06-27 Eric ChristopherReduce indentation.
2014-06-27 Eric ChristopherRemove unnecessary caching of the subtarget for Hexagon...
2014-06-27 Eric ChristopherInstrItineraryData is already on the subtarget, no...
2014-06-26 Juergen Ributzka[StackMaps] Enable patchpoint liveness analysis per...
2014-06-26 Juergen Ributzka[Stackmaps] Remove the liveness calculation for stackma...
2014-06-26 Lang Hames[RuntimeDyld] Teach MachOObjectImage to deregister...
2014-06-26 Alp TokerRevert "Introduce a string_ostream string builder facilty"
2014-06-26 Eric ChristopherMove the various Subtarget dependent members down to...
2014-06-26 Eric ChristopherHave SparcSelectionDAGInfo take a DataLayout to initial...
2014-06-26 Eric ChristopherRemove the storage and use of the subtarget out of...
2014-06-26 Sanjay Patelfixed typo
2014-06-26 Tom RoederFix the new LTOCodeGenerator setup in gold to parse...
2014-06-26 Arnold SchwaighoferGVN: Preserve invariant.load metadata
2014-06-26 Eric ChristopherRemove extraneous includes from the target machines.
2014-06-26 Eric ChristopherMove all of the ARM subtarget features down onto the...
2014-06-26 Eric ChristopherMove the frame lowering constructors out of line to...
2014-06-26 Sanjay PatelChanged Phab 'CC' to 'subscriber'; fixed typo
2014-06-26 Matt ArsenaultR600/SI: Add FP mode bits to binary.
2014-06-26 Aaron BallmanSilencing a warning about isZExtFree hiding an inherite...
2014-06-26 Andrea Di BiagioSilence a warning due to a comparison between signed...
2014-06-26 Will SchmidtAdd support for ppc64/power8 as a host
2014-06-26 Will Schmidtadd ppc64/pwr8 as target
2014-06-26 Renato GolinAdded parsing co-processor names starting with "cr"
2014-06-26 Andrea Di Biagio[X86] Improve the selection of SSE3/AVX addsub instruct...
2014-06-26 Dinesh DwivediThis patch removed duplicate code for matching patterns
2014-06-26 Dinesh DwivediAdded instruction combine to transform few more negativ...
2014-06-26 David MajnemerGlobalOpt: Don't optimize thread_local for initializers
2014-06-26 Matt ArsenaultR600: Fix vector FMA
2014-06-26 Reid KlecknerRemove forward decl of SmallVectorImpl now that we...
2014-06-26 Hans WennborgDon't build switch tables for dllimport and TLS variabl...
2014-06-26 Alp TokerMSVC build fix following r211749
2014-06-26 Adam Nemet[X86] AVX512: Fix asm syntax for packed vcmp
2014-06-26 Alp TokerIntroduce a string_ostream string builder facilty
2014-06-25 Argyrios KyrtzidisFor CrashRecoveryContext::RunSafelyOnThread, propagate...
2014-06-25 Michael LiaoFix typo
2014-06-25 Juergen Ributzka[FastISel][X86] More refactoring of select lowering...
2014-06-25 Eric ChristopherThe includes were sorted. Revert r210578.
2014-06-25 Juergen Ributzka[FastISel][X86] Refactor XALU folding. NFC.
2014-06-25 Reid KlecknerMention that Phabricator users should subscribe to...
2014-06-25 Juergen Ributzka[FastISel][X86] Only fold the cmp into the select when...
2014-06-25 Rafael EspindolaMerge the used symbol scanning of MCObjectStreamer...
2014-06-25 David BlaikieRevert "PR20038: DebugInfo: Inlined call sites where...
2014-06-25 David BlaikiePR20038: DebugInfo: Inlined call sites where the caller...
2014-06-25 Tyler NowickiAdd Rpass-missed and Rpass-analysis reports to the...
2014-06-25 Andrea Di Biagio[X86] Always prefer to lower a VECTOR_SHUFFLE into...
2014-06-25 Juergen RibutzkaFix indentation.
2014-06-25 Rafael EspindolaFix the build.
2014-06-25 Rafael EspindolaMove expression visitation logic up to MCStreamer.
2014-06-25 Eli BenderskyAdd some test files for r211710.
2014-06-25 Eli BenderskyRename loop unrolling and loop vectorizer metadata...
2014-06-25 JF BastienFix = delete in MSVC build from r211705
2014-06-25 Rafael EspindolaSimplify the visitation of target expressions. No funct...
2014-06-25 JF BastienRandom Number Generator (llvm)
2014-06-25 Rafael EspindolaSimplify AddValueSymbols. No functionality change.
2014-06-25 Evgeniy Stepanov[msan] Fix bad interaction between with-calls mode...
2014-06-25 Rafael EspindolaDon't leak a file descriptor.
2014-06-25 Logan ChienCode cleanup.
2014-06-25 Chandler CarruthAdd Polly to the ignored trees.
2014-06-25 Chandler Carruth[x86] Add intrinsics for the pshufd, pshuflw, and pshuf...
2014-06-25 NAKAMURA TakumiRe-apply r211399, "Generate native unwind info on Win64...
2014-06-25 NAKAMURA TakumiReformat.
2014-06-25 Andrea Di Biagio[X86] Add target combine rule to select ADDSUB instruct...
2014-06-25 Evgeniy StepanovFactor out part of LICM::sink into a helper function.
2014-06-25 Alexey VolkovFix unresolved symbols when loading gold plugin
2014-06-25 Evgeniy Stepanov[LICM] Don't create more than one copy of an instructio...
2014-06-25 Rafael EspindolaFix another asserting method in the null streamer.
next