opencl/llvm.git
2013-09-17 Adrian Prantlmention command line parameters
2013-09-17 Adrian Prantlsimplify expression
2013-09-16 Adrian PrantlBe sure we run ARM tests only when an ARM backend is...
2013-09-16 Adrian PrantlDebug info: Fix PR16736 and rdar://problem/14990587.
2013-09-16 Matt ArsenaultMemCpyOptimizer: Use max legal int size instead of...
2013-09-16 Preston GurdAdd Atom Silvermont (slm) tests
2013-09-16 Jakub StaszakUse reference instead of copy.
2013-09-16 Jordan Rose[CMake] Hack GetSVN.cmake to handle unusual terminals.
2013-09-16 Krzysztof ParzyszekAdd testcase for r190631
2013-09-16 Tim NorthoverTableGen: fix constness of new comparison function.
2013-09-16 Bill Schmidt[PowerPC] Fix PR17155 - Ignore COPY_TO_REGCLASS during...
2013-09-16 Tim NorthoverTableGen: give asm match classes deterministic order.
2013-09-16 Tim NorthoverAsmMatcher: emit subtarget feature enum in deterministi...
2013-09-16 Arnold SchwaighoferDon't vectorize if there are outside loop users of...
2013-09-16 Evgeniy Stepanov[msan] Check return value of main().
2013-09-16 Vladimir MedicThis patch implements Mips load/store instructions...
2013-09-16 Benjamin KramerARM: Deduplicate ConstantPoolValues.
2013-09-16 Daniel SandersFix the build for git repositories with multiple remotes.
2013-09-16 Richard Sandiford[SystemZ] Improve extload handling
2013-09-16 Craig TopperMake F16C feature flag imply AVX rather than just check...
2013-09-16 Peter CollingbourneImplement function prefix data as an IR feature.
2013-09-15 Hal FinkelPPC: Don't restrict lvsl generation to after type legal...
2013-09-15 Benjamin KramerReplace some unnecessary vector copies with references.
2013-09-15 Benjamin KramerELF: Add support for the exclude section bit for gas...
2013-09-15 David MajnemerMC: Add support for '?' flags in .section directives
2013-09-15 Kai NackeFix alignment of unwind data.
2013-09-15 Kai NackeGenerate IMAGE_REL_AMD64_ADDR32NB relocations for SEH
2013-09-15 Hal FinkelRevert r190764: PPC: Don't restrict lvsl generation...
2013-09-15 Hal FinkelPPC: Don't restrict lvsl generation to after type legal...
2013-09-15 Hal FinkelPrevent assert in CombinerGlobalAA with null values
2013-09-15 Reed KotlerExpand the mask capability for deciding which functions...
2013-09-14 Benjamin KramerRemove unused StringRef that no compiler warned about...
2013-09-14 Ben LangmuirAdd the remaining Intel SHA instructions
2013-09-14 Robert WilhelmFix spelling.
2013-09-14 Robert WilhelmFix spelling.
2013-09-14 Chandler CarruthRemove the long, long defunct IR block placement pass.
2013-09-14 Zoran JovanovicFixed bug when generating Load Upper Immediate microMIP...
2013-09-14 Zoran JovanovicSupport for microMIPS DIV instructions.
2013-09-14 Zoran JovanovicSupport for misc microMIPS instructions.
2013-09-14 Matt ArsenaultAdd missing CHECK-LABEL
2013-09-14 Matt ArsenaultAdd test for untested path in SimplifyCFG
2013-09-14 Daniel Dunbar[lit] Add an --output option, for writing results in...
2013-09-13 Filip PizloMake PrettyStackTraceEntry use ManagedStatic for its...
2013-09-13 Hal FinkelAdd missing break statement in PPCISelLowering
2013-09-13 Preston GurdAdds support for Atom Silvermont (SLM) - -march=slm
2013-09-13 Quentin Colombet[Peephole] Rewrite copies to avoid cross register banks...
2013-09-13 Benjamin KramerAdd warn_unused_result to empty() on various containers.
2013-09-13 Nuno Lopestypo fix: use BUILD_ARCHIVE to build .a libs and not...
2013-09-13 Amaury de la... Fix tests for hasFPARMv8 name change (r190692)
2013-09-13 Joey Gouly[ARMv8] Change hasV8Fp to hasFPARMv8, and other command...
2013-09-13 Evgeniy Stepanov[msan] Add source file:line to stack origin reports.
2013-09-13 Daniel SandersFix build failure reported by Tobias Markmann in bug...
2013-09-13 Joey Gouly[ARMv8] Emit the proper .fpu directive.
2013-09-13 Amaury de la... Add "native" to config.available_features, to make...
2013-09-13 Patrik HagglundFix for executing AutoRegen.sh. Revert a part of r187209.
2013-09-13 Zoran JovanovicTest commit to verify that commit access works.
2013-09-13 Richard Sandiford[SystemZ] Use getTarget{Insert,Extract}Subreg rather...
2013-09-13 Richard Sandiford[SystemZ] Try to fold shifts into TMxx
2013-09-13 Duncan SandsAvoid a compiler warning about Found not being used...
2013-09-13 Tim NorthoverAArch64: use RegisterOperand for NEON registers.
2013-09-13 Craig TopperMove operator to end of previous line to match coding...
2013-09-13 Eric ChristopherAdd initial support for handling gnu style pubnames...
2013-09-13 Eric ChristopherReformat and hoist section grabbing to top level.
2013-09-12 Vincent LejeuneR600: Move clamp handling code to R600IselLowering.cpp
2013-09-12 Vincent LejeuneR600: Move code handling literal folding into R600ISelL...
2013-09-12 Vincent LejeuneR600: Move fabs/fneg/sel folding logic into PostProcessIsel
2013-09-12 Chandler CarruthRemove an unused variable, fixing -Werror build with...
2013-09-12 Hal FinkelRemove unnecessary TBAA metadata from r190636's test...
2013-09-12 Hal FinkelFix PPC ABI for ByVal structs with vector members
2013-09-12 Joe AbbeyPatch provide by Tom Roeder!
2013-09-12 Krzysztof ParzyszekIn AliasSetTracker, do not change the alias set to...
2013-09-12 Hal FinkelMake the PPC fast-math sqrt expansion safe at 0
2013-09-12 Roman DivackyImplement asm support for a few PowerPC bookIII that...
2013-09-12 Filip PizloThis switches CrashRecoveryContext to using ManagedStat...
2013-09-12 Ben LangmuirPartial support for Intel SHA Extensions (sha1rnds4)
2013-09-12 Hal FinkelMark PPC MFTB and DST (and friends) as deprecated
2013-09-12 Joey GoulySomehow this important part of the patch, where I actua...
2013-09-12 Joey Gouly[LTO] Fix the LTO tool, after my API breakage.
2013-09-12 Elena DemikhovskyLLVM interpreter: added a test for insert- extract...
2013-09-12 Elena DemikhovskyLLVM Interpreter: implementation of "insertvalue" and...
2013-09-12 Joey GoulyAdd an instruction deprecation feature to TableGen.
2013-09-12 Elena DemikhovskyAVX-512: implemented extractelement with variable index.
2013-09-12 Alexey SamsonovFixup for r190409: add dep on LZMA only if CMake is...
2013-09-12 Hal FinkelPPC: Enable aggressive anti-dependency breaking
2013-09-12 Hal FinkelFix crash in AggressiveAntiDepBreaker with empty Critic...
2013-09-12 Tom StellardR600/SI: expose TBUFFER_STORE_FORMAT_* for OpenGL trans...
2013-09-12 Tom StellardR600: Don't use trans slot for instructions that read...
2013-09-12 Rui UeyamaTypo fixes.
2013-09-12 Matt ArsenaultMove variable under condition where it is used
2013-09-12 Matt ArsenaultFix comment to match what the assert actually enforces
2013-09-12 Matt ArsenaultRemove pointless assertion after r190376
2013-09-11 Hal FinkelGreatly simplify the PPC A2 scheduling itinerary
2013-09-11 Hal FinkelEnable MI scheduling (and CodeGen AA) by default for...
2013-09-11 Jordan Rose[CMake] Update GetSVN.cmake to use LLVM version control...
2013-09-11 Nick LewyckyFix anachronism/typo in syntax of declaration of llvm...
2013-09-11 Bill WendlingUse the appropriate return type for the compact unwind...
2013-09-11 Hal FinkelImplement TTI getUnrollingPreferences for PowerPC
2013-09-11 Bill WendlingMove into an anonymous namespace and closer to where...
2013-09-11 Manman RenDebug info: add more comments.
2013-09-11 Hal FinkelAdd getUnrollingPreferences to TTI
next