opencl/llvm.git
2014-05-29 Adrian PrantlDebug Info: Remove unused code. The MInsn of an _abstra...
2014-05-29 Rafael EspindolaRename alias variables to make it easier to add new...
2014-05-29 Rafael Espindola[PPC] Use alias symbols in address computation.
2014-05-29 Rafael EspindolaAdd a test showing the ppc code sequence for getting...
2014-05-29 Rafael EspindolaRevert "Revert "Revert "InstCombine: Improvement to...
2014-05-29 Artyom SkrobovRestore getInvertedCondCode() from the phased-out backe...
2014-05-29 Artyom SkrobovAdd missing check when MatchInstructionImpl() reports...
2014-05-29 Simon Atanasyan[elf2yaml][ELF] Move Info field to the RelocationSectio...
2014-05-29 Hao LiuRename a test case to contain correct date info.
2014-05-29 Hao LiuFix an assertion failure caused by v1i64 in DAGCombiner...
2014-05-29 Dinesh DwivediLCSSA should be performed on the outermost affected...
2014-05-29 Michael J.... [LoadCombine] Missed a file.
2014-05-29 Michael J.... Add LoadCombine pass.
2014-05-29 Alexey Samsonov[ASan] Hoist blacklisting globals from init-order check...
2014-05-29 Michael J.... [x86] Fold extract_vector_elt of a load into the Load...
2014-05-29 Matt ArsenaultR600/SI: Fix pattern variable names.
2014-05-29 Alexey SamsonovFix typo in variable name
2014-05-29 Alexey Samsonov[ASan] Use llvm.global_ctors to insert init-order check...
2014-05-28 Reid KlecknerAdd a simple helper function to create a 64-bit integer.
2014-05-28 Rafael EspindolaRevert "Revert "InstCombine: Improvement to check if...
2014-05-28 Rafael EspindolaRevert "Add support for combining GEPs across PHI nodes"
2014-05-28 Matt ArsenaultFix wrong setcc result type when legalizing uaddo/usubo
2014-05-28 Jim GrosbachUpdate CREDITS to be at least moderately more current.
2014-05-28 Sanjay Patelfixed a few typos
2014-05-28 Sanjay Pateltest check-in: added missing parenthesis in comment
2014-05-28 Rafael EspindolaRevert "InstCombine: Improvement to check if signed...
2014-05-28 Reid KlecknerFix standard integer definitions for MSVC in DataTypes.h
2014-05-28 Rafael Espindola[pr19844] Add thread local mode to aliases.
2014-05-28 Louis GerbargAdd support for combining GEPs across PHI nodes
2014-05-28 Hal FinkelRevert "[DAGCombiner] Split up an indexed load if only...
2014-05-28 Rafael EspindolaInstCombine: Improvement to check if signed addition...
2014-05-28 Hal FinkelRevert "[PPC] Use alias symbols in address computation."
2014-05-28 Joerg SonnenbergerDon't hard-code ld when extracting host linker version...
2014-05-28 Evgeniy Stepanov[asancov] Don't emit extra runtime calls when compiling...
2014-05-28 Tilmann Scheller[AArch64] Add store post-index update folding regressio...
2014-05-28 Justin Bognerutils: Teach lldbDataFormatters to load automatically
2014-05-28 Tilmann Scheller[AArch64] Add load post-index update folding regression...
2014-05-27 Alexey SamsonovChange representation of instruction ranges where varia...
2014-05-27 Alexey SamsonovFactor out looking for prologue end into a function
2014-05-27 Sebastian Popavoid type mismatch when building SCEVs
2014-05-27 Sebastian Popdo not use the GCD to compute the delinearization strides
2014-05-27 Sebastian Popremove BasePointer before delinearizing
2014-05-27 Sebastian Popremove constant terms
2014-05-27 Alexey SamsonovDon't pre-populate the set of keys in the map with...
2014-05-27 Arnaud A. de... No need for those tests to go thru llvm-as and/or llvm...
2014-05-27 Arnaud A. de... Factor out comparison of Instruction "special" states.
2014-05-27 Reid KlecknerWording fix for llvm.global_dtors docs.
2014-05-27 David BlaikieDebugInfo: partially revert cleanup committed in r209680
2014-05-27 David BlaikieDebugInfo: Simplify solution to avoid DW_AT_artificial...
2014-05-27 Sasa Stankovic[mips] Optimize long branch for MIPS64 by removing...
2014-05-27 David BlaikieDebugInfo: Create abstract function definitions even...
2014-05-27 David BlaikieDebugInfo: Avoid an extra map lookup when finding abstr...
2014-05-27 David BlaikieDebugInfo: Lazily construct subprogram definition DIEs.
2014-05-27 David BlaikieDebugInfo: Lazily attach definition attributes to defin...
2014-05-27 David BlaikieDebugInfo: Separate out the addition of subprogram...
2014-05-27 Jingyue WuFixed a test in r209670
2014-05-27 Jingyue WuDistribute sext/zext to the operands of and/or/xor
2014-05-27 David BlaikieDebugInfo: Fix argument ordering in test by adding...
2014-05-27 Filipe CabecinhasPost-commit fixes for r209643
2014-05-27 Tim NorthoverAArch64: add test for NZCV cross-copy save.
2014-05-27 Tim NorthoverAArch64: add AArch64-specific test for 'c' and 'n'.
2014-05-27 Bill Schmidt[PATCH] Correct type used for VADD_SPLAT optimization...
2014-05-27 Zoran Jovanovic[mips][mips64r6] Add Relocations R_MIPS_PCHI16, R_MIPS_...
2014-05-27 Amara Emerson[ARM] Emit correct build attributes for the relocation...
2014-05-27 Zoran Jovanovic[mips][mips64r6] Add relocations R_MIPS_PC21_S2, R_MIPS...
2014-05-27 Evgeniy Stepanov[asancov] Emit an initializer passing number of coverag...
2014-05-27 Tim NorthoverAArch64: implement copies to/from NZCV as a last ditch...
2014-05-27 Tim NorthoverARM: teach AAPCS-VFP to deal with Cortex-M4.
2014-05-27 Daniel JasperFix bad assert.
2014-05-27 Tim NorthoverAArch64: support 'c' and 'n' inline asm modifiers.
2014-05-27 Dinesh DwivediAdding testcase for PR18886.
2014-05-27 Filipe CabecinhasConvert some X86 blendv* intrinsics into IR.
2014-05-26 Rafael EspindolaFix link.
2014-05-26 Rafael EspindolaUse existing helper function.
2014-05-26 Rafael Espindola[PPC] Use alias symbols in address computation.
2014-05-26 Tim NorthoverAArch64: force i1 to be zero-extended at an ABI boundary.
2014-05-26 Tim NorthoverAArch64: simplify calling conventions slightly.
2014-05-26 Michael ZolotukhinSome cleanup for r209568.
2014-05-26 Rafael EspindolaConvert a few loops to use ranges.
2014-05-26 Tilmann Scheller[AArch64] Add store + add folding regression tests...
2014-05-26 Tilmann Scheller[AArch64] Add more regression tests for the load/store...
2014-05-26 Kostya Serebryany[asan] decrease asan-instrumentation-with-call-threshol...
2014-05-26 Tim NorthoverAArch64: remove empty ARM64 directories from svn.
2014-05-26 Tilmann SchellerRemove accidentally committed whitespace.
2014-05-26 Tilmann Scheller[AArch64] Add a regression test for the load store...
2014-05-26 Owen AndersonMake the LoopRotate pass's maximum header size configur...
2014-05-26 David BlaikieDebugInfo: Test linkonce-odr functions under LTO.
2014-05-26 David BlaikieDwarfUnit: Remove some misleading no-op code introduced...
2014-05-26 Rafael EspindolaJust check the entire string.
2014-05-26 NAKAMURA TakumiReformat linefeeds.
2014-05-26 NAKAMURA TakumiTrailing whitespace.
2014-05-25 Saleem Abdulrasooltools: avoid use of std::function
2014-05-25 Saleem Abdulrasooltools: split out Win64EHDumper from COFFDumper
2014-05-25 Saleem Abdulrasooltools: inline simple single-use function
2014-05-25 Saleem Abdulrasooltools: refactor COFFDumper symbol resolution logic
2014-05-25 Saleem Abdulrasooltools: use references rather than out pointers in COFFD...
2014-05-25 David BlaikieDebugInfo: Fix inlining with #file directives a little...
2014-05-25 David BlaikieStreamline test case by avoiding a temporary file and...
2014-05-25 Rafael EspindolaEmit data or code export directives based on the type.
2014-05-25 Rafael EspindolaMake these CHECKs a bit more strict.
next