opencl/llvm.git
2014-03-14 Adrian PrantlRe-add checks that were in this testcase before it...
2014-03-14 Adrian Prantltypo
2014-03-14 Jim GrosbachMC: don't create a backtrace for diagnostics.
2014-03-14 Diego NovilloRe-format SampleProfile.cpp with clang-format. No funct...
2014-03-14 Diego NovilloUse DiagnosticInfo facility.
2014-03-14 Eric ChristopherRemove command line option for CU hashing. This is...
2014-03-14 Eric ChristopherMake the arbitrary section name be something mach-o...
2014-03-14 Eric ChristopherIf we see that we're emitting code for a function that...
2014-03-14 Eric ChristopherRemove the -generate-dwarf-cu-ranges flag.
2014-03-14 David BlaikieMCDwarf: Initialize MCLineTableHeader::Label
2014-03-14 David BlaikieMCContext: Remove redundant assignment
2014-03-14 Rafael EspindolaCorrectly handle an ELF symbol defined with "a = b...
2014-03-14 David BlaikieRemove unnecessary StringRef::str() call where an impli...
2014-03-14 David BlaikieDwarfDebug: Remove some needless recursion.
2014-03-14 Duncan P. N... x86: Add missing break to getCallPreservedMask()
2014-03-14 Duncan P. N... x86: NFC: Make getCallPreservedMask() more similar...
2014-03-14 Richard Osborne[docs] Add links to XMOS XCore documentation.
2014-03-14 Duncan P. N... x86: getCalleeSavedRegs() would crash on 0 (so don...
2014-03-14 Rafael EspindolaFix a bug introduced during the transition to PathV2.
2014-03-14 Alexey SamsonovDelete unused ObjectFile::{begin,end}_symbols()
2014-03-14 Alexey Samsonov[C++11] Introduce SectionRef::relocations() to use...
2014-03-14 Patrik HagglundSeparate out MVT in a separate header file: MachineValu...
2014-03-14 Ulrich Weigand[ppc64] Avoid copy relocs in named rodata sections
2014-03-14 Alexander Potapenko[ASan] Fix https://code.google.com/p/address-sanitizer...
2014-03-14 Alexey SamsonovUse ctor instead of initializer list to appease Windows...
2014-03-14 Alexey SamsonovUse temporary instead of a local variable here
2014-03-14 Oliver StannardGeneralise assembly tests to not rely on anonymous...
2014-03-14 Evgeniy StepanovAddressSanitizer instrumentation for MOV and MOVAPS.
2014-03-14 Stepan DyatkovskiyMergeFunctions, cmpType: fixed variable names from...
2014-03-14 Stepan DyatkovskiyMergeFunctions, cmpType: Fixed comments wrapping.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Use range-based for loops.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Refer to a section in the error message...
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Remove unused ELFState class field.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Assign name (.shstrtab) to the section...
2014-03-14 Simon Atanasyan[Mips] Add one more MIPS relocation type constant.
2014-03-14 Owen AndersonRevert r203883 (which was more of a bandaid) and fix...
2014-03-14 Sebastian Popstatic link polly into tools
2014-03-14 Pete CooperFix issue with r203865. The old behaviour would get...
2014-03-14 Galina KistanovaReverted r203879.
2014-03-14 Galina KistanovaFixed misuse of isascii. Also fixes mingw32 build,...
2014-03-13 Eric ChristopherUse DW_AT_linkage_name when we're emitting DWARF4 or...
2014-03-13 Rafael EspindolaRemove the linker_private and linker_private_weak linkages.
2014-03-13 Owen AndersonPhase 2 of the great MachineRegisterInfo cleanup. ...
2014-03-13 Owen AndersonFix a bug in InstCombine where we would incorrectly...
2014-03-13 David BlaikieMCDwarf: Rename MCDwarfFileTable to MCDwarfLineTable
2014-03-13 David BlaikieMCDwarf: Extract the DWARF line table header handling...
2014-03-13 Lang HamesMake GDBJITRegistrar thread safe. Patch by Jim Kearyn...
2014-03-13 Owen AndersonFix a subtle issue introduced my my recent changes...
2014-03-13 Kevin EnderbyAdd -mtriple=x86_64-linux to this test case to fix...
2014-03-13 David BlaikieMCDwarf: Sink file/directory creation down into MCDwarf...
2014-03-13 Stephan TolksdorfTest commit - remove trailing whitespace
2014-03-13 David BlaikieMCDwarf: Oh, and move the directory string over to...
2014-03-13 David BlaikieMCDwarf: Simplify MCDwarfFile to just use std::string...
2014-03-13 Ekaterina RomanovaFix for http://llvm.org/bugs/show_bug.cgi?id=18590
2014-03-13 David BlaikieMCDwarf: Simply MCDwarfFile since it really is just...
2014-03-13 Rafael EspindolaUse printable names to implement directional labels.
2014-03-13 Tim NorthoverUpdate my e-mail address in CODE_OWNERS.TXT
2014-03-13 David BlaikieRemove stale comment
2014-03-13 David BlaikieMCDwarf: Refactor line table handling into a single...
2014-03-13 Tom StellardR600: LDS instructions shouldn't implicitly define...
2014-03-13 Mark SeabornCleanup: Remove use of old "-enable-correct-eh-support...
2014-03-13 Hans Wennborg[ARM] Use symbolic register names in .cfi directives...
2014-03-13 Alexey Samsonov[C++11] Use ObjectFile::sections() in commandline llvm...
2014-03-13 Alexey Samsonov[C++11] Introduce ObjectFile::sections().
2014-03-13 Manuel JacobCodeGenPrep: sink extends of illegal types into use...
2014-03-13 Evgeniy Stepanov[msan] Fix handling of byval arguments in VarArg calls.
2014-03-13 Alexey Samsonov[CMake] Put -Werror to CMAKE_CXX_FLAGS instead of using...
2014-03-13 Rafael EspindolaRemove utils/llvm-native-gcc.
2014-03-13 Elena DemikhovskyAVX-512: masked load/store + intrinsics for them.
2014-03-13 Stepan DyatkovskiyFirst patch of patch series that improves MergeFunction...
2014-03-13 Chandler Carruth[PM] As was pointed out in review, I need to define...
2014-03-13 Chandler Carruth[PM] Stop playing fast and loose with rebinding of...
2014-03-13 Tim NorthoverAArch64: error when both positional & named operands...
2014-03-13 Alexey Samsonov[C++11] DWARF parser: use SmallVector<std::unique_ptr...
2014-03-13 Hal Finkel[PowerPC] Initial support for the VSX instruction set
2014-03-13 Hal Finkel[TableGen] Optionally forbid overlap between named...
2014-03-13 Alexey Samsonov[C++11] Convert DWARF parser to range-based for loops
2014-03-13 Saleem AbdulrasoolARM: ignore unused variable to fix -Wunused-variable...
2014-03-13 Saleem AbdulrasoolMC: fix silly typo
2014-03-13 Saleem AbdulrasoolARM: support emission of complex SO expressions
2014-03-13 Saleem AbdulrasoolSupport: add support to identify WinCOFF/ARM objects
2014-03-13 Ted Kremenek[CMake] Enable a bunch of Xcode build settings that...
2014-03-13 Owen AndersonPhase 1 of refactoring the MachineRegisterInfo iterator...
2014-03-13 Karthik BhatFix PR18800. llvm intrinsic memcpy takes 5 arguments...
2014-03-13 Andrew TrickFix a false error reported by the tblgen backend for...
2014-03-13 Saleem AbdulrasoolMC: fix possible NULL pointer dereference
2014-03-13 NAKAMURA Takumillvm/test/BugPoint/compile-custom.ll.py: Make it py3...
2014-03-13 Mark SeabornFix typo in comment: "inwoke" -> "invoke"
2014-03-12 Arnold SchwaighoferFix whitespace in vectorizer example
2014-03-12 Arnold SchwaighoferFix vectorizer docs.
2014-03-12 NAKAMURA Takumidecl-derived-member.ll: Try to unbreak. Don't add ...
2014-03-12 Rafael EspindolaRemove more empty directories.
2014-03-12 Rafael EspindolaRemove empty directories.
2014-03-12 Rafael EspindolaRemove projects/sample.
2014-03-12 David BlaikieMCDwarf: Remove unused parameter
2014-03-12 David BlaikieMCDwarf: Invert the Section+CU->LineEntries mapping...
2014-03-12 Rafael EspindolaThis test need the X86 backend, move it to the X86...
2014-03-12 Justin BognerBack out Profile library and dependent commits
2014-03-12 Michael ZolotukhinPR17473:
2014-03-12 Adam Nemet[X86] Add peephole for masked rotate amount
next