opencl/llvm.git
2014-10-13 Adrian PrantlAdd an assertion about the integrity of the iterator.
2014-10-13 Adrian Prantlconstify the getters in SDNodeDbgValue.
2014-10-13 Chad RosierRefactor debug statement and remove dead argument....
2014-10-13 Timur IskhodzhanovAdd VS2012-generated test inputs for test/tools/llvm...
2014-10-13 Filipe CabecinhasFix a broadcast related regression on the vector shuffl...
2014-10-13 Matt ArsenaultR600/SI: Minor cleanup of function
2014-10-13 Yuri Gorshenin[asan-asm-instrumentation] Follow-up fixes to r219602...
2014-10-13 Renato GolinAdds support for the Cortex-A17 to the ARM backend
2014-10-13 Daniel Sanders[mips] Mark redundant instructions with a comment in...
2014-10-13 Bradley Smith[AArch64] Add workaround for Cortex-A53 erratum (835769)
2014-10-13 Yuri Gorshenin[asan-asm-instrumentation] Fixed memory references...
2014-10-13 NAKAMURA TakumiUnix/Signals.inc: Let findModulesAndOffsets() built...
2014-10-13 NAKAMURA TakumiRevert r219584, "[X86] Memory folding for commutative...
2014-10-13 Richard Smith[modules] Stop excluding Support/Debug.h from the Suppo...
2014-10-12 Benjamin Kramer[Modules] Add some missing includes to make files compi...
2014-10-12 Benjamin KramerModernize old-style static asserts. NFC.
2014-10-12 Joerg SonnenbergerRevert r219223, it creates invalid PHI nodes.
2014-10-12 Benjamin KramerAPSInt: Simplify code to reduce the number of copies...
2014-10-12 Benjamin KramerInstCombine: Turn (x != 0 & x <u C) into the canonical...
2014-10-12 Simon Pilgrim[X86] Memory folding for commutative instructions.
2014-10-12 David MajnemerInstCombine: Simplify commonIDivTransforms
2014-10-12 NAKAMURA Takumillvm/test/CodeGen: Some tests don't REQUIRE asserts...
2014-10-11 NAKAMURA TakumiSuppress llvm-ar's MRI tests for now on win32, since...
2014-10-11 Simon PilgrimTest commit access (email fix)
2014-10-11 Benjamin KramerAssumptionTracker: Don't create temporary CallbackVHs.
2014-10-11 Benjamin KramerMC: Shrink MCSymbolRefExpr by only storing the bits...
2014-10-11 Benjamin KramerMC: Bit pack MCSymbolData.
2014-10-11 Simon PilgrimTest commit access
2014-10-11 David MajnemerInstCombine: Don't fold (X <<s log(INT_MIN)) /s INT_MIN...
2014-10-11 David MajnemerInstCombine, InstSimplify: (%X /s C1) /s C2 isn't alway...
2014-10-11 David MajnemerInstCombine: mul to shl shouldn't preserve nsw
2014-10-11 Chandler Carruth[SCEV] Fix one more caller blindly passing the latch...
2014-10-11 Chandler CarruthGuard the definition of the stack tracing function...
2014-10-11 Reed KotlerAdd basic conditional branches in mips fast-isel
2014-10-11 Chandler Carruth[SCEV] Add some asserts to the recently improved trip...
2014-10-10 Lang Hames[MCJIT] Replace memcpy with readBytesUnaligned in Runti...
2014-10-10 Sanjay PatelReturn undef on FP <-> Int conversions that overflow...
2014-10-10 Alexey SamsonovFollow-up to r219534 to make symbolization more robust.
2014-10-10 Matt ArsenaultR600/SI: Change how DS offsets are printed
2014-10-10 Matt ArsenaultR600/SI: Match read2/write2 stride 64 versions
2014-10-10 Alexey SamsonovRe-land r219354: Use llvm-symbolizer to symbolize LLVM...
2014-10-10 Matt ArsenaultR600/SI: Add load / store machine optimizer pass.
2014-10-10 Sanjoy DasThis patch teaches ScalarEvolution to pick and use...
2014-10-10 Chandler Carruth[mips] Actually mark that the default case is unreachab...
2014-10-10 Reed KotlerImplement floating point compare for mips fast-isel
2014-10-10 David BlaikieRevert "DebugInfo: Ensure that all debug location scope...
2014-10-10 Rafael Espindolallvm-ar: Start adding support for mri scripts.
2014-10-10 Matt ArsenaultR600/SI: Disable copying of SCC
2014-10-10 Reed Kotlerimplement integer compare in mips fast-isel
2014-10-10 Mark HeffernanThis patch de-pessimizes the calculation of loop trip...
2014-10-10 Fariborz JahanianAdd couple of missing 'override' keyword. NFC.
2014-10-10 Bill Schmidt[PowerPC] Reduce names from Power8Vector to P8Vector
2014-10-10 Hal Finkel[MiSched] Fix a logic error in tryPressure()
2014-10-10 Reed KotlerImplement floating point to integer conversion in mips...
2014-10-10 David BlaikieSimplify a few uses of DwarfDebug::SPMap
2014-10-10 Timur IskhodzhanovReorder functions in WinCodeViewLineTables.cpp [NFC]
2014-10-10 Frederic Riss[dwarfdump] Prettyprint DW_AT_APPLE_property_attribute...
2014-10-10 Frederic Riss[dwarfdump] Resolve also variable specifications/abstra...
2014-10-10 Benjamin KramerReduce double set lookups. NFC.
2014-10-10 Bill Schmidt[PowerPC] Add feature for Power8 vector extensions
2014-10-10 Zoran Jovanovic[mips][microMIPS] Implement ADDIUSP instruction
2014-10-10 Zoran Jovanovic[mips][microMIPS] Implement JR16 instruction
2014-10-10 Zoran Jovanovic[mips][microMIPS] Implement ADDIUS5 instruction
2014-10-10 Zoran Jovanovicps][microMIPS] Implement JRC instruction
2014-10-10 Zoran Jovanovic[mips][microMIPS] Implement JALRS16 instruction
2014-10-10 Timur IskhodzhanovFix a small typo, NFC
2014-10-10 Benjamin KramerAPInt: Unfold return expressions so RVO can work.
2014-10-10 Chandler Carruth[ADT] Add an (ADL-friendly) abs free function for APFlo...
2014-10-10 Chandler CarruthDon't use an unqualified 'abs' function call with a...
2014-10-10 David MajnemerAdd tests for r219479.
2014-10-10 David MajnemerObject, COFF: Relax aux symbols for section definitions
2014-10-10 David BlaikieSink the per-CU part of DwarfDebug::finishSubprogramDef...
2014-10-10 David BlaikieSink most of DwarfDebug::constructAbstractSubprogramSco...
2014-10-10 Matt ArsenaultAdd minnum / maxnum to APFloat
2014-10-10 Chandler Carruth[ADT] Replace the logb implementation with the simpler...
2014-10-10 Chandler Carruth[ADT] Add the scalbn function for APFloat.
2014-10-10 Chandler Carruth[ADT] Implement the 'logb' functionality for APFloat...
2014-10-10 Hal Finkel[LVI] Revert the remainder of "r218231 - Add two thresh...
2014-10-10 David BlaikieAvoid unnecessary map lookup/insertion.
2014-10-10 Matt ArsenaultAdd isInfinity to ConstantFP
2014-10-10 Arnold SchwaighoferSimplifyCFG: Don't convert phis into selects if we...
2014-10-10 Rafael EspindolaFix gcc warning in gold-plugin.cpp.
2014-10-10 David Majnemerobj2yaml, COFF: Handle long section names
2014-10-09 Chandler Carruth[ADT] Add basic operator overloads for arithmetic to...
2014-10-09 Sanjay PatelImprove sqrt estimate algorithm (fast-math)
2014-10-09 Sanjay Pateldelete function names from comments
2014-10-09 Sanjay Pateldelete function name from comment
2014-10-09 Frederic RissAdd ApplePropertyString dump helper to Dwarf.{h|cpp}.
2014-10-09 Samuel AntaoFix bug in GPR to FPR moves in PPC64LE.
2014-10-09 David BlaikieRemove unused parameter
2014-10-09 David BlaikieSink DwarfDebug::createAndAddScopeChildren down into...
2014-10-09 David BlaikieSink DwarfDebug::constructSubprogramScopeDIE down into...
2014-10-09 Chad Rosier[Reassociate] Don't canonicalize X - undef to X + ...
2014-10-09 Benjamin KramerRemove a compiler bug workaround from 2007. The affecte...
2014-10-09 Hal FinkelRevert "[BasicAA] Revert "Revert r218714 - Make better...
2014-10-09 Matt ArsenaultRemove unused field from Operand
2014-10-09 Matt ArsenaultFix typo
2014-10-09 Tom StellardR600/SI: Legalize CopyToReg during instruction selection
2014-10-09 Lang Hames[PBQP] Add missing headers from r219421.
2014-10-09 David BlaikieSink DwarfDebug::createScopeChildrenDIE down into Dwarf...
next