opencl/llvm.git
2015-01-06 Adrian PrantlReapply: Teach SROA how to update debug info for fragme...
2015-01-06 Filipe CabecinhasDon't loop endlessly for MachO files with 0 ncmds
2015-01-06 Colin LeMahieu[Hexagon] Fix 225267. GP register is not yet fully...
2015-01-06 Adrian PrantlImplement a very basic colored syntax highlighting...
2015-01-06 Hal Finkel[PowerPC] Add a regression test for r225251
2015-01-06 Colin LeMahieu[Hexagon] Adding dealloc_return encoding and absolute...
2015-01-06 Asiri Rathnayake[ARM] Cleanup so_imm* tblgen defintions
2015-01-06 Matt ArsenaultConvert fcmp with 0.0 from casted integers to icmp
2015-01-06 NAKAMURA Takumi[CMake] Silence stderr on "COMMAND ${CMAKE_C_COMPILER...
2015-01-06 NAKAMURA TakumiReformat.
2015-01-06 Chandler Carruth[PM] Hide a function we only use in an assert behind...
2015-01-06 Chandler Carruth[PM] Introduce a utility pass that preserves no analyses.
2015-01-06 Craig Topper[X86] Add OpSize32 to XBEGIN_4. Add XBEGIN_2 with OpSize16.
2015-01-06 David MajnemerInstCombine: Bitcast call arguments from/to pointer...
2015-01-06 Chandler Carruth[PM] Simplify how we parse the outer layer of the pass...
2015-01-06 Craig Topper[X86] Make isel select the 2-byte register form of...
2015-01-06 Hal Finkel[PowerPC] Remove old README.txt entry regarding struct...
2015-01-06 David MajnemerX86: Don't make illegal GOTTPOFF relocations
2015-01-06 Hal Finkel[PowerPC] Add some missing names in getTargetNodeName
2015-01-06 Hal Finkel[PowerPC] Improve int_to_fp(fp_to_int(x)) combining
2015-01-06 Chandler Carruth[PM] Add a utility pass template that synthesizes the...
2015-01-06 Chandler Carruth[PM] Simplify how we use the registry by including...
2015-01-06 Craig Topper[X86] Remove 16-bit and 32-bit offset jump instructions...
2015-01-06 Craig Topper[X86] Make isel select the shorter form of jump instruc...
2015-01-06 Chandler Carruth[PM] Add a collection of no-op analysis passes and...
2015-01-06 Chandler Carruth[PM] Sink the no-op pass parsing logic into the .def...
2015-01-06 Chandler Carruth[PM] Move the analysis registry into the Passes.cpp...
2015-01-06 Chandler Carruth[PM] Add a utility to the new pass manager for generati...
2015-01-06 Rafael EspindolaAdd a testcase that would have found the problem in...
2015-01-06 Eric ChristopherRemove dead variable.
2015-01-06 Eric ChristopherUse the same call off of the TargetMachine rather than...
2015-01-06 Eric ChristopherRewrite the Mips16HardFloat pass to avoid using the...
2015-01-06 Lang HamesRevert r225048: It broke ObjC on AArch64.
2015-01-06 Brad SmithRemove X86 .quad workaround for buggy GNU assembler...
2015-01-05 Duncan P. N... IR: Don't drop MDNode uniquing on null operands
2015-01-05 Duncan P. N... Revert "Use the integrated assembler by default on...
2015-01-05 Hal Finkel[PowerPC] Fix test to pass on Darwin hosts
2015-01-05 Hal Finkel[PowerPC] Remove old README.txt entry
2015-01-05 Simon Pilgrim[X86][SSE] lowerVectorShuffleAsByteShift tidyup
2015-01-05 Hal Finkel[PowerPC] Convert a README.txt entry into a better...
2015-01-05 Brad SmithUse the integrated assembler by default on 32-bit Power...
2015-01-05 Hal Finkel[PowerPC] Remove README.txt entry
2015-01-05 Colin LeMahieu[Hexagon] Adding add/sub with carry, logical shift...
2015-01-05 Hal Finkel[PowerPC] Add a test for truncating a shifted load
2015-01-05 Frederic RissMake DIE.h a public CodeGen header.
2015-01-05 Frederic Riss[dsymutil] Implement the BinaryHolder object and gain...
2015-01-05 NAKAMURA Takumi[autoconf] llvm/cmake/modules/Makefile: Make sure to...
2015-01-05 Hal Finkel[PowerPC] Add another test for load/store with update
2015-01-05 NAKAMURA Takumi[autoconf] Export LLVM_LIBDIR_SUFFIX with empty string...
2015-01-05 Hal Finkel[PowerPC] Fold i1 extensions with other ops
2015-01-05 Simon Pilgrim[X86][SSE] Fixed description for isSequentialOrUndefInR...
2015-01-05 Colin LeMahieu[Hexagon] Adding rounding reg/reg variants, accumulatin...
2015-01-05 Duncan P. N... IR: Prune arguments to ValueAsMetadata::ValueAsMetadata()
2015-01-05 Colin LeMahieu[Hexagon] Adding V4 bit manipulating instructions,...
2015-01-05 Colin LeMahieu[Hexagon] Adding V4 logic-logic instructions and tests.
2015-01-05 Colin LeMahieu[Hexagon] Adding orand, bitsplit reg/reg, and modwrap...
2015-01-05 Hal Finkel[PowerPC] Remove zexts after i32 ctlz
2015-01-05 Hal Finkel[PowerPC] Remove zexts after byte-swapping loads
2015-01-05 Colin LeMahieu[Hexagon] Adding round reg/imm and bitsplit instructions.
2015-01-05 Saleem AbdulrasoolSymbolRewriter: use iplist::splice
2015-01-05 Saleem AbdulrasoolSymbolRewriter: 80-column
2015-01-05 Ahmed Bougacha[AArch64] Improve codegen of store lane instructions...
2015-01-05 Ahmed Bougacha[AArch64] Improve codegen of store lane 0 instructions...
2015-01-05 NAKAMURA Takumillvm/test/lit.cfg: have_ld_plugin_support(): Use decode...
2015-01-05 Karthik BhatSelect lower fsub,fabs pattern to fabd on AArch64
2015-01-05 Charlie TurnerParse Tag_compatibility correctly.
2015-01-05 Charlie TurnerEmit the build attribute Tag_conformance.
2015-01-05 Karthik BhatSelect lower sub,abs pattern to sabd on AArch64
2015-01-05 Michael KupersteinFix broken test from r225159.
2015-01-05 Chandler Carruth[PM] Don't run the machinery of invalidating all the...
2015-01-05 Chandler Carruth[PM] Add names and debug logging for analysis passes...
2015-01-05 Craig TopperReplace several 'assert(false' with 'llvm_unreachable...
2015-01-05 Jiangning LiuFixed a bug in memory dependence checking module of...
2015-01-05 Michael GottesmanConvert SmallMapVector from a class to a struct.
2015-01-05 Craig Topper[X86] Remove the predicates from the register forms...
2015-01-05 Craig Topper[X86] Simplify code a little by just summing flags...
2015-01-05 Craig Topper[X86] Remove unnecessary redeclaration of a variable...
2015-01-05 Craig Topper[X86] Remove a strange fixme referring to a hack that...
2015-01-05 Craig Topper[x86] Reduce text duplication for similar operand class...
2015-01-05 Craig Topper[X86] Fix the immediate size to match the address size...
2015-01-05 Craig Topper[X86] Remove unused operand type from disassembler...
2015-01-05 Hal Finkel[PowerPC] Enable speculation of cttz/ctlz
2015-01-05 Chandler Carruth[SROA] Apply a somewhat heavy and unpleasant hammer...
2015-01-05 Hal Finkel[LangRef] Correct a typo
2015-01-05 Hal Finkel[PowerPC] Materialize i64 constants using rotation...
2015-01-05 Chandler Carruth[PM] Cleanup a place where I forgot to update the heade...
2015-01-05 Chandler Carruth[PM] Switch the new pass manager to use a reference...
2015-01-05 Chandler Carruth[PM] Wire up support for explicitly running the verifie...
2015-01-04 Chandler Carruth[PM] Cleanup a const_cast and other machinery left...
2015-01-04 Simon Pilgrim[X86][SSE] Added vector packing test for pr12412
2015-01-04 Simon Pilgrim[X86][SSE] Added vector integer truncation tests -...
2015-01-04 Hal Finkel[PowerPC] Materialize i64 constants using rotation
2015-01-04 Michael KupersteinFix unused variable warning for non-asserts builds...
2015-01-04 Hal Finkel[PowerPC] Materialize i64 constants using bit inversion
2015-01-04 Chandler Carruth[PM] Split the AssumptionTracker immutable pass into...
2015-01-04 David MajnemerInstCombine: match can find ConstantExprs, don't assume...
2015-01-04 David MajnemerValueTracking: ComputeNumSignBits should tolerate missh...
2015-01-04 Lang Hames[APFloat][ADT] Fix sign handling logic for FMA results...
2015-01-03 Saleem Abdulrasoolllvm-readobj: add support to dump COFF export tables
2015-01-03 Saleem AbdulrasoolARM: permit tail calls to weak externals on COFF
next