opencl/llvm.git
2014-03-18 Adrian PrantlReplace unnecessary #include directive with forward...
2014-03-18 Eric ChristopherAdd explanatory comment.
2014-03-18 Eric ChristopherShorten DotDebugLocEntry to just DebugLocEntry and...
2014-03-18 David BlaikieDebugInfo: Avoid emitting standard opcode lengths in...
2014-03-18 David BlaikieDebugInfo: Implement debug_line.dwo for file names...
2014-03-18 David BlaikieDebugInfo: Flag test as requiring object emission support
2014-03-18 David BlaikieDebugInfo: Do not rely on the compilation dir (index...
2014-03-17 David BlaikieDebugInfo: Move getOrCreateSourceID from DwarfDebug...
2014-03-17 David BlaikieDebugInfo: Move line table zero-directory-index (compil...
2014-03-17 Matt ArsenaultMake methods static
2014-03-17 Dan GohmanUse range metadata instead of introducing selects.
2014-03-17 Owen AndersonSwitch a number of loops in lib/CodeGen over to range...
2014-03-17 Owen AndersonReally REALLY finish adding const to the MachineRegiste...
2014-03-17 Kevin EnderbyMaking a guess to fix the test case with r204056 to...
2014-03-17 Matt ArsenaultR600: Match sign_extend_inreg to BFE instructions
2014-03-17 Matt ArsenaultMake DAGCombiner work on vector bitshifts with constant...
2014-03-17 Owen AndersonAdd one more const marker that I missed.
2014-03-17 David BlaikieDebugInfo: Use MC line table file entry uniquing for...
2014-03-17 Owen AndersonMark MachineRegisterInfo's iterator range methods as...
2014-03-17 Owen AndersonAdd iterator range definitions for the MachineRegisterI...
2014-03-17 Adam Nemet[X86] Fix unused variable warning with NDEBUG from...
2014-03-17 Saleem AbdulrasoolMC: change runtime check to an assertion
2014-03-17 Saleem AbdulrasoolARM IAS: support .thumb_set
2014-03-17 Adam Nemet[VectorLegalizer/X86] Don't unvectorize fp_to_uint...
2014-03-17 Tom StellardR600/SI: Fix implementation of isInlineConstant() used...
2014-03-17 Tom StellardR600/SI: Use correct dest register class for V_READFIRS...
2014-03-17 Tom StellardR600/SI: Add generic checks to SIInstrInfo::verifyInstr...
2014-03-17 Eli BenderskyConsistent use of the noduplicate attribute.
2014-03-17 Alexey Samsonov[C++11] Introduce ObjectFile::symbols() to use range...
2014-03-17 NAKAMURA Takumillvm/test/MC/MachO/gen-dwarf-cpp.s: Relax an expression...
2014-03-17 Rafael EspindolaConsider the base pointer for setting the symbol type.
2014-03-17 David BlaikieDebugInfo: Improve reuse of file table entries in asm...
2014-03-17 David BlaikieTest case
2014-03-17 Lang HamesDeleted copy-constructor/copy-assignment broke a buildb...
2014-03-17 Nico Rieckllvm-readobj: Print referred symbol name for CLR token...
2014-03-17 Nico Rieckllvm-readobj: Add test for COFF auxiliary symbols as...
2014-03-17 Lang HamesRename PBQP RegAllocSolver local variables to conform...
2014-03-17 Lang Hames[X86] New and improved VZeroUpperInserter optimization.
2014-03-16 NAKAMURA TakumiUntabify.
2014-03-16 Manman RenAdd FIXMEs to use DIScopeRef instead of DIScope for...
2014-03-16 NAKAMURA Takumi[CMake][cygming] Disable --out-implib from executables.
2014-03-16 David BlaikieRemove named Twine.
2014-03-15 Benjamin KramerUse a fixed subtarget for test so atom scheduling can...
2014-03-15 Arnaud A. de... Remove some dead assignements found by scan-build
2014-03-15 Benjamin KramerMake some assertions on constant expressions static.
2014-03-15 Benjamin KramerPointerIntPair: Avoid an (academic) case of undefined...
2014-03-15 Benjamin KramerLSR: Compress a pair (and get rid of the DenseMapInfo...
2014-03-15 Patrik HagglundReplace ValueTypes.h with MachineValueType.h if possible.
2014-03-15 Justin BognerSupport: Make error_category's constructor public
2014-03-15 NAKAMURA Takumillvm/test/Transforms/SampleProfile/syntax.ll: Suppress...
2014-03-15 NAKAMURA TakumiSampleProfile.cpp: Fix take #2. The issue was abuse...
2014-03-15 NAKAMURA TakumiSampleProfile.cpp: Quick fix to r203976 about abuse...
2014-03-15 Matt ArsenaultR600: Remove unnecessary attempt to zext a pointer.
2014-03-15 Matt ArsenaultR600: Code cleanup.
2014-03-15 Rui UeyamaObject/COFF: change data type of SymbolNumber from...
2014-03-14 Adrian PrantlDebug info: Unique types before emitting them to DWARF...
2014-03-14 Adrian PrantlDebug Info: Fix LTO type uniquing for C++ member declar...
2014-03-14 Adrian PrantlRe-add checks that were in this testcase before it...
2014-03-14 Adrian Prantltypo
2014-03-14 Jim GrosbachMC: don't create a backtrace for diagnostics.
2014-03-14 Diego NovilloRe-format SampleProfile.cpp with clang-format. No funct...
2014-03-14 Diego NovilloUse DiagnosticInfo facility.
2014-03-14 Eric ChristopherRemove command line option for CU hashing. This is...
2014-03-14 Eric ChristopherMake the arbitrary section name be something mach-o...
2014-03-14 Eric ChristopherIf we see that we're emitting code for a function that...
2014-03-14 Eric ChristopherRemove the -generate-dwarf-cu-ranges flag.
2014-03-14 David BlaikieMCDwarf: Initialize MCLineTableHeader::Label
2014-03-14 David BlaikieMCContext: Remove redundant assignment
2014-03-14 Rafael EspindolaCorrectly handle an ELF symbol defined with "a = b...
2014-03-14 David BlaikieRemove unnecessary StringRef::str() call where an impli...
2014-03-14 David BlaikieDwarfDebug: Remove some needless recursion.
2014-03-14 Duncan P. N... x86: Add missing break to getCallPreservedMask()
2014-03-14 Duncan P. N... x86: NFC: Make getCallPreservedMask() more similar...
2014-03-14 Richard Osborne[docs] Add links to XMOS XCore documentation.
2014-03-14 Duncan P. N... x86: getCalleeSavedRegs() would crash on 0 (so don...
2014-03-14 Rafael EspindolaFix a bug introduced during the transition to PathV2.
2014-03-14 Alexey SamsonovDelete unused ObjectFile::{begin,end}_symbols()
2014-03-14 Alexey Samsonov[C++11] Introduce SectionRef::relocations() to use...
2014-03-14 Patrik HagglundSeparate out MVT in a separate header file: MachineValu...
2014-03-14 Ulrich Weigand[ppc64] Avoid copy relocs in named rodata sections
2014-03-14 Alexander Potapenko[ASan] Fix https://code.google.com/p/address-sanitizer...
2014-03-14 Alexey SamsonovUse ctor instead of initializer list to appease Windows...
2014-03-14 Alexey SamsonovUse temporary instead of a local variable here
2014-03-14 Oliver StannardGeneralise assembly tests to not rely on anonymous...
2014-03-14 Evgeniy StepanovAddressSanitizer instrumentation for MOV and MOVAPS.
2014-03-14 Stepan DyatkovskiyMergeFunctions, cmpType: fixed variable names from...
2014-03-14 Stepan DyatkovskiyMergeFunctions, cmpType: Fixed comments wrapping.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Use range-based for loops.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Refer to a section in the error message...
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Remove unused ELFState class field.
2014-03-14 Simon Atanasyan[yaml2obj][ELF] Assign name (.shstrtab) to the section...
2014-03-14 Simon Atanasyan[Mips] Add one more MIPS relocation type constant.
2014-03-14 Owen AndersonRevert r203883 (which was more of a bandaid) and fix...
2014-03-14 Sebastian Popstatic link polly into tools
2014-03-14 Pete CooperFix issue with r203865. The old behaviour would get...
2014-03-14 Galina KistanovaReverted r203879.
2014-03-14 Galina KistanovaFixed misuse of isascii. Also fixes mingw32 build,...
2014-03-13 Eric ChristopherUse DW_AT_linkage_name when we're emitting DWARF4 or...
2014-03-13 Rafael EspindolaRemove the linker_private and linker_private_weak linkages.
2014-03-13 Owen AndersonPhase 2 of the great MachineRegisterInfo cleanup. ...
next