opencl/llvm.git
2013-11-15 Adrian PrantlReplace the dangling context hotfix with an assertion.
2013-11-15 Lang HamesRemove unused arguments.
2013-11-15 Lang HamesDuring folding for patchpoint/stackmap instructions...
2013-11-15 David BlaikieDwarfDebug: Push DISubprogram through updateSubprogramS...
2013-11-15 Arnold SchwaighoferLoopVectorizer: Use abi alignment for accesses with...
2013-11-15 David BlaikieDwarfCompileUnit: Push DIDescriptors through a getDIE...
2013-11-15 Juergen RibutzkaFix previous commit (r194865)
2013-11-15 David BlaikieDwarfCompileUnit: Push DIDescriptor usage out from...
2013-11-15 Matt ArsenaultFix typos.
2013-11-15 Juergen Ributzka[weak vtables] Remove a bunch of weak vtables
2013-11-15 Matt ArsenaultFix confusing machine verifier error.
2013-11-15 Andrew KaylorFix a problem in MCJIT identifying the module containin...
2013-11-15 Matt ArsenaultMake method static
2013-11-15 Chandler Carruth[PM] Fix an iterator problem spotted by the MSVC debug...
2013-11-15 Chandler Carruth[PM] Run clang-format on a few lines that I missed...
2013-11-15 Chad Rosier[AArch64] Fix the scalar NEON ACLE functions so that...
2013-11-15 Rui UeyamaPath: Recognize COFF import library file magic.
2013-11-15 Adrian PrantlReimplement r194843 in a slightly less broken way.
2013-11-15 Manman RenArgumentPromotion: correctly transfer TBAA tags and...
2013-11-15 Rui UeyamaReadobj: If NumbersOfSections is 0xffff, it's an COFF...
2013-11-15 Adrian PrantlRestore the behaviour from before r194728.
2013-11-15 Bob WilsonAvoid illegal integer promotion in fastisel
2013-11-15 Tom StellardR600/SI: Add VReg_96 register class to SIRegisterInfo...
2013-11-15 Andrew KaylorResolve JIT runtime linking problems on Android.
2013-11-15 Andrew KaylorDon't try to initialize memory for a global if the...
2013-11-15 Chad RosierUpdate contact information.
2013-11-15 Daniel Sanders[mips][msa] Merge basic_operations_little.ll into basic...
2013-11-15 Cameron McInallyAdd AVX512 unmasked FMA intrinsics and support.
2013-11-15 Justin Holewinski[NVPTX] Fix type in usage doc
2013-11-15 Daniel Sanders[mips][msa] lowerMSABitClear() should use SelectionDAG...
2013-11-15 Alexey SamsonovHopefully fix uninitialized memory read in AArch64AsmPa...
2013-11-15 Justin Holewinski[NVPTX] Update the usage document
2013-11-15 Daniel SandersFix illegal DAG produced by SelectionDAG::getConstant...
2013-11-15 Justin Holewinski[NVPTX] Fix handling of indirect calls
2013-11-15 Yaron KerenCorrect spelling.
2013-11-15 Daniel Sanders[mips][msa] Build all the tests in little and big endia...
2013-11-15 Chandler CarruthMove all of the GoogleTest files back to the same locat...
2013-11-15 Kostya Serebryany[asan] use GlobalValue::PrivateLinkage for coverage...
2013-11-15 Benjamin Kramerllvm-cov: Clean up memory leaks.
2013-11-15 Alexey SamsonovRedirect unused test case output to /dev/null
2013-11-15 Benjamin KramerGive unit test its own LLVMContext so MDNodes aren...
2013-11-15 Renato GolinAdding some info about stability of ARM boards
2013-11-15 Zoran JovanovicUse instr mapping for microMIPS in llvm-mc.
2013-11-15 Bob WilsonReapply "[asan] Poor man's coverage that works with...
2013-11-15 Andrew TrickPlatform proof a test case.
2013-11-15 Matt ArsenaultAdd instcombine visitor for addrspacecast
2013-11-15 Matt ArsenaultFix grammar in addrspacecast description
2013-11-15 Matt ArsenaultAdd target hook to prevent folding some bitcasted loads.
2013-11-15 Peter Zotov[OCaml] Add REQUIRES: native, object-emission to the...
2013-11-15 Bob WilsonRevert "[asan] Poor man's coverage that works with...
2013-11-15 Peter Zotov[OCaml] Use native target in testsuite instead of hardc...
2013-11-15 Peter Zotov[OCaml] Add Target and TargetMachine bindings to Llvm_t...
2013-11-15 Peter Zotov[OCaml] Refactor Llvm_target interface
2013-11-15 Peter Zotov[OCaml] Fix building of stub libraries
2013-11-15 Peter Zotov[llvm-c] Make LLVMGetTargetFromName actually work
2013-11-15 Peter Zotov[llvm-c] Add missing const qualifiers to LLVMCreateTarg...
2013-11-15 Peter Zotov[llvm-c] Simplify signature of LLVMGetTargetFromName
2013-11-15 Reed KotlerMake all the conditional Mips 16 branches get initially...
2013-11-15 Eric ChristopherUse a reference rather than a pointer as we don't expec...
2013-11-15 Matt ArsenaultAdd addrspacecast instruction.
2013-11-15 Rui UeyamaInclude raw_ostream.h.
2013-11-15 Tom StellardR600: Fix scheduling of instructions that use the LDS...
2013-11-14 Chandler CarruthTeach the Makefile build system how to handle SOURCES...
2013-11-14 Tom StellardR600/SI: Add processor type for Hawaii
2013-11-14 Andrew TrickWhen folding memory operands, preserve existing Machine...
2013-11-14 Matt ArsenaultR600/SI: Remove redundant legalizeOperands call
2013-11-14 Eric ChristopherSimplify testcase.
2013-11-14 Hans WennborgAdd #include raw_ostream.h in lib/Target/R600/SIFixSGPR...
2013-11-14 Matt ArsenaultR600/SI: Specify S_ADDK/S_MULK set SCC and are commutable
2013-11-14 David BlaikieDebugInfo: Simplify/narrow null-check for getOrCreateType
2013-11-14 Rui UeyamaRecognize 0x0000 as a COFF file magic.
2013-11-14 Chad Rosier[AArch64] Remove redundant Neon_immAllOnes/Neon_immAllZ...
2013-11-14 David BlaikieDwarfCompileUnit::getOrCreateContext: Return the compil...
2013-11-14 David BlaikieRemove unnecessary 'else' after return.
2013-11-14 Paul RobinsonTypos. (Test commit.)
2013-11-14 Dmitri GribenkoFix regular expression to work with multiple-digit...
2013-11-14 Tim NorthoverARM: produce friendly error for invalid inline asm
2013-11-14 Rafael EspindolaAdd a triple and switch test to FileCheck.
2013-11-14 NAKAMURA Takumillvm-cov.test: Remove XFAIL:arm. Seems this is passing...
2013-11-14 Rafael EspindolaError if we see an alias to a declaration.
2013-11-14 Kostya Serebryany[asan] Poor man's coverage that works with ASan
2013-11-14 Evgeniy Stepanov[msan] Use CHECK-DAG instead of CHECK where order of...
2013-11-14 Evgeniy Stepanov[msan] Fast path optimization for wrap-indirect-calls...
2013-11-14 NAKAMURA Takumillvm-cov requires IR and Support as libraries. Instrume...
2013-11-14 NAKAMURA Takumillvm-cov.test: Tweak win32 hosts not confused by \r...
2013-11-14 NAKAMURA TakumiIR/GCOV.cpp: Use PRIu64 as format string with uint64_t.
2013-11-14 NAKAMURA TakumiWhitespace.
2013-11-14 Elena DemikhovskyAVX-512: Handled extractelement from mask vector;
2013-11-14 Chandler CarruthFix the header comment of the new pass manager stuff...
2013-11-14 Matt ArsenaultIndentation fixes
2013-11-14 Matt ArsenaultAdd a comment
2013-11-14 Matt ArsenaultFix trailing whitespace in debug printing
2013-11-14 Matt ArsenaultR600/SI: Add testcase for problem I ran into
2013-11-14 NAKAMURA Takumiyaml::Input::mapTag(): Don't use StringRef to hold...
2013-11-14 NAKAMURA TakumiWhitespace.
2013-11-14 NAKAMURA TakumiAArch64DAGToDAGISel::SelectVTBL(): Fix a warning. ...
2013-11-14 Andrew TrickMinor extension to llvm.experimental.patchpoint: don...
2013-11-14 Kevin QinAdd test case for AArch64 NEON instruction set misc.
2013-11-14 Peter Zotov[OCaml] Build stub OCaml libraries for all configured...
2013-11-14 Peter Zotov[OCaml] Expose LLVM's fatal error and stacktrace APIs
next