]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/shortlog
opencl/llvm.git
2014-08-07 Adrian PrantlMake these regexes stricter by disallowing any addition...
2014-08-07 Arnold SchwaighoferSLPVectorizer: Use the type of the value loaded/stored...
2014-08-07 Adrian PrantlAdd a separate testcase for a DWARF expression describi...
2014-08-07 Adrian PrantlReflow this comment.
2014-08-07 David BlaikieDebugInfo: Fix overwriting/loss of inlined arguments...
2014-08-07 Reed Kotlerfix materialization of one bit constants and global...
2014-08-07 Eric ChristopherTemporarily Revert "Nuke the old JIT." as it's not...
2014-08-07 Gerolf HoflehnerDebugging Utility - optional ability for dumping critic...
2014-08-07 Gerolf HoflehnerMachineCombiner Pass for selecting faster instruction...
2014-08-07 Kevin EnderbyAdd two missing ARM cpusubtypes to the switch statement in
2014-08-07 Owen AndersonFix a case in SROA where lifetime intrinsics could...
2014-08-07 Lang Hames[MCJIT] Replace a c-style cast with reinterpret_cast...
2014-08-07 Richard SmithRemove Support/IncludeFile.h and its only user. This...
2014-08-07 Rafael EspindolaFix test failure on ARM.
2014-08-07 Richard Smith[modules] Update module map workaround to cope with...
2014-08-07 Frederic Risstest commit: remove trailing whitespace.
2014-08-07 Rafael EspindolaRemove a few XFAILs.
2014-08-07 Akira Hatanaka[Branch probability] Recompute branch weights of tail...
2014-08-07 Joerg SonnenbergerAdd the majority of the remaining SPE instructions.
2014-08-07 Justin BognerFileCheck: Add a flag to allow checking empty input
2014-08-07 Joerg SonnenbergerIndent
2014-08-07 Adam Nemet[AVX512] Generate masking instruction variants with...
2014-08-07 NAKAMURA Takumillvm/test/tools/llvm-objdump: Reorganize target-depende...
2014-08-07 Rafael EspindolaFix the ocaml bindings.
2014-08-07 Rafael Espindolafix configure+make build
2014-08-07 Rafael EspindolaRemove empty directories.
2014-08-07 Rafael EspindolaNuke the old JIT.
2014-08-07 Joerg SonnenbergerAdd mfasr and mtasr
2014-08-07 Joerg SonnenbergerAdd mfrtcu and mfrtcl instructions
2014-08-07 Joerg SonnenbergerSupport mttbl and mttbu mnemonic
2014-08-07 Joerg SonnenbergerAdd RFID instruction.
2014-08-07 Joerg SonnenbergerFix Itineray class of rfi
2014-08-07 Joerg SonnenbergerSpell e500 feature in lower case.
2014-08-07 Joerg SonnenbergerAdd first bunch of SPE instructions. As they overlap...
2014-08-07 Alexander KornienkoInsert parens to avoid a warning:
2014-08-07 Aaron BallmanSilencing an MSVC C4334 warning ('<<' : result of 32...
2014-08-07 Daniel Sanders[mips] Add assembler support for .set msa/nomsa directive.
2014-08-07 Pavel ChupinFix lld-x86_64-win7 Build #11969
2014-08-07 Chandler Carruth[x86] Fix another miscompile found through fuzz testing...
2014-08-07 Chandler Carruth[x86] Fix another miscompile in the new vector shuffle...
2014-08-07 Chandler Carruth[x86] Fix another miscompile in the new vector shuffle...
2014-08-07 Pavel Chupin[x32] Use ebp/esp as frame and stack pointer
2014-08-07 Chandler Carruth[x86] Fix a miscompile in the new shuffle lowering...
2014-08-07 Pete CooperUpdate Tablegen documents given that binary literals...
2014-08-07 Pete CooperUpdate BitRecTy::convertValue to allow if expressions...
2014-08-07 Pete CooperChange the { } expression in tablegen to accept sized...
2014-08-07 Pete CooperChange BitsInit to inherit from TypedInit.
2014-08-07 Pete CooperChange TableGen so that binary literals such as 0b001...
2014-08-07 Pete CooperTableGen: Change { } to only accept bits<n> entries...
2014-08-07 Pete CooperFix a whole bunch of binary literals which were the...
2014-08-07 Chandler CarruthAdd an option to the shuffle fuzzer that lets you fuzz...
2014-08-07 Bill WendlingUse the minor number for the revision numbers.
2014-08-07 Chandler CarruthAdd a vector shuffle fuzzer.
2014-08-07 Justin BognerDebugInfo: Make a test more portable
2014-08-07 Saleem AbdulrasoolMC: split Win64EHUnwindEmitter into a shared streamer
2014-08-07 Quentin Colombet[X86][SchedModel] Fixed missing/wrong scheduling model...
2014-08-06 Kevin EnderbyAdd the -mcpu= option to llvm-objdump for use with...
2014-08-06 Reid KlecknerMC X86: Accept ".att_syntax prefix" and diagnose noprefix
2014-08-06 David BlaikieRevert "Reapply "DebugInfo: Ensure that all debug locat...
2014-08-06 Sanjay Patelfix typo
2014-08-06 Yaron KerengetNewMemBuffer memsets the buffer to zeros,
2014-08-06 Sanjay PatelFix a test that has no checks.
2014-08-06 Matt ArsenaultR600: Cleanup fadd and fsub tests
2014-08-06 Rui UeyamaRevert "r214897 - Remove dead zero store to calloc...
2014-08-06 Eric ChristopherRemove the target machine from CCState. Previously...
2014-08-06 Adrian PrantlImprove performance of calculateDbgValueHistory.
2014-08-06 Adrian PrantlCleanup collectChangingRegs
2014-08-06 David BlaikieDebugInfo: Fix ranges+gmlt test case to actually exerci...
2014-08-06 Reid KlecknerAdd a triple to this test to get the right IR mangling
2014-08-06 Reid KlecknerDon't count inreg params when mangling fastcall functions
2014-08-06 Reid KlecknerRound up the size of byval arguments to MinAlign
2014-08-06 Duncan P. N... UseListOrder: Use std::vector
2014-08-06 Chad Rosier[AArch64] Add a few isTarget* API to AArch64 Subtarget.
2014-08-06 Chad RosierAdd test case omitted in r214974.
2014-08-06 Chad Rosier[AArch64] Fix OS ABI flag for aarch64-linux-gnu target.
2014-08-06 Sanjay Pateluse register iterators that include self to reduce...
2014-08-06 Robert Khasanov[AVX512] Added load/store instructions to Register2Memo...
2014-08-06 James Molloy[AArch64] Add a testcase for r214957.
2014-08-06 James MolloyAdd a new option -run-slp-after-loop-vectorization.
2014-08-06 Tim NorthoverARM: do not generate BLX instructions on Cortex-M CPUs.
2014-08-06 Tim NorthoverARM-MachO: materialize callee address correctly on...
2014-08-06 James Molloy[AArch64] Conditional selects are expensive on out...
2014-08-06 Chandler Carruth[x86] Fix two independent miscompiles in the process...
2014-08-06 Chandler Carruth[x86] Switch to a formulation of a for loop that is...
2014-08-06 Adam Nemet[X86] Fixes commit r214890 to match the posted patch
2014-08-06 Matt ArsenaultCorrect comment
2014-08-06 Peter Collingbourne[dfsan] Try not to create too many additional basic...
2014-08-06 Matt ArsenaultR600: Increase nearby load scheduling threshold.
2014-08-06 Matt ArsenaultR600/SI: Implement areLoadsFromSameBasePtr
2014-08-06 Quentin Colombet[X86][SchedModel] Fixed some wrong scheduling model...
2014-08-06 David BlaikieDebugInfo: Assert that any CU for which debug_loc lists...
2014-08-05 David BlaikieDebugInfo: Fix a bunch of tests that, owing to their...
2014-08-05 Matt ArsenaultR600/SI: Add definitions for ds_read2st64_ / ds_write2st64_
2014-08-05 JF BastienFix typos in comments and doc
2014-08-05 David BlaikieDebugInfo: Move the reference to the CU from the locati...
2014-08-05 Rafael EspindolaRemove a virtual function from TargetMachine. NFC.
2014-08-05 Jonathan RoelofsRe-apply r214881: Fix return sequence on armv4 thumb
2014-08-05 Lang Hames[MCJIT] Make llvm-rtdyld check RuntimeDyld's error...
2014-08-05 Bill Schmidt[PowerPC] Swap arguments and adjust shift count for...
2014-08-05 Sanjay PatelImproved test cases that were added with r214892.
next