opencl/llvm.git
2013-10-08 Adrian PrantlReduce testcase from 1r92011.
2013-10-08 Nick Kledzikupdate mach-o EXPORT_SYMBOL_* names
2013-10-07 Hans Wennborgcmake: don't set LLVM_COMPILER_IS_GCC_COMPATIBLE when...
2013-10-07 David MajnemerWindows: Avoiding resizing, use uninitialized data...
2013-10-07 Akira Hatanaka[mips] Test case for r192124.
2013-10-07 Arnold SchwaighoferLoopVectorize: External uses must use the last value...
2013-10-07 Reed KotlerAdd Mips16 patterns for sign extend byte and sign exten...
2013-10-07 Manman RenStruct byval: use the correct alignment for loads gener...
2013-10-07 Akira Hatanaka[mips] Coding style clean up.
2013-10-07 Akira Hatanaka[mips] Disable tail merging when long branch pass is...
2013-10-07 Benjamin KramerX86: Fix type check. Just because an integer type is...
2013-10-07 Akira Hatanaka[mips] Define method MipsSubtarget::enableLongBranchPass.
2013-10-07 Alexey SamsonovRevert r191834 until we measure the effect of this...
2013-10-07 Akira Hatanaka[mips] Fix definition of mfhi and mflo instructions...
2013-10-07 Richard MittonFormally added an explicit enum for DWARF TLS support...
2013-10-07 Matt ArsenaultChange objectsize intrinsic to accept different address...
2013-10-07 Amara Emerson[ARM] Improve build attributes emission.
2013-10-07 Chad Rosier[AArch64] Add support for NEON scalar arithmetic instru...
2013-10-07 Joey Gouly[ARMv8] Add some disassembly tests for Thumb sevl/sevl.w
2013-10-07 NAKAMURA TakumiRevert r191088, corresponding to r191823 to re-enable...
2013-10-07 NAKAMURA TakumiWindows/Process.inc: Fix for +Asserts. &Buf[0] is not...
2013-10-07 Rafael EspindolaFix typo.
2013-10-07 Rafael EspindolaRemove dead code.
2013-10-07 Rafael EspindolaRemove getEHExceptionRegister and getEHHandlerRegister.
2013-10-07 Rafael EspindolaFix the documentation of getDefaultSubtargetFeatures.
2013-10-07 Tim NorthoverARM: allow cortex-m0 to use hint instructions
2013-10-07 David MajnemerWindows: Be more explicit with Win32 APIs
2013-10-07 Simon Atanasyan[Mips] Teach llvm-readobj to print MIPS-specific ELF...
2013-10-07 Craig TopperRemove some instructions that seem to only exist to...
2013-10-07 Craig TopperRemove FsMOVAPSrr and friends. They have no patterns...
2013-10-07 Craig TopperTeach X86 asm parser that VMOVAPSrr and other VEX-encod...
2013-10-07 Craig TopperAdd disassembler support for long encodings for INC...
2013-10-07 David MajnemerRevert "Revert "Windows: Add support for unicode comman...
2013-10-06 Craig TopperFix some assert messages to say the correct opcode...
2013-10-06 David MajnemerRevert "Windows: Add support for unicode command lines"
2013-10-06 David MajnemerWindows: Add support for unicode command lines
2013-10-06 Rafael EspindolaAdd support for aliases with linkonce_odr.
2013-10-06 Benjamin KramerForce a CPU that doesn't have AVX, otherwise this test...
2013-10-06 Benjamin KramerX86: Don't fold spills into SSE operations if the stack...
2013-10-06 Elena DemikhovskyAVX-512: added scalar convert instructions and intrinsics.
2013-10-06 Simon Atanasyan[Mips] Add MIPS program header types.
2013-10-06 Venkatraman... [Sparc] Do not emit nop after fcmp* instruction with V9.
2013-10-06 Elena DemikhovskyAVX-512: fixed shuffle lowering
2013-10-06 Venkatraman... [Sparc] Custom lower addc/adde/subc/sube on i64 in...
2013-10-06 Venkatraman... [Sparc] Use addxcc/subxcc for adde/sube instead of...
2013-10-05 Craig TopperAdd TBM instructions to loading folding tables.
2013-10-05 Nick LewyckyRename this feature to "cx16" to match gcc's flag name...
2013-10-05 Aaron BallmanSilencing an MSVC warning.
2013-10-05 Benjamin KramerEmit a better error when running out of registers on...
2013-10-05 Craig TopperRemove underscores from TBM instruction names for consi...
2013-10-05 Craig TopperRemove unneeded TBM intrinsics. The arithmetic/logical...
2013-10-05 Craig TopperAdd an additional pattern for BLCI since opt can turn...
2013-10-05 Rafael EspindolaRemove some really nasty uses of hasRawTextSupport.
2013-10-05 Benjamin Kramerlli: Plug leaks in the remote target external implement...
2013-10-05 Jiangning LiuImplement aarch64 neon instruction set AdvSIMD (Across).
2013-10-05 Craig TopperAdd OPC_CheckChildSame0-3 to the DAG isel matcher....
2013-10-05 Rafael EspindolaConvert test to FileCheck.
2013-10-05 Venkatraman... [Sparc] Use correct alignment while loading/storing...
2013-10-05 Andrew KaylorUpdating XFAILs for recent GOT tests
2013-10-05 Andrew KaylorAdding tests for multiple GOTs with MCJIT
2013-10-05 Andrew KaylorAdding multiple GOT handling to RuntimeDyldELF
2013-10-05 Manman RenDebug Info: In DIBuilder, the derived-from field of...
2013-10-05 Eric ChristopherReorganize some member variables and update a comment.
2013-10-05 Eric ChristopherFix one comment and update another. Slightly reformat.
2013-10-05 Venkatraman... [Sparc] Respect hasHardQuad parameter correctly when...
2013-10-05 Eric ChristopherAdd a resolve method on CompileUnit that forwards to...
2013-10-05 Adrian PrantlDebug info: Don't crash in SelectionDAGISel when a...
2013-10-05 Eric ChristopherMake a bunch of CompileUnit member functions private.
2013-10-04 Venkatraman... [Sparc] Correct the floating point conditional code...
2013-10-04 David BlaikieMinor formatting/comment rewording/etc.
2013-10-04 Eric ChristopherRemove odd use of this.
2013-10-04 Eric ChristopherReformat some odd formattings.
2013-10-04 Eric ChristopherTighten up some type arguments to functions. Where...
2013-10-04 Hal FinkelUpdatePHINodes in BasicBlockUtils should not crash...
2013-10-04 David BlaikieRemove some dead code.
2013-10-04 Eric ChristopherPull this out for a bit of readability.
2013-10-04 David BlaikieSimplify setting of DIE tag for type DIEs by setting...
2013-10-04 Eric ChristopherReformat.
2013-10-04 Eric ChristopherFormatting.
2013-10-04 Eric ChristopherPrune includes.
2013-10-04 Jack Carterforgot to remove this file as well
2013-10-04 Jack Carterreverting per request
2013-10-04 Eric ChristopherUse addFlag to add the enum class attribute.
2013-10-04 Eric ChristopherUse Die->addValue and DIEIntegerOne directly when we...
2013-10-04 Hal FinkelFix DAGCombiner::visitFP_EXTEND to ignore indexed loads
2013-10-04 Reed KotlerSupport tblockaddr for static compilation in Mips16.
2013-10-04 Rafael EspindolaFix object file writing in llvm-lto on Windows.
2013-10-04 Jack Carter[MC][AsmParser] Hook for post assembly file processing
2013-10-04 Andrew KaylorAttempting to fix lli build error
2013-10-04 Akira Hatanaka[mips] Fix a bug in MipsLongBranch::replaceBranch,...
2013-10-04 Arnold SchwaighoferSLPVectorizer: Sort inputs to commutative binary operations
2013-10-04 Andrew KaylorFixing container/pointer bug in remote-lli found by...
2013-10-04 Eric ChristopherTemporarily revert r176882 as it needs to be implemente...
2013-10-04 Benjamin Kramerlli: Check pipe creation for errors.
2013-10-04 Rafael EspindolaAdd lto_codegen_add_dso_symbol to the export list.
2013-10-04 Eric ChristopherTemporarily revert r191792 as it is causing some LTO...
2013-10-04 Matthias BraunFix comment
2013-10-04 Matthias BraunFix indentation
2013-10-04 Matthias BraunFix typo
2013-10-04 Matthias BraunARM: optimizeSelect has to consider the previous regist...
next