opencl/llvm.git
2014-11-01 Adrian PrantlTemporarily revert r220777 to sort out build bot breakage.
2014-11-01 Duncan P. N... IR: MDNode => Value: Instruction::getAllMetadata()
2014-11-01 Duncan P. N... IR: MDNode => Value: Instruction::getMetadata()
2014-10-31 Duncan P. N... IR: MDNode => Value: Add Instruction::getMDNode()
2014-10-31 Reid KlecknerRevert "R600: Add missing file to CMakeLists.txt"
2014-10-31 Reid KlecknerRevert "R600: Make sure to inline all internal functions"
2014-10-31 Reid KlecknerWork around bugs in MSVC "14" CTP 3's conversion logic
2014-10-31 Rafael EspindolaRefactor duplicated code in liking GlobalValues.
2014-10-31 Reid KlecknerDefine LLVM_NOEXCEPT with MSVC 14 CTP 3 or newer
2014-10-31 Reid KlecknerSuppress MSVC's equivalent of -Wshadow warnings
2014-10-31 David BlaikieSink some of DwarfDebug::collectDeadVariables down...
2014-10-31 Michael ZolotukhinCorrectly update dom-tree after loop vectorizer.
2014-10-31 David BlaikieSink most of DwarfDebug::constructAbstractSubprogramSco...
2014-10-31 Tom StellardR600: Add IPO to the list of required libraries
2014-10-31 Lang Hames[Object] Modify OwningBinary's interface to separate...
2014-10-31 Tom StellardR600: Add missing file to CMakeLists.txt
2014-10-31 Tom StellardR600: Don't promote allocas when one of the users is...
2014-10-31 Tom StellardR600: Make sure to inline all internal functions
2014-10-31 Duncan P. N... IR: Instruction::setMetadata() should use cast_or_null
2014-10-31 Duncan P. N... IR: MDNode => Value: Instruction::setMetadata()
2014-10-31 Bill Schmidt[PowerPC] Initial VSX intrinsic support, with min/max...
2014-10-31 Chad Rosier[AArch64] Check Dest Register Liveness in CondOpt pass.
2014-10-31 Kostya Serebryany[asan] do not treat inline asm calls as indirect calls
2014-10-31 Quentin Colombet[CodeGenPrepare] Move extractelement close to store...
2014-10-31 Kostya Serebryany[asan] fix caller-calee instrumentation to emit new...
2014-10-31 Justin BognerRemove the wrongly named and now empty Ocaml directory
2014-10-31 David BlaikieUpdate the non-pthreads fallback for RWMutex on Unix
2014-10-31 Rafael EspindolaUnify and update link-messages.ll and redefinition...
2014-10-31 David BlaikieCorrect assert text from r220923
2014-10-31 Rafael EspindolaMark a few variables const. NFC.
2014-10-31 NAKAMURA Takumi[CMake] llvm/examples: Update libdeps for unoptimized...
2014-10-31 Chad Rosier[AArch64] CondOpt pass is missing FCMP instructions...
2014-10-31 Bradley Smith[SCEV] Improve Scalar Evolution's use of no {un,}signed...
2014-10-31 Ulrich Weigand[PowerPC] Load BlockAddress values from the TOC in...
2014-10-31 Peter Zotov[OCaml] Ensure consistent naming.
2014-10-31 Peter Zotov[OCaml] Rework Llvm_executionengine using ctypes.
2014-10-31 Rafael EspindolaMove an input file to Inputs instead of using RUN:...
2014-10-31 David MajnemerObject, COFF: Cleanup symbol type code, improve binutil...
2014-10-31 Rafael Espindolamerge tests for constant linking.
2014-10-31 Rafael EspindolaMove definition closer to use. NFC.
2014-10-31 Hao LiuPR20557: Fix the bug that bogus cpu parameter crashes...
2014-10-31 NAKAMURA TakumiThreading.h: Give named parameters to llvm::call_once...
2014-10-30 Ahmed Bougacha[SelectionDAG] When scalarizing trunc, don't assert...
2014-10-30 Hans WennborgSpeculative fix for Windows build after r220932
2014-10-30 Chris BienemanEXPORTED_SYMBOL_FILE using mingw and cmake
2014-10-30 NAKAMURA Takumillvm/test/Transforms/SampleProfile/syntax.ll: Relax...
2014-10-30 Louis GerbargFix incorrect invariant check in DAG Combine
2014-10-30 Chris BienemanRemoving the static initializer in ManagedStatic.cpp...
2014-10-30 Justin Bognerllvm-cov: Follow LLVM naming conventions
2014-10-30 Justin Bognerllvm-cov: Don't manually parse an option for no reason
2014-10-30 Rafael EspindolaFix the merging of the constantness of declarations.
2014-10-30 Justin Bognerllvm-cov: Very basic top level help
2014-10-30 Philip ReamesAdd handling for range metadata in ValueTracking isKnow...
2014-10-30 Rafael EspindolaUpdate test to pass .ll to llvm-link and use Inputs.
2014-10-30 David BlaikiePR21408: Workaround the appearance of duplicate variabl...
2014-10-30 Diego NovilloFix comment spelling and tidy diagnostic call in profil...
2014-10-30 Peter Zotovlit: PR21417: don't try to update OCAMLPATH if LibDir...
2014-10-30 Diego NovilloFix Twine corruption problem with diagnostics.
2014-10-30 Diego NovilloAdd profile writing capabilities for sampling profiles.
2014-10-30 Tim NorthoverARM: test default values for TAG_CPU_unaligned_access...
2014-10-30 Simon Atanasyan[Mips] Add new Mips specific e_flags.
2014-10-30 Robert Khasanov[AVX512] Added VBROADCAST{SS/SD} encoding for VL subset.
2014-10-30 Peter Collingbourne[dfsan] New calling convention for custom functions...
2014-10-30 Peter Zotov[OCaml] Expose LLVMCloneModule.
2014-10-30 Peter Zotov[OCaml] Expose LLVM{Get,Set}DLLStorageClass.
2014-10-30 Peter Zotov[OCaml] Test code emission in Llvm_target.
2014-10-30 Peter Zotov[OCaml] Enable backtraces in tests.
2014-10-30 Peter Zotov[OCaml] [autoconf] Migrate to ocamlfind.
2014-10-30 Peter Zotov[OCaml] De-duplicate llvm_raise and llvm_string_of_message.
2014-10-30 Rafael EspindolaEnable the slp vectorizer in the gold plugin.
2014-10-30 Rafael EspindolaEnable the loop vectorizer in the gold plugin.
2014-10-29 Rafael EspindolaReplace also-emit-llvm with save-temps.
2014-10-29 NAKAMURA TakumiUntabify.
2014-10-29 NAKAMURA Takumillvm/test/Transforms/LoopRotate/nosimplifylatch.ll...
2014-10-29 Kevin EnderbyRun clang-format on tools/llvm-objdump/MachODump.cpp...
2014-10-29 Yi JiangTest Case for r220872:Do not simplifyLatch for loops...
2014-10-29 Yi JiangDo not simplifyLatch for loops where hoisting increment...
2014-10-29 Jan Wen VoungFix getRelocationValueString to return the symbol name...
2014-10-29 Alexander KornienkoEnable display of compiler diagnostics in clang-tidy...
2014-10-29 Robert Khasanov[AVX512] Implemented AVX512VL FP bnary packed instructi...
2014-10-29 NAKAMURA TakumiWhitespace.
2014-10-29 Michael KupersteinFix build with CMake if LLVM_USE_INTEL_JITEVENTS option...
2014-10-29 Peter Zotov[OCaml] Expose Llvm.parse_command_line_options.
2014-10-29 Peter Zotov[OCaml] Expose Llvm_target.TargetMachine.add_analysis_p...
2014-10-29 Peter Zotov[OCaml] If compiled without --enable-shared, hide packa...
2014-10-29 Peter Zotov[OCaml] Expose Llvm_bitwriter.write_bitcode_to_memory_b...
2014-10-29 Peter Zotov[OCaml] Drop support for 3.12.1 and earlier.
2014-10-29 Peter Zotov[OCaml] Synchronize transformations with LLVM-C.
2014-10-29 NAKAMURA Takumimacho-symbolized-disassembly.test: Don't check C++...
2014-10-29 Saleem Abdulrasooltest: tweak inlined-allocs test
2014-10-29 Seo SanghyeonVMCore was renamed to IR long time ago
2014-10-28 Kevin EnderbyUpdate llvm-objdump’s Mach-O symbolizer code to demangl...
2014-10-28 Peter Zotov[OCaml] PR5595: Pass LDFLAGS to tests via -cclib.
2014-10-28 Peter Zotov[OCaml] PR14083, PR9606: Only pick *.odoc files from...
2014-10-28 Peter Zotov[OCaml] Fix whitespace.
2014-10-28 Peter Zotov[OCaml] PR9719, PR14727: Make tests run without ocamlopt.
2014-10-28 Peter Zotov[OCaml] PR19859: Add functions to query and modify...
2014-10-28 Peter Zotov[C API] PR19859: Add functions to query and modify...
2014-10-28 Peter Zotov[OCaml] PR19859: Add tests for reading the values of...
2014-10-28 Peter Zotov[OCaml] PR19859: Add Llvm.{fcmp_predicate,float_of_const}.
next