opencl/llvm.git
2014-12-05 Adrian PrantlAdd a comment.
2014-12-05 Paul RobinsonMake GetSVN.cmake do its VCS queries with native CMake...
2014-12-05 Rafael EspindolalinkGlobalVariableProto never returns null. Simplify...
2014-12-05 Eric ChristopherRename the x86 isTargetMacho to isTargetMachO for unifo...
2014-12-05 Eric ChristopherBoth of these subtargets have functions that check...
2014-12-05 Rafael EspindolaMove merging of alignment to a central location. NFC.
2014-12-05 Rafael EspindolaAdd a few extra cases to the test. NFC.
2014-12-04 Kevin EnderbyRe-add support to llvm-objdump for Mach-O universal...
2014-12-04 Ahmed Bougacha[X86] Delete dead code in fcopysign lowering. NFC.
2014-12-04 Rafael EspindolaConvert test to use an extra Input file. NFC.
2014-12-04 Alexey SamsonovRevert "Fix UBSan report in StringMap implementation."
2014-12-04 Adrian PrantlSimplify implementation and testcase of r223401 based...
2014-12-04 Alexey SamsonovFix UBSan report in StringMap implementation.
2014-12-04 Adrian PrantlDebug info: If the RegisterCoalescer::reMaterializeTriv...
2014-12-04 Hans WennborgAdd some tests for SimplifyCFG's TurnSwitchRangeIntoICm...
2014-12-04 Hans WennborgAdd some tests for SimplifyCFG's ConstantFoldTerminator...
2014-12-04 Rafael EspindolaAlso use --icf=safe if we are being linked by gold.
2014-12-04 Roman DivackyAdd a FIXME as requested by Renato Golin.
2014-12-04 Yaron KerenSilence warning: variable 'buffer' set but not used.
2014-12-04 Bruno Cardoso... [x86] Fix isOffsetSuitableForCodeModel kernel code...
2014-12-04 Weiming Zhao[AArch64] Combining Load and IntToFp should check for...
2014-12-04 Asiri RathnayakeFix yet another unseen regression caused by r223113
2014-12-04 Jonathan RoelofsFix thumbv4t indirect calls
2014-12-04 Philip ReamesAdd a test case for argument type coercion in an invoke...
2014-12-04 Philip ReamesAdd a section to Statepoint docs mentioning shared...
2014-12-04 Rafael EspindolaDetect if the linker is gold and if so always use ...
2014-12-04 Hal FinkelRevert "r223364 - Revert r223347 which has caused crash...
2014-12-04 Philip ReamesFix a typo: use of cast where dyn_cast was intended
2014-12-04 Daniel Sanderstest-release.sh: Add a way to specify --build to configure
2014-12-04 Rafael EspindolaRemove dead code. NFC.
2014-12-04 Asiri RathnayakeFix a minor regression introduced in r223113
2014-12-04 Rafael EspindolaUse size_type in the interface exposed by SmallVector.
2014-12-04 Alexander PotapenkoRevert r223347 which has caused crashes on bootstrap...
2014-12-04 Rafael EspindolaRevert "[Thumb/Thumb2] Added restrictions on PC, LR...
2014-12-04 Michael Kuperstein[X86] Improve a dag-combine that handles a vector extra...
2014-12-04 Jyoti Allur[Thumb/Thumb2] Added restrictions on PC, LR, SP in...
2014-12-04 Andrea Di Biagio[X86] Simplify code. NFC.
2014-12-04 Daniel Sanderstest-release.sh: Correct the logged configure command...
2014-12-04 Patrik HagglundUse DomTree in MachineSink to sink over diamonds.
2014-12-04 Simon Pilgrim[InstCombine] Minor optimization for bswap with binary ops
2014-12-04 Elena DemikhovskyMasked Load / Store Intrinsics - the CodeGen part.
2014-12-04 Hal FinkelRestrict somewhat the memory-allocation pointer cmp...
2014-12-04 Jean-Daniel... Add missing test file
2014-12-04 Yaron Kerenclang-formatted ranged loops and assignment, NFC.
2014-12-04 Jean-Daniel... Add mach-o LC_RPATH support to llvm-objdump
2014-12-04 Michael Liao[X86] Clean up whitespace as well as minor coding style
2014-12-04 Rafael EspindolaRevert "Add missing test dependency and use a more...
2014-12-04 Rafael EspindolaAdd missing test dependency and use a more canonical...
2014-12-04 Colin LeMahieu[Hexagon] Adding lit exception if Hexagon isn't built.
2014-12-04 Colin LeMahieu[Hexagon] Marking some instructions as CodeGenOnly...
2014-12-04 NAKAMURA TakumiIntroduce "llvm-ranlib" as a name of targets since...
2014-12-04 NAKAMURA TakumiSort by alphabetical order.
2014-12-04 Michael Liao[X86] Restore X86 base pointer after call to llvm.eh...
2014-12-04 Hal Finkel[PowerPC] 'cc' should be an alias only to 'cr0'
2014-12-04 Philip ReamesMinor typo and link fixes for Statepoint documentation
2014-12-04 NAKAMURA TakumiHexagonMCInst.h: Qualify constants explicitly to appeas...
2014-12-04 Rafael EspindolaFor copy, cmake needs the full path to llvm-ar.
2014-12-04 Matt ArsenaultAllow target to specify prefix for labels
2014-12-04 Philip ReamesA few more checks for gc.statepoints in the Verifier
2014-12-04 Rafael EspindolaAdd missing dependency on llvm-ar. Should hopefully...
2014-12-03 Hal Finkel[PowerPC] Fix inline asm memory operands not to use r0
2014-12-03 Quentin Colombet[RegAllocFast] Handle implicit definitions conservatively.
2014-12-03 Rafael EspindolaThis reverts commit r223306 and r223277.
2014-12-03 Kostya Serebryany[msan] allow -fsanitize-coverage=N together with -fsani...
2014-12-03 Jacques PienaarTest commit.
2014-12-03 Rafael EspindolaMake llvm-ar a real build target and install it.
2014-12-03 Chris MatthewsAdd a test-case for lit xunit output
2014-12-03 Kevin EnderbyMove tests for llvm-objdump for universal files to...
2014-12-03 Chris MatthewsDon't allow test-suite names with . in them in xml...
2014-12-03 Rafael EspindolaSplit the set of identified struct types into opaque...
2014-12-03 Kevin EnderbyAdd support to llvm-objdump for Mach-O universal files...
2014-12-03 Sanjay Patelfix typos, grammar, formatting; NFC
2014-12-03 Philip ReamesStrength Verifier checks around the types involved...
2014-12-03 Matthias Brauncorrect spelling, NFC
2014-12-03 Matthias Braun[SimplifyLibCalls] Improve double->float shrinking...
2014-12-03 Matthias Braun[SimplifyLibCalls] Enable double to float shrinking...
2014-12-03 Colin LeMahieu[Hexagon] Converting member InstrDesc to static variable.
2014-12-03 Nico WeberFix grammar-o.
2014-12-03 Colin LeMahieu[Hexagon] Converting subclass members to an implicit...
2014-12-03 David Blaikierange-for some things
2014-12-03 David BlaikieSimplify CodeGenRegBank::inferMatchingSuperRegClass...
2014-12-03 David BlaikieSimplify ownership of RegClasses by using list<CodeGenR...
2014-12-03 David BlaikieRange-for some stuff related to RegClasses, and comment...
2014-12-03 Philip ReamesMake the Verifier more strict about gc.statepoints
2014-12-03 Will SchmidtAdd TableGen info for Power8.
2014-12-03 Roman DivackyChange the name to be in style.
2014-12-03 Matt ArsenaultFix sphinx error from Statepoints.rst
2014-12-03 Tom StellardR600/SI: Move SIInsertWaits into AMDGPUPassConfig:...
2014-12-03 Tom StellardR600/SI: Don't run SI passes on R600 subtargets
2014-12-03 Tim NorthoverAArch64: fix wrong-endian parameter passing.
2014-12-03 Colin LeMahieu[NFC] Fixing pendantic warning extra semicolons.
2014-12-03 Colin LeMahieu[Hexagon] [NFC] Moving function implementations out...
2014-12-03 Nick LewyckyFix test to use the right metadata node (reapply r22323...
2014-12-03 Colin LeMahieu[Hexagon] [NFC] Renaming *packetStart to *packetBegin
2014-12-03 Alexander PotapenkoRevert r223239, which broke some bots.
2014-12-03 Alexander PotapenkoFix the metadata number used by llvm.gcov to match...
2014-12-03 Aaron BallmanSilencing several "multiple copy constructors" warnings...
2014-12-03 Aaron BallmanSilencing a 32-bit implicit conversion warning in MSVC...
2014-12-03 Evgeniy Stepanovmsan] Add compile-time checks for missing origins.
2014-12-03 Erik EcksteinInstCombine: simplify signed range checks
next