opencl/llvm.git
2014-06-30 Reid KlecknerSpeculatively fix some code handling Power64 MachO...
2014-06-30 Reid Klecknermsan: Stop stripping the 'tail' modifier off of calls
2014-06-30 Ed Masteobjdump: Add test for ELF file with no section table
2014-06-30 Ehsan AkhgariRefactor the code in clang to find a file in a PATH...
2014-06-30 Alp TokerFix 'platform-specific' hyphenations
2014-06-30 Alp TokerBuild fix for systems without futimes/futimens
2014-06-30 Kevin EnderbyAdd the -arch flag support to llvm-nm to select the...
2014-06-30 Matt ArsenaultR600: Move mul combine to separate function
2014-06-30 Matt ArsenaultR600: Remove unused declarations leftover from AMDIL
2014-06-30 Adrian PrantlDebug info: split out complex DIVariable address expres...
2014-06-30 Andrea Di Biagio[X86] Add support for builtin to read performance monit...
2014-06-30 Peter Zotov[OCaml] Documentation improvements.
2014-06-30 Chad Rosier[AArch64] Unsized types don't specify an alignment.
2014-06-30 Chad Rosier[AArch64] Convert mul x, -(pow2 +/- 1) to shift + add...
2014-06-30 Tim Northovermacho-dump: add code to print LC_ID_DYLIB load commands.
2014-06-30 Scott DouglassARM: take care not to set the ThumbFunc bit on TLS...
2014-06-30 Scott Douglassundo test commit (whitespace only)
2014-06-30 Scott Douglasstest commit (whitespace only)
2014-06-30 Erik Ecksteintest commit: add a comment line in GVN test file
2014-06-30 Saleem AbdulrasoolX86: fix comment
2014-06-30 Saleem AbdulrasoolARM: use symbolic name for constant
2014-06-29 Saleem AbdulrasoolCodeGen: rename Win64 ExceptionHandling to WinEH
2014-06-29 Saleem AbdulrasoolMC: rename EmitWin64EH routines
2014-06-29 Craig TopperAdd ops() method to SDNode that returns an ArrayRef...
2014-06-28 Rafael EspindolaUse a range loop. No functionality change.
2014-06-28 Rafael EspindolaSimplify code a bit, no functionality change.
2014-06-28 Alp TokerFix build following r211956
2014-06-28 David MajnemerVerifier: Update assert message to reflect LangRef
2014-06-28 Chandler Carruth[x86] Fix a bug in the v8i16 shuffling exposed by the...
2014-06-28 Chandler CarruthFix this test to not write to the source tree, and...
2014-06-28 Chandler Carruth[x86] Add handling for splat-like widenings of v16i8...
2014-06-28 David MajnemerThis file wasn't supposed to be checked in
2014-06-27 Lang Hames[RuntimeDyld] Make sure that RuntimeDyld regression...
2014-06-27 Matt ArsenaultRevert "Temporary hack to try cleaning extra .s file...
2014-06-27 Matt ArsenaultTemporary hack to try cleaning extra .s file from bots.
2014-06-27 Lang Hames[RuntimeDyld] Use a raw_ostream and llvm::format for...
2014-06-27 Chad Rosier[AArch64] Fix memset ICE when memset value is f128.
2014-06-27 Justin Bognerllvm-cov: Support specifying multiple source files
2014-06-27 Lang Hames[RuntimeDyld] #include <cctype> header in RuntimeDyldCh...
2014-06-27 Lang Hames[RuntimeDyld] Add a framework for testing relocation...
2014-06-27 Chandler Carruth[x86] Fix another bug hit when bootstrapping with the...
2014-06-27 Aaron BallmanReverting r211950 -- it did not help resolve the -Wcomm...
2014-06-27 Justin Holewinski[NVPTX] Use GreatestCommonDivisor64 from MathExtras...
2014-06-27 Aaron BallmanAdding some trailing whitespace after a comment previou...
2014-06-27 David MajnemerInclude <tuple> to make buildbots happy
2014-06-27 Justin Holewinski[NVPTX] Add reflect intrinsic (better than matching...
2014-06-27 Justin Holewinski[NVPTX] Handle all possible vector types in getSetCCRes...
2014-06-27 Justin Holewinski[NVPTX] Add 'b' asm constraint
2014-06-27 Justin Holewinski[NVPTX] Simplify some argument lowering logic
2014-06-27 Justin Holewinski[NVPTX] Do not process samplers in GenericToNVVM
2014-06-27 Justin Holewinski[NVPTX] Error out if initializer is given for variable...
2014-06-27 Justin Holewinski[NVPTX] Add support for .managed variables for UVM
2014-06-27 Justin Holewinski[NVPTX] Emit .weak linkage for link_once, weak, availab...
2014-06-27 Justin Holewinski[NVPTX] Variables that start with llvm. or nvvm. are...
2014-06-27 Justin Holewinski[NVPTX] Fix handling of ldg/ldu intrinsics.
2014-06-27 Justin Holewinski[NVPTX] Clean up argument lowering code and properly...
2014-06-27 Justin Holewinski[NVPTX] Add missing boolean vector contents flag
2014-06-27 Justin Holewinski[NVPTX] Add support for [SHL,SRA,SRL]_PARTS
2014-06-27 Justin Holewinski[NVPTX] Implement fma and imad contraction as target...
2014-06-27 Justin Holewinski[NVPTX] Add support for efficient rotate instructions...
2014-06-27 Justin Holewinski[NVPTX] Add missing isel patterns for 64-bit atomics
2014-06-27 Justin Holewinski[NVPTX] Add isel patterns for bit-field extract (bfe)
2014-06-27 Justin Holewinski[NVPTX] Add support for isspacep instruction
2014-06-27 Justin Holewinski[NVPTX] Add support for envreg reads
2014-06-27 Justin Holewinski[NVPTX] Add target options for PTX 3.2/4.0 and SM 5...
2014-06-27 Justin Holewinski[NVPTX] Update sub-target feature detection
2014-06-27 Justin Holewinski[NVPTX] Directly control the Machine SSA passes that...
2014-06-27 Justin Holewinski[NVPTX] Emit .weak when linkage is not external, intern...
2014-06-27 Justin Holewinski[NVPTX] Just use getTypeAllocSize() when computing...
2014-06-27 Tyler NowickiVectorization documentation for loop hint pragmas and...
2014-06-27 Aaron BallmanSilencing some -Wcast-qual warnings. No functional...
2014-06-27 Chandler Carruth[x86] Fix a miscompile in the new shuffle lowering...
2014-06-27 David MajnemerIR: Add COMDATs to the IR
2014-06-27 Reid Klecknercmake: Don't do anything for LLVM_ENABLE_ASSERTIONS=OFF
2014-06-27 Julien Lerougelldb can interrupt waitpid, so EINTR shouldn't be an...
2014-06-27 Matt ArsenaultR600: Move trivial getters into header, use initializer...
2014-06-27 David BlaikieFix test so it doesn't try to write out temporary files...
2014-06-27 Logan ChienAvoid non-ascii character in the source code.
2014-06-27 David MajnemerMC: Fix associative sections on COFF
2014-06-27 Juergen Ributzka[FastISel][X86] Fix typos.
2014-06-27 Matt ArsenaultR600: Don't crash on unhandled instruction in promote...
2014-06-27 Ed Mastellvm-objdump: don't assert if ELF file has no sections
2014-06-27 Alexander KornienkoClean up unused variable warning in release build.
2014-06-27 Chandler CarruthRe-apply r211287: Remove support for LLVM runtime multi...
2014-06-27 Ulrich Weigand[PowerPC] Constrain base register in PPCRegisterInfo...
2014-06-27 Chandler Carruth[x86] Clean up some unused variables, especially in...
2014-06-27 Chandler Carruth[x86] Teach the target combine step to aggressively...
2014-06-27 Simon Atanasyan[ELF][Mips] Fix recognition of MIPS 64-bit arch in...
2014-06-27 Chandler Carruth[x86] Teach the target-specific combining how to aggres...
2014-06-27 Chandler Carruth[x86] Teach the X86 backend to DAG-combine SSE2 shuffle...
2014-06-27 Chandler Carruth[x86] Begin a significant overhaul of how vector loweri...
2014-06-27 Ulrich Weigand[RuntimeDyld, PowerPC] Fix/improve handling of TOC...
2014-06-27 Alp TokerIRReader: don't mark MemoryBuffers const
2014-06-27 Dinesh DwivediAdded instruction combine to transform few more negativ...
2014-06-27 Eric ChristopherRemove the caching of the target machine from SystemZTa...
2014-06-27 David MajnemerGlobalOpt: Fix constantfold-initializers.ll test
2014-06-27 Eric ChristopherRemove target machine caching from SystemZInstrInfo and
2014-06-27 David BlaikieRevert "Revert "Revert "PR20038: DebugInfo: Inlined...
2014-06-27 David BlaikieArgumentPromotion: Propagate debug locations on calls...
2014-06-27 David BlaikieRevert "Revert "PR20038: DebugInfo: Inlined call sites...
next