opencl/llvm.git
2015-01-22 Jon Humphreys- Added some stub implementations for C6000 target...
2015-01-22 Jon HumphreysAdded C6000 LLVM target specialization files.
2015-01-22 Jon Humphreys modified: include/llvm/IR/Intrinsics.td
2015-01-22 Jon HumphreysAdded TI generic and C6x specific intrinsics
2015-01-22 Duncan P. N... IR: Change GenericDwarfNode::getHeader() to StringRef
2015-01-22 Duncan P. N... IR: DwarfNode => DebugNode, NFC
2015-01-22 Simon Pilgrim[X86][AVX] Added (V)MOVDDUP / (V)MOVSLDUP / (V)MOVSHDUP...
2015-01-22 Simon PilgrimLine endings fixes. NFC.
2015-01-22 Simon Pilgrim[X86][SSE] Simplified PSUBUS tests
2015-01-22 Lang Hames[Object] Fix a bug in a condition introduced in r226217...
2015-01-22 Chandler Carruth[PM] Actually add the new pass manager support for...
2015-01-22 Benjamin KramerRemove dead leak detector parts that fell out of use...
2015-01-22 Duncan P. N... IR: Update references to temporaries before deleting
2015-01-22 Chris BienemanRefactoring cl::parser construction and initialization.
2015-01-22 Rafael EspindolaDon't use -z,defs on FreeBSD.
2015-01-22 Ramkumar Ramachandra[emacs] Use c-mode-common-hook, derive from "gnu"
2015-01-22 Ramkumar RamachandraIntrinsics: introduce llvm_any_ty aka ValueType Any
2015-01-22 Reid KlecknerRevert "Don't remove a landing pad if the invoke requir...
2015-01-22 Kevin EnderbyAdd the option, -indirect-symbols, used with -macho...
2015-01-22 Sanjay Patelmerge consecutive stores of extracted vector elements...
2015-01-22 Adrian PrantlFix the condition in this assertion, and also make...
2015-01-22 David BlaikieRevert "PR21408: Workaround the appearance of duplicate...
2015-01-22 Tim NorthoverAArch64: decode all MRS/MSR forms early to avoid saving...
2015-01-22 Adrian PrantlRun clang-format on parts of DebugInfo.h
2015-01-22 Adrian PrantlDocument DIExpression.
2015-01-22 Adrian PrantlRewrite DIExpression::printInternal() to use the iterat...
2015-01-22 Adrian PrantlRename DIExpressionIterator to DIExpression::iterator.
2015-01-22 Adrian PrantlFix a comment.
2015-01-22 Rafael Espindola[pr21886] Change MCJIT/ELF to support MSVC C++ mangled...
2015-01-22 Rafael EspindolaPass -Wl,-z,defs when building shared libraries, but...
2015-01-22 Aaron BallmanSilencing a -Wsign-compare warning (all uses of this...
2015-01-22 Michael Kuperstein[DAGCombine] Produce better code for constant splats
2015-01-22 Alexander PotapenkoMark |TLI| variables used to suppress -Wunused-variable...
2015-01-22 Michael KupersteinRevert r226811, MSVC accepts code sane compilers don't.
2015-01-22 Michael Kuperstein[DAGCombine] Produce better code for constant splats
2015-01-22 Timur Iskhodzhanov[ASan/Win] Move the shadow to 0x30000000
2015-01-22 Elena DemikhovskyFixed a bug in type legalizer for masked load/store...
2015-01-22 Elena DemikhovskyFixed a comment
2015-01-22 Elena DemikhovskyFixed a bug in narrowing store operation.
2015-01-22 Sanjoy Das[NFC] Introduce a 'struct Range' for IRCE
2015-01-22 Craig TopperRevert r226798. Guess I missed the patterns.
2015-01-22 Craig TopperUse u8imm instead of i32i8imm on a couple instructions...
2015-01-22 Craig Topper[X86] Remove some unused multiclasses from AVX512 instr...
2015-01-22 Sanjoy DasFix crashes in IRCE caused by mismatched types
2015-01-22 Erik EcksteinSLPVectorizer: add a second limit for the number of...
2015-01-22 Elena DemikhovskyFixed a bug in masked load/store in reversed loop.
2015-01-22 Chandler Carruth[PM] Rename InstCombine.h to InstCombineInternal.h...
2015-01-22 Chandler Carruth[canonicalize] Teach InstCombine to canonicalize loads...
2015-01-22 Saleem AbdulrasoolARM: fail less catastrophically on invalid Windows...
2015-01-22 Chandler Carruth[canonicalize] Move a helper function further up the...
2015-01-22 Duncan P. N... DIBuilder: Make header iterator constructor explicit...
2015-01-22 Duncan P. N... DIBuilder: Extract header_begin() and header_end()...
2015-01-22 Duncan P. N... DIBuilder: Stop abusing DIExpressionIterator::operator...
2015-01-22 Duncan P. N... DIBuilder: Extract DIHeaderFieldIterator::getNumber...
2015-01-22 Duncan P. N... DIBuilder: Create a getHeaderIterator() helper, NFC
2015-01-22 Chris BienemanMaking deleted copy constructors and operators to be...
2015-01-22 Reid KlecknerSEH: Finish writing the catch-all test case
2015-01-22 Reid KlecknerWin64 SEH: Emit the constant 1 for catch-all into xdata
2015-01-22 Chris BienemanAssigning and copying command line option objects shoul...
2015-01-22 Sanjoy DasMake ScalarEvolution less aggressive with respect to...
2015-01-22 Paul RobinsonExplicitly describe '///' versus '//' comment delimiters.
2015-01-22 Adrian PrantlMake DwarfExpression use the new DIExpressionIterator...
2015-01-22 Adrian PrantlRewrite DIExpression::Verify() using an iterator. NFC.
2015-01-21 Chandler Carruth[canonicalization] Refactor how we create new stores...
2015-01-21 Simon Pilgrim[X86][SSE] Missing SSE/AVX1 memory folding integer...
2015-01-21 Tim NorthoverDAGCombine: fold (or (and X, M), (and X, N)) -> (and...
2015-01-21 David BlaikieDebugInfo: Use distinct inlinedAt MDLocations to avoid...
2015-01-21 Matt ArsenaultR600: Add checks for urem/srem by a constant
2015-01-21 Matthias BraunLiveIntervalAnalysis: Mark subregister defs as undef...
2015-01-21 Chris BienemanAdding a new cl::HideUnrelatedOptions API to allow...
2015-01-21 Simon Pilgrim[X86][SSE] Added support for SSE3 lane duplication...
2015-01-21 Matt ArsenaultR600: Add missing tests for i64 srem
2015-01-21 Jonathan RoelofsFix load-store optimizer on thumbv4t
2015-01-21 George Burgess IVAdded test to cover the CFLAA bitset indexing bug.
2015-01-21 David MajnemerInstCombine: Don't strip bitcasts off of callsites...
2015-01-21 Simon Pilgrim[X86][SSE] movddup shuffle mask decodes
2015-01-21 Adrian Prantlsimplify expression
2015-01-21 Adrian PrantlFix a compile issue on MSVC and call finalize().
2015-01-21 Matthias BraunLiveIntervalAnalysis: Factor out code to update livenes...
2015-01-21 Matthias BraunLiveIntervalAnalysis: document removePhysRegDefAt(...
2015-01-21 Matthias BraunLiveIntervalAnalysis: Factor out code to update livenes...
2015-01-21 Matthias BraunLiveIntervalAnalysis: Remove unused pruneValue() variant.
2015-01-21 Adrian PrantlLet subprograms with instructions without parent scopes...
2015-01-21 Matt ArsenaultR600/SI: Custom lower fround
2015-01-21 Colin LeMahieu[Hexagon] Converting multiply and accumulate with immed...
2015-01-21 Ahmed Bougacha[X86] Declare SSE4.1/AVX2 vector extloads covered by...
2015-01-21 Eric Fiselier[lit] Format JSONMetricValue strings better.
2015-01-21 George Burgess IVFixed a bug with how we determine bitset indices.
2015-01-21 Yaron KerenAdd missing include guards to WindowsSupport.h.
2015-01-21 Tim NorthoverRevert "DAGCombine: fold (or (and X, M), (and X, N...
2015-01-21 Tim NorthoverAArch64: add backend option to reserve x18 (platform...
2015-01-21 Tim NorthoverDAGCombine: fold (or (and X, M), (and X, N)) -> (and...
2015-01-21 Michael Kuperstein[x32] Fast ISel should use LEA64_32r instead of LEA32r...
2015-01-21 Alexander PotapenkoUse a smaller pragma unroll threshold to reduce test...
2015-01-21 Evgeniy Stepanov[msan] Update origin for the entire destination range...
2015-01-21 Jozef Kolek[mips][microMIPS] MicroMIPS 16-bit unconditional branch...
2015-01-21 Jozef Kolek[mips][microMIPS] Implement ADDIUPC instruction
2015-01-21 Chandler Carruth[PM] Refactor the InstCombiner interface to use an...
2015-01-21 Chandler Carruth[PM] Simplify (ha! ha!) the way that instcombine calls the
2015-01-21 Vladimir Medic[Mips][Disassembler]When disassembler meets load/store...
next