]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/shortlog
opencl/llvm.git
2014-12-24 Chandler Carruth[SROA] Refactor the integer and vector promotion testin...
2014-12-24 Colin LeMahieu[Hexagon] Removing old classes.
2014-12-24 Kevin EnderbyAnother attempt to fix the LLVM Windows build bot lld...
2014-12-23 Kevin EnderbyAttempt to fix the LLVM Windows build bot lld-x86_64...
2014-12-23 Kevin EnderbyAdd printing the LC_THREAD load commands with llvm...
2014-12-23 Kostya Serebryany[asan] change the coverage collection scheme so that...
2014-12-23 Hal Finkel[PowerPC] Ensure that the TOC reload directly follows...
2014-12-23 Colin LeMahieu[Hexagon] Adding doubleword load.
2014-12-23 Colin LeMahieu[Hexagon] Reapplying 224775 load words.
2014-12-23 Jozef Kolek[mips][microMIPS] Implement CACHE, PREF, SSNOP, EHB...
2014-12-23 Colin LeMahieuReverting 224775 until mayLoad flag is addressed.
2014-12-23 Rafael EspindolaFinish removing DestroySource.
2014-12-23 Adrian PrantlDIBuilder: Similar to createPointerType, make createMem...
2014-12-23 Mehdi AminiAlways assert in DAGCombine and not only when -debug...
2014-12-23 Rafael EspindolaPass LSAN_OPTIONS down so that it is possible to add...
2014-12-23 Rafael EspindolaFix a leak found by asan.
2014-12-23 Colin LeMahieu[Hexagon] Adding word loads.
2014-12-23 Colin LeMahieu[Hexagon] Adding signed halfword loads.
2014-12-23 Rafael EspindolaFix a leak found by asan.
2014-12-23 Colin LeMahieu[Hexagon] Adding unsigned halfword load.
2014-12-23 Jozef Kolek[mips][microMIPS] Implement LWSP and SWSP instructions
2014-12-23 Peter Zotov[OCaml] PR22014: OCaml bindings didn't link to libLLVM...
2014-12-23 Michael Kuperstein[ValueTracking] Move GlobalAlias handling to be after...
2014-12-23 Elena DemikhovskyAVX-512: Added FMA instructions, intrinsics an tests...
2014-12-23 Hal Finkel[PowerPC] Don't mark the return-address slot as immutable
2014-12-23 Elena DemikhovskyAVX-512: BLENDM - fixed encoding of the broadcast version
2014-12-23 Michael Kuperstein[DagCombine] Improve DAGCombiner BUILD_VECTOR when...
2014-12-23 Hal Finkel[PowerPC] Don't attempt a 64-bit pow2 division on PPC32
2014-12-23 Michael Liao[SimplifyCFG] Revise common code sinking
2014-12-23 Michael KupersteinRemove a bad cast in CloneModule()
2014-12-23 Ahmed Bougacha[ARM] Don't break alignment when combining base updates...
2014-12-23 Alexey SamsonovFix UBSan bootstrap: replace shift of negative value...
2014-12-23 Alexey SamsonovFix UBSan bootstrap: don't bind reference to nullptr.
2014-12-23 Chandler CarruthRevert r224739: Debug info: Teach SROA how to update...
2014-12-23 Jim GrosbachX86: Don't over-align combined loads.
2014-12-22 Reid KlecknerMake musttail more robust for vector types on x86
2014-12-22 David BlaikieRemove dynamic allocation/indirection from GCOVBlocks...
2014-12-22 Adrian PrantlThumb1 frame lowering: Mark CFI instructions with the...
2014-12-22 Chandler Carruth[SROA] Lift the logic for traversing the alloca slices...
2014-12-22 Bruno Cardoso... [LCSSA] Handle PHI insertion in disjoint loops
2014-12-22 Adrian PrantlDebug info: Teach SROA how to update debug info for...
2014-12-22 Reid KlecknerFix Windows unwind info for functions in sections other...
2014-12-22 Colin LeMahieu[Hexagon] Adding memb instruction. Fixing whitespace...
2014-12-22 David BlaikieUse iterators rather than indices to make this forwards...
2014-12-22 David Blaikieunique_ptrify MatchableInfo(const CodeGenInstAlias...
2014-12-22 Colin LeMahieu[Hexagon] Adding classes and load unsigned byte instruc...
2014-12-22 Bruno Cardoso... [x86] Add vector @llvm.ctpop intrinsic custom lowering
2014-12-22 Juergen RibutzkaRemove unused header. NFC.
2014-12-22 Adrian PrantlAdd a C++ marker to this header file.
2014-12-22 Peter Zotov[C API] Expose LLVMGetGlobalValueAddress and LLVMGetFun...
2014-12-22 Quentin Colombet[CodeGenPrepare] Handle properly the promotion of opera...
2014-12-22 Elena DemikhovskyAVX-512: Added all forms of BLENDM instructions,
2014-12-22 Karthik BhatLower multiply-negate operation to mneg on AArch64
2014-12-22 Rafael EspindolaConvert a few tests to FileCheck. NFC.
2014-12-22 Rafael EspindolaThe leak detector is dead, long live asan and valgrind.
2014-12-21 Saleem AbdulrasoolCodeGen: minor style tweaks to SSP
2014-12-21 Craig Topper[X86] Add hasSideEffects = 0 to CALLpcrel16. This match...
2014-12-21 Matt ArsenaultEnable (sext x) == C --> x == (trunc C) combine
2014-12-20 Craig Topper[X86] Swap operand order in Intel syntax on a bunch...
2014-12-20 Craig Topper[X86] Swap operand order of imul aliases in Intel synta...
2014-12-20 Craig Topper[X86] Remove '*' from asm strings in far call/jump...
2014-12-20 Craig Topper[X86] Don't swap the order of segment and offset in...
2014-12-20 Saleem AbdulrasoolCodeGen: constify and use range loop for SSP
2014-12-20 Saleem AbdulrasoolARM: further improve deprecated diagnosis (LDM)
2014-12-20 David Majnemerstrnlen isn't available on some platforms, use StringRe...
2014-12-20 Craig Topper[X86] Immediate forms of far call/jump are not valid...
2014-12-20 David MajnemerThis should have been part of r224676.
2014-12-20 David MajnemerInstCombine: Squash an icmp+select into bitwise arithmetic
2014-12-20 David MajnemerInstSimplify: Don't bother if getScalarSizeInBits retur...
2014-12-20 David MajnemerSimplify the code
2014-12-20 Eric FiselierSplit executeShTest into two parts so that it can be...
2014-12-20 David MajnemerInstSimplify: Optimize away pointless comparisons
2014-12-20 Chandler Carruth[SROA] Run clang-format over the entire SROA pass as...
2014-12-20 Chandler Carruth[x86] Change the test added in r223774 to first check...
2014-12-20 Matthias BraunLiveIntervalAnalysis: No kill flags for partially undef...
2014-12-20 Matthias BraunLiveIntervalAnalysis: cleanup addKills(), NFC
2014-12-20 Matthias BraunUnbreak cmake build with shared libraries enabled.
2014-12-20 Eric ChristopherRemove unused variable and initialization.
2014-12-19 Eric ChristopherRemove unused variable, initializer, and accessor.
2014-12-19 Matt ArsenaultR600: Remove outdated comment
2014-12-19 Elena DemikhovskyMasked load and store codegen - fixed 128-bit vectors
2014-12-19 Matt ArsenaultR600/SI: Only form min/max with 1 use.
2014-12-19 Reid KlecknerEH: Sink computation of local PadMap variable into...
2014-12-19 Eric Fiselier[LIT] Add JSONMetricValue type to wrap types supported...
2014-12-19 Kevin EnderbyAdd printing the LC_ROUTINES load commands with llvm...
2014-12-19 Reid KlecknerAdd the ExceptionHandling::MSVC enumeration
2014-12-19 Sanjay PatelModel sqrtss as a binary operation with one source...
2014-12-19 Tom StellardR600/SI: isLegalOperand() shouldn't check constant...
2014-12-19 Tom StellardR600/SI: Make sure non-inline constants aren't folded...
2014-12-19 Yaron KerenRemove isSubroutineType test for isCompositeType, getTa...
2014-12-19 David BlaikieUpdate SmallPtrSet::insert's doc comment to match the...
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_CLIENT load command with llvm...
2014-12-19 Peter CollingbourneCodeGen: do not attempt to invalidate virtual registers...
2014-12-19 Colin LeMahieu[Hexagon] Removing old variants of instructions and...
2014-12-19 Sanjay Patelmerge consecutive stores of extracted vector elements
2014-12-19 Colin LeMahieu[Hexagon] Adding bit extraction and table indexing...
2014-12-19 Colin LeMahieu[Hexagon] Adding bit insertion instructions.
2014-12-19 Colin LeMahieu[Hexagon] Adding more xtype shift instructions.
2014-12-19 Kevin EnderbyAdd printing the LC_SUB_LIBRARY load command with llvm...
2014-12-19 Colin LeMahieu[Hexagon] Adding xtype shift instructions.
next