opencl/llvm.git
2015-01-10 Ramkumar Ramachandra.gitignore: add some rules for tagging programs
2015-01-10 Hal Finkel[PowerPC] Mark zext of a small scalar load as free
2015-01-10 Justin HibbitsRemove some whitespace.
2015-01-10 Dmitri GribenkoConvertUTFTest: fix misleading empty line
2015-01-10 Saleem Abdulrasooltests: fix previous commit
2015-01-10 Saleem Abdulrasooltest: merge ARM relocations test
2015-01-10 Saleem Abdulrasooltests: convert a couple of ARM relocation tests to...
2015-01-10 Justin HibbitsFully fix Bug #22115.
2015-01-10 Alexey SamsonovFix undefined behavior (shift of negative value) in...
2015-01-10 Hal Finkel[PowerPC] Readjust the loop unrolling threshold
2015-01-10 Hal Finkel[LoopUnroll] Fix the partial unrolling threshold for...
2015-01-10 Rafael EspindolaUse the DiagnosticHandler to print diagnostics when...
2015-01-09 Alexey SamsonovFix UBSan error reports in ValueMapCallbackVH and Asser...
2015-01-09 Alexey SamsonovDisable Go bindings test under UBSan.
2015-01-09 Andrew KaylorFix the JIT event listeners and replace the associated...
2015-01-09 Michael ZolotukhinUpdate comment.
2015-01-09 Hans WennborgSimplifyCFG: check uses of constant-foldable instrs...
2015-01-09 Simon Pilgrim[X86][SSE] Avoid vector byte shuffles with zero by...
2015-01-09 Kevin EnderbyFix an ASAN failure introduced with r225537 (adding...
2015-01-09 Rafael EspindolaAdd a testcase of llvm-lto error handling.
2015-01-09 Michael ZolotukhinRemove duplicating code. NFC.
2015-01-09 Kevin EnderbyAdd the option, -universal-headers, used with -macho...
2015-01-09 Tim NorthoverRe-reapply r221924: "[GVN] Perform Scalar PRE on gep...
2015-01-09 Lang HamesRecommit r224935 with a fix for the ObjC++/AArch64...
2015-01-09 Duncan P. N... Revert "Bitcode: Move the DEBUG_LOC record to DEBUG_LOC...
2015-01-09 Daniel Sanders[mips] Add support for accessing $gp as a named register.
2015-01-09 Sanjay Patelfix typos; remove names from comments; NFC
2015-01-09 Sanjay Patelremove names from comments; NFC
2015-01-09 Sanjay Patelfix typos; NFC
2015-01-09 Sanjay Patelfix typo; NFC
2015-01-09 Sanjay Patelmore efficient use of a dyn_cast; no functional change...
2015-01-09 Hal Finkel[PowerPC] Enable late partial unrolling on the POWER7
2015-01-09 Toma Tabacu[mips] Add comment which explains why we need to change...
2015-01-09 Suyog SardaAssumption that "VectorizedValue" will always be an...
2015-01-09 Saleem AbdulrasoolARM: add support for R_ARM_ABS16
2015-01-09 Saleem Abdulrasooltest: add additional test for SVN r225507
2015-01-09 Saleem AbdulrasoolARM: add support for R_ARM_ABS8 relocations
2015-01-09 Matthias BraunRegisterCoalescer: Fix removeCopyByCommutingDef with...
2015-01-09 Matthias BraunRegisterCoalescer: Some cleanup in removeCopyByCommutin...
2015-01-09 Matthias BraunRegisterCoalescer: No need to set kill flags, they...
2015-01-09 Matthias BraunRegisterCoalescer: Turn some impossible conditions...
2015-01-09 Duncan P. N... Bitcode: Share logic for last instruction, NFC
2015-01-09 Duncan P. N... Bitcode: Move the DEBUG_LOC record to DEBUG_LOC_OLD
2015-01-09 Hal Finkel[PowerPC] Add a flag for experimenting with subreg...
2015-01-09 Hal Finkel[PowerPC] Fold [sz]ext with fp_to_int lowering where...
2015-01-09 Hal Finkel[DAGCombine] Remainder of fix to r225380 (More FMA...
2015-01-09 Chandler Carruth[x86] Add a flag to control the vector shuffle legality...
2015-01-09 Chandler CarruthCleaup ValueHandle to no longer keep a PointerIntPair...
2015-01-09 Hal FinkelPartial fix to r225380 (More FMA folding opportunities)
2015-01-09 Philip Reames[REFACTOR] Push logic from MemDepPrinter into getNonLoc...
2015-01-09 Hans WennborgReleaseNotes.rst: these are for 3.6
2015-01-09 Philip Reames[Refactor] Have getNonLocalPointerDependency take the...
2015-01-08 Duncan P. N... LangRef: Add usage points for distinct MDNodes
2015-01-08 Duncan P. N... IR: Drop TODO now that PR22111 is finished
2015-01-08 Duncan P. N... Utils: Keep distinct MDNodes distinct in MapMetadata()
2015-01-08 Duncan P. N... IR: Add 'distinct' MDNodes to bitcode and assembly
2015-01-08 Sanjay Patelremove function names from comments; NFC
2015-01-08 Hal Finkel[PowerPC] Mark all instructions as non-cheap for Machin...
2015-01-08 Hal Finkel[MachineLICM] A command-line option to hoist even cheap...
2015-01-08 Duncan P. N... CodeGen: Use handy new-fangled post-increment, NFC
2015-01-08 Akira Hatanaka[ARM] Fix a bug in constant island pass that was trigge...
2015-01-08 Duncan P. N... CodeGen: Use range-based for loops, NFC
2015-01-08 Matt ArsenaultFix fcmp + fabs instcombines when using the intrinsic
2015-01-08 Eric ChristopherThe Kaleidoscope tutorial should be using "mcjit" for...
2015-01-08 Lang Hames[MCJIT] Remove a few redundant MCJIT tests, and drop...
2015-01-08 Eric ChristopherMake the TargetMachine in MipsSubtarget a reference...
2015-01-08 Eric ChristopherUpdate include - this class doesn't use the target...
2015-01-08 Eric ChristopherFix a couple of odd formatting issues.
2015-01-08 Eric ChristopherThis routine is in InstrInfo, there's no need to access...
2015-01-08 Ahmed Bougacha[X86] Reflow comment. NFC.
2015-01-08 Rafael Espindolaclang-format. NFC.
2015-01-08 Rafael EspindolaMake this test a bit stricter.
2015-01-08 Justin HibbitsAdd saving and restoring of r30 to the prologue and...
2015-01-08 Rafael EspindolaExplicitly handle LinkOnceODRAutoHideLinkage. NFC....
2015-01-08 Rafael EspindolaUpdate naming style and clang-format. NFC.
2015-01-08 Kristof BeylsFix large stack alignment codegen for ARM and Thumb2...
2015-01-08 Tom StellardR600/SI: Remove SIISelLowering::legalizeOperands()
2015-01-08 Elena DemikhovskyMasked Load/Store - fixed a bug in type legalization.
2015-01-08 Michael KupersteinFix a think-o in the test for r225438.
2015-01-08 Michael KupersteinFix include ordering, NFC.
2015-01-08 Michael Kuperstein[X86] Don't try to generate direct calls to TLS globals
2015-01-08 Michael KupersteinMove SPAdj logic from PEI into the targets (NFC)
2015-01-08 Craig TopperFix test case I missed in r225432.
2015-01-08 Craig Topper[X86] Don't print 'dword ptr' or 'qword ptr' on the...
2015-01-08 Adrian PrantlRevert "Reapply: Teach SROA how to update debug info...
2015-01-08 Quentin Colombet[RegAllocGreedy] Introduce a late pass to repair broken...
2015-01-08 Ahmed Bougacha[SelectionDAG] Allow targets to specify legality of...
2015-01-08 Nick LewyckyRemove empty statement. No functionality change.
2015-01-08 Matthias BraunX86: VZeroUpperInserter: shortcut should not trigger...
2015-01-08 Kevin EnderbyRun clang-format on tools/llvm-objdump/MachODump.cpp...
2015-01-08 Matthias BraunRegisterCoalescer: Do not remove IMPLICIT_DEFS if they...
2015-01-07 Matthias BraunRegisterCoalescer: Fix valuesIdentical() in some subran...
2015-01-07 Matthias BraunLiveInterval: Implement feedback by Quentin Colombet.
2015-01-07 Philip Reames[GC] improve testing around gc.relocate and fix a test
2015-01-07 Ahmed Bougacha[CodeGen] Add MVT::isValid to replace manual validity...
2015-01-07 Tom StellardR600/SI: Commute instructions to enable more folding...
2015-01-07 Duncan P. N... IR: Add MDNode::getDistinct()
2015-01-07 Tom StellardR600/SI: Only fold immediates that have one use
2015-01-07 Sean SilvaTest commit.
2015-01-07 Duncan P. N... IR: Add MDNode::isDistinct()
next