diff --git a/docs/sphinx-doc/source/getting_started.rst b/docs/sphinx-doc/source/getting_started.rst
index ff2faa01c81c50c9d3e3432c21a72441bae0a471..1b5b4222bba9cb270c37d7d3d1e21328d3e61834 100644 (file)
---------------------
The OpenMP Accelerator Model runtime implementation utilizes :ref:`TI's OpenCL runtime <opencl:ti-opencl-home>`. It also relies on TI's C6000
-Code Generation Tools version 8.1.x. Set the following environment variables to the correct paths:
+Code Generation Tools version 8.1.x. Set the following environment variables to the correct paths:
-.. envvar:: TI_OCL_CGT_INSTALL
+.. envvar:: TI_OCL_CGT_INSTALL
The OpenCL runtime is dependent on the C66 DSP compiler product for
compilation of OpenCL C kernels. When OpenCL C kernels are compiled on the
standard linux locations. However, offline cross compilation of OpenCL C
kernels is also supported from x86 Ubuntu machines and in that use case, it
is required that this environment variable is set to the top level
- directory path where the C66 cross compiler tools are installed.
+ directory path where the C66 cross compiler tools are installed.
.. envvar:: TARGET_ROOTDIR
Location of target filesystem if cross-compiling on x86/x86-64
-If cross-compiling, source the ``ompacc_env.sh`` environment setup script provided in ``$TARGET_ROOTDIR/usr/share/ti/examples/openmpacc/``
-
.. _ompa_clacc:
clacc
.. figure:: images/TIOpenMPAccClacc.png
:scale: 50%
:align: center
-
+
clacc wrapper compiler
-Building a program using clacc is accomplished with the command:
+Building a program using clacc is accomplished with the command:
:command:`clacc [options] [object-files] C-source-files`
-A summary of **clacc** options are specified below:
+A summary of **clacc** options are specified below:
-h, --help Show help message
-v, --verbose Show debug output
- ``$ cd vecadd``
- ``$ make``
-To run an example:
+To run an example:
- Ensure the OpenCL package is installed
- Ensure the OpenMPAcc package is installed