include: j721e: am65x: Add new types and subtypes from SYSFW 2019.12
[processor-firmware/system-firmware-image-gen.git] / README.md
1 System Firmware (SYSFW) and Configuration Image Generator TI K3 Family SoCs
2 ===========================================================================
4 Overview
5 --------
6 This tool is intended to be a simple solution to allow users to create an image
7 tree blob (a.k.a. FIT image) comprising a signed System Firmware image as well
8 as the binary configuration artifacts needed to bring up SYSFW as part of the
9 U-Boot SPL startup. Note that the final SYSFW configuration itself is expected
10 to be performed by the end user by directly modifying different C source files
11 included into this project as needed for an application and board-specific use
12 case. The domain-specific configuration artifacts to be tailored are:
14 * *board-cfg.c* contains the general board configuration
15 * *pm-cfg.c* contains the power management / clock related configuration
16 * *rm-cfg.c* contains the resource management / allocation related configuration
17 * *sec-cfg.c* contains the security configuration
19 These files exist under {srcroot}/soc/{soc}/{configuration}/ folders, Where:
20 * srcroot - Is the root folder of source code
21 * soc - Is one of the supported SoCs. Example: am65x
22 * configuration - This is one of the supported configurations for various
23   resource division desired. Example: evm
25 NOTE: The definitions for the same are available under
26 {srcroot}/include/soc/{soc} folder
28 The build process consumes a raw (unsigned) SYSFW binary image as released by
29 the SYSFW development team and signs it by adding an X.509 certificate using a
30 random key.
32 The signed SYSFW image as well as the configuration artifacts will then all get
33 build into an ITB blob (FIT image) named **sysfw-{soc}-{configuration}.itb**
34 ready for consumption by U-Boot SPL.
37 Building SYSFW Image and Configuration Data
38 -------------------------------------------
39 First, ensure you have a current mkimage tool and ARMv7 cross toolchain
40 installed. The SYSFW configuration generator was developed and tested using...
42     $ mkimage -V
43     mkimage version 2013.10
45     $ arm-linux-gnueabihf-gcc --version
46     arm-linux-gnueabihf-gcc (Linaro GCC 7.2-2017.11) 7.2.1 20171011
47     Copyright (C) 2017 Free Software Foundation, Inc.
48     This is free software; see the source for copying conditions.  There is NO
49     warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
51 Also make sure to have a proper unsigned SYSFW image populated at the root of
52 this project, otherwise a version specified in the Makefile via Git commit hash
53 will be downloaded from the TI SYSFW release URL (see download location below).
55 The default SYSFW image consumed by the build process is called
56 **ti-sci-firmware-{soc}-gp.bin** however this may be overwritten and customized
57 using the **SYSFW_PATH** make variable. The build process will fail if the
58 image can't be downloaded to {srcroot} or no such file has gotten populated into
59 that folder by other means.
61 Further note by default the SYSFW image for use with general purpose (GP) devices
62 (as opposed to high security devices) is signed with the TI degenerate key to
63 optimize boot time (less processing time needed by ROM) but can also be signed
64 with a random cryptoraphic key or another user-provided key. This signing behavior
65 is controlled through the **KEY** make variable. Not explicitly setting **KEY**
66 will result in the use of the TI degenerate key. To use a custom key populate the
67 **KEY** variable to point to the key to get used. By clearing the default key
68 setting by passing in **KEY=""** a random key will get generated and used during
69 the build process.
71 In order to download the SYSFW release image (if needed) and build the final
72 **sysfw-{soc}-{configuration}.itb** for consumption by U-Boot SPL simply by
73 perform a make.
75     $ make
77 Note that in case of filesystem-based boot such as booting from SD card
78 **sysfw-{soc}-{configuration}.itb** needs to be manually renamed to
79 **syswfw.itb** before populating it to the (SD card) boot media as this is the
80 file name U-Boot SPL will be trying to load early during the boot process. This
81 renaming step is not necessary for RAW boot modes such as eMMC (in RAW mode),
82 (x)SPI, and others.
84     $ mv sysfw-{soc}-{configuration}.itb syswfw.itb
86 To extract and show the release version of the SYSFW image being used...
88     $ make sysfw_version
89     SYSFW Version: v2018.08a (Curious Crow)
91 To extract the 'creator' information from the final generated
92 **sysfw-{soc}-{configuration}.itb** image tree blob...
94     $ fdtget sysfw-am65x-evm.itb / creator
95     SIG am65x/evm-ti2019.01-14-g47b8d
97 The workspace can be cleaned up by doing...
99     $ make clean
101 To also remove the SYSFW image do this...
103     $ make mrproper
105 The following flags further modify the build steps:
106 * SOC - Choose one of the supported SoCs (see folder name under {srcroot}/soc).
107   Defaults to am65x
108 * CONFIG - Choose of various configurations supported (see folder name under
109   {srcroot}/soc/{soc}). Defaults to evm
110 * O - Choose where the intermediate build files need to be located
111 * BIN_DIR - Choose where the final output sysfw-{soc}-{configuration}.itb needs
112   to be generated to.
113 * KEY - Choose key to use for the signing system firmware image
114 * ENABLE_TRACE=1 - Choose to enable sysfw traces while booting.
117 Building SYSFW Image for High-Security(HS) devices
118 --------------------------------------------------
119 The process for building and image suitable for use with HS devices is similar
120 to the above process with the following differences:
122 The make commands should be appended with HS=1,
124     $ make HS=1
126 The environment variable **TI_SECURE_DEV_PKG** should be defined to point to
127 the TI Secure Development Tools package.
129 There are two images downloaded and consumed by the build process.
131     * ti-sci-firmware-{soc}-hs-enc.bin: Encrypted HS SYSFW image
132     * ti-sci-firmware-{soc}-hs-cert.bin: Inner-certificate for HS SYSFW image
134 The inner-certificate is signed by the key provided by the **TI_SECURE_DEV_PKG**
135 path producing an outer-certificate. These images are then appended to produce
136 the final **sysfw-{soc}-{configuration}.bin** which is bundled with the
137 configuration data exactly as the non-HS version above.
140 Important Notes
141 ---------------
142 There is a strong dependency of the used System Firmware release version and
143 how the board configuration data needs to be structured and/or filled in. Using
144 config data that is not compatible with a given SYSFW release may lead to
145 failures during loading of the data by U-Boot SPL, or failures later downstream
146 in U-Boot or during Linux boot.
148 It is strongly recommended to review System Firmware release documentation in
149 great detail(!) to make sure suitable board configuration is provided. Common
150 pitfalls preventing proper system operation include but are not limited to using
151 an unsuitable or invalid resource management configuration.
154 References
155 ----------
156 * [Latest SYSFW Release Documentation](http://software-dl.ti.com/tisci/esd/latest/)
157 * [Official SYSFW Release Download Location](https://git.ti.com/processor-firmware/ti-linux-firmware/trees/ti-linux-firmware/ti-sysfw)