System Firmware (SYSFW) and Configuration Image Generator for AM65x =================================================================== Overview -------- This tool is intended to be a simple solution to allow users to create an image tree blob (a.k.a. FIT image) comprising a signed System Firmware image as well as the binary configuration artifacts needed to bring up SYSFW as part of the U-Boot SPL startup. Note that the final SYSFW configuration itself is expected to be performed by the end user by directly modifying different C source files included into this project as needed for an application and board-specific use case. The domain-specific configuration artifacts to be tailored are: * *board-cfg.c* contains the general board configuration * *pm-cfg.c* contains the power management / clock related configuration * *rm-cfg.c* contains the resource management / allocation related configuration * *sec-cfg.c* contains the security configuration The build process consumes a raw (unsigned) SYSFW binary image as released by the SYSFW development team and signs it by adding an X.509 certificate using a random key. The signed SYSFW image as well as the configuration artifacts will then all get build into an ITB blob (FIT image) named **sysfw.itb** ready for consumption by U-Boot SPL. Building SYSFW Image and Configuration Data ------------------------------------------- First, ensure you have a current mkimage tool and ARMv7 cross toolchain installed. The SYSFW configuration generator was developed and tested using... $ mkimage -V mkimage version 2013.10 $ arm-linux-gnueabihf-gcc --version arm-linux-gnueabihf-gcc (Linaro GCC 7.2-2017.11) 7.2.1 20171011 Copyright (C) 2017 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. Also make sure to have a proper unsigned SYSFW image populated at the root of this project, otherwise a version specified in the Makefile via Git commit hash will be downloaded from the TI SYSFW release URL (see download location below). The default SYSFW image consumed by the build process is called **ti-sci-firmware-am65x-gp.bin** however this may be overwritten and customized using the **SYSFW_PATH** make variable. The build process will fail if the image can't be downloaded or no such file is provided. In order to download the SYSFW release image (if needed) and build the final **sysfw.itb** for consumption by U-Boot simply perform a make... $ make To extract and show the release version of the SYSFW image being used... $ make sysfw_version SYSFW Version: v2018.08a (Curious Crow) The workspace can be cleaned up by doing... $ make clean To also remove the SYSFW image do this... $ make mrproper Building SYSFW Image for High-Security(HS) devices -------------------------------------------------- The process for building and image suitable for use with HS devices is similar to the above process with the following differences: The make commands should be appended with HS=1, $ make HS=1 The environment variable **TI_SECURE_DEV_PKG** should be defined to point to the TI Secure Development Tools package. There are two images downloaded and consumed by the build process. * ti-sci-firmware-am65x-hs-enc.bin: Encrypted HS SYSFW image * ti-sci-firmware-am65x-hs-cert.bin: Inner-certificate for HS SYSFW image The inner-certificate is signed by the key provided by the **TI_SECURE_DEV_PKG** path producing an outer-certificate. These images are then appended to produce the final **sysfw.bin** which is bundled with the configuration data exactly as the non-HS version above. Important Notes --------------- There is a strong dependency of the used System Firmware release version and how the board configuration data needs to be structured and/or filled in. Using config data that is not compatible with a given SYSFW release may lead to failures during loading of the data by U-Boot SPL, or failures later downstream in U-Boot or during Linux boot. It is strongly recommended to review System Firmware release documentation in great detail(!) to make sure suitable board configuration is provided. Common pitfalls preventing proper system operation include but are not limited to using an unsuitable or invalid resource management configuration. References ---------- * [Latest SYSFW Release Documentation](http://software-dl.ti.com/tisci/esd/latest/) * [Official SYSFW Release Download Location](https://git.ti.com/processor-firmware/ti-linux-firmware/trees/ti-linux-firmware-4.1.y/ti-sysfw)