diff --git a/README.md b/README.md
index 494914daa2d32bb0556fd604e00d5c78f5544c63..043c7a8a17181ccab90cac09c2041b9869957a0c 100644 (file)
--- a/README.md
+++ b/README.md
-System Firmware (SYSFW) and Configuration Image Generator for AM65x
-===================================================================
+System Firmware (SYSFW) and Configuration Image Generator TI K3 Family SoCs
+===========================================================================
Overview
--------
* *rm-cfg.c* contains the resource management / allocation related configuration
* *sec-cfg.c* contains the security configuration
+These files exist under {srcroot}/soc/{soc}/{configuration}/ folders, Where:
+* srcroot - Is the root folder of source code
+* soc - Is one of the supported SoCs. Example: am65x
+* configuration - This is one of the supported configurations for various
+ resource division desired. Example: evm
+
+NOTE: The definitions for the same are available under
+{srcroot}/include/soc/{soc} folder
+
The build process consumes a raw (unsigned) SYSFW binary image as released by
the SYSFW development team and signs it by adding an X.509 certificate using a
random key.
The signed SYSFW image as well as the configuration artifacts will then all get
-build into an ITB blob (FIT image) named **sysfw.itb** ready for consumption by
-U-Boot SPL.
+build into an ITB blob (FIT image) named **sysfw-{soc}-{configuration}.itb**
+ready for consumption by U-Boot SPL.
Building SYSFW Image and Configuration Data
will be downloaded from the TI SYSFW release URL (see download location below).
The default SYSFW image consumed by the build process is called
-**ti-sci-firmware-am65x-gp.bin** however this may be overwritten and customized
+**ti-sci-firmware-{soc}-gp.bin** however this may be overwritten and customized
using the **SYSFW_PATH** make variable. The build process will fail if the
-image can't be downloaded or no such file is provided.
+image can't be downloaded to {srcroot} or no such file has gotten populated into
+that folder by other means.
+
+Further note by default the SYSFW image for use with general purpose (GP) devices
+(as opposed to high security devices) is signed with the TI degenerate key to
+optimize boot time (less processing time needed by ROM) but can also be signed
+with a random cryptoraphic key or another user-provided key. This signing behavior
+is controlled through the **KEY** make variable. Not explicitly setting **KEY**
+will result in the use of the TI degenerate key. To use a custom key populate the
+**KEY** variable to point to the key to get used. By clearing the default key
+setting by passing in **KEY=""** a random key will get generated and used during
+the build process.
In order to download the SYSFW release image (if needed) and build the final
-**sysfw.itb** for consumption by U-Boot simply perform a make...
+**sysfw-{soc}-{configuration}.itb** for consumption by U-Boot SPL simply by
+perform a make.
$ make
+Note that in case of filesystem-based boot such as booting from SD card
+**sysfw-{soc}-{configuration}.itb** needs to be manually renamed to
+**syswfw.itb** before populating it to the (SD card) boot media as this is the
+file name U-Boot SPL will be trying to load early during the boot process. This
+renaming step is not necessary for RAW boot modes such as eMMC (in RAW mode),
+(x)SPI, and others.
+
+ $ mv sysfw-{soc}-{configuration}.itb syswfw.itb
+
To extract and show the release version of the SYSFW image being used...
$ make sysfw_version
SYSFW Version: v2018.08a (Curious Crow)
+To extract the 'creator' information from the final generated
+**sysfw-{soc}-{configuration}.itb** image tree blob...
+
+ $ fdtget sysfw-am65x-evm.itb / creator
+ SIG am65x/evm-ti2019.01-14-g47b8d
+
The workspace can be cleaned up by doing...
$ make clean
$ make mrproper
+The following flags further modify the build steps:
+* SOC - Choose one of the supported SoCs (see folder name under {srcroot}/soc).
+ Defaults to am65x
+* CONFIG - Choose of various configurations supported (see folder name under
+ {srcroot}/soc/{soc}). Defaults to evm
+* O - Choose where the intermediate build files need to be located
+* BIN_DIR - Choose where the final output sysfw-{soc}-{configuration}.itb needs
+ to be generated to.
+* KEY - Choose key to use for the signing system firmware image
+
+
+Building SYSFW Image for High-Security(HS) devices
+--------------------------------------------------
+The process for building and image suitable for use with HS devices is similar
+to the above process with the following differences:
+
+The make commands should be appended with HS=1,
+
+ $ make HS=1
+
+The environment variable **TI_SECURE_DEV_PKG** should be defined to point to
+the TI Secure Development Tools package.
+
+There are two images downloaded and consumed by the build process.
+
+ * ti-sci-firmware-{soc}-hs-enc.bin: Encrypted HS SYSFW image
+ * ti-sci-firmware-{soc}-hs-cert.bin: Inner-certificate for HS SYSFW image
+
+The inner-certificate is signed by the key provided by the **TI_SECURE_DEV_PKG**
+path producing an outer-certificate. These images are then appended to produce
+the final **sysfw-{soc}-{configuration}.bin** which is bundled with the
+configuration data exactly as the non-HS version above.
+
Important Notes
---------------
References
----------
* [Latest SYSFW Release Documentation](http://software-dl.ti.com/tisci/esd/latest/)
-* [Official SYSFW Release Download Location](https://git.ti.com/processor-firmware/ti-linux-firmware/trees/ti-linux-firmware-4.1.y/ti-sysfw)
+* [Official SYSFW Release Download Location](https://git.ti.com/processor-firmware/ti-linux-firmware/trees/ti-linux-firmware/ti-sysfw)