2 Linux firmware
3 ==============
5 <http://git.kernel.org/?p=linux/kernel/git/firmware/linux-firmware.git>
7 git://git.kernel.org/pub/scm/linux/kernel/git/firmware/linux-firmware.git
9 This repository contains all these firmware images which have been
10 extracted from older drivers, as well various new firmware images which
11 we were never permitted to include in a GPL'd work, but which we _have_
12 been permitted to redistribute under separate cover.
14 To submit firmware to this repository, please send either a git binary
15 diff or preferably a git pull request to:
16 linux-firmware@kernel.org
17 and also cc: to related mailing lists.
19 If your commit adds new firmware, it must update the WHENCE file to
20 clearly state the license under which the firmware is available, and
21 that it is redistributable. Being redistributable includes ensuring
22 the firmware license provided includes an implicit or explicit
23 patent grant to end users to ensure full functionality of device
24 operation with the firmware. If the license is long and involved, it's
25 permitted to include it in a separate file and refer to it from the
26 WHENCE file ('See LICENSE.foo for details.').
27 And if it were possible, a changelog of the firmware itself.
29 Run 'make check' to check that WHENCE is consistent with the
30 repository contents.
32 Ideally, your commit should contain a Signed-Off-By: from someone
33 authoritative on the licensing of the firmware in question (i.e. from
34 within the company that owns the code).
37 WARNING:
38 =======
40 Don't send any "CONFIDENTIALITY STATEMENT" in your e-mail, patch or
41 request. Otherwise your firmware _will never be accepted_.
43 Maintainers are really busy, so don't expect a prompt reply.