b4fe73200b5ade8453dc59daee1e63a4984802b2
1 <!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.01 Transitional//EN">\r
2 <html><head><meta http-equiv="Content-Type" content="text/html;charset=iso-8859-1">\r
3 <title>VPE 3.6.0.0 Release Notes</title>\r
4 <link href="doxygen.css" rel="stylesheet" type="text/css">\r
5 <link href="tabs.css" rel="stylesheet" type="text/css">\r
6 </head><body>\r
7 <table width=100%>\r
8 <tr>\r
9 <td bgcolor="black" width="1"><a href="http://www.ti.com"><img border=0 src="docs/relnotes_archive/tilogo.gif"></a></td>\r
10 <td bgcolor="red"><img src="docs/relnotes_archive/titagline.gif"></td>\r
11 </tr>\r
12 </table>\r
13 <!-- Generated by Doxygen 1.5.1-p1 -->\r
14 <h1 align="center"><a name="XDC_TOP"></a>VPE 3.6.0.0 Release Notes</h1>\r
15 <h2 align="center">June 28, 2013</h2>\r
16 <h1></h1>\r
17 <p>\r
18 <a href="#Introduction">Introduction</a> <br>\r
19 <a href="#Documentation">Documentation</a> <br>\r
20 <a href="#Whats_New">What's New</a> <br>\r
21 <a href="#Compatibility">Upgrade and Compatibility Information</a> <br>\r
22 <a href="#Host_Support">Host Support</a> <br>\r
23 <a href="#Device_Support">Device Support</a> <br>\r
24 <a href="#Validation">Validation Information</a> <br>\r
25 <a href="#Known_Issues">Known Issues</a> <br>\r
26 <a href="#Version">Version Information</a> <br>\r
27 <a href="#Support">Technical Support</a> <br>\r
28 <p>\r
29 <hr>\r
30 <p>\r
31 <h2><a class="anchor" name="Introduction"></a>Introduction</h2>\r
32 <p>\r
33 The Voice Processing Elements (VPE) component is a collection of voice processing modules that each perform specific functionality for a voice channel.<p>\r
34 <br>\r
35 <a href="#XDC_TOP">back to top</a><p>\r
36 <hr>\r
37 <p>\r
38 <h2><a class="anchor" name="Documentation"></a>Documentation</h2>\r
39 <p>\r
40 The following documentation is available: <ul>\r
41 <li><a href="docs/doxygen/VPEAPI.chm">VPE API Reference's Guide</a></li><li><a href="docs/doxygen/VPE.chm">VPE Source Reference's Guide (Source Release Only)</a></li><li><a href="docs/manifest/Software_Manifest.html">VPE Component Software Manifest</a></li></ul>\r
42 <p>\r
43 Release notes from previous releases are also available in the <a href="docs/relnotes_archive">Release Notes Archive</a> directory.<p>\r
44 <br>\r
45 <a href="#XDC_TOP">back to top</a><p>\r
46 <hr>\r
47 <p>\r
48 <h2><a class="anchor" name="Whats_New"></a>What's New</h2>\r
49 <p>\r
50 The following new features were added:<ul>\r
51 <li>Added Adaptive Spectral Noise Reduction (ASNR) module </li></ul>\r
52 <p>\r
53 <br>\r
54 <a href="#XDC_TOP">back to top</a><p>\r
55 <hr>\r
56 <p>\r
57 <h2><a class="anchor" name="Compatibility"></a>Upgrade and Compatibility Information</h2>\r
58 <p>\r
59 This <b>ti.mas.vpe</b> version <b>is</b> compatible with the last released <b>ti.mas.vpe</b> version.<p>\r
60 Please note that the package compatibility keys are independent of XDC product release numbers.<p>\r
61 Package compatibility keys are intended to:<p>\r
62 <ol type=1>\r
63 <li>Enable tooling to identify incompatibilities between components, and</li><li>Convey a level of compatibility between different releases to set end user expectations.</li></ol>\r
64 <p>\r
65 Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:<p>\r
66 <ul>\r
67 <li><b>M = Major</b> - A difference in M indicates a break in compatibility. The package consumer is required to re-write its source code in order to use the package.</li><li><b>S = Source</b> - A difference in S indicates source compatibility. The package consumer\92s source code doesn't require change, but does require a recompile.</li><li><b>R = Radix</b> - A difference in R indicates an introduction of new features, but compatibility with previous interfaces is not broken. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.</li><li><b>P = Patch</b> - A difference in P indicates that only bugs have been fixed in the latest package and no new features have been introduced. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.</li></ul>\r
68 <p>\r
69 <br>\r
70 <a href="#XDC_TOP">back to top</a><p>\r
71 <hr>\r
72 <p>\r
73 <h2><a class="anchor" name="Host_Support"></a>Host Support</h2>\r
74 <p>\r
75 The current XDC toolset can be used to build components on the following hosts:<ul>\r
76 <li>Windows XP</li></ul>\r
77 <p>\r
78 <br>\r
79 <a href="#XDC_TOP">back to top</a><p>\r
80 <hr>\r
81 <p>\r
82 <h2><a class="anchor" name="Device_Support"></a>Device Support</h2>\r
83 <p>\r
84 This release supports the following device families:<ul>\r
85 <li>C55</li><li>C64P</li><li>C66</li><li>C674</li></ul>\r
86 <p>\r
87 <br>\r
88 <a href="#XDC_TOP">back to top</a><p>\r
89 <hr>\r
90 <p>\r
91 <h2><a class="anchor" name="Validation"></a>Validation Information</h2>\r
92 <p>\r
93 This release was built and validated using the following components and tools:<p>\r
94 <b>Component Dependencies</b><ul>\r
95 <li>ti.mas.types 5.5.5 (Common data type definitions)</li><li>ti.mas.swtools 5.0.4 (Internally used s/w tools)</li><li>ti.mas.util 4.7.6 (Common utilities)</li><li>ti.mas.fract 2.4.6 (Common Fractional utilities)</li></ul>\r
96 <p>\r
97 <b>Component Test Dependencies</b><ul>\r
98 <li>ti.mas.sdk 3.3.9 (Signal Generators)</li><li>CCS Version 5.2</li></ul>\r
99 <p>\r
100 <b>Tool Dependencies for Source Release</b><ul>\r
101 <li>XDC Tools version 3.20.05.76</li><li>RTSC Packaging Standard version 2.00.00</li><li>C55x Code Generation Tools version 4.4.1</li><li>C6x Code Generation Tools version 7.4.2</li></ul>\r
102 <p>\r
103 <br>\r
104 <a href="#XDC_TOP">back to top</a><p>\r
105 <hr>\r
106 <p>\r
107 <h2><a class="anchor" name="Known_Issues"></a>Known Issues</h2>\r
108 <p>\r
109 <ul>\r
110 <li>None</li></ul>\r
111 <p>\r
112 <br>\r
113 <a href="#XDC_TOP">back to top</a><p>\r
114 <hr>\r
115 <p>\r
116 <h2><a class="anchor" name="Version"></a>Versioning</h2>\r
117 <p>\r
118 This product's version follows a version format, <b>M.m.p.b</b>, where:<ul>\r
119 <li><b>M</b> is a single digit Major number</li><li><b>m</b> is a single digit minor number</li><li><b>p</b> is a single digit patch number</li><li><b>b</b> is an unrestricted set of digits used as an incrementing build counter.</li></ul>\r
120 <p>\r
121 Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the '<a href="#Compatibility">Upgrade and Compatibility Information</a>' section.<p>\r
122 <br>\r
123 <a href="#XDC_TOP">back to top</a><p>\r
124 <hr>\r
125 <p>\r
126 <h2><a class="anchor" name="Support"></a>Technical Support</h2>\r
127 <p>\r
128 Questions regarding VPE should be directed to the Texas Instruments BIOS E2E Forum. Please include the text "VoLIB" in the title.<p>\r
129 <br>\r
130 <a href="#XDC_TOP">back to top</a> <hr size="1"><small>\r
131 Copyright 2013, Texas Instruments Incorporated</small>\r
132 </body>\r
133 </html>\r