1 Date: 12/12/2006 Jianzhong Xu \r
2 Version 1.0.0.0\r
3 \r
4 The initial version of the package has three files: mhm.h, c55x/mhmport.h, mhm.c.\r
5 1. mhm.h: This file was taken from the latest of main branch. It was chagned in branch \r
6 blr_ggxvipp_r001_04_12_01_videoDSP_framework_start. The change was ignored since that brach is for video.\r
7 \r
8 2. mhmport.h: This file was taken from the latest of main branch. It is the same among all branches.\r
9 \r
10 3. mhm.c: This file was taken from the latest of main branch. It was changed in branch \r
11 blr_ggxcore_r10_03_06_14_core_10_0_0_5_core10_2 and ggdcm_desktop_vc_port. \r
12 Changes were ignored sicne the changes were not done properly. They should be outside of mhm.c.